]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - post/tests.c
Sync'd u-boot-net with mainline
[glsdk/glsdk-u-boot.git] / post / tests.c
1 /*
2  * (C) Copyright 2002
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  *
23  * Be sure to mark tests to be run before relocation as such with the
24  * CFG_POST_PREREL flag so that logging is done correctly if the
25  * logbuffer support is enabled.
26  */
28 #include <common.h>
30 #ifdef CONFIG_POST
32 #include <post.h>
34 extern int cache_post_test (int flags);
35 extern int watchdog_post_test (int flags);
36 extern int i2c_post_test (int flags);
37 extern int rtc_post_test (int flags);
38 extern int memory_post_test (int flags);
39 extern int cpu_post_test (int flags);
40 extern int fpu_post_test (int flags);
41 extern int uart_post_test (int flags);
42 extern int ether_post_test (int flags);
43 extern int spi_post_test (int flags);
44 extern int usb_post_test (int flags);
45 extern int spr_post_test (int flags);
46 extern int sysmon_post_test (int flags);
47 extern int dsp_post_test (int flags);
48 extern int codec_post_test (int flags);
50 extern int sysmon_init_f (void);
52 extern void sysmon_reloc (void);
55 struct post_test post_list[] =
56 {
57 #if CONFIG_POST & CFG_POST_CACHE
58     {
59         "Cache test",
60         "cache",
61         "This test verifies the CPU cache operation.",
62         POST_RAM | POST_ALWAYS,
63         &cache_post_test,
64         NULL,
65         NULL,
66         CFG_POST_CACHE
67     },
68 #endif
69 #if CONFIG_POST & CFG_POST_WATCHDOG
70     {
71         "Watchdog timer test",
72         "watchdog",
73         "This test checks the watchdog timer.",
74         POST_RAM | POST_POWERON | POST_SLOWTEST | POST_MANUAL | POST_REBOOT,
75         &watchdog_post_test,
76         NULL,
77         NULL,
78         CFG_POST_WATCHDOG
79     },
80 #endif
81 #if CONFIG_POST & CFG_POST_I2C
82     {
83         "I2C test",
84         "i2c",
85         "This test verifies the I2C operation.",
86         POST_RAM | POST_ALWAYS,
87         &i2c_post_test,
88         NULL,
89         NULL,
90         CFG_POST_I2C
91     },
92 #endif
93 #if CONFIG_POST & CFG_POST_RTC
94     {
95         "RTC test",
96         "rtc",
97         "This test verifies the RTC operation.",
98         POST_RAM | POST_SLOWTEST | POST_MANUAL,
99         &rtc_post_test,
100         NULL,
101         NULL,
102         CFG_POST_RTC
103     },
104 #endif
105 #if CONFIG_POST & CFG_POST_MEMORY
106     {
107         "Memory test",
108         "memory",
109         "This test checks RAM.",
110         POST_ROM | POST_POWERON | POST_SLOWTEST | POST_PREREL,
111         &memory_post_test,
112         NULL,
113         NULL,
114         CFG_POST_MEMORY
115     },
116 #endif
117 #if CONFIG_POST & CFG_POST_CPU
118     {
119         "CPU test",
120         "cpu",
121         "This test verifies the arithmetic logic unit of"
122         " CPU.",
123         POST_RAM | POST_ALWAYS,
124         &cpu_post_test,
125         NULL,
126         NULL,
127         CFG_POST_CPU
128     },
129 #endif
130 #if CONFIG_POST & CFG_POST_FPU
131     {
132         "FPU test",
133         "fpu",
134         "This test verifies the arithmetic logic unit of"
135         " FPU.",
136         POST_RAM | POST_ALWAYS,
137         &fpu_post_test,
138         NULL,
139         NULL,
140         CFG_POST_FPU
141     },
142 #endif
143 #if CONFIG_POST & CFG_POST_UART
144     {
145         "UART test",
146         "uart",
147         "This test verifies the UART operation.",
148         POST_RAM | POST_SLOWTEST | POST_MANUAL,
149         &uart_post_test,
150         NULL,
151         NULL,
152         CFG_POST_UART
153     },
154 #endif
155 #if CONFIG_POST & CFG_POST_ETHER
156     {
157         "ETHERNET test",
158         "ethernet",
159         "This test verifies the ETHERNET operation.",
160         POST_RAM | POST_ALWAYS | POST_MANUAL,
161         &ether_post_test,
162         NULL,
163         NULL,
164         CFG_POST_ETHER
165     },
166 #endif
167 #if CONFIG_POST & CFG_POST_SPI
168     {
169         "SPI test",
170         "spi",
171         "This test verifies the SPI operation.",
172         POST_RAM | POST_ALWAYS | POST_MANUAL,
173         &spi_post_test,
174         NULL,
175         NULL,
176         CFG_POST_SPI
177     },
178 #endif
179 #if CONFIG_POST & CFG_POST_USB
180     {
181         "USB test",
182         "usb",
183         "This test verifies the USB operation.",
184         POST_RAM | POST_ALWAYS | POST_MANUAL,
185         &usb_post_test,
186         NULL,
187         NULL,
188         CFG_POST_USB
189     },
190 #endif
191 #if CONFIG_POST & CFG_POST_SPR
192     {
193         "SPR test",
194         "spr",
195         "This test checks SPR contents.",
196         POST_ROM | POST_ALWAYS | POST_PREREL,
197         &spr_post_test,
198         NULL,
199         NULL,
200         CFG_POST_SPR
201     },
202 #endif
203 #if CONFIG_POST & CFG_POST_SYSMON
204     {
205         "SYSMON test",
206         "sysmon",
207         "This test monitors system hardware.",
208         POST_RAM | POST_ALWAYS,
209         &sysmon_post_test,
210         &sysmon_init_f,
211         &sysmon_reloc,
212         CFG_POST_SYSMON
213     },
214 #endif
215 #if CONFIG_POST & CFG_POST_DSP
216     {
217         "DSP test",
218         "dsp",
219         "This test checks any connected DSP(s).",
220         POST_RAM | POST_MANUAL,
221         &dsp_post_test,
222         NULL,
223         NULL,
224         CFG_POST_DSP
225     },
226 #endif
227 #if CONFIG_POST & CFG_POST_DSP
228     {
229         "CODEC test",
230         "codec",
231         "This test checks any connected codec(s).",
232         POST_RAM | POST_MANUAL,
233         &codec_post_test,
234         NULL,
235         NULL,
236         CFG_POST_CODEC
237     },
238 #endif
239 };
241 unsigned int post_list_size = sizeof (post_list) / sizeof (struct post_test);
243 #endif /* CONFIG_POST */