]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - tools/mkimage.h
HACK: ARM: DRA7xx: Add Ethernet crossbar setting
[glsdk/glsdk-u-boot.git] / tools / mkimage.h
1 /*
2  * (C) Copyright 2000-2004
3  * DENX Software Engineering
4  * Wolfgang Denk, wd@denx.de
5  *
6  * This program is free software; you can redistribute it and/or
7  * modify it under the terms of the GNU General Public License as
8  * published by the Free Software Foundation; either version 2 of
9  * the License, or (at your option) any later version.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19  * MA 02111-1307 USA
20  */
22 #ifndef _MKIIMAGE_H_
23 #define _MKIIMAGE_H_
25 #include "os_support.h"
26 #include <errno.h>
27 #include <fcntl.h>
28 #include <stdio.h>
29 #include <stdlib.h>
30 #include <string.h>
31 #include <sys/stat.h>
32 #include <time.h>
33 #include <unistd.h>
34 #include <sha1.h>
35 #include "fdt_host.h"
37 #undef MKIMAGE_DEBUG
39 #ifdef MKIMAGE_DEBUG
40 #define debug(fmt,args...)      printf (fmt ,##args)
41 #else
42 #define debug(fmt,args...)
43 #endif /* MKIMAGE_DEBUG */
45 #define MKIMAGE_TMPFILE_SUFFIX          ".tmp"
46 #define MKIMAGE_MAX_TMPFILE_LEN         256
47 #define MKIMAGE_DEFAULT_DTC_OPTIONS     "-I dts -O dtb -p 500"
48 #define MKIMAGE_MAX_DTC_CMDLINE_LEN     512
49 #define MKIMAGE_DTC                     "dtc"   /* assume dtc is in $PATH */
51 /*
52  * This structure defines all such variables those are initialized by
53  * mkimage main core and need to be referred by image type specific
54  * functions
55  */
56 struct mkimage_params {
57         int dflag;
58         int eflag;
59         int fflag;
60         int lflag;
61         int vflag;
62         int xflag;
63         int skipcpy;
64         int os;
65         int arch;
66         int type;
67         int comp;
68         char *dtc;
69         unsigned int addr;
70         unsigned int ep;
71         char *imagename;
72         char *imagename2;
73         char *datafile;
74         char *imagefile;
75         char *cmdname;
76 };
78 /*
79  * image type specific variables and callback functions
80  */
81 struct image_type_params {
82         /* name is an identification tag string for added support */
83         char *name;
84         /*
85          * header size is local to the specific image type to be supported,
86          * mkimage core treats this as number of bytes
87          */
88         uint32_t header_size;
89         /* Image type header pointer */
90         void *hdr;
91         /*
92          * There are several arguments that are passed on the command line
93          * and are registered as flags in mkimage_params structure.
94          * This callback function can be used to check the passed arguments
95          * are in-lined with the image type to be supported
96          *
97          * Returns 1 if parameter check is successful
98          */
99         int (*check_params) (struct mkimage_params *);
100         /*
101          * This function is used by list command (i.e. mkimage -l <filename>)
102          * image type verification code must be put here
103          *
104          * Returns 0 if image header verification is successful
105          * otherwise, returns respective negative error codes
106          */
107         int (*verify_header) (unsigned char *, int, struct mkimage_params *);
108         /* Prints image information abstracting from image header */
109         void (*print_header) (const void *);
110         /*
111          * The header or image contents need to be set as per image type to
112          * be generated using this callback function.
113          * further output file post processing (for ex. checksum calculation,
114          * padding bytes etc..) can also be done in this callback function.
115          */
116         void (*set_header) (void *, struct stat *, int,
117                                         struct mkimage_params *);
118         /*
119          * Some image generation support for ex (default image type) supports
120          * more than one type_ids, this callback function is used to check
121          * whether input (-T <image_type>) is supported by registered image
122          * generation/list low level code
123          */
124         int (*check_image_type) (uint8_t);
125         /* This callback function will be executed if fflag is defined */
126         int (*fflag_handle) (struct mkimage_params *);
127         /*
128          * This callback function will be executed for variable size record
129          * It is expected to build this header in memory and return its length
130          * and a pointer to it
131          */
132         int (*vrec_header) (struct mkimage_params *,
133                 struct image_type_params *);
134         /* pointer to the next registered entry in linked list */
135         struct image_type_params *next;
136 };
138 /*
139  * Exported functions
140  */
141 void mkimage_register (struct image_type_params *tparams);
143 /*
144  * There is a c file associated with supported image type low level code
145  * for ex. default_image.c, fit_image.c
146  * init is the only function referred by mkimage core.
147  * to avoid a single lined header file, you can define them here
148  *
149  * Supported image types init functions
150  */
151 void pbl_load_uboot(int fd, struct mkimage_params *mparams);
152 void init_pbl_image_type(void);
153 void init_ais_image_type(void);
154 void init_kwb_image_type (void);
155 void init_imx_image_type (void);
156 void init_default_image_type (void);
157 void init_fit_image_type (void);
158 void init_ubl_image_type(void);
159 void init_omap_image_type(void);
161 #endif /* _MKIIMAGE_H_ */