1 # Copyright (c) 2011 The Chromium OS Authors.
2 #
3 # See file CREDITS for list of people who contributed to this
4 # project.
5 #
6 # This program is free software; you can redistribute it and/or
7 # modify it under the terms of the GNU General Public License as
8 # published by the Free Software Foundation; either version 2 of
9 # the License, or (at your option) any later version.
10 #
11 # This program is distributed in the hope that it will be useful,
12 # but WITHOUT ANY WARRANTY; without even the implied warranty of
13 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 # GNU General Public License for more details.
15 #
16 # You should have received a copy of the GNU General Public License
17 # along with this program; if not, write to the Free Software
18 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19 # MA 02111-1307 USA
20 #
22 What is this?
23 =============
25 This tool is a Python script which:
26 - Creates patch directly from your branch
27 - Cleans them up by removing unwanted tags
28 - Inserts a cover letter with change lists
29 - Runs the patches through checkpatch.pl and its own checks
30 - Optionally emails them out to selected people
32 It is intended to automate patch creation and make it a less
33 error-prone process. It is useful for U-Boot and Linux work so far,
34 since it uses the checkpatch.pl script.
36 It is configured almost entirely by tags it finds in your commits.
37 This means that you can work on a number of different branches at
38 once, and keep the settings with each branch rather than having to
39 git format-patch, git send-email, etc. with the correct parameters
40 each time. So for example if you put:
42 Series-to: fred.blogs@napier.co.nz
44 in one of your commits, the series will be sent there.
46 In Linux this will also call get_maintainer.pl on each of your
47 patches automatically.
50 How to use this tool
51 ====================
53 This tool requires a certain way of working:
55 - Maintain a number of branches, one for each patch series you are
56 working on
57 - Add tags into the commits within each branch to indicate where the
58 series should be sent, cover letter, version, etc. Most of these are
59 normally in the top commit so it is easy to change them with 'git
60 commit --amend'
61 - Each branch tracks the upstream branch, so that this script can
62 automatically determine the number of commits in it (optional)
63 - Check out a branch, and run this script to create and send out your
64 patches. Weeks later, change the patches and repeat, knowing that you
65 will get a consistent result each time.
68 How to configure it
69 ===================
71 For most cases of using patman for U-Boot development, patman will
72 locate and use the file 'doc/git-mailrc' in your U-Boot directory.
73 This contains most of the aliases you will need.
75 For Linux the 'scripts/get_maintainer.pl' handles figuring out where
76 to send patches pretty well.
78 During the first run patman creates a config file for you by taking the default
79 user name and email address from the global .gitconfig file.
81 To add your own, create a file ~/.patman like this:
83 >>>>
84 # patman alias file
86 [alias]
87 me: Simon Glass <sjg@chromium.org>
89 u-boot: U-Boot Mailing List <u-boot@lists.denx.de>
90 wolfgang: Wolfgang Denk <wd@denx.de>
91 others: Mike Frysinger <vapier@gentoo.org>, Fred Bloggs <f.bloggs@napier.net>
93 <<<<
95 Aliases are recursive.
97 The checkpatch.pl in the U-Boot tools/ subdirectory will be located and
98 used. Failing that you can put it into your path or ~/bin/checkpatch.pl
101 If you want to change the defaults for patman's command-line arguments,
102 you can add a [settings] section to your .patman file. This can be used
103 for any command line option by referring to the "dest" for the option in
104 patman.py. For reference, the useful ones (at the moment) shown below
105 (all with the non-default setting):
107 >>>
109 [settings]
110 ignore_errors: True
111 process_tags: False
112 verbose: True
114 <<<
117 If you want to adjust settings (or aliases) that affect just a single
118 project you can add a section that looks like [project_settings] or
119 [project_alias]. If you want to use tags for your linux work, you could
120 do:
122 >>>
124 [linux_settings]
125 process_tags: True
127 <<<
130 How to run it
131 =============
133 First do a dry run:
135 $ ./tools/patman/patman -n
137 If it can't detect the upstream branch, try telling it how many patches
138 there are in your series:
140 $ ./tools/patman/patman -n -c5
142 This will create patch files in your current directory and tell you who
143 it is thinking of sending them to. Take a look at the patch files.
145 $ ./tools/patman/patman -n -c5 -s1
147 Similar to the above, but skip the first commit and take the next 5. This
148 is useful if your top commit is for setting up testing.
151 How to add tags
152 ===============
154 To make this script useful you must add tags like the following into any
155 commit. Most can only appear once in the whole series.
157 Series-to: email / alias
158 Email address / alias to send patch series to (you can add this
159 multiple times)
161 Series-cc: email / alias, ...
162 Email address / alias to Cc patch series to (you can add this
163 multiple times)
165 Series-version: n
166 Sets the version number of this patch series
168 Series-prefix: prefix
169 Sets the subject prefix. Normally empty but it can be RFC for
170 RFC patches, or RESEND if you are being ignored.
172 Series-name: name
173 Sets the name of the series. You don't need to have a name, and
174 patman does not yet use it, but it is convenient to put the branch
175 name here to help you keep track of multiple upstreaming efforts.
177 Cover-letter:
178 This is the patch set title
179 blah blah
180 more blah blah
181 END
182 Sets the cover letter contents for the series. The first line
183 will become the subject of the cover letter
185 Cover-letter-cc: email / alias
186 Additional email addresses / aliases to send cover letter to (you
187 can add this multiple times)
189 Series-notes:
190 blah blah
191 blah blah
192 more blah blah
193 END
194 Sets some notes for the patch series, which you don't want in
195 the commit messages, but do want to send, The notes are joined
196 together and put after the cover letter. Can appear multiple
197 times.
199 Signed-off-by: Their Name <email>
200 A sign-off is added automatically to your patches (this is
201 probably a bug). If you put this tag in your patches, it will
202 override the default signoff that patman automatically adds.
204 Tested-by: Their Name <email>
205 Reviewed-by: Their Name <email>
206 Acked-by: Their Name <email>
207 These indicate that someone has tested/reviewed/acked your patch.
208 When you get this reply on the mailing list, you can add this
209 tag to the relevant commit and the script will include it when
210 you send out the next version. If 'Tested-by:' is set to
211 yourself, it will be removed. No one will believe you.
213 Series-changes: n
214 - Guinea pig moved into its cage
215 - Other changes ending with a blank line
216 <blank line>
217 This can appear in any commit. It lists the changes for a
218 particular version n of that commit. The change list is
219 created based on this information. Each commit gets its own
220 change list and also the whole thing is repeated in the cover
221 letter (where duplicate change lines are merged).
223 By adding your change lists into your commits it is easier to
224 keep track of what happened. When you amend a commit, remember
225 to update the log there and then, knowing that the script will
226 do the rest.
228 Cc: Their Name <email>
229 This copies a single patch to another email address.
231 Series-process-log: sort, uniq
232 This tells patman to sort and/or uniq the change logs. It is
233 assumed that each change log entry is only a single line long.
234 Use 'sort' to sort the entries, and 'uniq' to include only
235 unique entries. If omitted, no change log processing is done.
236 Separate each tag with a comma.
238 Various other tags are silently removed, like these Chrome OS and
239 Gerrit tags:
241 BUG=...
242 TEST=...
243 Change-Id:
244 Review URL:
245 Reviewed-on:
248 Exercise for the reader: Try adding some tags to one of your current
249 patch series and see how the patches turn out.
252 Where Patches Are Sent
253 ======================
255 Once the patches are created, patman sends them using git send-email. The
256 whole series is sent to the recipients in Series-to: and Series-cc.
257 You can Cc individual patches to other people with the Cc: tag. Tags in the
258 subject are also picked up to Cc patches. For example, a commit like this:
260 >>>>
261 commit 10212537b85ff9b6e09c82045127522c0f0db981
262 Author: Mike Frysinger <vapier@gentoo.org>
263 Date: Mon Nov 7 23:18:44 2011 -0500
265 x86: arm: add a git mailrc file for maintainers
267 This should make sending out e-mails to the right people easier.
269 Cc: sandbox, mikef, ag
270 Cc: afleming
271 <<<<
273 will create a patch which is copied to x86, arm, sandbox, mikef, ag and
274 afleming.
276 If you have a cover letter it will get sent to the union of the CC lists of
277 all of the other patches. If you want to sent it to additional people you
278 can add a tag:
280 Cover-letter-cc: <list of addresses>
282 These people will get the cover letter even if they are not on the To/Cc
283 list for any of the patches.
286 Example Work Flow
287 =================
289 The basic workflow is to create your commits, add some tags to the top
290 commit, and type 'patman' to check and send them.
292 Here is an example workflow for a series of 4 patches. Let's say you have
293 these rather contrived patches in the following order in branch us-cmd in
294 your tree where 'us' means your upstreaming activity (newest to oldest as
295 output by git log --oneline):
297 7c7909c wip
298 89234f5 Don't include standard parser if hush is used
299 8d640a7 mmc: sparc: Stop using builtin_run_command()
300 0c859a9 Rename run_command2() to run_command()
301 a74443f sandbox: Rename run_command() to builtin_run_command()
303 The first patch is some test things that enable your code to be compiled,
304 but that you don't want to submit because there is an existing patch for it
305 on the list. So you can tell patman to create and check some patches
306 (skipping the first patch) with:
308 patman -s1 -n
310 If you want to do all of them including the work-in-progress one, then
311 (if you are tracking an upstream branch):
313 patman -n
315 Let's say that patman reports an error in the second patch. Then:
317 git rebase -i HEAD~6
318 <change 'pick' to 'edit' in 89234f5>
319 <use editor to make code changes>
320 git add -u
321 git rebase --continue
323 Now you have an updated patch series. To check it:
325 patman -s1 -n
327 Let's say it is now clean and you want to send it. Now you need to set up
328 the destination. So amend the top commit with:
330 git commit --amend
332 Use your editor to add some tags, so that the whole commit message is:
334 The current run_command() is really only one of the options, with
335 hush providing the other. It really shouldn't be called directly
336 in case the hush parser is bring used, so rename this function to
337 better explain its purpose.
339 Series-to: u-boot
340 Series-cc: bfin, marex
341 Series-prefix: RFC
342 Cover-letter:
343 Unified command execution in one place
345 At present two parsers have similar code to execute commands. Also
346 cmd_usage() is called all over the place. This series adds a single
347 function which processes commands called cmd_process().
348 END
350 Change-Id: Ica71a14c1f0ecb5650f771a32fecb8d2eb9d8a17
353 You want this to be an RFC and Cc the whole series to the bfin alias and
354 to Marek. Two of the patches have tags (those are the bits at the front of
355 the subject that say mmc: sparc: and sandbox:), so 8d640a7 will be Cc'd to
356 mmc and sparc, and the last one to sandbox.
358 Now to send the patches, take off the -n flag:
360 patman -s1
362 The patches will be created, shown in your editor, and then sent along with
363 the cover letter. Note that patman's tags are automatically removed so that
364 people on the list don't see your secret info.
366 Of course patches often attract comments and you need to make some updates.
367 Let's say one person sent comments and you get an Acked-by: on one patch.
368 Also, the patch on the list that you were waiting for has been merged,
369 so you can drop your wip commit. So you resync with upstream:
371 git fetch origin (or whatever upstream is called)
372 git rebase origin/master
374 and use git rebase -i to edit the commits, dropping the wip one. You add
375 the ack tag to one commit:
377 Acked-by: Heiko Schocher <hs@denx.de>
379 update the Series-cc: in the top commit:
381 Series-cc: bfin, marex, Heiko Schocher <hs@denx.de>
383 and remove the Series-prefix: tag since it it isn't an RFC any more. The
384 series is now version two, so the series info in the top commit looks like
385 this:
387 Series-to: u-boot
388 Series-cc: bfin, marex, Heiko Schocher <hs@denx.de>
389 Series-version: 2
390 Cover-letter:
391 ...
393 Finally, you need to add a change log to the two commits you changed. You
394 add change logs to each individual commit where the changes happened, like
395 this:
397 Series-changes: 2
398 - Updated the command decoder to reduce code size
399 - Wound the torque propounder up a little more
401 (note the blank line at the end of the list)
403 When you run patman it will collect all the change logs from the different
404 commits and combine them into the cover letter, if you have one. So finally
405 you have a new series of commits:
407 faeb973 Don't include standard parser if hush is used
408 1b2f2fe mmc: sparc: Stop using builtin_run_command()
409 cfbe330 Rename run_command2() to run_command()
410 0682677 sandbox: Rename run_command() to builtin_run_command()
412 so to send them:
414 patman
416 and it will create and send the version 2 series.
418 General points:
420 1. When you change back to the us-cmd branch days or weeks later all your
421 information is still there, safely stored in the commits. You don't need
422 to remember what version you are up to, who you sent the last lot of patches
423 to, or anything about the change logs.
425 2. If you put tags in the subject, patman will Cc the maintainers
426 automatically in many cases.
428 3. If you want to keep the commits from each series you sent so that you can
429 compare change and see what you did, you can either create a new branch for
430 each version, or just tag the branch before you start changing it:
432 git tag sent/us-cmd-rfc
433 ...later...
434 git tag sent/us-cmd-v2
436 4. If you want to modify the patches a little before sending, you can do
437 this in your editor, but be careful!
439 5. If you want to run git send-email yourself, use the -n flag which will
440 print out the command line patman would have used.
442 6. It is a good idea to add the change log info as you change the commit,
443 not later when you can't remember which patch you changed. You can always
444 go back and change or remove logs from commits.
447 Other thoughts
448 ==============
450 This script has been split into sensible files but still needs work.
451 Most of these are indicated by a TODO in the code.
453 It would be nice if this could handle the In-reply-to side of things.
455 The tests are incomplete, as is customary. Use the -t flag to run them,
456 and make sure you are in the tools/scripts/patman directory first:
458 $ cd /path/to/u-boot
459 $ cd tools/scripts/patman
460 $ patman -t
462 Error handling doesn't always produce friendly error messages - e.g.
463 putting an incorrect tag in a commit may provide a confusing message.
465 There might be a few other features not mentioned in this README. They
466 might be bugs. In particular, tags are case sensitive which is probably
467 a bad thing.
470 Simon Glass <sjg@chromium.org>
471 v1, v2, 19-Oct-11
472 revised v3 24-Nov-11