1 # Copyright (c) 2012 The Chromium OS Authors.
2 #
3 # See file CREDITS for list of people who contributed to this
4 # project.
5 #
6 # This program is free software; you can redistribute it and/or
7 # modify it under the terms of the GNU General Public License as
8 # published by the Free Software Foundation; either version 2 of
9 # the License, or (at your option) any later version.
10 #
11 # This program is distributed in the hope that it will be useful,
12 # but WITHOUT ANY WARRANTY; without even the implied warranty of
13 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 # GNU General Public License for more details.
15 #
16 # You should have received a copy of the GNU General Public License
17 # along with this program; if not, write to the Free Software
18 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19 # MA 02111-1307 USA
20 #
22 import os.path
24 import gitutil
26 def DetectProject():
27 """Autodetect the name of the current project.
29 This looks for signature files/directories that are unlikely to exist except
30 in the given project.
32 Returns:
33 The name of the project, like "linux" or "u-boot". Returns "unknown"
34 if we can't detect the project.
35 """
36 top_level = gitutil.GetTopLevel()
38 if os.path.exists(os.path.join(top_level, "include", "u-boot")):
39 return "u-boot"
40 elif os.path.exists(os.path.join(top_level, "kernel")):
41 return "linux"
43 return "unknown"