/* * armboot - Startup Code for ARM926EJS CPU-core * * Copyright (c) 2003 Texas Instruments * * ----- Adapted for OMAP1610 OMAP730 from ARM925t code ------ * * Copyright (c) 2001 Marius Gröger * Copyright (c) 2002 Alex Züpke * Copyright (c) 2002 Gary Jennejohn * Copyright (c) 2003 Richard Woodruff * Copyright (c) 2003 Kshitij * Copyright (c) 2010 Albert Aribaud * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #include #include #include #include #if defined(CONFIG_OMAP1610) #include <./configs/omap1510.h> #elif defined(CONFIG_OMAP730) #include <./configs/omap730.h> #endif /* ************************************************************************* * * Jump vector table as in table 3.1 in [1] * ************************************************************************* */ #ifdef CONFIG_SYS_DV_NOR_BOOT_CFG .globl _start _start: .globl _NOR_BOOT_CFG _NOR_BOOT_CFG: .word CONFIG_SYS_DV_NOR_BOOT_CFG b reset #else .globl _start _start: b reset #endif #ifdef CONFIG_SPL_BUILD /* No exception handlers in preloader */ ldr pc, _hang ldr pc, _hang ldr pc, _hang ldr pc, _hang ldr pc, _hang ldr pc, _hang ldr pc, _hang _hang: .word do_hang /* pad to 64 byte boundary */ .word 0x12345678 .word 0x12345678 .word 0x12345678 .word 0x12345678 .word 0x12345678 .word 0x12345678 .word 0x12345678 #else ldr pc, _undefined_instruction ldr pc, _software_interrupt ldr pc, _prefetch_abort ldr pc, _data_abort ldr pc, _not_used ldr pc, _irq ldr pc, _fiq _undefined_instruction: .word undefined_instruction _software_interrupt: .word software_interrupt _prefetch_abort: .word prefetch_abort _data_abort: .word data_abort _not_used: .word not_used _irq: .word irq _fiq: .word fiq #endif /* CONFIG_SPL_BUILD */ .balignl 16,0xdeadbeef /* ************************************************************************* * * Startup Code (reset vector) * * do important init only if we don't start from memory! * setup Memory and board specific bits prior to relocation. * relocate armboot to ram * setup stack * ************************************************************************* */ .globl _TEXT_BASE _TEXT_BASE: #ifdef CONFIG_NAND_SPL /* deprecated, use instead CONFIG_SPL_BUILD */ .word CONFIG_SYS_TEXT_BASE #else #ifdef CONFIG_SPL_BUILD .word CONFIG_SPL_TEXT_BASE #else .word CONFIG_SYS_TEXT_BASE #endif #endif /* * These are defined in the board-specific linker script. * Subtracting _start from them lets the linker put their * relative position in the executable instead of leaving * them null. */ .globl _bss_start_ofs _bss_start_ofs: .word __bss_start - _start .globl _bss_end_ofs _bss_end_ofs: .word __bss_end__ - _start .globl _end_ofs _end_ofs: .word _end - _start #ifdef CONFIG_NAND_U_BOOT .globl _end _end: .word __bss_end__ #endif #ifdef CONFIG_USE_IRQ /* IRQ stack memory (calculated at run-time) */ .globl IRQ_STACK_START IRQ_STACK_START: .word 0x0badc0de /* IRQ stack memory (calculated at run-time) */ .globl FIQ_STACK_START FIQ_STACK_START: .word 0x0badc0de #endif /* IRQ stack memory (calculated at run-time) + 8 bytes */ .globl IRQ_STACK_START_IN IRQ_STACK_START_IN: .word 0x0badc0de /* * the actual reset code */ reset: /* * set the cpu to SVC32 mode */ mrs r0,cpsr bic r0,r0,#0x1f orr r0,r0,#0xd3 msr cpsr,r0 /* * we do sys-critical inits only at reboot, * not when booting from ram! */ #ifndef CONFIG_SKIP_LOWLEVEL_INIT bl cpu_init_crit #endif /* Set stackpointer in internal RAM to call board_init_f */ call_board_init_f: #ifdef CONFIG_NAND_SPL /* deprecated, use instead CONFIG_SPL_BUILD */ ldr sp, =(CONFIG_SYS_INIT_SP_ADDR) #else #ifdef CONFIG_SPL_BUILD ldr sp, =(CONFIG_SPL_STACK) #else ldr sp, =(CONFIG_SYS_INIT_SP_ADDR) #endif #endif bic sp, sp, #7 /* 8-byte alignment for ABI compliance */ ldr r0,=0x00000000 bl board_init_f /*------------------------------------------------------------------------------*/ /* * void relocate_code (addr_sp, gd, addr_moni) * * This "function" does not return, instead it continues in RAM * after relocating the monitor code. * */ .globl relocate_code relocate_code: mov r4, r0 /* save addr_sp */ mov r5, r1 /* save addr of gd */ mov r6, r2 /* save addr of destination */ /* Set up the stack */ stack_setup: mov sp, r4 adr r0, _start sub r9, r6, r0 /* r9 <- relocation offset */ cmp r0, r6 beq clear_bss /* skip relocation */ mov r1, r6 /* r1 <- scratch for copy loop */ ldr r3, _bss_start_ofs add r2, r0, r3 /* r2 <- source end address */ copy_loop: ldmia r0!, {r9-r10} /* copy from source address [r0] */ stmia r1!, {r9-r10} /* copy to target address [r1] */ cmp r0, r2 /* until source end address [r2] */ blo copy_loop #ifndef CONFIG_SPL_BUILD /* * fix .rel.dyn relocations */ ldr r0, _TEXT_BASE /* r0 <- Text base */ sub r9, r6, r0 /* r9 <- relocation offset */ ldr r10, _dynsym_start_ofs /* r10 <- sym table ofs */ add r10, r10, r0 /* r10 <- sym table in FLASH */ ldr r2, _rel_dyn_start_ofs /* r2 <- rel dyn start ofs */ add r2, r2, r0 /* r2 <- rel dyn start in FLASH */ ldr r3, _rel_dyn_end_ofs /* r3 <- rel dyn end ofs */ add r3, r3, r0 /* r3 <- rel dyn end in FLASH */ fixloop: ldr r0, [r2] /* r0 <- location to fix up, IN FLASH! */ add r0, r0, r9 /* r0 <- location to fix up in RAM */ ldr r1, [r2, #4] and r7, r1, #0xff cmp r7, #23 /* relative fixup? */ beq fixrel cmp r7, #2 /* absolute fixup? */ beq fixabs /* ignore unknown type of fixup */ b fixnext fixabs: /* absolute fix: set location to (offset) symbol value */ mov r1, r1, LSR #4 /* r1 <- symbol index in .dynsym */ add r1, r10, r1 /* r1 <- address of symbol in table */ ldr r1, [r1, #4] /* r1 <- symbol value */ add r1, r1, r9 /* r1 <- relocated sym addr */ b fixnext fixrel: /* relative fix: increase location by offset */ ldr r1, [r0] add r1, r1, r9 fixnext: str r1, [r0] add r2, r2, #8 /* each rel.dyn entry is 8 bytes */ cmp r2, r3 blo fixloop #endif clear_bss: #ifdef CONFIG_SPL_BUILD /* No relocation for SPL */ ldr r0, =__bss_start ldr r1, =__bss_end__ #else ldr r0, _bss_start_ofs ldr r1, _bss_end_ofs mov r4, r6 /* reloc addr */ add r0, r0, r4 add r1, r1, r4 #endif mov r2, #0x00000000 /* clear */ clbss_l:cmp r0, r1 /* clear loop... */ bhs clbss_e /* if reached end of bss, exit */ str r2, [r0] add r0, r0, #4 b clbss_l clbss_e: #ifndef CONFIG_SPL_BUILD bl coloured_LED_init bl red_led_on #endif /* * We are done. Do not return, instead branch to second part of board * initialization, now running from RAM. */ #ifdef CONFIG_NAND_SPL ldr r0, _nand_boot_ofs mov pc, r0 _nand_boot_ofs: .word nand_boot #else ldr r0, _board_init_r_ofs ldr r1, _TEXT_BASE add lr, r0, r1 add lr, lr, r9 /* setup parameters for board_init_r */ mov r0, r5 /* gd_t */ mov r1, r6 /* dest_addr */ /* jump to it ... */ mov pc, lr _board_init_r_ofs: .word board_init_r - _start #endif _rel_dyn_start_ofs: .word __rel_dyn_start - _start _rel_dyn_end_ofs: .word __rel_dyn_end - _start _dynsym_start_ofs: .word __dynsym_start - _start /* ************************************************************************* * * CPU_init_critical registers * * setup important registers * setup memory timing * ************************************************************************* */ #ifndef CONFIG_SKIP_LOWLEVEL_INIT cpu_init_crit: /* * flush D cache before disabling it */ mov r0, #0 flush_dcache: mrc p15, 0, r15, c7, c10, 3 bne flush_dcache mcr p15, 0, r0, c8, c7, 0 /* invalidate TLB */ mcr p15, 0, r0, c7, c5, 0 /* invalidate I Cache */ /* * disable MMU and D cache * enable I cache if CONFIG_SYS_ICACHE_OFF is not defined */ mrc p15, 0, r0, c1, c0, 0 bic r0, r0, #0x00000300 /* clear bits 9:8 (---- --RS) */ bic r0, r0, #0x00000087 /* clear bits 7, 2:0 (B--- -CAM) */ #ifdef CONFIG_SYS_EXCEPTION_VECTORS_HIGH orr r0, r0, #0x00002000 /* set bit 13 (--V- ----) */ #else bic r0, r0, #0x00002000 /* clear bit 13 (--V- ----) */ #endif orr r0, r0, #0x00000002 /* set bit 2 (A) Align */ #ifndef CONFIG_SYS_ICACHE_OFF orr r0, r0, #0x00001000 /* set bit 12 (I) I-Cache */ #endif mcr p15, 0, r0, c1, c0, 0 /* * Go setup Memory and board specific bits prior to relocation. */ mov ip, lr /* perserve link reg across call */ bl lowlevel_init /* go setup pll,mux,memory */ mov lr, ip /* restore link */ mov pc, lr /* back to my caller */ #endif /* CONFIG_SKIP_LOWLEVEL_INIT */ #ifndef CONFIG_SPL_BUILD /* ************************************************************************* * * Interrupt handling * ************************************************************************* */ @ @ IRQ stack frame. @ #define S_FRAME_SIZE 72 #define S_OLD_R0 68 #define S_PSR 64 #define S_PC 60 #define S_LR 56 #define S_SP 52 #define S_IP 48 #define S_FP 44 #define S_R10 40 #define S_R9 36 #define S_R8 32 #define S_R7 28 #define S_R6 24 #define S_R5 20 #define S_R4 16 #define S_R3 12 #define S_R2 8 #define S_R1 4 #define S_R0 0 #define MODE_SVC 0x13 #define I_BIT 0x80 /* * use bad_save_user_regs for abort/prefetch/undef/swi ... * use irq_save_user_regs / irq_restore_user_regs for IRQ/FIQ handling */ .macro bad_save_user_regs @ carve out a frame on current user stack sub sp, sp, #S_FRAME_SIZE stmia sp, {r0 - r12} @ Save user registers (now in svc mode) r0-r12 ldr r2, IRQ_STACK_START_IN @ get values for "aborted" pc and cpsr (into parm regs) ldmia r2, {r2 - r3} add r0, sp, #S_FRAME_SIZE @ grab pointer to old stack add r5, sp, #S_SP mov r1, lr stmia r5, {r0 - r3} @ save sp_SVC, lr_SVC, pc, cpsr mov r0, sp @ save current stack into r0 (param register) .endm .macro irq_save_user_regs sub sp, sp, #S_FRAME_SIZE stmia sp, {r0 - r12} @ Calling r0-r12 @ !!!! R8 NEEDS to be saved !!!! a reserved stack spot would be good. add r8, sp, #S_PC stmdb r8, {sp, lr}^ @ Calling SP, LR str lr, [r8, #0] @ Save calling PC mrs r6, spsr str r6, [r8, #4] @ Save CPSR str r0, [r8, #8] @ Save OLD_R0 mov r0, sp .endm .macro irq_restore_user_regs ldmia sp, {r0 - lr}^ @ Calling r0 - lr mov r0, r0 ldr lr, [sp, #S_PC] @ Get PC add sp, sp, #S_FRAME_SIZE subs pc, lr, #4 @ return & move spsr_svc into cpsr .endm .macro get_bad_stack ldr r13, IRQ_STACK_START_IN @ setup our mode stack str lr, [r13] @ save caller lr in position 0 of saved stack mrs lr, spsr @ get the spsr str lr, [r13, #4] @ save spsr in position 1 of saved stack mov r13, #MODE_SVC @ prepare SVC-Mode @ msr spsr_c, r13 msr spsr, r13 @ switch modes, make sure moves will execute mov lr, pc @ capture return pc movs pc, lr @ jump to next instruction & switch modes. .endm .macro get_irq_stack @ setup IRQ stack ldr sp, IRQ_STACK_START .endm .macro get_fiq_stack @ setup FIQ stack ldr sp, FIQ_STACK_START .endm #endif /* CONFIG_SPL_BUILD */ /* * exception handlers */ #ifdef CONFIG_SPL_BUILD .align 5 do_hang: ldr sp, _TEXT_BASE /* switch to abort stack */ 1: bl 1b /* hang and never return */ #else /* !CONFIG_SPL_BUILD */ .align 5 undefined_instruction: get_bad_stack bad_save_user_regs bl do_undefined_instruction .align 5 software_interrupt: get_bad_stack bad_save_user_regs bl do_software_interrupt .align 5 prefetch_abort: get_bad_stack bad_save_user_regs bl do_prefetch_abort .align 5 data_abort: get_bad_stack bad_save_user_regs bl do_data_abort .align 5 not_used: get_bad_stack bad_save_user_regs bl do_not_used #ifdef CONFIG_USE_IRQ .align 5 irq: get_irq_stack irq_save_user_regs bl do_irq irq_restore_user_regs .align 5 fiq: get_fiq_stack /* someone ought to write a more effiction fiq_save_user_regs */ irq_save_user_regs bl do_fiq irq_restore_user_regs #else .align 5 irq: get_bad_stack bad_save_user_regs bl do_irq .align 5 fiq: get_bad_stack bad_save_user_regs bl do_fiq #endif #endif /* CONFIG_SPL_BUILD */