/* * Copyright (C) 2009 Texas Instruments Incorporated * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef _GPIO_DEFS_H_ #define _GPIO_DEFS_H_ #ifndef CONFIG_SOC_DA8XX #define DAVINCI_GPIO_BINTEN 0x01C67008 #define DAVINCI_GPIO_BANK01 0x01C67010 #define DAVINCI_GPIO_BANK23 0x01C67038 #define DAVINCI_GPIO_BANK45 0x01C67060 #define DAVINCI_GPIO_BANK67 0x01C67088 #else /* CONFIG_SOC_DA8XX */ #define DAVINCI_GPIO_BINTEN 0x01E26008 #define DAVINCI_GPIO_BANK01 0x01E26010 #define DAVINCI_GPIO_BANK23 0x01E26038 #define DAVINCI_GPIO_BANK45 0x01E26060 #define DAVINCI_GPIO_BANK67 0x01E26088 #define DAVINCI_GPIO_BANK8 0x01E260B0 #endif /* CONFIG_SOC_DA8XX */ struct davinci_gpio { unsigned int dir; unsigned int out_data; unsigned int set_data; unsigned int clr_data; unsigned int in_data; unsigned int set_rising; unsigned int clr_rising; unsigned int set_falling; unsigned int clr_falling; unsigned int intstat; }; struct davinci_gpio_bank { int num_gpio; unsigned int irq_num; unsigned int irq_mask; unsigned long *in_use; unsigned long base; }; #define davinci_gpio_bank01 ((struct davinci_gpio *)DAVINCI_GPIO_BANK01) #define davinci_gpio_bank23 ((struct davinci_gpio *)DAVINCI_GPIO_BANK23) #define davinci_gpio_bank45 ((struct davinci_gpio *)DAVINCI_GPIO_BANK45) #define davinci_gpio_bank67 ((struct davinci_gpio *)DAVINCI_GPIO_BANK67) #define davinci_gpio_bank8 ((struct davinci_gpio *)DAVINCI_GPIO_BANK8) #define gpio_status() gpio_info() #define GPIO_NAME_SIZE 20 #define MAX_NUM_GPIOS 144 #define GPIO_BANK(gp) (davinci_gpio_bank01 + ((gp) >> 5)) #define GPIO_BIT(gp) ((gp) & 0x1F) void gpio_info(void); #endif