/* * (C) Copyright 2010 * Texas Instruments, * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef _SYS_PROTO_H_ #define _SYS_PROTO_H_ #include #include #include #include #include struct omap_sysinfo { char *board_string; }; extern const struct omap_sysinfo sysinfo; extern struct omap4_prcm_regs *const prcm; void gpmc_init(void); void watchdog_init(void); u32 get_device_type(void); void do_set_mux(u32 base, struct pad_conf_entry const *array, int size); void set_muxconf_regs_non_essential(void); void sr32(void *, u32, u32, u32); u32 wait_on_value(u32, u32, void *, u32); void sdelay(unsigned long); void set_pl310_ctrl_reg(u32 val); void setup_clocks_for_console(void); void prcm_init(void); void bypass_dpll(u32 *const base); void freq_update_core(void); u32 get_sys_clk_freq(void); u32 omap4_ddr_clk(void); void cancel_out(u32 *num, u32 *den, u32 den_limit); void sdram_init(void); u32 omap4_sdram_size(void); static inline u32 running_from_sdram(void) { u32 pc; asm volatile ("mov %0, pc" : "=r" (pc)); return ((pc >= OMAP44XX_DRAM_ADDR_SPACE_START) && (pc < OMAP44XX_DRAM_ADDR_SPACE_END)); } static inline u8 uboot_loaded_by_spl(void) { /* * Configuration Header is not supported yet, so u-boot init running * from SDRAM implies that it was loaded by SPL. When this situation * changes one of these approaches could be taken: * i. Pass a magic from SPL to U-Boot and U-Boot save it at a known * location. * ii. Check the OPP. CH can support only 50% OPP while SPL initializes * the DPLLs at 100% OPP. */ return running_from_sdram(); } /* * The basic hardware init of OMAP(s_init()) can happen in 4 * different contexts: * 1. SPL running from SRAM * 2. U-Boot running from FLASH * 3. Non-XIP U-Boot loaded to SDRAM by SPL * 4. Non-XIP U-Boot loaded to SDRAM by ROM code using the * Configuration Header feature * * This function finds this context. * Defining as inline may help in compiling out unused functions in SPL */ static inline u32 omap4_hw_init_context(void) { #ifdef CONFIG_SPL_BUILD return OMAP_INIT_CONTEXT_SPL; #else if (uboot_loaded_by_spl()) return OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL; else if (running_from_sdram()) return OMAP_INIT_CONTEXT_UBOOT_AFTER_CH; else return OMAP_INIT_CONTEXT_UBOOT_FROM_NOR; #endif } static inline u32 omap_revision(void) { extern u32 *const omap4_revision; return *omap4_revision; } #endif