/* * Copyright (c) 2009 Wind River Systems, Inc. * Tom Rix * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA * * This work is derived from the linux 2.6.27 kernel source * To fetch, use the kernel repository * git://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux-2.6.git * Use the v2.6.27 tag. * * Below is the original's header including its copyright * * linux/arch/arm/plat-omap/gpio.c * * Support functions for OMAP GPIO * * Copyright (C) 2003-2005 Nokia Corporation * Written by Juha Yrjölä * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #ifndef _GPIO_H #define _GPIO_H #include struct gpio_bank { void *base; int method; }; extern const struct gpio_bank *const omap_gpio_bank; #define METHOD_GPIO_24XX 4 #endif /* _GPIO_H_ */