/* * (C) Copyright 2002 * Sysgo Real-Time Solutions, GmbH * Marius Groeger * * (C) Copyright 2002 * Sysgo Real-Time Solutions, GmbH * Alex Zuepke * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA * ******************************************************************** * NOTE: This header file defines an interface to U-Boot. Including * this (unmodified) header file in another file is considered normal * use of U-Boot, and does *not* fall under the heading of "derived * work". ******************************************************************** */ #ifndef _U_BOOT_H_ #define _U_BOOT_H_ 1 typedef struct bd_info { int bi_baudrate; /* serial console baudrate */ ulong bi_arch_number; /* unique id for this board */ ulong bi_boot_params; /* where this board expects params */ unsigned long bi_arm_freq; /* arm frequency */ unsigned long bi_dsp_freq; /* dsp core frequency */ unsigned long bi_ddr_freq; /* ddr frequency */ struct /* RAM configuration */ { ulong start; ulong size; } bi_dram[CONFIG_NR_DRAM_BANKS]; } bd_t; /* For image.h:image_check_target_arch() */ #define IH_ARCH_DEFAULT IH_ARCH_ARM #endif /* _U_BOOT_H_ */