# # (C) Copyright 2003 # Wolfgang Denk, DENX Software Engineering, wd@denx.de. # # See file CREDITS for list of people who contributed to this # project. # # This program is free software; you can redistribute it and/or # modify it under the terms of the GNU General Public License as # published by the Free Software Foundation; either version 2 of # the License, or (at your option) any later version. # # This program is distributed in the hope that it will be useful, # but WITHOUT ANY WARRANTY; without even the implied warranty of # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the # GNU General Public License for more details. # # You should have received a copy of the GNU General Public License # along with this program; if not, write to the Free Software # Foundation, Inc., 59 Temple Place, Suite 330, Boston, # MA 02111-1307 USA # CROSS_COMPILE ?= mips_4KC- # Handle special prefix in ELDK 4.0 toolchain ifneq (,$(findstring 4KCle,$(CROSS_COMPILE))) ENDIANNESS := -EL endif ifdef CONFIG_SYS_LITTLE_ENDIAN ENDIANNESS := -EL endif ifdef CONFIG_SYS_BIG_ENDIAN ENDIANNESS := -EB endif # Default to EB if no endianess is configured ENDIANNESS ?= -EB PLATFORM_CPPFLAGS += -DCONFIG_MIPS -D__MIPS__ # # From Linux arch/mips/Makefile # # GCC uses -G 0 -mabicalls -fpic as default. We don't want PIC in the kernel # code since it only slows down the whole thing. At some point we might make # use of global pointer optimizations but their use of $28 conflicts with # the current pointer optimization. # # The DECStation requires an ECOFF kernel for remote booting, other MIPS # machines may also. Since BFD is incredibly buggy with respect to # crossformat linking we rely on the elf2ecoff tool for format conversion. # # cflags-y += -G 0 -mno-abicalls -fno-pic -pipe # cflags-y += -msoft-float # LDFLAGS_vmlinux += -G 0 -static -n -nostdlib # MODFLAGS += -mlong-calls # # On the other hand, we want PIC in the U-Boot code to relocate it from ROM # to RAM. $28 is always used as gp. # PLATFORM_CPPFLAGS += -G 0 -mabicalls -fpic $(ENDIANNESS) PLATFORM_CPPFLAGS += -msoft-float PLATFORM_LDFLAGS += -G 0 -static -n -nostdlib $(ENDIANNESS) PLATFORM_RELFLAGS += -ffunction-sections -fdata-sections LDFLAGS_FINAL += --gc-sections -pie OBJCFLAGS += --remove-section=.dynsym