/* * (C) Copyright 2007 * Gerald Van Baren, Custom IDEAS, vanbaren@cideas.com * Based on code written by: * Pantelis Antoniou and * Matthew McClintock * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #include #include #include #include #include #include #include #include #define MAX_LEVEL 32 /* how deeply nested we will go */ #define SCRATCHPAD 1024 /* bytes of scratchpad memory */ #ifndef CONFIG_CMD_FDT_MAX_DUMP #define CONFIG_CMD_FDT_MAX_DUMP 64 #endif /* * Global data (for the gd->bd) */ DECLARE_GLOBAL_DATA_PTR; static int fdt_valid(void); static int fdt_parse_prop(char *const*newval, int count, char *data, int *len); static int fdt_print(const char *pathp, char *prop, int depth); static int is_printable_string(const void *data, int len); /* * The working_fdt points to our working flattened device tree. */ struct fdt_header *working_fdt; void set_working_fdt_addr(void *addr) { char buf[17]; working_fdt = addr; sprintf(buf, "%lx", (unsigned long)addr); setenv("fdtaddr", buf); } /* * Get a value from the fdt and format it to be set in the environment */ static int fdt_value_setenv(const void *nodep, int len, const char *var) { if (is_printable_string(nodep, len)) setenv(var, (void *)nodep); else if (len == 4) { char buf[11]; sprintf(buf, "0x%08X", *(uint32_t *)nodep); setenv(var, buf); } else if (len%4 == 0 && len <= 20) { /* Needed to print things like sha1 hashes. */ char buf[41]; int i; for (i = 0; i < len; i += sizeof(unsigned int)) sprintf(buf + (i * 2), "%08x", *(unsigned int *)(nodep + i)); setenv(var, buf); } else { printf("error: unprintable value\n"); return 1; } return 0; } /* * Flattened Device Tree command, see the help for parameter definitions. */ int do_fdt (cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[]) { if (argc < 2) return CMD_RET_USAGE; /* * Set the address of the fdt */ if (argv[1][0] == 'a') { unsigned long addr; /* * Set the address [and length] of the fdt. */ if (argc == 2) { if (!fdt_valid()) { return 1; } printf("The address of the fdt is %p\n", working_fdt); return 0; } addr = simple_strtoul(argv[2], NULL, 16); set_working_fdt_addr((void *)addr); if (!fdt_valid()) { return 1; } if (argc >= 4) { int len; int err; /* * Optional new length */ len = simple_strtoul(argv[3], NULL, 16); if (len < fdt_totalsize(working_fdt)) { printf ("New length %d < existing length %d, " "ignoring.\n", len, fdt_totalsize(working_fdt)); } else { /* * Open in place with a new length. */ err = fdt_open_into(working_fdt, working_fdt, len); if (err != 0) { printf ("libfdt fdt_open_into(): %s\n", fdt_strerror(err)); } } } return CMD_RET_SUCCESS; } if (!working_fdt) { puts( "No FDT memory address configured. Please configure\n" "the FDT address via \"fdt addr
\" command.\n" "Aborting!\n"); return CMD_RET_FAILURE; } /* * Move the working_fdt */ if (strncmp(argv[1], "mo", 2) == 0) { struct fdt_header *newaddr; int len; int err; if (argc < 4) return CMD_RET_USAGE; /* * Set the address and length of the fdt. */ working_fdt = (struct fdt_header *)simple_strtoul(argv[2], NULL, 16); if (!fdt_valid()) { return 1; } newaddr = (struct fdt_header *)simple_strtoul(argv[3],NULL,16); /* * If the user specifies a length, use that. Otherwise use the * current length. */ if (argc <= 4) { len = fdt_totalsize(working_fdt); } else { len = simple_strtoul(argv[4], NULL, 16); if (len < fdt_totalsize(working_fdt)) { printf ("New length 0x%X < existing length " "0x%X, aborting.\n", len, fdt_totalsize(working_fdt)); return 1; } } /* * Copy to the new location. */ err = fdt_open_into(working_fdt, newaddr, len); if (err != 0) { printf ("libfdt fdt_open_into(): %s\n", fdt_strerror(err)); return 1; } working_fdt = newaddr; /* * Make a new node */ } else if (strncmp(argv[1], "mk", 2) == 0) { char *pathp; /* path */ char *nodep; /* new node to add */ int nodeoffset; /* node offset from libfdt */ int err; /* * Parameters: Node path, new node to be appended to the path. */ if (argc < 4) return CMD_RET_USAGE; pathp = argv[2]; nodep = argv[3]; nodeoffset = fdt_path_offset (working_fdt, pathp); if (nodeoffset < 0) { /* * Not found or something else bad happened. */ printf ("libfdt fdt_path_offset() returned %s\n", fdt_strerror(nodeoffset)); return 1; } err = fdt_add_subnode(working_fdt, nodeoffset, nodep); if (err < 0) { printf ("libfdt fdt_add_subnode(): %s\n", fdt_strerror(err)); return 1; } /* * Set the value of a property in the working_fdt. */ } else if (argv[1][0] == 's') { char *pathp; /* path */ char *prop; /* property */ int nodeoffset; /* node offset from libfdt */ static char data[SCRATCHPAD]; /* storage for the property */ int len; /* new length of the property */ int ret; /* return value */ /* * Parameters: Node path, property, optional value. */ if (argc < 4) return CMD_RET_USAGE; pathp = argv[2]; prop = argv[3]; if (argc == 4) { len = 0; } else { ret = fdt_parse_prop(&argv[4], argc - 4, data, &len); if (ret != 0) return ret; } nodeoffset = fdt_path_offset (working_fdt, pathp); if (nodeoffset < 0) { /* * Not found or something else bad happened. */ printf ("libfdt fdt_path_offset() returned %s\n", fdt_strerror(nodeoffset)); return 1; } ret = fdt_setprop(working_fdt, nodeoffset, prop, data, len); if (ret < 0) { printf ("libfdt fdt_setprop(): %s\n", fdt_strerror(ret)); return 1; } /******************************************************************** * Get the value of a property in the working_fdt. ********************************************************************/ } else if (argv[1][0] == 'g') { char *subcmd; /* sub-command */ char *pathp; /* path */ char *prop; /* property */ char *var; /* variable to store result */ int nodeoffset; /* node offset from libfdt */ const void *nodep; /* property node pointer */ int len = 0; /* new length of the property */ /* * Parameters: Node path, property, optional value. */ if (argc < 5) return CMD_RET_USAGE; subcmd = argv[2]; if (argc < 6 && subcmd[0] != 's') return CMD_RET_USAGE; var = argv[3]; pathp = argv[4]; prop = argv[5]; nodeoffset = fdt_path_offset(working_fdt, pathp); if (nodeoffset < 0) { /* * Not found or something else bad happened. */ printf("libfdt fdt_path_offset() returned %s\n", fdt_strerror(nodeoffset)); return 1; } if (subcmd[0] == 'n' || (subcmd[0] == 's' && argc == 5)) { int reqIndex = -1; int startDepth = fdt_node_depth( working_fdt, nodeoffset); int curDepth = startDepth; int curIndex = -1; int nextNodeOffset = fdt_next_node( working_fdt, nodeoffset, &curDepth); if (subcmd[0] == 'n') reqIndex = simple_strtoul(argv[5], NULL, 16); while (curDepth > startDepth) { if (curDepth == startDepth + 1) curIndex++; if (subcmd[0] == 'n' && curIndex == reqIndex) { const char *nodeName = fdt_get_name( working_fdt, nextNodeOffset, NULL); setenv(var, (char *)nodeName); return 0; } nextNodeOffset = fdt_next_node( working_fdt, nextNodeOffset, &curDepth); if (nextNodeOffset < 0) break; } if (subcmd[0] == 's') { /* get the num nodes at this level */ char buf[11]; sprintf(buf, "%d", curIndex + 1); setenv(var, buf); } else { /* node index not found */ printf("libfdt node not found\n"); return 1; } } else { nodep = fdt_getprop( working_fdt, nodeoffset, prop, &len); if (len == 0) { /* no property value */ setenv(var, ""); return 0; } else if (len > 0) { if (subcmd[0] == 'v') { int ret; ret = fdt_value_setenv(nodep, len, var); if (ret != 0) return ret; } else if (subcmd[0] == 'a') { /* Get address */ char buf[11]; sprintf(buf, "0x%08X", (uint32_t)nodep); setenv(var, buf); } else if (subcmd[0] == 's') { /* Get size */ char buf[11]; sprintf(buf, "0x%08X", len); setenv(var, buf); } else return CMD_RET_USAGE; return 0; } else { printf("libfdt fdt_getprop(): %s\n", fdt_strerror(len)); return 1; } } /* * Print (recursive) / List (single level) */ } else if ((argv[1][0] == 'p') || (argv[1][0] == 'l')) { int depth = MAX_LEVEL; /* how deep to print */ char *pathp; /* path */ char *prop; /* property */ int ret; /* return value */ static char root[2] = "/"; /* * list is an alias for print, but limited to 1 level */ if (argv[1][0] == 'l') { depth = 1; } /* * Get the starting path. The root node is an oddball, * the offset is zero and has no name. */ if (argc == 2) pathp = root; else pathp = argv[2]; if (argc > 3) prop = argv[3]; else prop = NULL; ret = fdt_print(pathp, prop, depth); if (ret != 0) return ret; /* * Remove a property/node */ } else if (strncmp(argv[1], "rm", 2) == 0) { int nodeoffset; /* node offset from libfdt */ int err; /* * Get the path. The root node is an oddball, the offset * is zero and has no name. */ nodeoffset = fdt_path_offset (working_fdt, argv[2]); if (nodeoffset < 0) { /* * Not found or something else bad happened. */ printf ("libfdt fdt_path_offset() returned %s\n", fdt_strerror(nodeoffset)); return 1; } /* * Do the delete. A fourth parameter means delete a property, * otherwise delete the node. */ if (argc > 3) { err = fdt_delprop(working_fdt, nodeoffset, argv[3]); if (err < 0) { printf("libfdt fdt_delprop(): %s\n", fdt_strerror(err)); return err; } } else { err = fdt_del_node(working_fdt, nodeoffset); if (err < 0) { printf("libfdt fdt_del_node(): %s\n", fdt_strerror(err)); return err; } } /* * Display header info */ } else if (argv[1][0] == 'h') { u32 version = fdt_version(working_fdt); printf("magic:\t\t\t0x%x\n", fdt_magic(working_fdt)); printf("totalsize:\t\t0x%x (%d)\n", fdt_totalsize(working_fdt), fdt_totalsize(working_fdt)); printf("off_dt_struct:\t\t0x%x\n", fdt_off_dt_struct(working_fdt)); printf("off_dt_strings:\t\t0x%x\n", fdt_off_dt_strings(working_fdt)); printf("off_mem_rsvmap:\t\t0x%x\n", fdt_off_mem_rsvmap(working_fdt)); printf("version:\t\t%d\n", version); printf("last_comp_version:\t%d\n", fdt_last_comp_version(working_fdt)); if (version >= 2) printf("boot_cpuid_phys:\t0x%x\n", fdt_boot_cpuid_phys(working_fdt)); if (version >= 3) printf("size_dt_strings:\t0x%x\n", fdt_size_dt_strings(working_fdt)); if (version >= 17) printf("size_dt_struct:\t\t0x%x\n", fdt_size_dt_struct(working_fdt)); printf("number mem_rsv:\t\t0x%x\n", fdt_num_mem_rsv(working_fdt)); printf("\n"); /* * Set boot cpu id */ } else if (strncmp(argv[1], "boo", 3) == 0) { unsigned long tmp = simple_strtoul(argv[2], NULL, 16); fdt_set_boot_cpuid_phys(working_fdt, tmp); /* * memory command */ } else if (strncmp(argv[1], "me", 2) == 0) { uint64_t addr, size; int err; addr = simple_strtoull(argv[2], NULL, 16); size = simple_strtoull(argv[3], NULL, 16); err = fdt_fixup_memory(working_fdt, addr, size); if (err < 0) return err; /* * mem reserve commands */ } else if (strncmp(argv[1], "rs", 2) == 0) { if (argv[2][0] == 'p') { uint64_t addr, size; int total = fdt_num_mem_rsv(working_fdt); int j, err; printf("index\t\t start\t\t size\n"); printf("-------------------------------" "-----------------\n"); for (j = 0; j < total; j++) { err = fdt_get_mem_rsv(working_fdt, j, &addr, &size); if (err < 0) { printf("libfdt fdt_get_mem_rsv(): %s\n", fdt_strerror(err)); return err; } printf(" %x\t%08x%08x\t%08x%08x\n", j, (u32)(addr >> 32), (u32)(addr & 0xffffffff), (u32)(size >> 32), (u32)(size & 0xffffffff)); } } else if (argv[2][0] == 'a') { uint64_t addr, size; int err; addr = simple_strtoull(argv[3], NULL, 16); size = simple_strtoull(argv[4], NULL, 16); err = fdt_add_mem_rsv(working_fdt, addr, size); if (err < 0) { printf("libfdt fdt_add_mem_rsv(): %s\n", fdt_strerror(err)); return err; } } else if (argv[2][0] == 'd') { unsigned long idx = simple_strtoul(argv[3], NULL, 16); int err = fdt_del_mem_rsv(working_fdt, idx); if (err < 0) { printf("libfdt fdt_del_mem_rsv(): %s\n", fdt_strerror(err)); return err; } } else { /* Unrecognized command */ return CMD_RET_USAGE; } } #ifdef CONFIG_OF_BOARD_SETUP /* Call the board-specific fixup routine */ else if (strncmp(argv[1], "boa", 3) == 0) ft_board_setup(working_fdt, gd->bd); #endif /* Create a chosen node */ else if (argv[1][0] == 'c') { unsigned long initrd_start = 0, initrd_end = 0; if ((argc != 2) && (argc != 4)) return CMD_RET_USAGE; if (argc == 4) { initrd_start = simple_strtoul(argv[2], NULL, 16); initrd_end = simple_strtoul(argv[3], NULL, 16); } fdt_chosen(working_fdt, 1); fdt_initrd(working_fdt, initrd_start, initrd_end, 1); } /* resize the fdt */ else if (strncmp(argv[1], "re", 2) == 0) { fdt_resize(working_fdt); } else { /* Unrecognized command */ return CMD_RET_USAGE; } return 0; } /****************************************************************************/ static int fdt_valid(void) { int err; if (working_fdt == NULL) { printf ("The address of the fdt is invalid (NULL).\n"); return 0; } err = fdt_check_header(working_fdt); if (err == 0) return 1; /* valid */ if (err < 0) { printf("libfdt fdt_check_header(): %s", fdt_strerror(err)); /* * Be more informative on bad version. */ if (err == -FDT_ERR_BADVERSION) { if (fdt_version(working_fdt) < FDT_FIRST_SUPPORTED_VERSION) { printf (" - too old, fdt %d < %d", fdt_version(working_fdt), FDT_FIRST_SUPPORTED_VERSION); working_fdt = NULL; } if (fdt_last_comp_version(working_fdt) > FDT_LAST_SUPPORTED_VERSION) { printf (" - too new, fdt %d > %d", fdt_version(working_fdt), FDT_LAST_SUPPORTED_VERSION); working_fdt = NULL; } return 0; } printf("\n"); return 0; } return 1; } /****************************************************************************/ /* * Parse the user's input, partially heuristic. Valid formats: * <0x00112233 4 05> - an array of cells. Numbers follow standard * C conventions. * [00 11 22 .. nn] - byte stream * "string" - If the the value doesn't start with "<" or "[", it is * treated as a string. Note that the quotes are * stripped by the parser before we get the string. * newval: An array of strings containing the new property as specified * on the command line * count: The number of strings in the array * data: A bytestream to be placed in the property * len: The length of the resulting bytestream */ static int fdt_parse_prop(char * const *newval, int count, char *data, int *len) { char *cp; /* temporary char pointer */ char *newp; /* temporary newval char pointer */ unsigned long tmp; /* holds converted values */ int stridx = 0; *len = 0; newp = newval[0]; /* An array of cells */ if (*newp == '<') { newp++; while ((*newp != '>') && (stridx < count)) { /* * Keep searching until we find that last ">" * That way users don't have to escape the spaces */ if (*newp == '\0') { newp = newval[++stridx]; continue; } cp = newp; tmp = simple_strtoul(cp, &newp, 0); *(uint32_t *)data = __cpu_to_be32(tmp); data += 4; *len += 4; /* If the ptr didn't advance, something went wrong */ if ((newp - cp) <= 0) { printf("Sorry, I could not convert \"%s\"\n", cp); return 1; } while (*newp == ' ') newp++; } if (*newp != '>') { printf("Unexpected character '%c'\n", *newp); return 1; } } else if (*newp == '[') { /* * Byte stream. Convert the values. */ newp++; while ((stridx < count) && (*newp != ']')) { while (*newp == ' ') newp++; if (*newp == '\0') { newp = newval[++stridx]; continue; } if (!isxdigit(*newp)) break; tmp = simple_strtoul(newp, &newp, 16); *data++ = tmp & 0xFF; *len = *len + 1; } if (*newp != ']') { printf("Unexpected character '%c'\n", *newp); return 1; } } else { /* * Assume it is one or more strings. Copy it into our * data area for convenience (including the * terminating '\0's). */ while (stridx < count) { size_t length = strlen(newp) + 1; strcpy(data, newp); data += length; *len += length; newp = newval[++stridx]; } } return 0; } /****************************************************************************/ /* * Heuristic to guess if this is a string or concatenated strings. */ static int is_printable_string(const void *data, int len) { const char *s = data; /* zero length is not */ if (len == 0) return 0; /* must terminate with zero or '\n' */ if (s[len - 1] != '\0' && s[len - 1] != '\n') return 0; /* printable or a null byte (concatenated strings) */ while (((*s == '\0') || isprint(*s) || isspace(*s)) && (len > 0)) { /* * If we see a null, there are three possibilities: * 1) If len == 1, it is the end of the string, printable * 2) Next character also a null, not printable. * 3) Next character not a null, continue to check. */ if (s[0] == '\0') { if (len == 1) return 1; if (s[1] == '\0') return 0; } s++; len--; } /* Not the null termination, or not done yet: not printable */ if (*s != '\0' || (len != 0)) return 0; return 1; } /* * Print the property in the best format, a heuristic guess. Print as * a string, concatenated strings, a byte, word, double word, or (if all * else fails) it is printed as a stream of bytes. */ static void print_data(const void *data, int len) { int j; /* no data, don't print */ if (len == 0) return; /* * It is a string, but it may have multiple strings (embedded '\0's). */ if (is_printable_string(data, len)) { puts("\""); j = 0; while (j < len) { if (j > 0) puts("\", \""); puts(data); j += strlen(data) + 1; data += strlen(data) + 1; } puts("\""); return; } if ((len %4) == 0) { if (len > CONFIG_CMD_FDT_MAX_DUMP) printf("* 0x%08x [0x%08x]", (unsigned int)data, len); else { const u32 *p; printf("<"); for (j = 0, p = data; j < len/4; j++) printf("0x%08x%s", fdt32_to_cpu(p[j]), j < (len/4 - 1) ? " " : ""); printf(">"); } } else { /* anything else... hexdump */ if (len > CONFIG_CMD_FDT_MAX_DUMP) printf("* 0x%08x [0x%08x]", (unsigned int)data, len); else { const u8 *s; printf("["); for (j = 0, s = data; j < len; j++) printf("%02x%s", s[j], j < len - 1 ? " " : ""); printf("]"); } } } /****************************************************************************/ /* * Recursively print (a portion of) the working_fdt. The depth parameter * determines how deeply nested the fdt is printed. */ static int fdt_print(const char *pathp, char *prop, int depth) { static char tabs[MAX_LEVEL+1] = "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t" "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t"; const void *nodep; /* property node pointer */ int nodeoffset; /* node offset from libfdt */ int nextoffset; /* next node offset from libfdt */ uint32_t tag; /* tag */ int len; /* length of the property */ int level = 0; /* keep track of nesting level */ const struct fdt_property *fdt_prop; nodeoffset = fdt_path_offset (working_fdt, pathp); if (nodeoffset < 0) { /* * Not found or something else bad happened. */ printf ("libfdt fdt_path_offset() returned %s\n", fdt_strerror(nodeoffset)); return 1; } /* * The user passed in a property as well as node path. * Print only the given property and then return. */ if (prop) { nodep = fdt_getprop (working_fdt, nodeoffset, prop, &len); if (len == 0) { /* no property value */ printf("%s %s\n", pathp, prop); return 0; } else if (len > 0) { printf("%s = ", prop); print_data (nodep, len); printf("\n"); return 0; } else { printf ("libfdt fdt_getprop(): %s\n", fdt_strerror(len)); return 1; } } /* * The user passed in a node path and no property, * print the node and all subnodes. */ while(level >= 0) { tag = fdt_next_tag(working_fdt, nodeoffset, &nextoffset); switch(tag) { case FDT_BEGIN_NODE: pathp = fdt_get_name(working_fdt, nodeoffset, NULL); if (level <= depth) { if (pathp == NULL) pathp = "/* NULL pointer error */"; if (*pathp == '\0') pathp = "/"; /* root is nameless */ printf("%s%s {\n", &tabs[MAX_LEVEL - level], pathp); } level++; if (level >= MAX_LEVEL) { printf("Nested too deep, aborting.\n"); return 1; } break; case FDT_END_NODE: level--; if (level <= depth) printf("%s};\n", &tabs[MAX_LEVEL - level]); if (level == 0) { level = -1; /* exit the loop */ } break; case FDT_PROP: fdt_prop = fdt_offset_ptr(working_fdt, nodeoffset, sizeof(*fdt_prop)); pathp = fdt_string(working_fdt, fdt32_to_cpu(fdt_prop->nameoff)); len = fdt32_to_cpu(fdt_prop->len); nodep = fdt_prop->data; if (len < 0) { printf ("libfdt fdt_getprop(): %s\n", fdt_strerror(len)); return 1; } else if (len == 0) { /* the property has no value */ if (level <= depth) printf("%s%s;\n", &tabs[MAX_LEVEL - level], pathp); } else { if (level <= depth) { printf("%s%s = ", &tabs[MAX_LEVEL - level], pathp); print_data (nodep, len); printf(";\n"); } } break; case FDT_NOP: printf("%s/* NOP */\n", &tabs[MAX_LEVEL - level]); break; case FDT_END: return 1; default: if (level <= depth) printf("Unknown tag 0x%08X\n", tag); return 1; } nodeoffset = nextoffset; } return 0; } /********************************************************************/ U_BOOT_CMD( fdt, 255, 0, do_fdt, "flattened device tree utility commands", "addr [] - Set the fdt location to \n" #ifdef CONFIG_OF_BOARD_SETUP "fdt boardsetup - Do board-specific set up\n" #endif "fdt move - Copy the fdt to and make it active\n" "fdt resize - Resize fdt to size + padding to 4k addr\n" "fdt print [] - Recursive print starting at \n" "fdt list [] - Print one level starting at \n" "fdt get value - Get and store in \n" "fdt get name - Get name of node and store in \n" "fdt get addr - Get start address of and store in \n" "fdt get size [] - Get size of [] or num nodes and store in \n" "fdt set [] - Set [to ]\n" "fdt mknode - Create a new node after \n" "fdt rm [] - Delete the node or \n" "fdt header - Display header info\n" "fdt bootcpu - Set boot cpuid\n" "fdt memory - Add/Update memory node\n" "fdt rsvmem print - Show current mem reserves\n" "fdt rsvmem add - Add a mem reserve\n" "fdt rsvmem delete - Delete a mem reserves\n" "fdt chosen [ ] - Add/update the /chosen branch in the tree\n" " / - initrd start/end addr\n" "NOTE: Dereference aliases by omiting the leading '/', " "e.g. fdt print ethernet0." );