/* * (C) Copyright 2008 * Ricado Ribalda-Universidad Autonoma de Madrid-ricardo.ribalda@uam.es * This work has been supported by: QTechnology http://qtec.com/ * This program is free software: you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation, either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * You should have received a copy of the GNU General Public License * along with this program. If not, see . */ #ifndef __CONFIG_H #define __CONFIG_H /*CPU*/ #define CONFIG_440 1 #define CONFIG_XILINX_PPC440_GENERIC 1 #include "../board/xilinx/ppc440-generic/xparameters.h" /*Mem Map*/ #define CONFIG_SYS_SDRAM_SIZE_MB 256 /*Env*/ #define CONFIG_ENV_IS_IN_FLASH 1 #define CONFIG_ENV_SIZE 0x20000 #define CONFIG_ENV_SECT_SIZE 0x20000 #define CONFIG_ENV_OFFSET 0x340000 #define CONFIG_ENV_ADDR (XPAR_FLASH_MEM0_BASEADDR+CONFIG_ENV_OFFSET) /*Misc*/ #define CONFIG_SYS_PROMPT "board:/# " /* Monitor Command Prompt */ #define CONFIG_PREBOOT "echo U-Boot is up and runnining;" /*Flash*/ #define CONFIG_SYS_FLASH_SIZE (32*1024*1024) #define CONFIG_SYS_MAX_FLASH_SECT 259 #define MTDIDS_DEFAULT "nor0=ml507-flash" #define MTDPARTS_DEFAULT "mtdparts=ml507-flash:-(user)" /*Generic Configs*/ #include #endif /* __CONFIG_H */