/* * (C) Copyright 2012 * Joe Hershberger, National Instruments, joe.hershberger@ni.com * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef __ENV_ATTR_H__ #define __ENV_ATTR_H__ #define ENV_ATTR_LIST_DELIM ',' #define ENV_ATTR_SEP ':' /* * env_attr_walk takes as input an "attr_list" that takes the form: * attributes = [^,:\s]* * entry = name[:attributes] * list = entry[,list] * It will call the "callback" function with the "name" and attribute as "value" * The callback may return a non-0 to abort the list walk. * This return value will be passed through to the caller. * 0 is returned on success. */ extern int env_attr_walk(const char *attr_list, int (*callback)(const char *name, const char *value)); /* * env_attr_lookup takes as input an "attr_list" with the same form as above. * It also takes as input a "name" to look for. * If the name is found in the list, it's value is copied into "attributes". * There is no protection on attributes being too small for the value. * It returns -1 if attributes is NULL, 1 if "name" is not found, 2 if * "attr_list" is NULL. * Returns 0 on success. */ extern int env_attr_lookup(const char *attr_list, const char *name, char *attributes); #endif /* __ENV_ATTR_H__ */