/* * Copyright (c) 2012 The Chromium OS Authors. * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef _HASH_H #define _HASH_H #if defined(CONFIG_SHA1SUM_VERIFY) || defined(CONFIG_CRC32_VERIFY) #define CONFIG_HASH_VERIFY #endif struct hash_algo { const char *name; /* Name of algorithm */ int digest_size; /* Length of digest */ /** * hash_func_ws: Generic hashing function * * This is the generic prototype for a hashing function. We only * have the watchdog version at present. * * @input: Input buffer * @ilen: Input buffer length * @output: Checksum result (length depends on algorithm) * @chunk_sz: Trigger watchdog after processing this many bytes */ void (*hash_func_ws)(const unsigned char *input, unsigned int ilen, unsigned char *output, unsigned int chunk_sz); int chunk_size; /* Watchdog chunk size */ }; /* * Maximum digest size for all algorithms we support. Having this value * avoids a malloc() or C99 local declaration in common/cmd_hash.c. */ #define HASH_MAX_DIGEST_SIZE 32 enum { HASH_FLAG_VERIFY = 1 << 0, /* Enable verify mode */ HASH_FLAG_ENV = 1 << 1, /* Allow env vars */ }; /** * hash_command: Process a hash command for a particular algorithm * * This common function is used to implement specific hash commands. * * @algo_name: Hash algorithm being used (lower case!) * @flags: Flags value (HASH_FLAG_...) * @cmdtp: Pointer to command table entry * @flag: Some flags normally 0 (see CMD_FLAG_.. above) * @argc: Number of arguments (arg 0 must be the command text) * @argv: Arguments */ int hash_command(const char *algo_name, int flags, cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]); #endif