/* * (C) Copyright 2008 Semihalf * * (C) Copyright 2000-2005 * Wolfgang Denk, DENX Software Engineering, wd@denx.de. * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA * ******************************************************************** * NOTE: This header file defines an interface to U-Boot. Including * this (unmodified) header file in another file is considered normal * use of U-Boot, and does *not* fall under the heading of "derived * work". ******************************************************************** */ #ifndef __IMAGE_H__ #define __IMAGE_H__ #include "compiler.h" #ifdef USE_HOSTCC /* new uImage format support enabled on host */ #define CONFIG_FIT 1 #define CONFIG_OF_LIBFDT 1 #define CONFIG_FIT_VERBOSE 1 /* enable fit_format_{error,warning}() */ #else #include #include #include #endif /* USE_HOSTCC */ #if defined(CONFIG_FIT) #include #include #include #define CONFIG_MD5 /* FIT images need MD5 support */ #define CONFIG_SHA1 /* and SHA1 */ #endif /* * Operating System Codes */ #define IH_OS_INVALID 0 /* Invalid OS */ #define IH_OS_OPENBSD 1 /* OpenBSD */ #define IH_OS_NETBSD 2 /* NetBSD */ #define IH_OS_FREEBSD 3 /* FreeBSD */ #define IH_OS_4_4BSD 4 /* 4.4BSD */ #define IH_OS_LINUX 5 /* Linux */ #define IH_OS_SVR4 6 /* SVR4 */ #define IH_OS_ESIX 7 /* Esix */ #define IH_OS_SOLARIS 8 /* Solaris */ #define IH_OS_IRIX 9 /* Irix */ #define IH_OS_SCO 10 /* SCO */ #define IH_OS_DELL 11 /* Dell */ #define IH_OS_NCR 12 /* NCR */ #define IH_OS_LYNXOS 13 /* LynxOS */ #define IH_OS_VXWORKS 14 /* VxWorks */ #define IH_OS_PSOS 15 /* pSOS */ #define IH_OS_QNX 16 /* QNX */ #define IH_OS_U_BOOT 17 /* Firmware */ #define IH_OS_RTEMS 18 /* RTEMS */ #define IH_OS_ARTOS 19 /* ARTOS */ #define IH_OS_UNITY 20 /* Unity OS */ #define IH_OS_INTEGRITY 21 /* INTEGRITY */ #define IH_OS_OSE 22 /* OSE */ /* * CPU Architecture Codes (supported by Linux) */ #define IH_ARCH_INVALID 0 /* Invalid CPU */ #define IH_ARCH_ALPHA 1 /* Alpha */ #define IH_ARCH_ARM 2 /* ARM */ #define IH_ARCH_I386 3 /* Intel x86 */ #define IH_ARCH_IA64 4 /* IA64 */ #define IH_ARCH_MIPS 5 /* MIPS */ #define IH_ARCH_MIPS64 6 /* MIPS 64 Bit */ #define IH_ARCH_PPC 7 /* PowerPC */ #define IH_ARCH_S390 8 /* IBM S390 */ #define IH_ARCH_SH 9 /* SuperH */ #define IH_ARCH_SPARC 10 /* Sparc */ #define IH_ARCH_SPARC64 11 /* Sparc 64 Bit */ #define IH_ARCH_M68K 12 /* M68K */ #define IH_ARCH_MICROBLAZE 14 /* MicroBlaze */ #define IH_ARCH_NIOS2 15 /* Nios-II */ #define IH_ARCH_BLACKFIN 16 /* Blackfin */ #define IH_ARCH_AVR32 17 /* AVR32 */ #define IH_ARCH_ST200 18 /* STMicroelectronics ST200 */ /* * Image Types * * "Standalone Programs" are directly runnable in the environment * provided by U-Boot; it is expected that (if they behave * well) you can continue to work in U-Boot after return from * the Standalone Program. * "OS Kernel Images" are usually images of some Embedded OS which * will take over control completely. Usually these programs * will install their own set of exception handlers, device * drivers, set up the MMU, etc. - this means, that you cannot * expect to re-enter U-Boot except by resetting the CPU. * "RAMDisk Images" are more or less just data blocks, and their * parameters (address, size) are passed to an OS kernel that is * being started. * "Multi-File Images" contain several images, typically an OS * (Linux) kernel image and one or more data images like * RAMDisks. This construct is useful for instance when you want * to boot over the network using BOOTP etc., where the boot * server provides just a single image file, but you want to get * for instance an OS kernel and a RAMDisk image. * * "Multi-File Images" start with a list of image sizes, each * image size (in bytes) specified by an "uint32_t" in network * byte order. This list is terminated by an "(uint32_t)0". * Immediately after the terminating 0 follow the images, one by * one, all aligned on "uint32_t" boundaries (size rounded up to * a multiple of 4 bytes - except for the last file). * * "Firmware Images" are binary images containing firmware (like * U-Boot or FPGA images) which usually will be programmed to * flash memory. * * "Script files" are command sequences that will be executed by * U-Boot's command interpreter; this feature is especially * useful when you configure U-Boot to use a real shell (hush) * as command interpreter (=> Shell Scripts). */ #define IH_TYPE_INVALID 0 /* Invalid Image */ #define IH_TYPE_STANDALONE 1 /* Standalone Program */ #define IH_TYPE_KERNEL 2 /* OS Kernel Image */ #define IH_TYPE_RAMDISK 3 /* RAMDisk Image */ #define IH_TYPE_MULTI 4 /* Multi-File Image */ #define IH_TYPE_FIRMWARE 5 /* Firmware Image */ #define IH_TYPE_SCRIPT 6 /* Script file */ #define IH_TYPE_FILESYSTEM 7 /* Filesystem Image (any type) */ #define IH_TYPE_FLATDT 8 /* Binary Flat Device Tree Blob */ #define IH_TYPE_KWBIMAGE 9 /* Kirkwood Boot Image */ #define IH_TYPE_IMXIMAGE 10 /* Freescale IMXBoot Image */ /* * Compression Types */ #define IH_COMP_NONE 0 /* No Compression Used */ #define IH_COMP_GZIP 1 /* gzip Compression Used */ #define IH_COMP_BZIP2 2 /* bzip2 Compression Used */ #define IH_COMP_LZMA 3 /* lzma Compression Used */ #define IH_COMP_LZO 4 /* lzo Compression Used */ #define IH_MAGIC 0x27051956 /* Image Magic Number */ #define IH_NMLEN 32 /* Image Name Length */ /* * Legacy format image header, * all data in network byte order (aka natural aka bigendian). */ typedef struct image_header { uint32_t ih_magic; /* Image Header Magic Number */ uint32_t ih_hcrc; /* Image Header CRC Checksum */ uint32_t ih_time; /* Image Creation Timestamp */ uint32_t ih_size; /* Image Data Size */ uint32_t ih_load; /* Data Load Address */ uint32_t ih_ep; /* Entry Point Address */ uint32_t ih_dcrc; /* Image Data CRC Checksum */ uint8_t ih_os; /* Operating System */ uint8_t ih_arch; /* CPU architecture */ uint8_t ih_type; /* Image Type */ uint8_t ih_comp; /* Compression Type */ uint8_t ih_name[IH_NMLEN]; /* Image Name */ } image_header_t; typedef struct image_info { ulong start, end; /* start/end of blob */ ulong image_start, image_len; /* start of image within blob, len of image */ ulong load; /* load addr for the image */ uint8_t comp, type, os; /* compression, type of image, os type */ } image_info_t; /* * Legacy and FIT format headers used by do_bootm() and do_bootm_() * routines. */ typedef struct bootm_headers { /* * Legacy os image header, if it is a multi component image * then boot_get_ramdisk() and get_fdt() will attempt to get * data from second and third component accordingly. */ image_header_t *legacy_hdr_os; /* image header pointer */ image_header_t legacy_hdr_os_copy; /* header copy */ ulong legacy_hdr_valid; #if defined(CONFIG_FIT) const char *fit_uname_cfg; /* configuration node unit name */ void *fit_hdr_os; /* os FIT image header */ const char *fit_uname_os; /* os subimage node unit name */ int fit_noffset_os; /* os subimage node offset */ void *fit_hdr_rd; /* init ramdisk FIT image header */ const char *fit_uname_rd; /* init ramdisk subimage node unit name */ int fit_noffset_rd; /* init ramdisk subimage node offset */ void *fit_hdr_fdt; /* FDT blob FIT image header */ const char *fit_uname_fdt; /* FDT blob subimage node unit name */ int fit_noffset_fdt;/* FDT blob subimage node offset */ #endif #ifndef USE_HOSTCC image_info_t os; /* os image info */ ulong ep; /* entry point of OS */ ulong rd_start, rd_end;/* ramdisk start/end */ #ifdef CONFIG_OF_LIBFDT char *ft_addr; /* flat dev tree address */ #endif ulong ft_len; /* length of flat device tree */ ulong initrd_start; ulong initrd_end; ulong cmdline_start; ulong cmdline_end; bd_t *kbd; #endif int verify; /* getenv("verify")[0] != 'n' */ #define BOOTM_STATE_START (0x00000001) #define BOOTM_STATE_LOADOS (0x00000002) #define BOOTM_STATE_RAMDISK (0x00000004) #define BOOTM_STATE_FDT (0x00000008) #define BOOTM_STATE_OS_CMDLINE (0x00000010) #define BOOTM_STATE_OS_BD_T (0x00000020) #define BOOTM_STATE_OS_PREP (0x00000040) #define BOOTM_STATE_OS_GO (0x00000080) int state; #ifdef CONFIG_LMB struct lmb lmb; /* for memory mgmt */ #endif } bootm_headers_t; /* * Some systems (for example LWMON) have very short watchdog periods; * we must make sure to split long operations like memmove() or * checksum calculations into reasonable chunks. */ #ifndef CHUNKSZ #define CHUNKSZ (64 * 1024) #endif #ifndef CHUNKSZ_CRC32 #define CHUNKSZ_CRC32 (64 * 1024) #endif #ifndef CHUNKSZ_MD5 #define CHUNKSZ_MD5 (64 * 1024) #endif #ifndef CHUNKSZ_SHA1 #define CHUNKSZ_SHA1 (64 * 1024) #endif #define uimage_to_cpu(x) be32_to_cpu(x) #define cpu_to_uimage(x) cpu_to_be32(x) /* * Translation table for entries of a specific type; used by * get_table_entry_id() and get_table_entry_name(). */ typedef struct table_entry { int id; char *sname; /* short (input) name to find table entry */ char *lname; /* long (output) name to print for messages */ } table_entry_t; /* * get_table_entry_id() scans the translation table trying to find an * entry that matches the given short name. If a matching entry is * found, it's id is returned to the caller. */ int get_table_entry_id(const table_entry_t *table, const char *table_name, const char *name); /* * get_table_entry_name() scans the translation table trying to find * an entry that matches the given id. If a matching entry is found, * its long name is returned to the caller. */ char *get_table_entry_name(const table_entry_t *table, char *msg, int id); const char *genimg_get_os_name (uint8_t os); const char *genimg_get_arch_name (uint8_t arch); const char *genimg_get_type_name (uint8_t type); const char *genimg_get_comp_name (uint8_t comp); int genimg_get_os_id (const char *name); int genimg_get_arch_id (const char *name); int genimg_get_type_id (const char *name); int genimg_get_comp_id (const char *name); void genimg_print_size (uint32_t size); #ifndef USE_HOSTCC /* Image format types, returned by _get_format() routine */ #define IMAGE_FORMAT_INVALID 0x00 #define IMAGE_FORMAT_LEGACY 0x01 /* legacy image_header based format */ #define IMAGE_FORMAT_FIT 0x02 /* new, libfdt based format */ int genimg_get_format (void *img_addr); int genimg_has_config (bootm_headers_t *images); ulong genimg_get_image (ulong img_addr); int boot_get_ramdisk (int argc, char * const argv[], bootm_headers_t *images, uint8_t arch, ulong *rd_start, ulong *rd_end); #ifdef CONFIG_OF_LIBFDT int boot_get_fdt (int flag, int argc, char * const argv[], bootm_headers_t *images, char **of_flat_tree, ulong *of_size); int boot_relocate_fdt (struct lmb *lmb, ulong bootmap_base, char **of_flat_tree, ulong *of_size); #endif #ifdef CONFIG_SYS_BOOT_RAMDISK_HIGH int boot_ramdisk_high (struct lmb *lmb, ulong rd_data, ulong rd_len, ulong *initrd_start, ulong *initrd_end); #endif /* CONFIG_SYS_BOOT_RAMDISK_HIGH */ #ifdef CONFIG_SYS_BOOT_GET_CMDLINE int boot_get_cmdline (struct lmb *lmb, ulong *cmd_start, ulong *cmd_end, ulong bootmap_base); #endif /* CONFIG_SYS_BOOT_GET_CMDLINE */ #ifdef CONFIG_SYS_BOOT_GET_KBD int boot_get_kbd (struct lmb *lmb, bd_t **kbd, ulong bootmap_base); #endif /* CONFIG_SYS_BOOT_GET_KBD */ #endif /* !USE_HOSTCC */ /*******************************************************************/ /* Legacy format specific code (prefixed with image_) */ /*******************************************************************/ static inline uint32_t image_get_header_size (void) { return (sizeof (image_header_t)); } #define image_get_hdr_l(f) \ static inline uint32_t image_get_##f(const image_header_t *hdr) \ { \ return uimage_to_cpu (hdr->ih_##f); \ } image_get_hdr_l (magic) /* image_get_magic */ image_get_hdr_l (hcrc) /* image_get_hcrc */ image_get_hdr_l (time) /* image_get_time */ image_get_hdr_l (size) /* image_get_size */ image_get_hdr_l (load) /* image_get_load */ image_get_hdr_l (ep) /* image_get_ep */ image_get_hdr_l (dcrc) /* image_get_dcrc */ #define image_get_hdr_b(f) \ static inline uint8_t image_get_##f(const image_header_t *hdr) \ { \ return hdr->ih_##f; \ } image_get_hdr_b (os) /* image_get_os */ image_get_hdr_b (arch) /* image_get_arch */ image_get_hdr_b (type) /* image_get_type */ image_get_hdr_b (comp) /* image_get_comp */ static inline char *image_get_name (const image_header_t *hdr) { return (char *)hdr->ih_name; } static inline uint32_t image_get_data_size (const image_header_t *hdr) { return image_get_size (hdr); } /** * image_get_data - get image payload start address * @hdr: image header * * image_get_data() returns address of the image payload. For single * component images it is image data start. For multi component * images it points to the null terminated table of sub-images sizes. * * returns: * image payload data start address */ static inline ulong image_get_data (const image_header_t *hdr) { return ((ulong)hdr + image_get_header_size ()); } static inline uint32_t image_get_image_size (const image_header_t *hdr) { return (image_get_size (hdr) + image_get_header_size ()); } static inline ulong image_get_image_end (const image_header_t *hdr) { return ((ulong)hdr + image_get_image_size (hdr)); } #define image_set_hdr_l(f) \ static inline void image_set_##f(image_header_t *hdr, uint32_t val) \ { \ hdr->ih_##f = cpu_to_uimage (val); \ } image_set_hdr_l (magic) /* image_set_magic */ image_set_hdr_l (hcrc) /* image_set_hcrc */ image_set_hdr_l (time) /* image_set_time */ image_set_hdr_l (size) /* image_set_size */ image_set_hdr_l (load) /* image_set_load */ image_set_hdr_l (ep) /* image_set_ep */ image_set_hdr_l (dcrc) /* image_set_dcrc */ #define image_set_hdr_b(f) \ static inline void image_set_##f(image_header_t *hdr, uint8_t val) \ { \ hdr->ih_##f = val; \ } image_set_hdr_b (os) /* image_set_os */ image_set_hdr_b (arch) /* image_set_arch */ image_set_hdr_b (type) /* image_set_type */ image_set_hdr_b (comp) /* image_set_comp */ static inline void image_set_name (image_header_t *hdr, const char *name) { strncpy (image_get_name (hdr), name, IH_NMLEN); } int image_check_hcrc (const image_header_t *hdr); int image_check_dcrc (const image_header_t *hdr); #ifndef USE_HOSTCC int getenv_yesno (char *var); ulong getenv_bootm_low(void); phys_size_t getenv_bootm_size(void); void memmove_wd (void *to, void *from, size_t len, ulong chunksz); #endif static inline int image_check_magic (const image_header_t *hdr) { return (image_get_magic (hdr) == IH_MAGIC); } static inline int image_check_type (const image_header_t *hdr, uint8_t type) { return (image_get_type (hdr) == type); } static inline int image_check_arch (const image_header_t *hdr, uint8_t arch) { return (image_get_arch (hdr) == arch); } static inline int image_check_os (const image_header_t *hdr, uint8_t os) { return (image_get_os (hdr) == os); } ulong image_multi_count (const image_header_t *hdr); void image_multi_getimg (const image_header_t *hdr, ulong idx, ulong *data, ulong *len); void image_print_contents (const void *hdr); #ifndef USE_HOSTCC static inline int image_check_target_arch (const image_header_t *hdr) { #if defined(__ARM__) if (!image_check_arch (hdr, IH_ARCH_ARM)) #elif defined(__avr32__) if (!image_check_arch (hdr, IH_ARCH_AVR32)) #elif defined(__bfin__) if (!image_check_arch (hdr, IH_ARCH_BLACKFIN)) #elif defined(__I386__) if (!image_check_arch (hdr, IH_ARCH_I386)) #elif defined(__M68K__) if (!image_check_arch (hdr, IH_ARCH_M68K)) #elif defined(__microblaze__) if (!image_check_arch (hdr, IH_ARCH_MICROBLAZE)) #elif defined(__mips__) if (!image_check_arch (hdr, IH_ARCH_MIPS)) #elif defined(__nios2__) if (!image_check_arch (hdr, IH_ARCH_NIOS2)) #elif defined(__PPC__) if (!image_check_arch (hdr, IH_ARCH_PPC)) #elif defined(__sh__) if (!image_check_arch (hdr, IH_ARCH_SH)) #elif defined(__sparc__) if (!image_check_arch (hdr, IH_ARCH_SPARC)) #else # error Unknown CPU type #endif return 0; return 1; } #endif /* USE_HOSTCC */ /*******************************************************************/ /* New uImage format specific code (prefixed with fit_) */ /*******************************************************************/ #if defined(CONFIG_FIT) #define FIT_IMAGES_PATH "/images" #define FIT_CONFS_PATH "/configurations" /* hash node */ #define FIT_HASH_NODENAME "hash" #define FIT_ALGO_PROP "algo" #define FIT_VALUE_PROP "value" /* image node */ #define FIT_DATA_PROP "data" #define FIT_TIMESTAMP_PROP "timestamp" #define FIT_DESC_PROP "description" #define FIT_ARCH_PROP "arch" #define FIT_TYPE_PROP "type" #define FIT_OS_PROP "os" #define FIT_COMP_PROP "compression" #define FIT_ENTRY_PROP "entry" #define FIT_LOAD_PROP "load" /* configuration node */ #define FIT_KERNEL_PROP "kernel" #define FIT_RAMDISK_PROP "ramdisk" #define FIT_FDT_PROP "fdt" #define FIT_DEFAULT_PROP "default" #define FIT_MAX_HASH_LEN 20 /* max(crc32_len(4), sha1_len(20)) */ /* cmdline argument format parsing */ inline int fit_parse_conf (const char *spec, ulong addr_curr, ulong *addr, const char **conf_name); inline int fit_parse_subimage (const char *spec, ulong addr_curr, ulong *addr, const char **image_name); void fit_print_contents (const void *fit); void fit_image_print (const void *fit, int noffset, const char *p); void fit_image_print_hash (const void *fit, int noffset, const char *p); /** * fit_get_end - get FIT image size * @fit: pointer to the FIT format image header * * returns: * size of the FIT image (blob) in memory */ static inline ulong fit_get_size (const void *fit) { return fdt_totalsize (fit); } /** * fit_get_end - get FIT image end * @fit: pointer to the FIT format image header * * returns: * end address of the FIT image (blob) in memory */ static inline ulong fit_get_end (const void *fit) { return (ulong)fit + fdt_totalsize (fit); } /** * fit_get_name - get FIT node name * @fit: pointer to the FIT format image header * * returns: * NULL, on error * pointer to node name, on success */ static inline const char *fit_get_name (const void *fit_hdr, int noffset, int *len) { return fdt_get_name (fit_hdr, noffset, len); } int fit_get_desc (const void *fit, int noffset, char **desc); int fit_get_timestamp (const void *fit, int noffset, time_t *timestamp); int fit_image_get_node (const void *fit, const char *image_uname); int fit_image_get_os (const void *fit, int noffset, uint8_t *os); int fit_image_get_arch (const void *fit, int noffset, uint8_t *arch); int fit_image_get_type (const void *fit, int noffset, uint8_t *type); int fit_image_get_comp (const void *fit, int noffset, uint8_t *comp); int fit_image_get_load (const void *fit, int noffset, ulong *load); int fit_image_get_entry (const void *fit, int noffset, ulong *entry); int fit_image_get_data (const void *fit, int noffset, const void **data, size_t *size); int fit_image_hash_get_algo (const void *fit, int noffset, char **algo); int fit_image_hash_get_value (const void *fit, int noffset, uint8_t **value, int *value_len); int fit_set_timestamp (void *fit, int noffset, time_t timestamp); int fit_set_hashes (void *fit); int fit_image_set_hashes (void *fit, int image_noffset); int fit_image_hash_set_value (void *fit, int noffset, uint8_t *value, int value_len); int fit_image_check_hashes (const void *fit, int noffset); int fit_all_image_check_hashes (const void *fit); int fit_image_check_os (const void *fit, int noffset, uint8_t os); int fit_image_check_arch (const void *fit, int noffset, uint8_t arch); int fit_image_check_type (const void *fit, int noffset, uint8_t type); int fit_image_check_comp (const void *fit, int noffset, uint8_t comp); int fit_check_format (const void *fit); int fit_conf_get_node (const void *fit, const char *conf_uname); int fit_conf_get_kernel_node (const void *fit, int noffset); int fit_conf_get_ramdisk_node (const void *fit, int noffset); int fit_conf_get_fdt_node (const void *fit, int noffset); void fit_conf_print (const void *fit, int noffset, const char *p); #ifndef USE_HOSTCC static inline int fit_image_check_target_arch (const void *fdt, int node) { #if defined(__ARM__) if (!fit_image_check_arch (fdt, node, IH_ARCH_ARM)) #elif defined(__avr32__) if (!fit_image_check_arch (fdt, node, IH_ARCH_AVR32)) #elif defined(__bfin__) if (!fit_image_check_arch (fdt, node, IH_ARCH_BLACKFIN)) #elif defined(__I386__) if (!fit_image_check_arch (fdt, node, IH_ARCH_I386)) #elif defined(__M68K__) if (!fit_image_check_arch (fdt, node, IH_ARCH_M68K)) #elif defined(__microblaze__) if (!fit_image_check_arch (fdt, node, IH_ARCH_MICROBLAZE)) #elif defined(__mips__) if (!fit_image_check_arch (fdt, node, IH_ARCH_MIPS)) #elif defined(__nios2__) if (!fit_image_check_arch (fdt, node, IH_ARCH_NIOS2)) #elif defined(__PPC__) if (!fit_image_check_arch (fdt, node, IH_ARCH_PPC)) #elif defined(__sh__) if (!fit_image_check_arch (fdt, node, IH_ARCH_SH)) #elif defined(__sparc__) if (!fit_image_check_arch (fdt, node, IH_ARCH_SPARC)) #else # error Unknown CPU type #endif return 0; return 1; } #endif /* USE_HOSTCC */ #ifdef CONFIG_FIT_VERBOSE #define fit_unsupported(msg) printf ("! %s:%d " \ "FIT images not supported for '%s'\n", \ __FILE__, __LINE__, (msg)) #define fit_unsupported_reset(msg) printf ("! %s:%d " \ "FIT images not supported for '%s' " \ "- must reset board to recover!\n", \ __FILE__, __LINE__, (msg)) #else #define fit_unsupported(msg) #define fit_unsupported_reset(msg) #endif /* CONFIG_FIT_VERBOSE */ #endif /* CONFIG_FIT */ #endif /* __IMAGE_H__ */