/* * Interface to SPI flash * * Copyright (C) 2008 Atmel Corporation * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * version 2 as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef _SPI_FLASH_H_ #define _SPI_FLASH_H_ #include #include #include struct spi_flash { struct spi_slave *spi; const char *name; /* Total flash size */ u32 size; /* Write (page) size */ u32 page_size; /* Erase (sector) size */ u32 sector_size; #ifdef CONFIG_SPI_FLASH_BAR /* Bank read cmd */ u8 bank_read_cmd; /* Bank write cmd */ u8 bank_write_cmd; /* Current flash bank */ u8 bank_curr; #endif /* Poll cmd - for flash erase/program */ u8 poll_cmd; void *memory_map; /* Address of read-only SPI flash access */ int (*read)(struct spi_flash *flash, u32 offset, size_t len, void *buf); int (*write)(struct spi_flash *flash, u32 offset, size_t len, const void *buf); int (*erase)(struct spi_flash *flash, u32 offset, size_t len); }; /** * spi_flash_do_alloc - Allocate a new spi flash structure * * The structure is allocated and cleared with default values for * read, write and erase, which the caller can modify. The caller must set * up size, page_size and sector_size. * * Use the helper macro spi_flash_alloc() to call this. * * @offset: Offset of struct spi_slave within slave structure * @size: Size of slave structure * @spi: SPI slave * @name: Name of SPI flash device */ void *spi_flash_do_alloc(int offset, int size, struct spi_slave *spi, const char *name); /** * spi_flash_alloc - Allocate a new SPI flash structure * * @_struct: Name of structure to allocate (e.g. struct ramtron_spi_fram). This * structure must contain a member 'struct spi_flash *flash'. * @spi: SPI slave * @name: Name of SPI flash device */ #define spi_flash_alloc(_struct, spi, name) \ spi_flash_do_alloc(offsetof(_struct, flash), sizeof(_struct), \ spi, name) /** * spi_flash_alloc_base - Allocate a new SPI flash structure with no private data * * @spi: SPI slave * @name: Name of SPI flash device */ #define spi_flash_alloc_base(spi, name) \ spi_flash_do_alloc(0, sizeof(struct spi_flash), spi, name) struct spi_flash *spi_flash_probe(unsigned int bus, unsigned int cs, unsigned int max_hz, unsigned int spi_mode); void spi_flash_free(struct spi_flash *flash); static inline int spi_flash_read(struct spi_flash *flash, u32 offset, size_t len, void *buf) { return flash->read(flash, offset, len, buf); } static inline int spi_flash_write(struct spi_flash *flash, u32 offset, size_t len, const void *buf) { return flash->write(flash, offset, len, buf); } static inline int spi_flash_erase(struct spi_flash *flash, u32 offset, size_t len) { return flash->erase(flash, offset, len); } void spi_boot(void) __noreturn; #endif /* _SPI_FLASH_H_ */