/* * NAND boot for Freescale Enhanced Local Bus Controller, Flash Control Machine * * (C) Copyright 2006-2008 * Stefan Roese, DENX Software Engineering, sr@denx.de. * * Copyright (c) 2008 Freescale Semiconductor, Inc. * Author: Scott Wood * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #include #include #include #include #include #define WINDOW_SIZE 8192 static void nand_wait(void) { fsl_lbus_t *regs = (fsl_lbus_t *)(CONFIG_SYS_IMMR + 0x5000); for (;;) { uint32_t status = in_be32(®s->ltesr); if (status == 1) return; if (status & 1) { puts("read failed (ltesr)\n"); for (;;); } } } static void nand_load(unsigned int offs, int uboot_size, uchar *dst) { fsl_lbus_t *regs = (fsl_lbus_t *)(CONFIG_SYS_IMMR + 0x5000); uchar *buf = (uchar *)CONFIG_SYS_NAND_BASE; int large = in_be32(®s->bank[0].or) & OR_FCM_PGS; int block_shift = large ? 17 : 14; int block_size = 1 << block_shift; int page_size = large ? 2048 : 512; int bad_marker = large ? page_size + 0 : page_size + 5; int fmr = (15 << FMR_CWTO_SHIFT) | (2 << FMR_AL_SHIFT) | 2; int pos = 0; if (offs & (block_size - 1)) { puts("bad offset\n"); for (;;); } if (large) { fmr |= FMR_ECCM; out_be32(®s->fcr, (NAND_CMD_READ0 << FCR_CMD0_SHIFT) | (NAND_CMD_READSTART << FCR_CMD1_SHIFT)); out_be32(®s->fir, (FIR_OP_CW0 << FIR_OP0_SHIFT) | (FIR_OP_CA << FIR_OP1_SHIFT) | (FIR_OP_PA << FIR_OP2_SHIFT) | (FIR_OP_CW1 << FIR_OP3_SHIFT) | (FIR_OP_RBW << FIR_OP4_SHIFT)); } else { out_be32(®s->fcr, NAND_CMD_READ0 << FCR_CMD0_SHIFT); out_be32(®s->fir, (FIR_OP_CW0 << FIR_OP0_SHIFT) | (FIR_OP_CA << FIR_OP1_SHIFT) | (FIR_OP_PA << FIR_OP2_SHIFT) | (FIR_OP_RBW << FIR_OP3_SHIFT)); } out_be32(®s->fbcr, 0); clrsetbits_be32(®s->bank[0].br, BR_DECC, BR_DECC_CHK_GEN); while (pos < uboot_size) { int i = 0; out_be32(®s->fbar, offs >> block_shift); do { int j; unsigned int page_offs = (offs & (block_size - 1)) << 1; out_be32(®s->ltesr, ~0); out_be32(®s->lteatr, 0); out_be32(®s->fpar, page_offs); out_be32(®s->fmr, fmr); out_be32(®s->lsor, 0); nand_wait(); page_offs %= WINDOW_SIZE; /* * If either of the first two pages are marked bad, * continue to the next block. */ if (i++ < 2 && buf[page_offs + bad_marker] != 0xff) { puts("skipping\n"); offs = (offs + block_size) & ~(block_size - 1); pos &= ~(block_size - 1); break; } for (j = 0; j < page_size; j++) dst[pos + j] = buf[page_offs + j]; pos += page_size; offs += page_size; } while (offs & (block_size - 1)); } } /* * The main entry for NAND booting. It's necessary that SDRAM is already * configured and available since this code loads the main U-Boot image * from NAND into SDRAM and starts it from there. */ void nand_boot(void) { __attribute__((noreturn)) void (*uboot)(void); /* * Load U-Boot image from NAND into RAM */ nand_load(CONFIG_SYS_NAND_U_BOOT_OFFS, CONFIG_SYS_NAND_U_BOOT_SIZE, (uchar *)CONFIG_SYS_NAND_U_BOOT_DST); /* * Jump to U-Boot image */ puts("transfering control\n"); uboot = (void *)CONFIG_SYS_NAND_U_BOOT_START; uboot(); }