/* * (C) Copyright 2010 * Linaro LTD, www.linaro.org * Author: John Rigby * Based on TI's signGP.c * * (C) Copyright 2009 * Stefano Babic, DENX Software Engineering, sbabic@denx.de. * * (C) Copyright 2008 * Marvell Semiconductor * Written-by: Prafulla Wadaskar * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ /* Required to obtain the getline prototype from stdio.h */ #define _GNU_SOURCE #include "mkimage.h" #include #include "omapimage.h" /* Header size is CH header rounded up to 512 bytes plus GP header */ #define OMAP_CH_HDR_SIZE 512 #define OMAP_GP_HDR_SIZE (sizeof(struct gp_header)) #define OMAP_FILE_HDR_SIZE (OMAP_CH_HDR_SIZE+OMAP_GP_HDR_SIZE) static int do_swap32 = 0; static uint32_t omapimage_swap32(uint32_t data) { uint32_t result = 0; result = (data & 0xFF000000) >> 24; result |= (data & 0x00FF0000) >> 8; result |= (data & 0x0000FF00) << 8; result |= (data & 0x000000FF) << 24; return result; } static uint8_t omapimage_header[OMAP_FILE_HDR_SIZE]; static int omapimage_check_image_types(uint8_t type) { if (type == IH_TYPE_OMAPIMAGE) return EXIT_SUCCESS; else { return EXIT_FAILURE; } } /* * Only the simplest image type is currently supported: * TOC pointing to CHSETTINGS * TOC terminator * CHSETTINGS * * padding to OMAP_CH_HDR_SIZE bytes * * gp header * size * load_addr */ static int valid_gph_size(uint32_t size) { return size; } static int valid_gph_load_addr(uint32_t load_addr) { return load_addr; } static int omapimage_verify_header(unsigned char *ptr, int image_size, struct mkimage_params *params) { struct ch_toc *toc = (struct ch_toc *)ptr; struct gp_header *gph = (struct gp_header *)(ptr+OMAP_CH_HDR_SIZE); uint32_t offset, size, gph_size, gph_load_addr; while (toc->section_offset != 0xffffffff && toc->section_size != 0xffffffff) { if (do_swap32) { offset = omapimage_swap32(toc->section_offset); size = omapimage_swap32(toc->section_size); } else { offset = toc->section_offset; size = toc->section_size; } if (!offset || !size) return -1; if (offset >= OMAP_CH_HDR_SIZE || offset+size >= OMAP_CH_HDR_SIZE) return -1; toc++; } if (do_swap32) { gph_size = omapimage_swap32(gph->size); gph_load_addr = omapimage_swap32(gph->load_addr); } else { gph_size = gph->size; gph_load_addr = gph->load_addr; } if (!valid_gph_size(gph_size)) return -1; if (!valid_gph_load_addr(gph_load_addr)) return -1; return 0; } static void omapimage_print_section(struct ch_settings *chs) { const char *section_name; if (chs->section_key) section_name = "CHSETTINGS"; else section_name = "UNKNOWNKEY"; printf("%s (%x) " "valid:%x " "version:%x " "reserved:%x " "flags:%x\n", section_name, chs->section_key, chs->valid, chs->version, chs->reserved, chs->flags); } static void omapimage_print_header(const void *ptr) { const struct ch_toc *toc = (struct ch_toc *)ptr; const struct gp_header *gph = (struct gp_header *)(ptr+OMAP_CH_HDR_SIZE); uint32_t offset, size, gph_size, gph_load_addr; while (toc->section_offset != 0xffffffff && toc->section_size != 0xffffffff) { if (do_swap32) { offset = omapimage_swap32(toc->section_offset); size = omapimage_swap32(toc->section_size); } else { offset = toc->section_offset; size = toc->section_size; } if (offset >= OMAP_CH_HDR_SIZE || offset+size >= OMAP_CH_HDR_SIZE) exit(EXIT_FAILURE); printf("Section %s offset %x length %x\n", toc->section_name, toc->section_offset, toc->section_size); omapimage_print_section((struct ch_settings *)(ptr+offset)); toc++; } if (do_swap32) { gph_size = omapimage_swap32(gph->size); gph_load_addr = omapimage_swap32(gph->load_addr); } else { gph_size = gph->size; gph_load_addr = gph->load_addr; } if (!valid_gph_size(gph_size)) { fprintf(stderr, "Error: invalid image size %x\n", gph_size); exit(EXIT_FAILURE); } if (!valid_gph_load_addr(gph_load_addr)) { fprintf(stderr, "Error: invalid image load address %x\n", gph_load_addr); exit(EXIT_FAILURE); } printf("GP Header: Size %x LoadAddr %x\n", gph_size, gph_load_addr); } static int toc_offset(void *hdr, void *member) { return member - hdr; } static void omapimage_set_header(void *ptr, struct stat *sbuf, int ifd, struct mkimage_params *params) { struct ch_toc *toc = (struct ch_toc *)ptr; struct ch_settings *chs = (struct ch_settings *) (ptr + 2 * sizeof(*toc)); struct gp_header *gph = (struct gp_header *)(ptr + OMAP_CH_HDR_SIZE); toc->section_offset = toc_offset(ptr, chs); toc->section_size = sizeof(struct ch_settings); strcpy((char *)toc->section_name, "CHSETTINGS"); chs->section_key = KEY_CHSETTINGS; chs->valid = 0; chs->version = 1; chs->reserved = 0; chs->flags = 0; toc++; memset(toc, 0xff, sizeof(*toc)); gph->size = sbuf->st_size - OMAP_FILE_HDR_SIZE; gph->load_addr = params->addr; if (strncmp(params->imagename, "byteswap", 8) == 0) { do_swap32 = 1; int swapped = 0; uint32_t *data = (uint32_t *)ptr; while (swapped <= (sbuf->st_size / sizeof(uint32_t))) { *data = omapimage_swap32(*data); swapped++; data++; } } } int omapimage_check_params(struct mkimage_params *params) { return (params->dflag && (params->fflag || params->lflag)) || (params->fflag && (params->dflag || params->lflag)) || (params->lflag && (params->dflag || params->fflag)); } /* * omapimage parameters */ static struct image_type_params omapimage_params = { .name = "TI OMAP CH/GP Boot Image support", .header_size = OMAP_FILE_HDR_SIZE, .hdr = (void *)&omapimage_header, .check_image_type = omapimage_check_image_types, .verify_header = omapimage_verify_header, .print_header = omapimage_print_header, .set_header = omapimage_set_header, .check_params = omapimage_check_params, }; void init_omap_image_type(void) { mkimage_register(&omapimage_params); }