/* * (C) Copyright 2010 * Linaro LTD, www.linaro.org * Author John Rigby * Based on TI's signGP.c * * See file CREDITS for list of people who contributed to this * project. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #ifndef _OMAPIMAGE_H_ #define _OMAPIMAGE_H_ struct ch_toc { uint32_t section_offset; uint32_t section_size; uint8_t unused[12]; uint8_t section_name[12]; }; struct ch_settings { uint32_t section_key; uint8_t valid; uint8_t version; uint16_t reserved; uint32_t flags; }; struct gp_header { uint32_t size; uint32_t load_addr; }; #define KEY_CHSETTINGS 0xC0C0C0C1 #endif /* _OMAPIMAGE_H_ */