]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blobdiff - README
Merge branch 'u-boot/master' into 'u-boot-arm/master'
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 67a071fccac5f909a2193d39350757fd14235611..14c83f4bb1796698e3a88b192a390395c51febeb 100644 (file)
--- a/README
+++ b/README
@@ -634,14 +634,6 @@ The following options need to be configured:
                boot loader that has already initialized the UART.  Define this
                variable to flush the UART at init time.
 
-               CONFIG_SYS_NS16550_BROKEN_TEMT
-
-               16550 UART set the Transmitter Empty (TEMT) Bit when all output
-               has finished and the transmitter is totally empty. U-Boot waits
-               for this bit to be set to initialize the serial console. On some
-               broken platforms this bit is not set in SPL making U-Boot to
-               hang while waiting for TEMT. Define this option to avoid it.
-
 
 - Console Interface:
                Depending on board, define exactly one serial port
@@ -2972,8 +2964,11 @@ FIT uImage format:
                Support for lib/libgeneric.o in SPL binary
 
                CONFIG_SPL_PAD_TO
-               Linker address to which the SPL should be padded before
-               appending the SPL payload.
+               Image offset to which the SPL should be padded before appending
+               the SPL payload. By default, this is defined as
+               CONFIG_SPL_MAX_SIZE, or 0 if CONFIG_SPL_MAX_SIZE is undefined.
+               CONFIG_SPL_PAD_TO must be either 0, meaning to append the SPL
+               payload without any padding, or >= CONFIG_SPL_MAX_SIZE.
 
                CONFIG_SPL_TARGET
                Final target image containing SPL and payload.  Some SPLs
@@ -3846,9 +3841,13 @@ Low Level (hardware related) configuration options:
 - CONFIG_SYS_SRIOn_MEM_SIZE:
                Size of SRIO port 'n' memory region
 
-- CONFIG_SYS_NDFC_16
-               Defined to tell the NDFC that the NAND chip is using a
-               16 bit bus.
+- CONFIG_SYS_NAND_BUSWIDTH_16BIT
+               Defined to tell the NAND controller that the NAND chip is using
+               a 16 bit bus.
+               Not all NAND drivers use this symbol.
+               Example of drivers that use it:
+               - drivers/mtd/nand/ndfc.c
+               - drivers/mtd/nand/mxc_nand.c
 
 - CONFIG_SYS_NDFC_EBC0_CFG
                Sets the EBC0_CFG register for the NDFC. If not defined