index 4428205b86aa5273c95ca6f820667ffb5d63e2d8..5793b0a2069ad5c2fac40f29c7b9c9a5c4d1e5f2 100644 (file)
--- a/README
+++ b/README
symbol should be set to the TLB1 entry to be used for this
purpose.
+ CONFIG_SYS_FSL_ERRATUM_A004510
+
+ Enables a workaround for erratum A004510. If set,
+ then CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV and
+ CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY must be set.
+
+ CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV
+ CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV2 (optional)
+
+ Defines one or two SoC revisions (low 8 bits of SVR)
+ for which the A004510 workaround should be applied.
+
+ The rest of SVR is either not relevant to the decision
+ of whether the erratum is present (e.g. p2040 versus
+ p2041) or is implied by the build target, which controls
+ whether CONFIG_SYS_FSL_ERRATUM_A004510 is set.
+
+ See Freescale App Note 4493 for more information about
+ this erratum.
+
+ CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY
+
+ This is the value to write into CCSR offset 0x18600
+ according to the A004510 workaround.
+
- Generic CPU options:
CONFIG_SYS_BIG_ENDIAN, CONFIG_SYS_LITTLE_ENDIAN
These two #defines specify the address and size of the
environment area within the remote memory space. The
local device can get the environment from remote memory
- space by SRIO or other links.
+ space by SRIO or PCIE links.
BE CAREFUL! For some special cases, the local device can not use
"saveenv" command. For example, the local device will get the
-environment stored in a remote NOR flash by SRIO link, but it can
-not erase, write this NOR flash by SRIO interface.
+environment stored in a remote NOR flash by SRIO or PCIE link,
+but it can not erase, write this NOR flash by SRIO or PCIE interface.
- CONFIG_ENV_IS_IN_NAND:
- CONFIG_SYS_QE_FMAN_FW_IN_REMOTE
Specifies that QE/FMAN firmware is located in the remote (master)
memory space. CONFIG_SYS_FMAN_FW_ADDR is a virtual address which
- can be mapped from slave TLB->slave LAW->slave SRIO outbound window
- ->master inbound window->master LAW->the ucode address in master's
- NOR flash.
+ can be mapped from slave TLB->slave LAW->slave SRIO or PCIE outbound
+ window->master inbound window->master LAW->the ucode address in
+ master's memory space.
Building the Software:
======================