]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blobdiff - README
Merge branch 'master' of git://git.denx.de/u-boot-x86
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 61e2e1ffc7952935ee150b1397483befeff21e6a..5a86ae9c5f9188dd53a8b54ce3eb9554f2485f41 100644 (file)
--- a/README
+++ b/README
@@ -54,6 +54,11 @@ In case of problems see the CHANGELOG and CREDITS files to find out
 who contributed the specific port. The MAINTAINERS file lists board
 maintainers.
 
+Note: There is no CHANGELOG file in the actual U-Boot source tree;
+it can be created dynamically from the Git log using:
+
+       make CHANGELOG
+
 
 Where to get help:
 ==================
@@ -363,6 +368,12 @@ The following options need to be configured:
                ICache only when Code runs from RAM.
 
 - 85xx CPU Options:
+               CONFIG_SYS_PPC64
+
+               Specifies that the core is a 64-bit PowerPC implementation (implements
+               the "64" category of the Power ISA). This is necessary for ePAPR
+               compliance, among other possible reasons.
+
                CONFIG_SYS_FSL_TBCLK_DIV
 
                Defines the core time base clock divider ratio compared to the
@@ -805,9 +816,11 @@ The following options need to be configured:
                CONFIG_CMD_EEPROM       * EEPROM read/write support
                CONFIG_CMD_ELF          * bootelf, bootvx
                CONFIG_CMD_EXPORTENV    * export the environment
+               CONFIG_CMD_EXT2         * ext2 command support
+               CONFIG_CMD_EXT4         * ext4 command support
                CONFIG_CMD_SAVEENV        saveenv
                CONFIG_CMD_FDC          * Floppy Disk Support
-               CONFIG_CMD_FAT          * FAT partition support
+               CONFIG_CMD_FAT          * FAT command support
                CONFIG_CMD_FDOS         * Dos diskette Support
                CONFIG_CMD_FLASH          flinfo, erase, protect
                CONFIG_CMD_FPGA           FPGA device initialization support
@@ -1037,6 +1050,9 @@ The following options need to be configured:
                devices.
                CONFIG_SYS_SCSI_SYM53C8XX_CCF to fix clock timing (80Mhz)
 
+                The environment variable 'scsidevs' is set to the number of
+                SCSI devices found during the last scan.
+
 - NETWORK Support (PCI):
                CONFIG_E1000
                Support for Intel 8254x/8257x gigabit chips.
@@ -1088,7 +1104,7 @@ The following options need to be configured:
                CONFIG_CALXEDA_XGMAC
                Support for the Calxeda XGMAC device
 
-               CONFIG_DRIVER_LAN91C96
+               CONFIG_LAN91C96
                Support for SMSC's LAN91C96 chips.
 
                        CONFIG_LAN91C96_BASE
@@ -1098,7 +1114,7 @@ The following options need to be configured:
                        CONFIG_LAN91C96_USE_32_BIT
                        Define this to enable 32 bit addressing
 
-               CONFIG_DRIVER_SMC91111
+               CONFIG_SMC91111
                Support for SMSC's LAN91C111 chip
 
                        CONFIG_SMC91111_BASE
@@ -1320,6 +1336,13 @@ The following options need to be configured:
                This will also enable the command "fatwrite" enabling the
                user to write files to FAT.
 
+CBFS (Coreboot Filesystem) support
+               CONFIG_CMD_CBFS
+
+               Define this to enable support for reading from a Coreboot
+               filesystem. Available commands are cbfsinit, cbfsinfo, cbfsls
+               and cbfsload.
+
 - Keyboard Support:
                CONFIG_ISA_KEYBOARD
 
@@ -1391,6 +1414,13 @@ The following options need to be configured:
                boot.  See the documentation file README.video for a
                description of this variable.
 
+               CONFIG_VIDEO_VGA
+
+               Enable the VGA video / BIOS for x86. The alternative if you
+               are using coreboot is to use the coreboot frame buffer
+               driver.
+
+
 - Keyboard Support:
                CONFIG_KEYBOARD
 
@@ -1451,6 +1481,11 @@ The following options need to be configured:
                Normally display is black on white background; define
                CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
 
+               CONFIG_LCD_BMP_RLE8
+
+               Support drawing of RLE8-compressed bitmaps on the LCD.
+
+
 - Splash Screen Support: CONFIG_SPLASH_SCREEN
 
                If this option is set, the environment is checked for
@@ -2173,10 +2208,18 @@ The following options need to be configured:
                following board configurations are known to be
                "pRAM-clean":
 
-                       ETX094, IVMS8, IVML24, SPD8xx, TQM8xxL,
-                       HERMES, IP860, RPXlite, LWMON, LANTEC,
+                       IVMS8, IVML24, SPD8xx, TQM8xxL,
+                       HERMES, IP860, RPXlite, LWMON,
                        FLAGADM, TQM8260
 
+- Access to physical memory region (> 4GB)
+               Some basic support is provided for operations on memory not
+               normally accessible to U-Boot - e.g. some architectures
+               support access to more than 4GB of memory on 32-bit
+               machines using physical address extension or similar.
+               Define CONFIG_PHYSMEM to access this basic support, which
+               currently only supports clearing the memory.
+
 - Error Recovery:
                CONFIG_PANIC_HANG
 
@@ -2300,6 +2343,12 @@ The following options need to be configured:
                - CONFIG_SYS_VENDOR
                - CONFIG_SYS_SOC
 
+               CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
+
+               Define this in order to add variables describing certain
+               run-time determined information about the hardware to the
+               environment.  These will be named board_name, board_rev.
+
 - DataFlash Support:
                CONFIG_HAS_DATAFLASH
 
@@ -2573,6 +2622,17 @@ FIT uImage format:
  -150  common/cmd_nand.c       Incorrect FIT image format
   151  common/cmd_nand.c       FIT image format OK
 
+- FIT image support:
+               CONFIG_FIT
+               Enable support for the FIT uImage format.
+
+               CONFIG_FIT_BEST_MATCH
+               When no configuration is explicitly selected, default to the
+               one whose fdt's compatibility field best matches that of
+               U-Boot itself. A match is considered "best" if it matches the
+               most specific compatibility entry of U-Boot's fdt's root node.
+               The order of entries in the configuration's fdt is ignored.
+
 - Standalone program support:
                CONFIG_STANDALONE_LOAD_ADDR
 
@@ -2624,6 +2684,10 @@ FIT uImage format:
                CONFIG_SPL_TEXT_BASE
                TEXT_BASE for linking the SPL binary.
 
+               CONFIG_SPL_RELOC_TEXT_BASE
+               Address to relocate to.  If unspecified, this is equal to
+               CONFIG_SPL_TEXT_BASE (i.e. no relocation is done).
+
                CONFIG_SPL_BSS_START_ADDR
                Link address for the BSS within the SPL binary.
 
@@ -2633,6 +2697,11 @@ FIT uImage format:
                CONFIG_SPL_STACK
                Adress of the start of the stack SPL will use
 
+               CONFIG_SPL_RELOC_STACK
+               Adress of the start of the stack SPL will use after
+               relocation.  If unspecified, this is equal to
+               CONFIG_SPL_STACK.
+
                CONFIG_SYS_SPL_MALLOC_START
                Starting address of the malloc pool used in SPL.
 
@@ -2648,6 +2717,9 @@ FIT uImage format:
                For ARM, enable an optional function to print more information
                about the running system.
 
+               CONFIG_SPL_INIT_MINIMAL
+               Arch init code should be built for a very small image
+
                CONFIG_SPL_LIBCOMMON_SUPPORT
                Support for common/libcommon.o in SPL binary
 
@@ -2675,8 +2747,19 @@ FIT uImage format:
                CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME
                Filename to read to load U-Boot when reading from FAT
 
+               CONFIG_SPL_NAND_BASE
+               Include nand_base.c in the SPL.  Requires
+               CONFIG_SPL_NAND_DRIVERS.
+
+               CONFIG_SPL_NAND_DRIVERS
+               SPL uses normal NAND drivers, not minimal drivers.
+
+               CONFIG_SPL_NAND_ECC
+               Include standard software ECC in the SPL
+
                CONFIG_SPL_NAND_SIMPLE
-               Support for drivers/mtd/nand/libnand.o in SPL binary
+               Support for NAND boot using simple NAND drivers that
+               expose the cmd_ctrl() interface.
 
                CONFIG_SYS_NAND_5_ADDR_CYCLE, CONFIG_SYS_NAND_PAGE_COUNT,
                CONFIG_SYS_NAND_PAGE_SIZE, CONFIG_SYS_NAND_OOBSIZE,
@@ -2684,15 +2767,19 @@ FIT uImage format:
                CONFIG_SYS_NAND_ECCPOS, CONFIG_SYS_NAND_ECCSIZE,
                CONFIG_SYS_NAND_ECCBYTES
                Defines the size and behavior of the NAND that SPL uses
-               to read U-Boot with CONFIG_SPL_NAND_SIMPLE
+               to read U-Boot
 
                CONFIG_SYS_NAND_U_BOOT_OFFS
-               Location in NAND for CONFIG_SPL_NAND_SIMPLE to read U-Boot
-               from.
+               Location in NAND to read U-Boot from
+
+               CONFIG_SYS_NAND_U_BOOT_DST
+               Location in memory to load U-Boot to
+
+               CONFIG_SYS_NAND_U_BOOT_SIZE
+               Size of image to load
 
                CONFIG_SYS_NAND_U_BOOT_START
-               Location in memory for CONFIG_SPL_NAND_SIMPLE to load U-Boot
-               to.
+               Entry point in loaded image to jump to
 
                CONFIG_SYS_NAND_HW_ECC_OOBFIRST
                Define this if you need to first read the OOB and then the
@@ -2717,6 +2804,11 @@ FIT uImage format:
                CONFIG_SPL_LIBGENERIC_SUPPORT
                Support for lib/libgeneric.o in SPL binary
 
+               CONFIG_SPL_TARGET
+               Final target image containing SPL and payload.  Some SPLs
+               use an arch-specific makefile fragment instead, for
+               example if more than one image needs to be produced.
+
 Modem Support:
 --------------
 
@@ -3592,6 +3684,16 @@ Low Level (hardware related) configuration options:
                be used if available. These functions may be faster under some
                conditions but may increase the binary size.
 
+- CONFIG_X86_NO_RESET_VECTOR
+               If defined, the x86 reset vector code is excluded. You will need
+               to do this when U-Boot is running from Coreboot.
+
+- CONFIG_X86_NO_REAL_MODE
+               If defined, x86 real mode code is omitted. This assumes a
+               32-bit environment where such code is not needed. You will
+               need to do this when U-Boot is running from Coreboot.
+
+
 Freescale QE/FMAN Firmware Support:
 -----------------------------------
 
@@ -3819,6 +3921,7 @@ saveenv - save environment variables to persistent storage
 protect - enable or disable FLASH write protection
 erase  - erase FLASH memory
 flinfo - print FLASH memory information
+nand   - NAND memory operations (see doc/README.nand)
 bdinfo - print Board Info structure
 iminfo - print header information for application image
 coninfo - print console devices and informations