index bb1b725672a7dab8ad435aaa8ef5813514f282d5..5a86ae9c5f9188dd53a8b54ce3eb9554f2485f41 100644 (file)
--- a/README
+++ b/README
who contributed the specific port. The MAINTAINERS file lists board
maintainers.
+Note: There is no CHANGELOG file in the actual U-Boot source tree;
+it can be created dynamically from the Git log using:
+
+ make CHANGELOG
+
Where to get help:
==================
ICache only when Code runs from RAM.
- 85xx CPU Options:
+ CONFIG_SYS_PPC64
+
+ Specifies that the core is a 64-bit PowerPC implementation (implements
+ the "64" category of the Power ISA). This is necessary for ePAPR
+ compliance, among other possible reasons.
+
CONFIG_SYS_FSL_TBCLK_DIV
Defines the core time base clock divider ratio compared to the
symbol should be set to the TLB1 entry to be used for this
purpose.
+ CONFIG_SYS_FSL_ERRATUM_A004510
+
+ Enables a workaround for erratum A004510. If set,
+ then CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV and
+ CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY must be set.
+
+ CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV
+ CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV2 (optional)
+
+ Defines one or two SoC revisions (low 8 bits of SVR)
+ for which the A004510 workaround should be applied.
+
+ The rest of SVR is either not relevant to the decision
+ of whether the erratum is present (e.g. p2040 versus
+ p2041) or is implied by the build target, which controls
+ whether CONFIG_SYS_FSL_ERRATUM_A004510 is set.
+
+ See Freescale App Note 4493 for more information about
+ this erratum.
+
+ CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY
+
+ This is the value to write into CCSR offset 0x18600
+ according to the A004510 workaround.
+
- Generic CPU options:
CONFIG_SYS_BIG_ENDIAN, CONFIG_SYS_LITTLE_ENDIAN
additional board info beside
the logo
+ When CONFIG_CFB_CONSOLE_ANSI is defined, console will support
+ a limited number of ANSI escape sequences (cursor control,
+ erase functions and limited graphics rendition control).
+
When CONFIG_CFB_CONSOLE is defined, video console is
default i/o. Serial console can be forced with
environment 'console=serial'.
- Boot Delay: CONFIG_BOOTDELAY - in seconds
Delay before automatically booting the default image;
set to -1 to disable autoboot.
+ set to -2 to autoboot with no delay and not check for abort
+ (even when CONFIG_ZERO_BOOTDELAY_CHECK is defined).
See doc/README.autoboot for these options that
work with CONFIG_BOOTDELAY. None are required.
- Monitor Functions:
Monitor commands can be included or excluded
from the build by using the #include files
- "config_cmd_all.h" and #undef'ing unwanted
- commands, or using "config_cmd_default.h"
+ <config_cmd_all.h> and #undef'ing unwanted
+ commands, or using <config_cmd_default.h>
and augmenting with additional #define's
for wanted commands.
CONFIG_CMD_EEPROM * EEPROM read/write support
CONFIG_CMD_ELF * bootelf, bootvx
CONFIG_CMD_EXPORTENV * export the environment
+ CONFIG_CMD_EXT2 * ext2 command support
+ CONFIG_CMD_EXT4 * ext4 command support
CONFIG_CMD_SAVEENV saveenv
CONFIG_CMD_FDC * Floppy Disk Support
- CONFIG_CMD_FAT * FAT partition support
+ CONFIG_CMD_FAT * FAT command support
CONFIG_CMD_FDOS * Dos diskette Support
CONFIG_CMD_FLASH flinfo, erase, protect
CONFIG_CMD_FPGA FPGA device initialization support
CONFIG_CMD_IMLS List all found images
CONFIG_CMD_IMMAP * IMMR dump support
CONFIG_CMD_IMPORTENV * import an environment
+ CONFIG_CMD_INI * import data from an ini file into the env
CONFIG_CMD_IRQ * irqinfo
CONFIG_CMD_ITEST Integer/string test of 2 values
CONFIG_CMD_JFFS2 * JFFS2 Support
CONFIG_CMD_SPI * SPI serial bus support
CONFIG_CMD_TFTPSRV * TFTP transfer in server mode
CONFIG_CMD_TFTPPUT * TFTP put command (upload)
- CONFIG_CMD_TIME * run command and report execution time
+ CONFIG_CMD_TIME * run command and report execution time (ARM specific)
+ CONFIG_CMD_TIMER * access to the system tick timer
CONFIG_CMD_USB * USB support
CONFIG_CMD_CDP * Cisco Discover Protocol support
CONFIG_CMD_MFSL * Microblaze FSL support
If this variable is defined, an environment variable
named "ver" is created by U-Boot showing the U-Boot
version as printed by the "version" command.
- This variable is readonly.
+ Any change to this variable will be reverted at the
+ next reset.
- Real-Time Clock:
commands like bootm or iminfo. This option is
automatically enabled when you select CONFIG_CMD_DATE .
-- Partition Support:
- CONFIG_MAC_PARTITION and/or CONFIG_DOS_PARTITION
- and/or CONFIG_ISO_PARTITION and/or CONFIG_EFI_PARTITION
+- Partition Labels (disklabels) Supported:
+ Zero or more of the following:
+ CONFIG_MAC_PARTITION Apple's MacOS partition table.
+ CONFIG_DOS_PARTITION MS Dos partition table, traditional on the
+ Intel architecture, USB sticks, etc.
+ CONFIG_ISO_PARTITION ISO partition table, used on CDROM etc.
+ CONFIG_EFI_PARTITION GPT partition table, common when EFI is the
+ bootloader. Note 2TB partition limit; see
+ disk/part_efi.c
+ CONFIG_MTD_PARTITIONS Memory Technology Device partition table.
If IDE or SCSI support is enabled (CONFIG_CMD_IDE or
CONFIG_CMD_SCSI) you must configure support for at
- least one partition type as well.
+ least one non-MTD partition type as well.
- IDE Reset method:
CONFIG_IDE_RESET_ROUTINE - this is defined in several
devices.
CONFIG_SYS_SCSI_SYM53C8XX_CCF to fix clock timing (80Mhz)
+ The environment variable 'scsidevs' is set to the number of
+ SCSI devices found during the last scan.
+
- NETWORK Support (PCI):
CONFIG_E1000
Support for Intel 8254x/8257x gigabit chips.
CONFIG_CALXEDA_XGMAC
Support for the Calxeda XGMAC device
- CONFIG_DRIVER_LAN91C96
+ CONFIG_LAN91C96
Support for SMSC's LAN91C96 chips.
CONFIG_LAN91C96_BASE
CONFIG_LAN91C96_USE_32_BIT
Define this to enable 32 bit addressing
- CONFIG_DRIVER_SMC91111
+ CONFIG_SMC91111
Support for SMSC's LAN91C111 chip
CONFIG_SMC91111_BASE
viewport is supported.
To enable the ULPI layer support, define CONFIG_USB_ULPI and
CONFIG_USB_ULPI_VIEWPORT in your board configuration file.
+ If your ULPI phy needs a different reference clock than the
+ standard 24 MHz then you have to define CONFIG_ULPI_REF_CLK to
+ the appropriate value in Hz.
- MMC Support:
The MMC controller on the Intel PXA is supported. To
This will also enable the command "fatwrite" enabling the
user to write files to FAT.
+CBFS (Coreboot Filesystem) support
+ CONFIG_CMD_CBFS
+
+ Define this to enable support for reading from a Coreboot
+ filesystem. Available commands are cbfsinit, cbfsinfo, cbfsls
+ and cbfsload.
+
- Keyboard Support:
CONFIG_ISA_KEYBOARD
boot. See the documentation file README.video for a
description of this variable.
+ CONFIG_VIDEO_VGA
+
+ Enable the VGA video / BIOS for x86. The alternative if you
+ are using coreboot is to use the coreboot frame buffer
+ driver.
+
+
- Keyboard Support:
CONFIG_KEYBOARD
Normally display is black on white background; define
CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
+ CONFIG_LCD_BMP_RLE8
+
+ Support drawing of RLE8-compressed bitmaps on the LCD.
+
+
- Splash Screen Support: CONFIG_SPLASH_SCREEN
If this option is set, the environment is checked for
can be displayed via the splashscreen support or the
bmp command.
+- Do compresssing for memory range:
+ CONFIG_CMD_ZIP
+
+ If this option is set, it would use zlib deflate method
+ to compress the specified memory at its best effort.
+
- Compression support:
CONFIG_BZIP2
following board configurations are known to be
"pRAM-clean":
- ETX094, IVMS8, IVML24, SPD8xx, TQM8xxL,
- HERMES, IP860, RPXlite, LWMON, LANTEC,
+ IVMS8, IVML24, SPD8xx, TQM8xxL,
+ HERMES, IP860, RPXlite, LWMON,
FLAGADM, TQM8260
+- Access to physical memory region (> 4GB)
+ Some basic support is provided for operations on memory not
+ normally accessible to U-Boot - e.g. some architectures
+ support access to more than 4GB of memory on 32-bit
+ machines using physical address extension or similar.
+ Define CONFIG_PHYSMEM to access this basic support, which
+ currently only supports clearing the memory.
+
- Error Recovery:
CONFIG_PANIC_HANG
Timeout waiting for an ARP reply in milliseconds.
+ CONFIG_NFS_TIMEOUT
+
+ Timeout in milliseconds used in NFS protocol.
+ If you encounter "ERROR: Cannot umount" in nfs command,
+ try longer timeout such as
+ #define CONFIG_NFS_TIMEOUT 10000UL
+
- Command Interpreter:
CONFIG_AUTO_COMPLETE
the environment like the "source" command or the
boot command first.
+ CONFIG_ENV_VARS_UBOOT_CONFIG
+
+ Define this in order to add variables describing the
+ U-Boot build configuration to the default environment.
+ These will be named arch, cpu, board, vendor, and soc.
+
+ Enabling this option will cause the following to be defined:
+
+ - CONFIG_SYS_ARCH
+ - CONFIG_SYS_CPU
+ - CONFIG_SYS_BOARD
+ - CONFIG_SYS_VENDOR
+ - CONFIG_SYS_SOC
+
+ CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
+
+ Define this in order to add variables describing certain
+ run-time determined information about the hardware to the
+ environment. These will be named board_name, board_rev.
+
- DataFlash Support:
CONFIG_HAS_DATAFLASH
29,916,167 26,005,792 bootm_start
30,361,327 445,160 start_kernel
+ CONFIG_CMD_BOOTSTAGE
+ Add a 'bootstage' command which supports printing a report
+ and un/stashing of bootstage data.
+
+ CONFIG_BOOTSTAGE_FDT
+ Stash the bootstage information in the FDT. A root 'bootstage'
+ node is created with each bootstage id as a child. Each child
+ has a 'name' property and either 'mark' containing the
+ mark time in microsecond, or 'accum' containing the
+ accumulated time for that bootstage id in microseconds.
+ For example:
+
+ bootstage {
+ 154 {
+ name = "board_init_f";
+ mark = <3575678>;
+ };
+ 170 {
+ name = "lcd";
+ accum = <33482>;
+ };
+ };
+
+ Code in the Linux kernel can find this in /proc/devicetree.
+
Legacy uImage format:
Arg Where When
-150 common/cmd_nand.c Incorrect FIT image format
151 common/cmd_nand.c FIT image format OK
+- FIT image support:
+ CONFIG_FIT
+ Enable support for the FIT uImage format.
+
+ CONFIG_FIT_BEST_MATCH
+ When no configuration is explicitly selected, default to the
+ one whose fdt's compatibility field best matches that of
+ U-Boot itself. A match is considered "best" if it matches the
+ most specific compatibility entry of U-Boot's fdt's root node.
+ The order of entries in the configuration's fdt is ignored.
+
- Standalone program support:
CONFIG_STANDALONE_LOAD_ADDR
CONFIG_SPL_TEXT_BASE
TEXT_BASE for linking the SPL binary.
+ CONFIG_SPL_RELOC_TEXT_BASE
+ Address to relocate to. If unspecified, this is equal to
+ CONFIG_SPL_TEXT_BASE (i.e. no relocation is done).
+
CONFIG_SPL_BSS_START_ADDR
Link address for the BSS within the SPL binary.
CONFIG_SPL_STACK
Adress of the start of the stack SPL will use
+ CONFIG_SPL_RELOC_STACK
+ Adress of the start of the stack SPL will use after
+ relocation. If unspecified, this is equal to
+ CONFIG_SPL_STACK.
+
CONFIG_SYS_SPL_MALLOC_START
Starting address of the malloc pool used in SPL.
CONFIG_SYS_SPL_MALLOC_SIZE
The size of the malloc pool used in SPL.
+ CONFIG_SPL_FRAMEWORK
+ Enable the SPL framework under common/. This framework
+ supports MMC, NAND and YMODEM loading of U-Boot and NAND
+ NAND loading of the Linux Kernel.
+
+ CONFIG_SPL_DISPLAY_PRINT
+ For ARM, enable an optional function to print more information
+ about the running system.
+
+ CONFIG_SPL_INIT_MINIMAL
+ Arch init code should be built for a very small image
+
CONFIG_SPL_LIBCOMMON_SUPPORT
Support for common/libcommon.o in SPL binary
CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME
Filename to read to load U-Boot when reading from FAT
+ CONFIG_SPL_NAND_BASE
+ Include nand_base.c in the SPL. Requires
+ CONFIG_SPL_NAND_DRIVERS.
+
+ CONFIG_SPL_NAND_DRIVERS
+ SPL uses normal NAND drivers, not minimal drivers.
+
+ CONFIG_SPL_NAND_ECC
+ Include standard software ECC in the SPL
+
CONFIG_SPL_NAND_SIMPLE
- Support for drivers/mtd/nand/libnand.o in SPL binary
+ Support for NAND boot using simple NAND drivers that
+ expose the cmd_ctrl() interface.
CONFIG_SYS_NAND_5_ADDR_CYCLE, CONFIG_SYS_NAND_PAGE_COUNT,
CONFIG_SYS_NAND_PAGE_SIZE, CONFIG_SYS_NAND_OOBSIZE,
CONFIG_SYS_NAND_ECCPOS, CONFIG_SYS_NAND_ECCSIZE,
CONFIG_SYS_NAND_ECCBYTES
Defines the size and behavior of the NAND that SPL uses
- to read U-Boot with CONFIG_SPL_NAND_SIMPLE
+ to read U-Boot
CONFIG_SYS_NAND_U_BOOT_OFFS
- Location in NAND for CONFIG_SPL_NAND_SIMPLE to read U-Boot
- from.
+ Location in NAND to read U-Boot from
+
+ CONFIG_SYS_NAND_U_BOOT_DST
+ Location in memory to load U-Boot to
+
+ CONFIG_SYS_NAND_U_BOOT_SIZE
+ Size of image to load
CONFIG_SYS_NAND_U_BOOT_START
- Location in memory for CONFIG_SPL_NAND_SIMPLE to load U-Boot
- to.
+ Entry point in loaded image to jump to
CONFIG_SYS_NAND_HW_ECC_OOBFIRST
Define this if you need to first read the OOB and then the
CONFIG_SPL_SPI_SUPPORT
Support for drivers/spi/libspi.o in SPL binary
+ CONFIG_SPL_RAM_DEVICE
+ Support for running image already present in ram, in SPL binary
+
CONFIG_SPL_LIBGENERIC_SUPPORT
Support for lib/libgeneric.o in SPL binary
+ CONFIG_SPL_TARGET
+ Final target image containing SPL and payload. Some SPLs
+ use an arch-specific makefile fragment instead, for
+ example if more than one image needs to be produced.
+
Modem Support:
--------------
These two #defines specify the address and size of the
environment area within the remote memory space. The
local device can get the environment from remote memory
- space by SRIO or other links.
+ space by SRIO or PCIE links.
BE CAREFUL! For some special cases, the local device can not use
"saveenv" command. For example, the local device will get the
-environment stored in a remote NOR flash by SRIO link, but it can
-not erase, write this NOR flash by SRIO interface.
+environment stored in a remote NOR flash by SRIO or PCIE link,
+but it can not erase, write this NOR flash by SRIO or PCIE interface.
- CONFIG_ENV_IS_IN_NAND:
Disable PCI-Express on systems where it is supported but not
required.
+- CONFIG_PCI_ENUM_ONLY
+ Only scan through and get the devices on the busses.
+ Don't do any setup work, presumably because someone or
+ something has already done it, and we don't need to do it
+ a second time. Useful for platforms that are pre-booted
+ by coreboot or similar.
+
- CONFIG_SYS_SRIO:
Chip has SRIO or not
be used if available. These functions may be faster under some
conditions but may increase the binary size.
+- CONFIG_X86_NO_RESET_VECTOR
+ If defined, the x86 reset vector code is excluded. You will need
+ to do this when U-Boot is running from Coreboot.
+
+- CONFIG_X86_NO_REAL_MODE
+ If defined, x86 real mode code is omitted. This assumes a
+ 32-bit environment where such code is not needed. You will
+ need to do this when U-Boot is running from Coreboot.
+
+
Freescale QE/FMAN Firmware Support:
-----------------------------------
- CONFIG_SYS_QE_FMAN_FW_IN_REMOTE
Specifies that QE/FMAN firmware is located in the remote (master)
memory space. CONFIG_SYS_FMAN_FW_ADDR is a virtual address which
- can be mapped from slave TLB->slave LAW->slave SRIO outbound window
- ->master inbound window->master LAW->the ucode address in master's
- NOR flash.
+ can be mapped from slave TLB->slave LAW->slave SRIO or PCIE outbound
+ window->master inbound window->master LAW->the ucode address in
+ master's memory space.
Building the Software:
======================
protect - enable or disable FLASH write protection
erase - erase FLASH memory
flinfo - print FLASH memory information
+nand - NAND memory operations (see doc/README.nand)
bdinfo - print Board Info structure
iminfo - print header information for application image
coninfo - print console devices and informations
consider minicom to be broken, and recommend not to use it. Under
Unix, I recommend to use C-Kermit for general purpose use (and
especially for kermit binary protocol download ("loadb" command), and
-use "cu" for S-Record download ("loads" command).
+use "cu" for S-Record download ("loads" command). See
+http://www.denx.de/wiki/view/DULG/SystemSetup#Section_4.3.
+for help with kermit.
+
Nevertheless, if you absolutely want to use it try adding this
configuration to your "File transfer protocols" section: