Merge branch 'master' of git://git.denx.de/u-boot-arm
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 1d2e1297d635dfa86134004dd91f7ea62eff2dbb..78f40dfb5aef64b476b7945166b55542a9f60cc1 100644 (file)
--- a/README
+++ b/README
@@ -1486,6 +1486,21 @@ CBFS (Coreboot Filesystem) support
                Normally display is black on white background; define
                CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
 
                Normally display is black on white background; define
                CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
 
+               CONFIG_LCD_ALIGNMENT
+
+               Normally the LCD is page-aligned (tyically 4KB). If this is
+               defined then the LCD will be aligned to this value instead.
+               For ARM it is sometimes useful to use MMU_SECTION_SIZE
+               here, since it is cheaper to change data cache settings on
+               a per-section basis.
+
+               CONFIG_CONSOLE_SCROLL_LINES
+
+               When the console need to be scrolled, this is the number of
+               lines to scroll by. It defaults to 1. Increasing this makes
+               the console jump but can help speed up operation when scrolling
+               is slow.
+
                CONFIG_LCD_BMP_RLE8
 
                Support drawing of RLE8-compressed bitmaps on the LCD.
                CONFIG_LCD_BMP_RLE8
 
                Support drawing of RLE8-compressed bitmaps on the LCD.
@@ -1495,7 +1510,6 @@ CBFS (Coreboot Filesystem) support
                Enables an 'i2c edid' command which can read EDID
                information over I2C from an attached LCD display.
 
                Enables an 'i2c edid' command which can read EDID
                information over I2C from an attached LCD display.
 
-
 - Splash Screen Support: CONFIG_SPLASH_SCREEN
 
                If this option is set, the environment is checked for
 - Splash Screen Support: CONFIG_SPLASH_SCREEN
 
                If this option is set, the environment is checked for