]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blobdiff - README
Merge branch 'master' of git://git.denx.de/u-boot-arm
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 4428205b86aa5273c95ca6f820667ffb5d63e2d8..78f40dfb5aef64b476b7945166b55542a9f60cc1 100644 (file)
--- a/README
+++ b/README
@@ -54,6 +54,11 @@ In case of problems see the CHANGELOG and CREDITS files to find out
 who contributed the specific port. The MAINTAINERS file lists board
 maintainers.
 
+Note: There is no CHANGELOG file in the actual U-Boot source tree;
+it can be created dynamically from the Git log using:
+
+       make CHANGELOG
+
 
 Where to get help:
 ==================
@@ -363,6 +368,12 @@ The following options need to be configured:
                ICache only when Code runs from RAM.
 
 - 85xx CPU Options:
+               CONFIG_SYS_PPC64
+
+               Specifies that the core is a 64-bit PowerPC implementation (implements
+               the "64" category of the Power ISA). This is necessary for ePAPR
+               compliance, among other possible reasons.
+
                CONFIG_SYS_FSL_TBCLK_DIV
 
                Defines the core time base clock divider ratio compared to the
@@ -383,6 +394,31 @@ The following options need to be configured:
                symbol should be set to the TLB1 entry to be used for this
                purpose.
 
+               CONFIG_SYS_FSL_ERRATUM_A004510
+
+               Enables a workaround for erratum A004510.  If set,
+               then CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV and
+               CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY must be set.
+
+               CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV
+               CONFIG_SYS_FSL_ERRATUM_A004510_SVR_REV2 (optional)
+
+               Defines one or two SoC revisions (low 8 bits of SVR)
+               for which the A004510 workaround should be applied.
+
+               The rest of SVR is either not relevant to the decision
+               of whether the erratum is present (e.g. p2040 versus
+               p2041) or is implied by the build target, which controls
+               whether CONFIG_SYS_FSL_ERRATUM_A004510 is set.
+
+               See Freescale App Note 4493 for more information about
+               this erratum.
+
+               CONFIG_SYS_FSL_CORENET_SNOOPVEC_COREONLY
+
+               This is the value to write into CCSR offset 0x18600
+               according to the A004510 workaround.
+
 - Generic CPU options:
                CONFIG_SYS_BIG_ENDIAN, CONFIG_SYS_LITTLE_ENDIAN
 
@@ -630,6 +666,10 @@ The following options need to be configured:
                                                additional board info beside
                                                the logo
 
+               When CONFIG_CFB_CONSOLE_ANSI is defined, console will support
+               a limited number of ANSI escape sequences (cursor control,
+               erase functions and limited graphics rendition control).
+
                When CONFIG_CFB_CONSOLE is defined, video console is
                default i/o. Serial console can be forced with
                environment 'console=serial'.
@@ -679,6 +719,8 @@ The following options need to be configured:
 - Boot Delay:  CONFIG_BOOTDELAY - in seconds
                Delay before automatically booting the default image;
                set to -1 to disable autoboot.
+               set to -2 to autoboot with no delay and not check for abort
+               (even when CONFIG_ZERO_BOOTDELAY_CHECK is defined).
 
                See doc/README.autoboot for these options that
                work with CONFIG_BOOTDELAY. None are required.
@@ -773,15 +815,21 @@ The following options need to be configured:
                CONFIG_CMD_EDITENV        edit env variable
                CONFIG_CMD_EEPROM       * EEPROM read/write support
                CONFIG_CMD_ELF          * bootelf, bootvx
+               CONFIG_CMD_ENV_CALLBACK * display details about env callbacks
+               CONFIG_CMD_ENV_FLAGS    * display details about env flags
                CONFIG_CMD_EXPORTENV    * export the environment
+               CONFIG_CMD_EXT2         * ext2 command support
+               CONFIG_CMD_EXT4         * ext4 command support
                CONFIG_CMD_SAVEENV        saveenv
                CONFIG_CMD_FDC          * Floppy Disk Support
-               CONFIG_CMD_FAT          * FAT partition support
+               CONFIG_CMD_FAT          * FAT command support
                CONFIG_CMD_FDOS         * Dos diskette Support
                CONFIG_CMD_FLASH          flinfo, erase, protect
                CONFIG_CMD_FPGA           FPGA device initialization support
+               CONFIG_CMD_GETTIME      * Get time since boot
                CONFIG_CMD_GO           * the 'go' command (exec code)
                CONFIG_CMD_GREPENV      * search environment
+               CONFIG_CMD_HASH         * calculate hash / digest
                CONFIG_CMD_HWFLOW       * RTS/CTS hw flow control
                CONFIG_CMD_I2C          * I2C serial bus support
                CONFIG_CMD_IDE          * IDE harddisk support
@@ -789,6 +837,7 @@ The following options need to be configured:
                CONFIG_CMD_IMLS           List all found images
                CONFIG_CMD_IMMAP        * IMMR dump support
                CONFIG_CMD_IMPORTENV    * import an environment
+               CONFIG_CMD_INI          * import data from an ini file into the env
                CONFIG_CMD_IRQ          * irqinfo
                CONFIG_CMD_ITEST          Integer/string test of 2 values
                CONFIG_CMD_JFFS2        * JFFS2 Support
@@ -815,6 +864,7 @@ The following options need to be configured:
                CONFIG_CMD_PING         * send ICMP ECHO_REQUEST to network
                                          host
                CONFIG_CMD_PORTIO       * Port I/O
+               CONFIG_CMD_READ         * Read raw data from partition
                CONFIG_CMD_REGINFO      * Register dump
                CONFIG_CMD_RUN            run command in env variable
                CONFIG_CMD_SAVES        * save S record dump
@@ -830,7 +880,8 @@ The following options need to be configured:
                CONFIG_CMD_SPI          * SPI serial bus support
                CONFIG_CMD_TFTPSRV      * TFTP transfer in server mode
                CONFIG_CMD_TFTPPUT      * TFTP put command (upload)
-               CONFIG_CMD_TIME         * run command and report execution time
+               CONFIG_CMD_TIME         * run command and report execution time (ARM specific)
+               CONFIG_CMD_TIMER        * access to the system tick timer
                CONFIG_CMD_USB          * USB support
                CONFIG_CMD_CDP          * Cisco Discover Protocol support
                CONFIG_CMD_MFSL         * Microblaze FSL support
@@ -1004,6 +1055,9 @@ The following options need to be configured:
                devices.
                CONFIG_SYS_SCSI_SYM53C8XX_CCF to fix clock timing (80Mhz)
 
+                The environment variable 'scsidevs' is set to the number of
+                SCSI devices found during the last scan.
+
 - NETWORK Support (PCI):
                CONFIG_E1000
                Support for Intel 8254x/8257x gigabit chips.
@@ -1055,7 +1109,7 @@ The following options need to be configured:
                CONFIG_CALXEDA_XGMAC
                Support for the Calxeda XGMAC device
 
-               CONFIG_DRIVER_LAN91C96
+               CONFIG_LAN91C96
                Support for SMSC's LAN91C96 chips.
 
                        CONFIG_LAN91C96_BASE
@@ -1065,7 +1119,7 @@ The following options need to be configured:
                        CONFIG_LAN91C96_USE_32_BIT
                        Define this to enable 32 bit addressing
 
-               CONFIG_DRIVER_SMC91111
+               CONFIG_SMC91111
                Support for SMSC's LAN91C111 chip
 
                        CONFIG_SMC91111_BASE
@@ -1239,6 +1293,9 @@ The following options need to be configured:
                viewport is supported.
                To enable the ULPI layer support, define CONFIG_USB_ULPI and
                CONFIG_USB_ULPI_VIEWPORT in your board configuration file.
+               If your ULPI phy needs a different reference clock than the
+               standard 24 MHz then you have to define CONFIG_ULPI_REF_CLK to
+               the appropriate value in Hz.
 
 - MMC Support:
                The MMC controller on the Intel PXA is supported. To
@@ -1284,6 +1341,13 @@ The following options need to be configured:
                This will also enable the command "fatwrite" enabling the
                user to write files to FAT.
 
+CBFS (Coreboot Filesystem) support
+               CONFIG_CMD_CBFS
+
+               Define this to enable support for reading from a Coreboot
+               filesystem. Available commands are cbfsinit, cbfsinfo, cbfsls
+               and cbfsload.
+
 - Keyboard Support:
                CONFIG_ISA_KEYBOARD
 
@@ -1355,6 +1419,13 @@ The following options need to be configured:
                boot.  See the documentation file README.video for a
                description of this variable.
 
+               CONFIG_VIDEO_VGA
+
+               Enable the VGA video / BIOS for x86. The alternative if you
+               are using coreboot is to use the coreboot frame buffer
+               driver.
+
+
 - Keyboard Support:
                CONFIG_KEYBOARD
 
@@ -1415,6 +1486,30 @@ The following options need to be configured:
                Normally display is black on white background; define
                CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
 
+               CONFIG_LCD_ALIGNMENT
+
+               Normally the LCD is page-aligned (tyically 4KB). If this is
+               defined then the LCD will be aligned to this value instead.
+               For ARM it is sometimes useful to use MMU_SECTION_SIZE
+               here, since it is cheaper to change data cache settings on
+               a per-section basis.
+
+               CONFIG_CONSOLE_SCROLL_LINES
+
+               When the console need to be scrolled, this is the number of
+               lines to scroll by. It defaults to 1. Increasing this makes
+               the console jump but can help speed up operation when scrolling
+               is slow.
+
+               CONFIG_LCD_BMP_RLE8
+
+               Support drawing of RLE8-compressed bitmaps on the LCD.
+
+               CONFIG_I2C_EDID
+
+               Enables an 'i2c edid' command which can read EDID
+               information over I2C from an attached LCD display.
+
 - Splash Screen Support: CONFIG_SPLASH_SCREEN
 
                If this option is set, the environment is checked for
@@ -1458,6 +1553,12 @@ The following options need to be configured:
                can be displayed via the splashscreen support or the
                bmp command.
 
+- Do compresssing for memory range:
+               CONFIG_CMD_ZIP
+
+               If this option is set, it would use zlib deflate method
+               to compress the specified memory at its best effort.
+
 - Compression support:
                CONFIG_BZIP2
 
@@ -2102,6 +2203,11 @@ The following options need to be configured:
                serial# is unaffected by this, i. e. it remains
                read-only.]
 
+               The same can be accomplished in a more flexible way
+               for any variable by configuring the type of access
+               to allow for those variables in the ".flags" variable
+               or define CONFIG_ENV_FLAGS_LIST_STATIC.
+
 - Protected RAM:
                CONFIG_PRAM
 
@@ -2131,10 +2237,18 @@ The following options need to be configured:
                following board configurations are known to be
                "pRAM-clean":
 
-                       ETX094, IVMS8, IVML24, SPD8xx, TQM8xxL,
-                       HERMES, IP860, RPXlite, LWMON, LANTEC,
+                       IVMS8, IVML24, SPD8xx, TQM8xxL,
+                       HERMES, IP860, RPXlite, LWMON,
                        FLAGADM, TQM8260
 
+- Access to physical memory region (> 4GB)
+               Some basic support is provided for operations on memory not
+               normally accessible to U-Boot - e.g. some architectures
+               support access to more than 4GB of memory on 32-bit
+               machines using physical address extension or similar.
+               Define CONFIG_PHYSMEM to access this basic support, which
+               currently only supports clearing the memory.
+
 - Error Recovery:
                CONFIG_PANIC_HANG
 
@@ -2258,6 +2372,12 @@ The following options need to be configured:
                - CONFIG_SYS_VENDOR
                - CONFIG_SYS_SOC
 
+               CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
+
+               Define this in order to add variables describing certain
+               run-time determined information about the hardware to the
+               environment.  These will be named board_name, board_rev.
+
 - DataFlash Support:
                CONFIG_HAS_DATAFLASH
 
@@ -2284,6 +2404,11 @@ The following options need to be configured:
                CONFIG_SF_DEFAULT_MODE          (see include/spi.h)
                CONFIG_SF_DEFAULT_SPEED         in Hz
 
+               CONFIG_CMD_SF_TEST
+
+               Define this option to include a destructive SPI flash
+               test ('sf test').
+
 - SystemACE Support:
                CONFIG_SYSTEMACE
 
@@ -2318,6 +2443,23 @@ The following options need to be configured:
                A better solution is to properly configure the firewall,
                but sometimes that is not allowed.
 
+- Hashing support:
+               CONFIG_CMD_HASH
+
+               This enables a generic 'hash' command which can produce
+               hashes / digests from a few algorithms (e.g. SHA1, SHA256).
+
+               CONFIG_HASH_VERIFY
+
+               Enable the hash verify command (hash -v). This adds to code
+               size a little.
+
+               CONFIG_SHA1 - support SHA1 hashing
+               CONFIG_SHA256 - support SHA256 hashing
+
+               Note: There is also a sha1sum command, which should perhaps
+               be deprecated in favour of 'hash sha1'.
+
 - Show boot progress:
                CONFIG_SHOW_BOOT_PROGRESS
 
@@ -2353,6 +2495,31 @@ The following options need to be configured:
                 29,916,167 26,005,792  bootm_start
                 30,361,327    445,160  start_kernel
 
+               CONFIG_CMD_BOOTSTAGE
+               Add a 'bootstage' command which supports printing a report
+               and un/stashing of bootstage data.
+
+               CONFIG_BOOTSTAGE_FDT
+               Stash the bootstage information in the FDT. A root 'bootstage'
+               node is created with each bootstage id as a child. Each child
+               has a 'name' property and either 'mark' containing the
+               mark time in microsecond, or 'accum' containing the
+               accumulated time for that bootstage id in microseconds.
+               For example:
+
+               bootstage {
+                       154 {
+                               name = "board_init_f";
+                               mark = <3575678>;
+                       };
+                       170 {
+                               name = "lcd";
+                               accum = <33482>;
+                       };
+               };
+
+               Code in the Linux kernel can find this in /proc/devicetree.
+
 Legacy uImage format:
 
   Arg  Where                   When
@@ -2506,6 +2673,17 @@ FIT uImage format:
  -150  common/cmd_nand.c       Incorrect FIT image format
   151  common/cmd_nand.c       FIT image format OK
 
+- FIT image support:
+               CONFIG_FIT
+               Enable support for the FIT uImage format.
+
+               CONFIG_FIT_BEST_MATCH
+               When no configuration is explicitly selected, default to the
+               one whose fdt's compatibility field best matches that of
+               U-Boot itself. A match is considered "best" if it matches the
+               most specific compatibility entry of U-Boot's fdt's root node.
+               The order of entries in the configuration's fdt is ignored.
+
 - Standalone program support:
                CONFIG_STANDALONE_LOAD_ADDR
 
@@ -2557,6 +2735,10 @@ FIT uImage format:
                CONFIG_SPL_TEXT_BASE
                TEXT_BASE for linking the SPL binary.
 
+               CONFIG_SPL_RELOC_TEXT_BASE
+               Address to relocate to.  If unspecified, this is equal to
+               CONFIG_SPL_TEXT_BASE (i.e. no relocation is done).
+
                CONFIG_SPL_BSS_START_ADDR
                Link address for the BSS within the SPL binary.
 
@@ -2566,12 +2748,29 @@ FIT uImage format:
                CONFIG_SPL_STACK
                Adress of the start of the stack SPL will use
 
+               CONFIG_SPL_RELOC_STACK
+               Adress of the start of the stack SPL will use after
+               relocation.  If unspecified, this is equal to
+               CONFIG_SPL_STACK.
+
                CONFIG_SYS_SPL_MALLOC_START
                Starting address of the malloc pool used in SPL.
 
                CONFIG_SYS_SPL_MALLOC_SIZE
                The size of the malloc pool used in SPL.
 
+               CONFIG_SPL_FRAMEWORK
+               Enable the SPL framework under common/.  This framework
+               supports MMC, NAND and YMODEM loading of U-Boot and NAND
+               NAND loading of the Linux Kernel.
+
+               CONFIG_SPL_DISPLAY_PRINT
+               For ARM, enable an optional function to print more information
+               about the running system.
+
+               CONFIG_SPL_INIT_MINIMAL
+               Arch init code should be built for a very small image
+
                CONFIG_SPL_LIBCOMMON_SUPPORT
                Support for common/libcommon.o in SPL binary
 
@@ -2599,8 +2798,19 @@ FIT uImage format:
                CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME
                Filename to read to load U-Boot when reading from FAT
 
+               CONFIG_SPL_NAND_BASE
+               Include nand_base.c in the SPL.  Requires
+               CONFIG_SPL_NAND_DRIVERS.
+
+               CONFIG_SPL_NAND_DRIVERS
+               SPL uses normal NAND drivers, not minimal drivers.
+
+               CONFIG_SPL_NAND_ECC
+               Include standard software ECC in the SPL
+
                CONFIG_SPL_NAND_SIMPLE
-               Support for drivers/mtd/nand/libnand.o in SPL binary
+               Support for NAND boot using simple NAND drivers that
+               expose the cmd_ctrl() interface.
 
                CONFIG_SYS_NAND_5_ADDR_CYCLE, CONFIG_SYS_NAND_PAGE_COUNT,
                CONFIG_SYS_NAND_PAGE_SIZE, CONFIG_SYS_NAND_OOBSIZE,
@@ -2608,15 +2818,19 @@ FIT uImage format:
                CONFIG_SYS_NAND_ECCPOS, CONFIG_SYS_NAND_ECCSIZE,
                CONFIG_SYS_NAND_ECCBYTES
                Defines the size and behavior of the NAND that SPL uses
-               to read U-Boot with CONFIG_SPL_NAND_SIMPLE
+               to read U-Boot
 
                CONFIG_SYS_NAND_U_BOOT_OFFS
-               Location in NAND for CONFIG_SPL_NAND_SIMPLE to read U-Boot
-               from.
+               Location in NAND to read U-Boot from
+
+               CONFIG_SYS_NAND_U_BOOT_DST
+               Location in memory to load U-Boot to
+
+               CONFIG_SYS_NAND_U_BOOT_SIZE
+               Size of image to load
 
                CONFIG_SYS_NAND_U_BOOT_START
-               Location in memory for CONFIG_SPL_NAND_SIMPLE to load U-Boot
-               to.
+               Entry point in loaded image to jump to
 
                CONFIG_SYS_NAND_HW_ECC_OOBFIRST
                Define this if you need to first read the OOB and then the
@@ -2635,9 +2849,17 @@ FIT uImage format:
                CONFIG_SPL_SPI_SUPPORT
                Support for drivers/spi/libspi.o in SPL binary
 
+               CONFIG_SPL_RAM_DEVICE
+               Support for running image already present in ram, in SPL binary
+
                CONFIG_SPL_LIBGENERIC_SUPPORT
                Support for lib/libgeneric.o in SPL binary
 
+               CONFIG_SPL_TARGET
+               Final target image containing SPL and payload.  Some SPLs
+               use an arch-specific makefile fragment instead, for
+               example if more than one image needs to be produced.
+
 Modem Support:
 --------------
 
@@ -2772,9 +2994,6 @@ Configuration Settings:
                non page size aligned address and this could cause major
                problems.
 
-- CONFIG_SYS_TFTP_LOADADDR:
-               Default load address for network file downloads
-
 - CONFIG_SYS_LOADS_BAUD_CHANGE:
                Enable temporary baudrate change while serial download
 
@@ -2916,6 +3135,49 @@ Configuration Settings:
        cases. This setting can be used to tune behaviour; see
        lib/hashtable.c for details.
 
+- CONFIG_ENV_FLAGS_LIST_DEFAULT
+- CONFIG_ENV_FLAGS_LIST_STATIC
+       Enable validation of the values given to enviroment variables when
+       calling env set.  Variables can be restricted to only decimal,
+       hexadecimal, or boolean.  If CONFIG_CMD_NET is also defined,
+       the variables can also be restricted to IP address or MAC address.
+
+       The format of the list is:
+               type_attribute = [s|d|x|b|i|m]
+               access_atribute = [a|r|o|c]
+               attributes = type_attribute[access_atribute]
+               entry = variable_name[:attributes]
+               list = entry[,list]
+
+       The type attributes are:
+               s - String (default)
+               d - Decimal
+               x - Hexadecimal
+               b - Boolean ([1yYtT|0nNfF])
+               i - IP address
+               m - MAC address
+
+       The access attributes are:
+               a - Any (default)
+               r - Read-only
+               o - Write-once
+               c - Change-default
+
+       - CONFIG_ENV_FLAGS_LIST_DEFAULT
+               Define this to a list (string) to define the ".flags"
+               envirnoment variable in the default or embedded environment.
+
+       - CONFIG_ENV_FLAGS_LIST_STATIC
+               Define this to a list (string) to define validation that
+               should be done if an entry is not found in the ".flags"
+               environment variable.  To override a setting in the static
+               list, simply add an entry for the same variable name to the
+               ".flags" variable.
+
+- CONFIG_ENV_ACCESS_IGNORE_FORCE
+       If defined, don't allow the -f switch to env set override variable
+       access flags.
+
 The following definitions that deal with the placement and management
 of environment data (variable area); in general, we support the
 following configurations:
@@ -3100,12 +3362,12 @@ to save the current settings.
          These two #defines specify the address and size of the
          environment area within the remote memory space. The
          local device can get the environment from remote memory
-         space by SRIO or other links.
+         space by SRIO or PCIE links.
 
 BE CAREFUL! For some special cases, the local device can not use
 "saveenv" command. For example, the local device will get the
-environment stored in a remote NOR flash by SRIO link, but it can
-not erase, write this NOR flash by SRIO interface.
+environment stored in a remote NOR flash by SRIO or PCIE link,
+but it can not erase, write this NOR flash by SRIO or PCIE interface.
 
 - CONFIG_ENV_IS_IN_NAND:
 
@@ -3513,6 +3775,16 @@ Low Level (hardware related) configuration options:
                be used if available. These functions may be faster under some
                conditions but may increase the binary size.
 
+- CONFIG_X86_NO_RESET_VECTOR
+               If defined, the x86 reset vector code is excluded. You will need
+               to do this when U-Boot is running from Coreboot.
+
+- CONFIG_X86_NO_REAL_MODE
+               If defined, x86 real mode code is omitted. This assumes a
+               32-bit environment where such code is not needed. You will
+               need to do this when U-Boot is running from Coreboot.
+
+
 Freescale QE/FMAN Firmware Support:
 -----------------------------------
 
@@ -3553,9 +3825,9 @@ within that device.
 - CONFIG_SYS_QE_FMAN_FW_IN_REMOTE
        Specifies that QE/FMAN firmware is located in the remote (master)
        memory space.   CONFIG_SYS_FMAN_FW_ADDR is a virtual address which
-       can be mapped from slave TLB->slave LAW->slave SRIO outbound window
-       ->master inbound window->master LAW->the ucode address in master's
-       NOR flash.
+       can be mapped from slave TLB->slave LAW->slave SRIO or PCIE outbound
+       window->master inbound window->master LAW->the ucode address in
+       master's memory space.
 
 Building the Software:
 ======================
@@ -3740,6 +4012,7 @@ saveenv - save environment variables to persistent storage
 protect - enable or disable FLASH write protection
 erase  - erase FLASH memory
 flinfo - print FLASH memory information
+nand   - NAND memory operations (see doc/README.nand)
 bdinfo - print Board Info structure
 iminfo - print header information for application image
 coninfo - print console devices and informations
@@ -4006,6 +4279,36 @@ Please note that changes to some configuration parameters may take
 only effect after the next boot (yes, that's just like Windoze :-).
 
 
+Callback functions for environment variables:
+---------------------------------------------
+
+For some environment variables, the behavior of u-boot needs to change
+when their values are changed.  This functionailty allows functions to
+be associated with arbitrary variables.  On creation, overwrite, or
+deletion, the callback will provide the opportunity for some side
+effect to happen or for the change to be rejected.
+
+The callbacks are named and associated with a function using the
+U_BOOT_ENV_CALLBACK macro in your board or driver code.
+
+These callbacks are associated with variables in one of two ways.  The
+static list can be added to by defining CONFIG_ENV_CALLBACK_LIST_STATIC
+in the board configuration to a string that defines a list of
+associations.  The list must be in the following format:
+
+       entry = variable_name[:callback_name]
+       list = entry[,list]
+
+If the callback name is not specified, then the callback is deleted.
+Spaces are also allowed anywhere in the list.
+
+Callbacks can also be associated by defining the ".callbacks" variable
+with the same list format above.  Any association in ".callbacks" will
+override any association in the static list. You can define
+CONFIG_ENV_CALLBACK_LIST_DEFAULT to a list (string) to define the
+".callbacks" envirnoment variable in the default or embedded environment.
+
+
 Command Line Parsing:
 =====================
 
@@ -4645,7 +4948,10 @@ Over time, many people have reported problems when trying to use the
 consider minicom to be broken, and recommend not to use it. Under
 Unix, I recommend to use C-Kermit for general purpose use (and
 especially for kermit binary protocol download ("loadb" command), and
-use "cu" for S-Record download ("loads" command).
+use "cu" for S-Record download ("loads" command).  See
+http://www.denx.de/wiki/view/DULG/SystemSetup#Section_4.3.
+for help with kermit.
+
 
 Nevertheless, if you absolutely want to use it try adding this
 configuration to your "File transfer protocols" section: