index ac61a32adf33c471887111515a9d677a902d4146..78f40dfb5aef64b476b7945166b55542a9f60cc1 100644 (file)
--- a/README
+++ b/README
CONFIG_CMD_EEPROM * EEPROM read/write support
CONFIG_CMD_ELF * bootelf, bootvx
CONFIG_CMD_ENV_CALLBACK * display details about env callbacks
+ CONFIG_CMD_ENV_FLAGS * display details about env flags
CONFIG_CMD_EXPORTENV * export the environment
CONFIG_CMD_EXT2 * ext2 command support
CONFIG_CMD_EXT4 * ext4 command support
Normally display is black on white background; define
CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
+ CONFIG_LCD_ALIGNMENT
+
+ Normally the LCD is page-aligned (tyically 4KB). If this is
+ defined then the LCD will be aligned to this value instead.
+ For ARM it is sometimes useful to use MMU_SECTION_SIZE
+ here, since it is cheaper to change data cache settings on
+ a per-section basis.
+
+ CONFIG_CONSOLE_SCROLL_LINES
+
+ When the console need to be scrolled, this is the number of
+ lines to scroll by. It defaults to 1. Increasing this makes
+ the console jump but can help speed up operation when scrolling
+ is slow.
+
CONFIG_LCD_BMP_RLE8
Support drawing of RLE8-compressed bitmaps on the LCD.
Enables an 'i2c edid' command which can read EDID
information over I2C from an attached LCD display.
-
- Splash Screen Support: CONFIG_SPLASH_SCREEN
If this option is set, the environment is checked for
serial# is unaffected by this, i. e. it remains
read-only.]
+ The same can be accomplished in a more flexible way
+ for any variable by configuring the type of access
+ to allow for those variables in the ".flags" variable
+ or define CONFIG_ENV_FLAGS_LIST_STATIC.
+
- Protected RAM:
CONFIG_PRAM
CONFIG_SF_DEFAULT_MODE (see include/spi.h)
CONFIG_SF_DEFAULT_SPEED in Hz
+ CONFIG_CMD_SF_TEST
+
+ Define this option to include a destructive SPI flash
+ test ('sf test').
+
- SystemACE Support:
CONFIG_SYSTEMACE
non page size aligned address and this could cause major
problems.
-- CONFIG_SYS_TFTP_LOADADDR:
- Default load address for network file downloads
-
- CONFIG_SYS_LOADS_BAUD_CHANGE:
Enable temporary baudrate change while serial download
cases. This setting can be used to tune behaviour; see
lib/hashtable.c for details.
+- CONFIG_ENV_FLAGS_LIST_DEFAULT
+- CONFIG_ENV_FLAGS_LIST_STATIC
+ Enable validation of the values given to enviroment variables when
+ calling env set. Variables can be restricted to only decimal,
+ hexadecimal, or boolean. If CONFIG_CMD_NET is also defined,
+ the variables can also be restricted to IP address or MAC address.
+
+ The format of the list is:
+ type_attribute = [s|d|x|b|i|m]
+ access_atribute = [a|r|o|c]
+ attributes = type_attribute[access_atribute]
+ entry = variable_name[:attributes]
+ list = entry[,list]
+
+ The type attributes are:
+ s - String (default)
+ d - Decimal
+ x - Hexadecimal
+ b - Boolean ([1yYtT|0nNfF])
+ i - IP address
+ m - MAC address
+
+ The access attributes are:
+ a - Any (default)
+ r - Read-only
+ o - Write-once
+ c - Change-default
+
+ - CONFIG_ENV_FLAGS_LIST_DEFAULT
+ Define this to a list (string) to define the ".flags"
+ envirnoment variable in the default or embedded environment.
+
+ - CONFIG_ENV_FLAGS_LIST_STATIC
+ Define this to a list (string) to define validation that
+ should be done if an entry is not found in the ".flags"
+ environment variable. To override a setting in the static
+ list, simply add an entry for the same variable name to the
+ ".flags" variable.
+
+- CONFIG_ENV_ACCESS_IGNORE_FORCE
+ If defined, don't allow the -f switch to env set override variable
+ access flags.
+
The following definitions that deal with the placement and management
of environment data (variable area); in general, we support the
following configurations: