index 14c83f4bb1796698e3a88b192a390395c51febeb..c40e3355e91e7cf5ab2220e89dea39c89181d6e8 100644 (file)
--- a/README
+++ b/README
Define this option to include a destructive SPI flash
test ('sf test').
+ CONFIG_SPI_FLASH_BAR Ban/Extended Addr Reg
+
+ Define this option to use the Bank addr/Extended addr
+ support on SPI flashes which has size > 16Mbytes.
+
- SystemACE Support:
CONFIG_SYSTEMACE
CONFIG_SPL_LDSCRIPT
LDSCRIPT for linking the SPL binary.
+ CONFIG_SPL_MAX_FOOTPRINT
+ Maximum size in memory allocated to the SPL, BSS included.
+ When defined, the linker checks that the actual memory
+ used by SPL from _start to __bss_end does not exceed it.
+ CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+ must not be both defined at the same time.
+
CONFIG_SPL_MAX_SIZE
- Maximum binary size (text, data and rodata) of the SPL binary.
+ Maximum size of the SPL image (text, data, rodata, and
+ linker lists sections), BSS excluded.
+ When defined, the linker checks that the actual size does
+ not exceed it.
CONFIG_SPL_TEXT_BASE
TEXT_BASE for linking the SPL binary.
Link address for the BSS within the SPL binary.
CONFIG_SPL_BSS_MAX_SIZE
- Maximum binary size of the BSS section of the SPL binary.
+ Maximum size in memory allocated to the SPL BSS.
+ When defined, the linker checks that the actual memory used
+ by SPL from __bss_start to __bss_end does not exceed it.
+ CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+ must not be both defined at the same time.
CONFIG_SPL_STACK
Adress of the start of the stack SPL will use
offset _bss_start_ofs from CONFIG_SYS_TEXT_BASE, rather than
directly. You should not need to touch this setting.
+- CONFIG_OMAP_PLATFORM_RESET_TIME_MAX_USEC (OMAP only)
+ This is set by OMAP boards for the max time that reset should
+ be asserted. See doc/README.omap-reset-time for details on how
+ the value can be calulated on a given board.
The following definitions that deal with the placement and management
of environment data (variable area); in general, we support the