]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blobdiff - README
ARM: DRA7xx: Lock DPLL_GMAC
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 81d3681dca70d4edb53de2ac9cb71facb98cb953..c40e3355e91e7cf5ab2220e89dea39c89181d6e8 100644 (file)
--- a/README
+++ b/README
@@ -634,14 +634,6 @@ The following options need to be configured:
                boot loader that has already initialized the UART.  Define this
                variable to flush the UART at init time.
 
-               CONFIG_SYS_NS16550_BROKEN_TEMT
-
-               16550 UART set the Transmitter Empty (TEMT) Bit when all output
-               has finished and the transmitter is totally empty. U-Boot waits
-               for this bit to be set to initialize the serial console. On some
-               broken platforms this bit is not set in SPL making U-Boot to
-               hang while waiting for TEMT. Define this option to avoid it.
-
 
 - Console Interface:
                Depending on board, define exactly one serial port
@@ -2490,6 +2482,11 @@ CBFS (Coreboot Filesystem) support
                Define this option to include a destructive SPI flash
                test ('sf test').
 
+               CONFIG_SPI_FLASH_BAR            Ban/Extended Addr Reg
+
+               Define this option to use the Bank addr/Extended addr
+               support on SPI flashes which has size > 16Mbytes.
+
 - SystemACE Support:
                CONFIG_SYSTEMACE
 
@@ -2814,6 +2811,11 @@ FIT uImage format:
 
                Requires also defining CONFIG_RBTREE
 
+               CONFIG_UBI_SILENCE_MSG
+
+               Make the verbose messages from UBI stop printing.  This leaves
+               warnings and errors enabled.
+
 - UBIFS support
                CONFIG_CMD_UBIFS
 
@@ -2822,6 +2824,11 @@ FIT uImage format:
 
                Requires UBI support as well as CONFIG_LZO
 
+               CONFIG_UBIFS_SILENCE_MSG
+
+               Make the verbose messages from UBIFS stop printing.  This leaves
+               warnings and errors enabled.
+
 - SPL framework
                CONFIG_SPL
                Enable building of SPL globally.
@@ -2829,8 +2836,18 @@ FIT uImage format:
                CONFIG_SPL_LDSCRIPT
                LDSCRIPT for linking the SPL binary.
 
+               CONFIG_SPL_MAX_FOOTPRINT
+               Maximum size in memory allocated to the SPL, BSS included.
+               When defined, the linker checks that the actual memory
+               used by SPL from _start to __bss_end does not exceed it.
+               CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+               must not be both defined at the same time.
+
                CONFIG_SPL_MAX_SIZE
-               Maximum binary size (text, data and rodata) of the SPL binary.
+               Maximum size of the SPL image (text, data, rodata, and
+               linker lists sections), BSS excluded.
+               When defined, the linker checks that the actual size does
+               not exceed it.
 
                CONFIG_SPL_TEXT_BASE
                TEXT_BASE for linking the SPL binary.
@@ -2843,7 +2860,11 @@ FIT uImage format:
                Link address for the BSS within the SPL binary.
 
                CONFIG_SPL_BSS_MAX_SIZE
-               Maximum binary size of the BSS section of the SPL binary.
+               Maximum size in memory allocated to the SPL BSS.
+               When defined, the linker checks that the actual memory used
+               by SPL from __bss_start to __bss_end does not exceed it.
+               CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+               must not be both defined at the same time.
 
                CONFIG_SPL_STACK
                Adress of the start of the stack SPL will use
@@ -2962,8 +2983,11 @@ FIT uImage format:
                Support for lib/libgeneric.o in SPL binary
 
                CONFIG_SPL_PAD_TO
-               Linker address to which the SPL should be padded before
-               appending the SPL payload.
+               Image offset to which the SPL should be padded before appending
+               the SPL payload. By default, this is defined as
+               CONFIG_SPL_MAX_SIZE, or 0 if CONFIG_SPL_MAX_SIZE is undefined.
+               CONFIG_SPL_PAD_TO must be either 0, meaning to append the SPL
+               payload without any padding, or >= CONFIG_SPL_MAX_SIZE.
 
                CONFIG_SPL_TARGET
                Final target image containing SPL and payload.  Some SPLs
@@ -3304,6 +3328,10 @@ Configuration Settings:
        offset _bss_start_ofs from CONFIG_SYS_TEXT_BASE, rather than
        directly. You should not need to touch this setting.
 
+- CONFIG_OMAP_PLATFORM_RESET_TIME_MAX_USEC (OMAP only)
+       This is set by OMAP boards for the max time that reset should
+       be asserted. See doc/README.omap-reset-time for details on how
+       the value can be calulated on a given board.
 
 The following definitions that deal with the placement and management
 of environment data (variable area); in general, we support the
@@ -3538,6 +3566,33 @@ but it can not erase, write this NOR flash by SRIO or PCIE interface.
        environment. If redundant environment is used, it will be copied to
        CONFIG_NAND_ENV_DST + CONFIG_ENV_SIZE.
 
+- CONFIG_ENV_IS_IN_UBI:
+
+       Define this if you have an UBI volume that you want to use for the
+       environment.  This has the benefit of wear-leveling the environment
+       accesses, which is important on NAND.
+
+       - CONFIG_ENV_UBI_PART:
+
+         Define this to a string that is the mtd partition containing the UBI.
+
+       - CONFIG_ENV_UBI_VOLUME:
+
+         Define this to the name of the volume that you want to store the
+         environment in.
+
+       - CONFIG_ENV_UBI_VOLUME_REDUND:
+
+         Define this to the name of another volume to store a second copy of
+         the environment in.  This will enable redundant environments in UBI.
+         It is assumed that both volumes are in the same MTD partition.
+
+       - CONFIG_UBI_SILENCE_MSG
+       - CONFIG_UBIFS_SILENCE_MSG
+
+         You will probably want to define these to avoid a really noisy system
+         when storing the env in UBI.
+
 - CONFIG_SYS_SPI_INIT_OFFSET
 
        Defines offset to the initial SPI buffer area in DPRAM. The
@@ -3809,9 +3864,13 @@ Low Level (hardware related) configuration options:
 - CONFIG_SYS_SRIOn_MEM_SIZE:
                Size of SRIO port 'n' memory region
 
-- CONFIG_SYS_NDFC_16
-               Defined to tell the NDFC that the NAND chip is using a
-               16 bit bus.
+- CONFIG_SYS_NAND_BUSWIDTH_16BIT
+               Defined to tell the NAND controller that the NAND chip is using
+               a 16 bit bus.
+               Not all NAND drivers use this symbol.
+               Example of drivers that use it:
+               - drivers/mtd/nand/ndfc.c
+               - drivers/mtd/nand/mxc_nand.c
 
 - CONFIG_SYS_NDFC_EBC0_CFG
                Sets the EBC0_CFG register for the NDFC. If not defined