index acb711a384c202bc20b0ff473b7f4de056eded62..c40e3355e91e7cf5ab2220e89dea39c89181d6e8 100644 (file)
--- a/README
+++ b/README
Thumb2 this flag will result in Thumb2 code generated by
GCC.
+ CONFIG_ARM_ERRATA_716044
+ CONFIG_ARM_ERRATA_742230
+ CONFIG_ARM_ERRATA_743622
+ CONFIG_ARM_ERRATA_751472
+
+ If set, the workarounds for these ARM errata are applied early
+ during U-Boot startup. Note that these options force the
+ workarounds to be applied; no CPU-type/version detection
+ exists, unlike the similar options in the Linux kernel. Do not
+ set these options unless they apply!
+
+- CPU timer options:
+ CONFIG_SYS_HZ
+
+ The frequency of the timer returned by get_timer().
+ get_timer() must operate in milliseconds and this CONFIG
+ option must be set to 1000.
+
- Linux Kernel Interface:
CONFIG_CLOCKS_IN_MHZ
CONFIG_CMD_EEPROM * EEPROM read/write support
CONFIG_CMD_ELF * bootelf, bootvx
CONFIG_CMD_ENV_CALLBACK * display details about env callbacks
+ CONFIG_CMD_ENV_FLAGS * display details about env flags
CONFIG_CMD_EXPORTENV * export the environment
CONFIG_CMD_EXT2 * ext2 command support
CONFIG_CMD_EXT4 * ext4 command support
CONFIG_CMD_I2C * I2C serial bus support
CONFIG_CMD_IDE * IDE harddisk support
CONFIG_CMD_IMI iminfo
- CONFIG_CMD_IMLS List all found images
+ CONFIG_CMD_IMLS List all images found in NOR flash
+ CONFIG_CMD_IMLS_NAND List all images found in NAND flash
CONFIG_CMD_IMMAP * IMMR dump support
CONFIG_CMD_IMPORTENV * import an environment
CONFIG_CMD_INI * import data from an ini file into the env
CONFIG_CMD_LOADS loads
CONFIG_CMD_MD5SUM print md5 message digest
(requires CONFIG_CMD_MEMORY and CONFIG_MD5)
+ CONFIG_CMD_MEMINFO * Display detailed memory information
CONFIG_CMD_MEMORY md, mm, nm, mw, cp, cmp, crc, base,
- loop, loopw, mtest
+ loop, loopw
+ CONFIG_CMD_MEMTEST mtest
CONFIG_CMD_MISC Misc functions like sleep etc
CONFIG_CMD_MMC * MMC memory mapped support
CONFIG_CMD_MII * MII utility commands
CONFIG_CMD_READ * Read raw data from partition
CONFIG_CMD_REGINFO * Register dump
CONFIG_CMD_RUN run command in env variable
+ CONFIG_CMD_SANDBOX * sb command to access sandbox features
CONFIG_CMD_SAVES * save S record dump
CONFIG_CMD_SCSI * SCSI Support
CONFIG_CMD_SDRAM * print SDRAM configuration information
CONFIG_SH_MMCIF_CLK
Define the clock frequency for MMCIF
+- USB Device Firmware Update (DFU) class support:
+ CONFIG_DFU_FUNCTION
+ This enables the USB portion of the DFU USB class
+
+ CONFIG_CMD_DFU
+ This enables the command "dfu" which is used to have
+ U-Boot create a DFU class device via USB. This command
+ requires that the "dfu_alt_info" environment variable be
+ set and define the alt settings to expose to the host.
+
+ CONFIG_DFU_MMC
+ This enables support for exposing (e)MMC devices via DFU.
+
+ CONFIG_DFU_NAND
+ This enables support for exposing NAND devices via DFU.
+
+ CONFIG_SYS_DFU_MAX_FILE_SIZE
+ When updating files rather than the raw storage device,
+ we use a static buffer to copy the file into and then write
+ the buffer once we've been given the whole file. Define
+ this to the maximum filesize (in bytes) for the buffer.
+ Default is 4 MiB if undefined.
+
- Journaling Flash filesystem support:
CONFIG_JFFS2_NAND, CONFIG_JFFS2_NAND_OFF, CONFIG_JFFS2_NAND_SIZE,
CONFIG_JFFS2_NAND_DEV
Normally display is black on white background; define
CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
+ CONFIG_LCD_ALIGNMENT
+
+ Normally the LCD is page-aligned (tyically 4KB). If this is
+ defined then the LCD will be aligned to this value instead.
+ For ARM it is sometimes useful to use MMU_SECTION_SIZE
+ here, since it is cheaper to change data cache settings on
+ a per-section basis.
+
+ CONFIG_CONSOLE_SCROLL_LINES
+
+ When the console need to be scrolled, this is the number of
+ lines to scroll by. It defaults to 1. Increasing this makes
+ the console jump but can help speed up operation when scrolling
+ is slow.
+
CONFIG_LCD_BMP_RLE8
Support drawing of RLE8-compressed bitmaps on the LCD.
Enables an 'i2c edid' command which can read EDID
information over I2C from an attached LCD display.
-
- Splash Screen Support: CONFIG_SPLASH_SCREEN
If this option is set, the environment is checked for
allows for a "silent" boot where a splash screen is
loaded very quickly after power-on.
+ CONFIG_SPLASHIMAGE_GUARD
+
+ If this option is set, then U-Boot will prevent the environment
+ variable "splashimage" from being set to a problematic address
+ (see README.displaying-bmps and README.arm-unaligned-accesses).
+ This option is useful for targets where, due to alignment
+ restrictions, an improperly aligned BMP image will cause a data
+ abort. If you think you will not have problems with unaligned
+ accesses (for example because your toolchain prevents them)
+ there is no need to set this option.
+
CONFIG_SPLASH_SCREEN_ALIGN
If this option is set the splash image can be freely positioned
=> vertically centered image
at x = dspWidth - bmpWidth - 9
+ CONFIG_SPLASH_SCREEN_PREPARE
+
+ If this option is set then the board_splash_screen_prepare()
+ function, which must be defined in your code, is called as part
+ of the splash screen display sequence. It gives the board an
+ opportunity to prepare the splash image data before it is
+ processed and sent to the frame buffer by U-Boot.
+
- Gzip compressed BMP image support: CONFIG_VIDEO_BMP_GZIP
If this option is set, additionally to standard BMP
I2C_READ
- Code that returns TRUE if the I2C data line is high,
- FALSE if it is low.
+ Code that returns true if the I2C data line is high,
+ false if it is low.
eg: #define I2C_READ ((immr->im_cpm.cp_pbdat & PB_SDA) != 0)
I2C_SDA(bit)
- If <bit> is TRUE, sets the I2C data line high. If it
- is FALSE, it clears it (low).
+ If <bit> is true, sets the I2C data line high. If it
+ is false, it clears it (low).
eg: #define I2C_SDA(bit) \
if(bit) immr->im_cpm.cp_pbdat |= PB_SDA; \
I2C_SCL(bit)
- If <bit> is TRUE, sets the I2C clock line high. If it
- is FALSE, it clears it (low).
+ If <bit> is true, sets the I2C clock line high. If it
+ is false, it clears it (low).
eg: #define I2C_SCL(bit) \
if(bit) immr->im_cpm.cp_pbdat |= PB_SCL; \
run-time determined information about the hardware to the
environment. These will be named board_name, board_rev.
+ CONFIG_DELAY_ENVIRONMENT
+
+ Normally the environment is loaded when the board is
+ intialised so that it is available to U-Boot. This inhibits
+ that so that the environment is not available until
+ explicitly loaded later by U-Boot code. With CONFIG_OF_CONTROL
+ this is instead controlled by the value of
+ /config/load-environment.
+
- DataFlash Support:
CONFIG_HAS_DATAFLASH
CONFIG_SF_DEFAULT_MODE (see include/spi.h)
CONFIG_SF_DEFAULT_SPEED in Hz
+ CONFIG_CMD_SF_TEST
+
+ Define this option to include a destructive SPI flash
+ test ('sf test').
+
+ CONFIG_SPI_FLASH_BAR Ban/Extended Addr Reg
+
+ Define this option to use the Bank addr/Extended addr
+ support on SPI flashes which has size > 16Mbytes.
+
- SystemACE Support:
CONFIG_SYSTEMACE
CONFIG_FB_ADDR
Define CONFIG_FB_ADDR if you want to use specific
- address for frame buffer.
- Then system will reserve the frame buffer address to
- defined address instead of lcd_setmem (this function
- grabs the memory for frame buffer by panel's size).
+ address for frame buffer. This is typically the case
+ when using a graphics controller has separate video
+ memory. U-Boot will then place the frame buffer at
+ the given address instead of dynamically reserving it
+ in system RAM by calling lcd_setmem(), which grabs
+ the memory for the frame buffer depending on the
+ configured panel size.
Please see board_init_f function.
Adds the MTD partitioning infrastructure from the Linux
kernel. Needed for UBI support.
+- UBI support
+ CONFIG_CMD_UBI
+
+ Adds commands for interacting with MTD partitions formatted
+ with the UBI flash translation layer
+
+ Requires also defining CONFIG_RBTREE
+
+ CONFIG_UBI_SILENCE_MSG
+
+ Make the verbose messages from UBI stop printing. This leaves
+ warnings and errors enabled.
+
+- UBIFS support
+ CONFIG_CMD_UBIFS
+
+ Adds commands for interacting with UBI volumes formatted as
+ UBIFS. UBIFS is read-only in u-boot.
+
+ Requires UBI support as well as CONFIG_LZO
+
+ CONFIG_UBIFS_SILENCE_MSG
+
+ Make the verbose messages from UBIFS stop printing. This leaves
+ warnings and errors enabled.
+
- SPL framework
CONFIG_SPL
Enable building of SPL globally.
CONFIG_SPL_LDSCRIPT
LDSCRIPT for linking the SPL binary.
+ CONFIG_SPL_MAX_FOOTPRINT
+ Maximum size in memory allocated to the SPL, BSS included.
+ When defined, the linker checks that the actual memory
+ used by SPL from _start to __bss_end does not exceed it.
+ CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+ must not be both defined at the same time.
+
CONFIG_SPL_MAX_SIZE
- Maximum binary size (text, data and rodata) of the SPL binary.
+ Maximum size of the SPL image (text, data, rodata, and
+ linker lists sections), BSS excluded.
+ When defined, the linker checks that the actual size does
+ not exceed it.
CONFIG_SPL_TEXT_BASE
TEXT_BASE for linking the SPL binary.
Link address for the BSS within the SPL binary.
CONFIG_SPL_BSS_MAX_SIZE
- Maximum binary size of the BSS section of the SPL binary.
+ Maximum size in memory allocated to the SPL BSS.
+ When defined, the linker checks that the actual memory used
+ by SPL from __bss_start to __bss_end does not exceed it.
+ CONFIG_SPL_MAX_FOOTPRINT and CONFIG_SPL_BSS_MAX_SIZE
+ must not be both defined at the same time.
CONFIG_SPL_STACK
Adress of the start of the stack SPL will use
CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME
Filename to read to load U-Boot when reading from FAT
+ CONFIG_SPL_MPC83XX_WAIT_FOR_NAND
+ Set this for NAND SPL on PPC mpc83xx targets, so that
+ start.S waits for the rest of the SPL to load before
+ continuing (the hardware starts execution after just
+ loading the first page rather than the full 4K).
+
CONFIG_SPL_NAND_BASE
Include nand_base.c in the SPL. Requires
CONFIG_SPL_NAND_DRIVERS.
CONFIG_SPL_LIBGENERIC_SUPPORT
Support for lib/libgeneric.o in SPL binary
+ CONFIG_SPL_PAD_TO
+ Image offset to which the SPL should be padded before appending
+ the SPL payload. By default, this is defined as
+ CONFIG_SPL_MAX_SIZE, or 0 if CONFIG_SPL_MAX_SIZE is undefined.
+ CONFIG_SPL_PAD_TO must be either 0, meaning to append the SPL
+ payload without any padding, or >= CONFIG_SPL_MAX_SIZE.
+
CONFIG_SPL_TARGET
Final target image containing SPL and payload. Some SPLs
use an arch-specific makefile fragment instead, for
non page size aligned address and this could cause major
problems.
-- CONFIG_SYS_TFTP_LOADADDR:
- Default load address for network file downloads
-
- CONFIG_SYS_LOADS_BAUD_CHANGE:
Enable temporary baudrate change while serial download
The format of the list is:
type_attribute = [s|d|x|b|i|m]
- attributes = type_attribute
+ access_atribute = [a|r|o|c]
+ attributes = type_attribute[access_atribute]
entry = variable_name[:attributes]
list = entry[,list]
i - IP address
m - MAC address
+ The access attributes are:
+ a - Any (default)
+ r - Read-only
+ o - Write-once
+ c - Change-default
+
- CONFIG_ENV_FLAGS_LIST_DEFAULT
Define this to a list (string) to define the ".flags"
envirnoment variable in the default or embedded environment.
list, simply add an entry for the same variable name to the
".flags" variable.
+- CONFIG_ENV_ACCESS_IGNORE_FORCE
+ If defined, don't allow the -f switch to env set override variable
+ access flags.
+
+- CONFIG_SYS_GENERIC_BOARD
+ This selects the architecture-generic board system instead of the
+ architecture-specific board files. It is intended to move boards
+ to this new framework over time. Defining this will disable the
+ arch/foo/lib/board.c file and use common/board_f.c and
+ common/board_r.c instead. To use this option your architecture
+ must support it (i.e. must define __HAVE_ARCH_GENERIC_BOARD in
+ its config.mk file). If you find problems enabling this option on
+ your board please report the problem and send patches!
+
+- CONFIG_SYS_SYM_OFFSETS
+ This is set by architectures that use offsets for link symbols
+ instead of absolute values. So bss_start is obtained using an
+ offset _bss_start_ofs from CONFIG_SYS_TEXT_BASE, rather than
+ directly. You should not need to touch this setting.
+
+- CONFIG_OMAP_PLATFORM_RESET_TIME_MAX_USEC (OMAP only)
+ This is set by OMAP boards for the max time that reset should
+ be asserted. See doc/README.omap-reset-time for details on how
+ the value can be calulated on a given board.
+
The following definitions that deal with the placement and management
of environment data (variable area); in general, we support the
following configurations:
environment. If redundant environment is used, it will be copied to
CONFIG_NAND_ENV_DST + CONFIG_ENV_SIZE.
+- CONFIG_ENV_IS_IN_UBI:
+
+ Define this if you have an UBI volume that you want to use for the
+ environment. This has the benefit of wear-leveling the environment
+ accesses, which is important on NAND.
+
+ - CONFIG_ENV_UBI_PART:
+
+ Define this to a string that is the mtd partition containing the UBI.
+
+ - CONFIG_ENV_UBI_VOLUME:
+
+ Define this to the name of the volume that you want to store the
+ environment in.
+
+ - CONFIG_ENV_UBI_VOLUME_REDUND:
+
+ Define this to the name of another volume to store a second copy of
+ the environment in. This will enable redundant environments in UBI.
+ It is assumed that both volumes are in the same MTD partition.
+
+ - CONFIG_UBI_SILENCE_MSG
+ - CONFIG_UBIFS_SILENCE_MSG
+
+ You will probably want to define these to avoid a really noisy system
+ when storing the env in UBI.
+
- CONFIG_SYS_SPI_INIT_OFFSET
Defines offset to the initial SPI buffer area in DPRAM. The
space for already greatly restricted images, including but not
limited to NAND_SPL configurations.
+- CONFIG_DISPLAY_BOARDINFO
+ Display information about the board that U-Boot is running on
+ when U-Boot starts up. The board function checkboard() is called
+ to do this.
+
+- CONFIG_DISPLAY_BOARDINFO_LATE
+ Similar to the previous option, but display this information
+ later, once stdio is running and output goes to the LCD, if
+ present.
+
Low Level (hardware related) configuration options:
---------------------------------------------------
- CONFIG_SYS_SRIOn_MEM_SIZE:
Size of SRIO port 'n' memory region
-- CONFIG_SYS_NDFC_16
- Defined to tell the NDFC that the NAND chip is using a
- 16 bit bus.
+- CONFIG_SYS_NAND_BUSWIDTH_16BIT
+ Defined to tell the NAND controller that the NAND chip is using
+ a 16 bit bus.
+ Not all NAND drivers use this symbol.
+ Example of drivers that use it:
+ - drivers/mtd/nand/ndfc.c
+ - drivers/mtd/nand/mxc_nand.c
- CONFIG_SYS_NDFC_EBC0_CFG
Sets the EBC0_CFG register for the NDFC. If not defined
that is executed before the actual U-Boot. E.g. when
compiling a NAND SPL.
+- CONFIG_ARCH_MAP_SYSMEM
+ Generally U-Boot (and in particular the md command) uses
+ effective address. It is therefore not necessary to regard
+ U-Boot address as virtual addresses that need to be translated
+ to physical addresses. However, sandbox requires this, since
+ it maintains its own little RAM buffer which contains all
+ addressable memory. This option causes some memory accesses
+ to be mapped through map_sysmem() / unmap_sysmem().
+
- CONFIG_USE_ARCH_MEMCPY
CONFIG_USE_ARCH_MEMSET
If these options are used a optimized version of memcpy/memset will
be used if available. These functions may be faster under some
conditions but may increase the binary size.
-- CONFIG_X86_NO_RESET_VECTOR
- If defined, the x86 reset vector code is excluded. You will need
- to do this when U-Boot is running from Coreboot.
+- CONFIG_X86_RESET_VECTOR
+ If defined, the x86 reset vector code is included. This is not
+ needed when U-Boot is running from Coreboot.
-- CONFIG_X86_NO_REAL_MODE
- If defined, x86 real mode code is omitted. This assumes a
- 32-bit environment where such code is not needed. You will
- need to do this when U-Boot is running from Coreboot.
+- CONFIG_SYS_MPUCLK
+ Defines the MPU clock speed (in MHz).
+ NOTE : currently only supported on AM335x platforms.
Freescale QE/FMAN Firmware Support:
-----------------------------------