Merge branch 'master' of git://git.denx.de/u-boot-i2c
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index cf6b8982490412e15aa399eee37b90aa4e48347a..cdd81d4efe3efafd8e8e3653303eec1af2e599f5 100644 (file)
--- a/README
+++ b/README
@@ -183,7 +183,7 @@ Directory Hierarchy:
   /nios2               Files generic to Altera NIOS2 architecture
     /cpu               CPU specific files
     /lib               Architecture specific library files
-  /ppc                 Files generic to PowerPC architecture
+  /powerpc             Files generic to PowerPC architecture
     /cpu               CPU specific files
       /74xx_7xx                Files specific to Freescale MPC74xx and 7xx CPUs
       /mpc5xx          Files specific to Freescale MPC5xx CPUs
@@ -1417,7 +1417,7 @@ The following options need to be configured:
                the CPU's i2c node address).
 
                Now, the u-boot i2c code for the mpc8xx
-               (arch/ppc/cpu/mpc8xx/i2c.c) sets the CPU up as a master node
+               (arch/powerpc/cpu/mpc8xx/i2c.c) sets the CPU up as a master node
                and so its address should therefore be cleared to 0 (See,
                eg, MPC823e User's Manual p.16-473). So, set
                CONFIG_SYS_I2C_SLAVE to 0.
@@ -1977,7 +1977,7 @@ Legacy uImage format:
 
    15  arch/<arch>/lib/bootm.c All preparation done, transferring control to OS
 
-  -30  arch/ppc/lib/board.c    Fatal error, hang the system
+  -30  arch/powerpc/lib/board.c        Fatal error, hang the system
   -31  post/post.c             POST test failed, detected by post_output_backlog()
   -32  post/post.c             POST test failed, detected by post_run_single()
 
@@ -2738,7 +2738,7 @@ Low Level (hardware related) configuration options:
   CONFIG_SYS_PCI_MSTR_MEMIO_SIZE, CONFIG_SYS_POCMR1_MASK_ATTRIB, CONFIG_SYS_PCI_MSTR_IO_LOCAL,
   CONFIG_SYS_PCI_MSTR_IO_BUS, CONFIG_SYS_CPU_PCI_IO_START, CONFIG_SYS_PCI_MSTR_IO_SIZE,
   CONFIG_SYS_POCMR2_MASK_ATTRIB: (MPC826x only)
-               Overrides the default PCI memory map in arch/ppc/cpu/mpc8260/pci.c if set.
+               Overrides the default PCI memory map in arch/powerpc/cpu/mpc8260/pci.c if set.
 
 - CONFIG_PCI_DISABLE_PCIE:
                Disable PCI-Express on systems where it is supported but not
@@ -3384,7 +3384,7 @@ configure the Linux device drivers for use with your target hardware
 (no, we don't intend to provide a full virtual machine interface to
 Linux :-).
 
-But now you can ignore ALL boot loader code (in arch/ppc/mbxboot).
+But now you can ignore ALL boot loader code (in arch/powerpc/mbxboot).
 
 Just make sure your machine specific header file (for instance
 include/asm-ppc/tqm8xx.h) includes the same definition of the Board
@@ -3482,7 +3482,7 @@ So a typical call to build a U-Boot image would read:
 
        -> tools/mkimage -n '2.4.4 kernel for TQM850L' \
        > -A ppc -O linux -T kernel -C gzip -a 0 -e 0 \
-       > -d /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/ppc/coffboot/vmlinux.gz \
+       > -d /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/powerpc/coffboot/vmlinux.gz \
        > examples/uImage.TQM850L
        Image Name:   2.4.4 kernel for TQM850L
        Created:      Wed Jul 19 02:34:59 2000
@@ -3506,10 +3506,10 @@ speed for memory and install an UNCOMPRESSED image instead: this
 needs more space in Flash, but boots much faster since it does not
 need to be uncompressed:
 
-       -> gunzip /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/ppc/coffboot/vmlinux.gz
+       -> gunzip /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/powerpc/coffboot/vmlinux.gz
        -> tools/mkimage -n '2.4.4 kernel for TQM850L' \
        > -A ppc -O linux -T kernel -C none -a 0 -e 0 \
-       > -d /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/ppc/coffboot/vmlinux \
+       > -d /opt/elsk/ppc_8xx/usr/src/linux-2.4.4/arch/powerpc/coffboot/vmlinux \
        > examples/uImage.TQM850L-uncompressed
        Image Name:   2.4.4 kernel for TQM850L
        Created:      Wed Jul 19 02:34:59 2000