index 2352e3862bfa81f4ad2bca262cc26529ac008fd7..d51ece946c309a37fa3fcf5c1d91f0174e2b016f 100644 (file)
--- a/README
+++ b/README
CONFIG_CMD_I2C * I2C serial bus support
CONFIG_CMD_IDE * IDE harddisk support
CONFIG_CMD_IMI iminfo
- CONFIG_CMD_IMLS List all found images
+ CONFIG_CMD_IMLS List all images found in NOR flash
+ CONFIG_CMD_IMLS_NAND List all images found in NAND flash
CONFIG_CMD_IMMAP * IMMR dump support
CONFIG_CMD_IMPORTENV * import an environment
CONFIG_CMD_INI * import data from an ini file into the env
CONFIG_CMD_READ * Read raw data from partition
CONFIG_CMD_REGINFO * Register dump
CONFIG_CMD_RUN run command in env variable
+ CONFIG_CMD_SANDBOX * sb command to access sandbox features
CONFIG_CMD_SAVES * save S record dump
CONFIG_CMD_SCSI * SCSI Support
CONFIG_CMD_SDRAM * print SDRAM configuration information
allows for a "silent" boot where a splash screen is
loaded very quickly after power-on.
+ CONFIG_SPLASHIMAGE_GUARD
+
+ If this option is set, then U-Boot will prevent the environment
+ variable "splashimage" from being set to a problematic address
+ (see README.displaying-bmps and README.arm-unaligned-accesses).
+ This option is useful for targets where, due to alignment
+ restrictions, an improperly aligned BMP image will cause a data
+ abort. If you think you will not have problems with unaligned
+ accesses (for example because your toolchain prevents them)
+ there is no need to set this option.
+
CONFIG_SPLASH_SCREEN_ALIGN
If this option is set the splash image can be freely positioned
=> vertically centered image
at x = dspWidth - bmpWidth - 9
+ CONFIG_SPLASH_SCREEN_PREPARE
+
+ If this option is set then the board_splash_screen_prepare()
+ function, which must be defined in your code, is called as part
+ of the splash screen display sequence. It gives the board an
+ opportunity to prepare the splash image data before it is
+ processed and sent to the frame buffer by U-Boot.
+
- Gzip compressed BMP image support: CONFIG_VIDEO_BMP_GZIP
If this option is set, additionally to standard BMP
that is executed before the actual U-Boot. E.g. when
compiling a NAND SPL.
+- CONFIG_ARCH_MAP_SYSMEM
+ Generally U-Boot (and in particular the md command) uses
+ effective address. It is therefore not necessary to regard
+ U-Boot address as virtual addresses that need to be translated
+ to physical addresses. However, sandbox requires this, since
+ it maintains its own little RAM buffer which contains all
+ addressable memory. This option causes some memory accesses
+ to be mapped through map_sysmem() / unmap_sysmem().
+
- CONFIG_USE_ARCH_MEMCPY
CONFIG_USE_ARCH_MEMSET
If these options are used a optimized version of memcpy/memset will
be used if available. These functions may be faster under some
conditions but may increase the binary size.
-- CONFIG_X86_NO_RESET_VECTOR
- If defined, the x86 reset vector code is excluded. You will need
- to do this when U-Boot is running from Coreboot.
-
-- CONFIG_X86_NO_REAL_MODE
- If defined, x86 real mode code is omitted. This assumes a
- 32-bit environment where such code is not needed. You will
- need to do this when U-Boot is running from Coreboot.
+- CONFIG_X86_RESET_VECTOR
+ If defined, the x86 reset vector code is included. This is not
+ needed when U-Boot is running from Coreboot.
Freescale QE/FMAN Firmware Support: