Merge u-boot/master into u-boot-ti/master
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index 42544cead64ef8d45dbd8834de1c36d5f292ed5a..d51ece946c309a37fa3fcf5c1d91f0174e2b016f 100644 (file)
--- a/README
+++ b/README
@@ -1532,6 +1532,17 @@ CBFS (Coreboot Filesystem) support
                allows for a "silent" boot where a splash screen is
                loaded very quickly after power-on.
 
+               CONFIG_SPLASHIMAGE_GUARD
+
+               If this option is set, then U-Boot will prevent the environment
+               variable "splashimage" from being set to a problematic address
+               (see README.displaying-bmps and README.arm-unaligned-accesses).
+               This option is useful for targets where, due to alignment
+               restrictions, an improperly aligned BMP image will cause a data
+               abort. If you think you will not have problems with unaligned
+               accesses (for example because your toolchain prevents them)
+               there is no need to set this option.
+
                CONFIG_SPLASH_SCREEN_ALIGN
 
                If this option is set the splash image can be freely positioned
@@ -1552,6 +1563,14 @@ CBFS (Coreboot Filesystem) support
                        => vertically centered image
                           at x = dspWidth - bmpWidth - 9
 
+               CONFIG_SPLASH_SCREEN_PREPARE
+
+               If this option is set then the board_splash_screen_prepare()
+               function, which must be defined in your code, is called as part
+               of the splash screen display sequence. It gives the board an
+               opportunity to prepare the splash image data before it is
+               processed and sent to the frame buffer by U-Boot.
+
 - Gzip compressed BMP image support: CONFIG_VIDEO_BMP_GZIP
 
                If this option is set, additionally to standard BMP