]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blobdiff - README
Merge u-boot/master into u-boot-ti/master
[glsdk/glsdk-u-boot.git] / README
diff --git a/README b/README
index afdf591c623f6cfa5c507d6918e738dea12b2c79..d51ece946c309a37fa3fcf5c1d91f0174e2b016f 100644 (file)
--- a/README
+++ b/README
@@ -54,6 +54,11 @@ In case of problems see the CHANGELOG and CREDITS files to find out
 who contributed the specific port. The MAINTAINERS file lists board
 maintainers.
 
+Note: There is no CHANGELOG file in the actual U-Boot source tree;
+it can be created dynamically from the Git log using:
+
+       make CHANGELOG
+
 
 Where to get help:
 ==================
@@ -611,6 +616,14 @@ The following options need to be configured:
                boot loader that has already initialized the UART.  Define this
                variable to flush the UART at init time.
 
+               CONFIG_SYS_NS16550_BROKEN_TEMT
+
+               16550 UART set the Transmitter Empty (TEMT) Bit when all output
+               has finished and the transmitter is totally empty. U-Boot waits
+               for this bit to be set to initialize the serial console. On some
+               broken platforms this bit is not set in SPL making U-Boot to
+               hang while waiting for TEMT. Define this option to avoid it.
+
 
 - Console Interface:
                Depending on board, define exactly one serial port
@@ -810,6 +823,8 @@ The following options need to be configured:
                CONFIG_CMD_EDITENV        edit env variable
                CONFIG_CMD_EEPROM       * EEPROM read/write support
                CONFIG_CMD_ELF          * bootelf, bootvx
+               CONFIG_CMD_ENV_CALLBACK * display details about env callbacks
+               CONFIG_CMD_ENV_FLAGS    * display details about env flags
                CONFIG_CMD_EXPORTENV    * export the environment
                CONFIG_CMD_EXT2         * ext2 command support
                CONFIG_CMD_EXT4         * ext4 command support
@@ -819,13 +834,16 @@ The following options need to be configured:
                CONFIG_CMD_FDOS         * Dos diskette Support
                CONFIG_CMD_FLASH          flinfo, erase, protect
                CONFIG_CMD_FPGA           FPGA device initialization support
+               CONFIG_CMD_GETTIME      * Get time since boot
                CONFIG_CMD_GO           * the 'go' command (exec code)
                CONFIG_CMD_GREPENV      * search environment
+               CONFIG_CMD_HASH         * calculate hash / digest
                CONFIG_CMD_HWFLOW       * RTS/CTS hw flow control
                CONFIG_CMD_I2C          * I2C serial bus support
                CONFIG_CMD_IDE          * IDE harddisk support
                CONFIG_CMD_IMI            iminfo
-               CONFIG_CMD_IMLS           List all found images
+               CONFIG_CMD_IMLS           List all images found in NOR flash
+               CONFIG_CMD_IMLS_NAND      List all images found in NAND flash
                CONFIG_CMD_IMMAP        * IMMR dump support
                CONFIG_CMD_IMPORTENV    * import an environment
                CONFIG_CMD_INI          * import data from an ini file into the env
@@ -840,6 +858,7 @@ The following options need to be configured:
                CONFIG_CMD_LOADS          loads
                CONFIG_CMD_MD5SUM         print md5 message digest
                                          (requires CONFIG_CMD_MEMORY and CONFIG_MD5)
+               CONFIG_CMD_MEMINFO      * Display detailed memory information
                CONFIG_CMD_MEMORY         md, mm, nm, mw, cp, cmp, crc, base,
                                          loop, loopw, mtest
                CONFIG_CMD_MISC           Misc functions like sleep etc
@@ -855,8 +874,10 @@ The following options need to be configured:
                CONFIG_CMD_PING         * send ICMP ECHO_REQUEST to network
                                          host
                CONFIG_CMD_PORTIO       * Port I/O
+               CONFIG_CMD_READ         * Read raw data from partition
                CONFIG_CMD_REGINFO      * Register dump
                CONFIG_CMD_RUN            run command in env variable
+               CONFIG_CMD_SANDBOX      * sb command to access sandbox features
                CONFIG_CMD_SAVES        * save S record dump
                CONFIG_CMD_SCSI         * SCSI Support
                CONFIG_CMD_SDRAM        * print SDRAM configuration information
@@ -1409,6 +1430,13 @@ CBFS (Coreboot Filesystem) support
                boot.  See the documentation file README.video for a
                description of this variable.
 
+               CONFIG_VIDEO_VGA
+
+               Enable the VGA video / BIOS for x86. The alternative if you
+               are using coreboot is to use the coreboot frame buffer
+               driver.
+
+
 - Keyboard Support:
                CONFIG_KEYBOARD
 
@@ -1469,6 +1497,30 @@ CBFS (Coreboot Filesystem) support
                Normally display is black on white background; define
                CONFIG_SYS_WHITE_ON_BLACK to get it inverted.
 
+               CONFIG_LCD_ALIGNMENT
+
+               Normally the LCD is page-aligned (tyically 4KB). If this is
+               defined then the LCD will be aligned to this value instead.
+               For ARM it is sometimes useful to use MMU_SECTION_SIZE
+               here, since it is cheaper to change data cache settings on
+               a per-section basis.
+
+               CONFIG_CONSOLE_SCROLL_LINES
+
+               When the console need to be scrolled, this is the number of
+               lines to scroll by. It defaults to 1. Increasing this makes
+               the console jump but can help speed up operation when scrolling
+               is slow.
+
+               CONFIG_LCD_BMP_RLE8
+
+               Support drawing of RLE8-compressed bitmaps on the LCD.
+
+               CONFIG_I2C_EDID
+
+               Enables an 'i2c edid' command which can read EDID
+               information over I2C from an attached LCD display.
+
 - Splash Screen Support: CONFIG_SPLASH_SCREEN
 
                If this option is set, the environment is checked for
@@ -1480,6 +1532,17 @@ CBFS (Coreboot Filesystem) support
                allows for a "silent" boot where a splash screen is
                loaded very quickly after power-on.
 
+               CONFIG_SPLASHIMAGE_GUARD
+
+               If this option is set, then U-Boot will prevent the environment
+               variable "splashimage" from being set to a problematic address
+               (see README.displaying-bmps and README.arm-unaligned-accesses).
+               This option is useful for targets where, due to alignment
+               restrictions, an improperly aligned BMP image will cause a data
+               abort. If you think you will not have problems with unaligned
+               accesses (for example because your toolchain prevents them)
+               there is no need to set this option.
+
                CONFIG_SPLASH_SCREEN_ALIGN
 
                If this option is set the splash image can be freely positioned
@@ -1500,6 +1563,14 @@ CBFS (Coreboot Filesystem) support
                        => vertically centered image
                           at x = dspWidth - bmpWidth - 9
 
+               CONFIG_SPLASH_SCREEN_PREPARE
+
+               If this option is set then the board_splash_screen_prepare()
+               function, which must be defined in your code, is called as part
+               of the splash screen display sequence. It gives the board an
+               opportunity to prepare the splash image data before it is
+               processed and sent to the frame buffer by U-Boot.
+
 - Gzip compressed BMP image support: CONFIG_VIDEO_BMP_GZIP
 
                If this option is set, additionally to standard BMP
@@ -2162,6 +2233,11 @@ CBFS (Coreboot Filesystem) support
                serial# is unaffected by this, i. e. it remains
                read-only.]
 
+               The same can be accomplished in a more flexible way
+               for any variable by configuring the type of access
+               to allow for those variables in the ".flags" variable
+               or define CONFIG_ENV_FLAGS_LIST_STATIC.
+
 - Protected RAM:
                CONFIG_PRAM
 
@@ -2195,6 +2271,14 @@ CBFS (Coreboot Filesystem) support
                        HERMES, IP860, RPXlite, LWMON,
                        FLAGADM, TQM8260
 
+- Access to physical memory region (> 4GB)
+               Some basic support is provided for operations on memory not
+               normally accessible to U-Boot - e.g. some architectures
+               support access to more than 4GB of memory on 32-bit
+               machines using physical address extension or similar.
+               Define CONFIG_PHYSMEM to access this basic support, which
+               currently only supports clearing the memory.
+
 - Error Recovery:
                CONFIG_PANIC_HANG
 
@@ -2324,6 +2408,15 @@ CBFS (Coreboot Filesystem) support
                run-time determined information about the hardware to the
                environment.  These will be named board_name, board_rev.
 
+               CONFIG_DELAY_ENVIRONMENT
+
+               Normally the environment is loaded when the board is
+               intialised so that it is available to U-Boot. This inhibits
+               that so that the environment is not available until
+               explicitly loaded later by U-Boot code. With CONFIG_OF_CONTROL
+               this is instead controlled by the value of
+               /config/load-environment.
+
 - DataFlash Support:
                CONFIG_HAS_DATAFLASH
 
@@ -2350,6 +2443,11 @@ CBFS (Coreboot Filesystem) support
                CONFIG_SF_DEFAULT_MODE          (see include/spi.h)
                CONFIG_SF_DEFAULT_SPEED         in Hz
 
+               CONFIG_CMD_SF_TEST
+
+               Define this option to include a destructive SPI flash
+               test ('sf test').
+
 - SystemACE Support:
                CONFIG_SYSTEMACE
 
@@ -2384,6 +2482,23 @@ CBFS (Coreboot Filesystem) support
                A better solution is to properly configure the firewall,
                but sometimes that is not allowed.
 
+- Hashing support:
+               CONFIG_CMD_HASH
+
+               This enables a generic 'hash' command which can produce
+               hashes / digests from a few algorithms (e.g. SHA1, SHA256).
+
+               CONFIG_HASH_VERIFY
+
+               Enable the hash verify command (hash -v). This adds to code
+               size a little.
+
+               CONFIG_SHA1 - support SHA1 hashing
+               CONFIG_SHA256 - support SHA256 hashing
+
+               Note: There is also a sha1sum command, which should perhaps
+               be deprecated in favour of 'hash sha1'.
+
 - Show boot progress:
                CONFIG_SHOW_BOOT_PROGRESS
 
@@ -2597,6 +2712,17 @@ FIT uImage format:
  -150  common/cmd_nand.c       Incorrect FIT image format
   151  common/cmd_nand.c       FIT image format OK
 
+- FIT image support:
+               CONFIG_FIT
+               Enable support for the FIT uImage format.
+
+               CONFIG_FIT_BEST_MATCH
+               When no configuration is explicitly selected, default to the
+               one whose fdt's compatibility field best matches that of
+               U-Boot itself. A match is considered "best" if it matches the
+               most specific compatibility entry of U-Boot's fdt's root node.
+               The order of entries in the configuration's fdt is ignored.
+
 - Standalone program support:
                CONFIG_STANDALONE_LOAD_ADDR
 
@@ -2609,10 +2735,13 @@ FIT uImage format:
                CONFIG_FB_ADDR
 
                Define CONFIG_FB_ADDR if you want to use specific
-               address for frame buffer.
-               Then system will reserve the frame buffer address to
-               defined address instead of lcd_setmem (this function
-               grabs the memory for frame buffer by panel's size).
+               address for frame buffer.  This is typically the case
+               when using a graphics controller has separate video
+               memory.  U-Boot will then place the frame buffer at
+               the given address instead of dynamically reserving it
+               in system RAM by calling lcd_setmem(), which grabs
+               the memory for the frame buffer depending on the
+               configured panel size.
 
                Please see board_init_f function.
 
@@ -2648,6 +2777,10 @@ FIT uImage format:
                CONFIG_SPL_TEXT_BASE
                TEXT_BASE for linking the SPL binary.
 
+               CONFIG_SPL_RELOC_TEXT_BASE
+               Address to relocate to.  If unspecified, this is equal to
+               CONFIG_SPL_TEXT_BASE (i.e. no relocation is done).
+
                CONFIG_SPL_BSS_START_ADDR
                Link address for the BSS within the SPL binary.
 
@@ -2657,6 +2790,11 @@ FIT uImage format:
                CONFIG_SPL_STACK
                Adress of the start of the stack SPL will use
 
+               CONFIG_SPL_RELOC_STACK
+               Adress of the start of the stack SPL will use after
+               relocation.  If unspecified, this is equal to
+               CONFIG_SPL_STACK.
+
                CONFIG_SYS_SPL_MALLOC_START
                Starting address of the malloc pool used in SPL.
 
@@ -2672,6 +2810,9 @@ FIT uImage format:
                For ARM, enable an optional function to print more information
                about the running system.
 
+               CONFIG_SPL_INIT_MINIMAL
+               Arch init code should be built for a very small image
+
                CONFIG_SPL_LIBCOMMON_SUPPORT
                Support for common/libcommon.o in SPL binary
 
@@ -2699,8 +2840,25 @@ FIT uImage format:
                CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME
                Filename to read to load U-Boot when reading from FAT
 
+               CONFIG_SPL_MPC83XX_WAIT_FOR_NAND
+               Set this for NAND SPL on PPC mpc83xx targets, so that
+               start.S waits for the rest of the SPL to load before
+               continuing (the hardware starts execution after just
+               loading the first page rather than the full 4K).
+
+               CONFIG_SPL_NAND_BASE
+               Include nand_base.c in the SPL.  Requires
+               CONFIG_SPL_NAND_DRIVERS.
+
+               CONFIG_SPL_NAND_DRIVERS
+               SPL uses normal NAND drivers, not minimal drivers.
+
+               CONFIG_SPL_NAND_ECC
+               Include standard software ECC in the SPL
+
                CONFIG_SPL_NAND_SIMPLE
-               Support for drivers/mtd/nand/libnand.o in SPL binary
+               Support for NAND boot using simple NAND drivers that
+               expose the cmd_ctrl() interface.
 
                CONFIG_SYS_NAND_5_ADDR_CYCLE, CONFIG_SYS_NAND_PAGE_COUNT,
                CONFIG_SYS_NAND_PAGE_SIZE, CONFIG_SYS_NAND_OOBSIZE,
@@ -2708,15 +2866,19 @@ FIT uImage format:
                CONFIG_SYS_NAND_ECCPOS, CONFIG_SYS_NAND_ECCSIZE,
                CONFIG_SYS_NAND_ECCBYTES
                Defines the size and behavior of the NAND that SPL uses
-               to read U-Boot with CONFIG_SPL_NAND_SIMPLE
+               to read U-Boot
 
                CONFIG_SYS_NAND_U_BOOT_OFFS
-               Location in NAND for CONFIG_SPL_NAND_SIMPLE to read U-Boot
-               from.
+               Location in NAND to read U-Boot from
+
+               CONFIG_SYS_NAND_U_BOOT_DST
+               Location in memory to load U-Boot to
+
+               CONFIG_SYS_NAND_U_BOOT_SIZE
+               Size of image to load
 
                CONFIG_SYS_NAND_U_BOOT_START
-               Location in memory for CONFIG_SPL_NAND_SIMPLE to load U-Boot
-               to.
+               Entry point in loaded image to jump to
 
                CONFIG_SYS_NAND_HW_ECC_OOBFIRST
                Define this if you need to first read the OOB and then the
@@ -2741,6 +2903,15 @@ FIT uImage format:
                CONFIG_SPL_LIBGENERIC_SUPPORT
                Support for lib/libgeneric.o in SPL binary
 
+               CONFIG_SPL_PAD_TO
+               Linker address to which the SPL should be padded before
+               appending the SPL payload.
+
+               CONFIG_SPL_TARGET
+               Final target image containing SPL and payload.  Some SPLs
+               use an arch-specific makefile fragment instead, for
+               example if more than one image needs to be produced.
+
 Modem Support:
 --------------
 
@@ -2875,9 +3046,6 @@ Configuration Settings:
                non page size aligned address and this could cause major
                problems.
 
-- CONFIG_SYS_TFTP_LOADADDR:
-               Default load address for network file downloads
-
 - CONFIG_SYS_LOADS_BAUD_CHANGE:
                Enable temporary baudrate change while serial download
 
@@ -3019,6 +3187,49 @@ Configuration Settings:
        cases. This setting can be used to tune behaviour; see
        lib/hashtable.c for details.
 
+- CONFIG_ENV_FLAGS_LIST_DEFAULT
+- CONFIG_ENV_FLAGS_LIST_STATIC
+       Enable validation of the values given to enviroment variables when
+       calling env set.  Variables can be restricted to only decimal,
+       hexadecimal, or boolean.  If CONFIG_CMD_NET is also defined,
+       the variables can also be restricted to IP address or MAC address.
+
+       The format of the list is:
+               type_attribute = [s|d|x|b|i|m]
+               access_atribute = [a|r|o|c]
+               attributes = type_attribute[access_atribute]
+               entry = variable_name[:attributes]
+               list = entry[,list]
+
+       The type attributes are:
+               s - String (default)
+               d - Decimal
+               x - Hexadecimal
+               b - Boolean ([1yYtT|0nNfF])
+               i - IP address
+               m - MAC address
+
+       The access attributes are:
+               a - Any (default)
+               r - Read-only
+               o - Write-once
+               c - Change-default
+
+       - CONFIG_ENV_FLAGS_LIST_DEFAULT
+               Define this to a list (string) to define the ".flags"
+               envirnoment variable in the default or embedded environment.
+
+       - CONFIG_ENV_FLAGS_LIST_STATIC
+               Define this to a list (string) to define validation that
+               should be done if an entry is not found in the ".flags"
+               environment variable.  To override a setting in the static
+               list, simply add an entry for the same variable name to the
+               ".flags" variable.
+
+- CONFIG_ENV_ACCESS_IGNORE_FORCE
+       If defined, don't allow the -f switch to env set override variable
+       access flags.
+
 The following definitions that deal with the placement and management
 of environment data (variable area); in general, we support the
 following configurations:
@@ -3294,6 +3505,16 @@ use the "saveenv" command to store a valid environment.
                space for already greatly restricted images, including but not
                limited to NAND_SPL configurations.
 
+- CONFIG_DISPLAY_BOARDINFO
+               Display information about the board that U-Boot is running on
+               when U-Boot starts up. The board function checkboard() is called
+               to do this.
+
+- CONFIG_DISPLAY_BOARDINFO_LATE
+               Similar to the previous option, but display this information
+               later, once stdio is running and output goes to the LCD, if
+               present.
+
 Low Level (hardware related) configuration options:
 ---------------------------------------------------
 
@@ -3610,12 +3831,26 @@ Low Level (hardware related) configuration options:
                that is executed before the actual U-Boot. E.g. when
                compiling a NAND SPL.
 
+- CONFIG_ARCH_MAP_SYSMEM
+               Generally U-Boot (and in particular the md command) uses
+               effective address. It is therefore not necessary to regard
+               U-Boot address as virtual addresses that need to be translated
+               to physical addresses. However, sandbox requires this, since
+               it maintains its own little RAM buffer which contains all
+               addressable memory. This option causes some memory accesses
+               to be mapped through map_sysmem() / unmap_sysmem().
+
 - CONFIG_USE_ARCH_MEMCPY
   CONFIG_USE_ARCH_MEMSET
                If these options are used a optimized version of memcpy/memset will
                be used if available. These functions may be faster under some
                conditions but may increase the binary size.
 
+- CONFIG_X86_RESET_VECTOR
+               If defined, the x86 reset vector code is included. This is not
+               needed when U-Boot is running from Coreboot.
+
+
 Freescale QE/FMAN Firmware Support:
 -----------------------------------
 
@@ -3843,6 +4078,7 @@ saveenv - save environment variables to persistent storage
 protect - enable or disable FLASH write protection
 erase  - erase FLASH memory
 flinfo - print FLASH memory information
+nand   - NAND memory operations (see doc/README.nand)
 bdinfo - print Board Info structure
 iminfo - print header information for application image
 coninfo - print console devices and informations
@@ -4109,6 +4345,36 @@ Please note that changes to some configuration parameters may take
 only effect after the next boot (yes, that's just like Windoze :-).
 
 
+Callback functions for environment variables:
+---------------------------------------------
+
+For some environment variables, the behavior of u-boot needs to change
+when their values are changed.  This functionailty allows functions to
+be associated with arbitrary variables.  On creation, overwrite, or
+deletion, the callback will provide the opportunity for some side
+effect to happen or for the change to be rejected.
+
+The callbacks are named and associated with a function using the
+U_BOOT_ENV_CALLBACK macro in your board or driver code.
+
+These callbacks are associated with variables in one of two ways.  The
+static list can be added to by defining CONFIG_ENV_CALLBACK_LIST_STATIC
+in the board configuration to a string that defines a list of
+associations.  The list must be in the following format:
+
+       entry = variable_name[:callback_name]
+       list = entry[,list]
+
+If the callback name is not specified, then the callback is deleted.
+Spaces are also allowed anywhere in the list.
+
+Callbacks can also be associated by defining the ".callbacks" variable
+with the same list format above.  Any association in ".callbacks" will
+override any association in the static list. You can define
+CONFIG_ENV_CALLBACK_LIST_DEFAULT to a list (string) to define the
+".callbacks" envirnoment variable in the default or embedded environment.
+
+
 Command Line Parsing:
 =====================