summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 803472b)
raw | patch | inline | side by side (parent: 803472b)
author | Minkyu Kang <mk7.kang@samsung.com> | |
Fri, 12 Feb 2010 09:17:52 +0000 (18:17 +0900) | ||
committer | trix <trix@windriver.com> | |
Sat, 13 Mar 2010 14:11:16 +0000 (08:11 -0600) |
This patch adds support the GPIO interface
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
cpu/arm_cortexa8/s5pc1xx/Makefile | patch | blob | history | |
cpu/arm_cortexa8/s5pc1xx/gpio.c | [new file with mode: 0644] | patch | blob |
include/asm-arm/arch-s5pc1xx/gpio.h | patch | blob | history |
index 4f922e686afeec24ef1e20da9f6516408c200046..7290c2f522378f78f829b5b5be22c1e079c3cb35 100644 (file)
COBJS += clock.o
COBJS += cpu_info.o
+COBJS += gpio.o
COBJS += timer.o
SRCS := $(SOBJS:.o=.S) $(COBJS:.o=.c)
diff --git a/cpu/arm_cortexa8/s5pc1xx/gpio.c b/cpu/arm_cortexa8/s5pc1xx/gpio.c
--- /dev/null
@@ -0,0 +1,143 @@
+/*
+ * (C) Copyright 2009 Samsung Electronics
+ * Minkyu Kang <mk7.kang@samsung.com>
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License as
+ * published by the Free Software Foundation; either version 2 of
+ * the License, or (at your option) any later version.
+ *
+ * This program is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
+ * GNU General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
+ * MA 02111-1307 USA
+ */
+
+#include <common.h>
+#include <asm/io.h>
+#include <asm/arch/gpio.h>
+
+#define CON_MASK(x) (0xf << ((x) << 2))
+#define CON_SFR(x, v) ((v) << ((x) << 2))
+
+#define DAT_MASK(x) (0x1 << (x))
+#define DAT_SET(x) (0x1 << (x))
+
+#define PULL_MASK(x) (0x3 << ((x) << 1))
+#define PULL_MODE(x, v) ((v) << ((x) << 1))
+
+#define DRV_MASK(x) (0x3 << ((x) << 1))
+#define DRV_SET(x, m) ((m) << ((x) << 1))
+#define RATE_MASK(x) (0x1 << (x + 16))
+#define RATE_SET(x) (0x1 << (x + 16))
+
+void gpio_cfg_pin(struct s5pc1xx_gpio_bank *bank, int gpio, int cfg)
+{
+ unsigned int value;
+
+ value = readl(&bank->con);
+ value &= ~CON_MASK(gpio);
+ value |= CON_SFR(gpio, cfg);
+ writel(value, &bank->con);
+}
+
+void gpio_direction_output(struct s5pc1xx_gpio_bank *bank, int gpio, int en)
+{
+ unsigned int value;
+
+ gpio_cfg_pin(bank, gpio, GPIO_OUTPUT);
+
+ value = readl(&bank->dat);
+ value &= ~DAT_MASK(gpio);
+ if (en)
+ value |= DAT_SET(gpio);
+ writel(value, &bank->dat);
+}
+
+void gpio_direction_input(struct s5pc1xx_gpio_bank *bank, int gpio)
+{
+ gpio_cfg_pin(bank, gpio, GPIO_INPUT);
+}
+
+void gpio_set_value(struct s5pc1xx_gpio_bank *bank, int gpio, int en)
+{
+ unsigned int value;
+
+ value = readl(&bank->dat);
+ value &= ~DAT_MASK(gpio);
+ if (en)
+ value |= DAT_SET(gpio);
+ writel(value, &bank->dat);
+}
+
+unsigned int gpio_get_value(struct s5pc1xx_gpio_bank *bank, int gpio)
+{
+ unsigned int value;
+
+ value = readl(&bank->dat);
+ return !!(value & DAT_MASK(gpio));
+}
+
+void gpio_set_pull(struct s5pc1xx_gpio_bank *bank, int gpio, int mode)
+{
+ unsigned int value;
+
+ value = readl(&bank->pull);
+ value &= ~PULL_MASK(gpio);
+
+ switch (mode) {
+ case GPIO_PULL_DOWN:
+ case GPIO_PULL_UP:
+ value |= PULL_MODE(gpio, mode);
+ break;
+ default:
+ return;
+ }
+
+ writel(value, &bank->pull);
+}
+
+void gpio_set_drv(struct s5pc1xx_gpio_bank *bank, int gpio, int mode)
+{
+ unsigned int value;
+
+ value = readl(&bank->drv);
+ value &= ~DRV_MASK(gpio);
+
+ switch (mode) {
+ case GPIO_DRV_1X:
+ case GPIO_DRV_2X:
+ case GPIO_DRV_3X:
+ case GPIO_DRV_4X:
+ value |= DRV_SET(gpio, mode);
+ break;
+ default:
+ return;
+ }
+
+ writel(value, &bank->drv);
+}
+
+void gpio_set_rate(struct s5pc1xx_gpio_bank *bank, int gpio, int mode)
+{
+ unsigned int value;
+
+ value = readl(&bank->drv);
+ value &= ~RATE_MASK(gpio);
+
+ switch (mode) {
+ case GPIO_DRV_FAST:
+ case GPIO_DRV_SLOW:
+ value |= RATE_SET(gpio);
+ break;
+ default:
+ return;
+ }
+
+ writel(value, &bank->drv);
+}
index afbc7ea5ae5a8d3d572621b56a1014cb93460953..8e4bb863f9cab9fc6b7b398953e17ccbbbf68bbc 100644 (file)
struct s5pc1xx_gpio_bank gpio_h2;
struct s5pc1xx_gpio_bank gpio_h3;
};
+
+/* functions */
+void gpio_cfg_pin(struct s5pc1xx_gpio_bank *bank, int gpio, int cfg);
+void gpio_direction_output(struct s5pc1xx_gpio_bank *bank, int gpio, int en);
+void gpio_direction_input(struct s5pc1xx_gpio_bank *bank, int gpio);
+void gpio_set_value(struct s5pc1xx_gpio_bank *bank, int gpio, int en);
+unsigned int gpio_get_value(struct s5pc1xx_gpio_bank *bank, int gpio);
+void gpio_set_pull(struct s5pc1xx_gpio_bank *bank, int gpio, int mode);
+void gpio_set_drv(struct s5pc1xx_gpio_bank *bank, int gpio, int mode);
+void gpio_set_rate(struct s5pc1xx_gpio_bank *bank, int gpio, int mode);
#endif
+/* Pin configurations */
+#define GPIO_INPUT 0x0
+#define GPIO_OUTPUT 0x1
+#define GPIO_IRQ 0xf
+#define GPIO_FUNC(x) (x)
+
+/* Pull mode */
+#define GPIO_PULL_NONE 0x0
+#define GPIO_PULL_DOWN 0x1
+#define GPIO_PULL_UP 0x2
+
+/* Drive Strength level */
+#define GPIO_DRV_1X 0x0
+#define GPIO_DRV_2X 0x1
+#define GPIO_DRV_3X 0x2
+#define GPIO_DRV_4X 0x3
+#define GPIO_DRV_FAST 0x0
+#define GPIO_DRV_SLOW 0x1
+
#endif