summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2c55123)
raw | patch | inline | side by side (parent: 2c55123)
author | Jagannadha Sutradharudu Teki <jaganna@xilinx.com> | |
Wed, 7 Aug 2013 12:36:55 +0000 (18:06 +0530) | ||
committer | Somnath Mukherjee <somnath@ti.com> | |
Thu, 8 Aug 2013 12:49:58 +0000 (18:19 +0530) |
This patch updated the spi_flash read func to support all
sizes of flashes using bank reg addr facility.
The same support has been added in below patch for erase/write
spi_flash functions:
"sf: Support all sizes of flashes using bank addr reg facility"
(sha1: c956f600cbb0943d0afe1004cdb503f4fcd8f415)
With these new updates on sf framework, the flashes which has < 16MB
are not effected as per as performance is concern and but the
u-boot.bin size incrased ~460 bytes.
sf update(for first 16MBytes), Changes before:
U-Boot> sf update 0x1000000 0x0 0x1000000
- N25Q256
16777216 bytes written, 0 bytes skipped in 199.72s, speed 86480 B/s
- W25Q128BV
16777216 bytes written, 0 bytes skipped in 351.739s, speed 48913 B/s
- S25FL256S_64K
16777216 bytes written, 0 bytes skipped in 65.659s, speed 262144 B/s
sf update(for first 16MBytes), Changes before:
U-Boot> sf update 0x1000000 0x0 0x1000000
- N25Q256
16777216 bytes written, 0 bytes skipped in 198.953s, speed 86480 B/s
- W25Q128BV
16777216 bytes written, 0 bytes skipped in 350.90s, speed 49200 B/s
- S25FL256S_64K
16777216 bytes written, 0 bytes skipped in 66.521s, speed 262144 B/s
Signed-off-by: Jagannadha Sutradharudu Teki <jaganna@xilinx.com>
Reviewed-by: Simon Glass <sjg@chromium.org>
sizes of flashes using bank reg addr facility.
The same support has been added in below patch for erase/write
spi_flash functions:
"sf: Support all sizes of flashes using bank addr reg facility"
(sha1: c956f600cbb0943d0afe1004cdb503f4fcd8f415)
With these new updates on sf framework, the flashes which has < 16MB
are not effected as per as performance is concern and but the
u-boot.bin size incrased ~460 bytes.
sf update(for first 16MBytes), Changes before:
U-Boot> sf update 0x1000000 0x0 0x1000000
- N25Q256
16777216 bytes written, 0 bytes skipped in 199.72s, speed 86480 B/s
- W25Q128BV
16777216 bytes written, 0 bytes skipped in 351.739s, speed 48913 B/s
- S25FL256S_64K
16777216 bytes written, 0 bytes skipped in 65.659s, speed 262144 B/s
sf update(for first 16MBytes), Changes before:
U-Boot> sf update 0x1000000 0x0 0x1000000
- N25Q256
16777216 bytes written, 0 bytes skipped in 198.953s, speed 86480 B/s
- W25Q128BV
16777216 bytes written, 0 bytes skipped in 350.90s, speed 49200 B/s
- S25FL256S_64K
16777216 bytes written, 0 bytes skipped in 66.521s, speed 262144 B/s
Signed-off-by: Jagannadha Sutradharudu Teki <jaganna@xilinx.com>
Reviewed-by: Simon Glass <sjg@chromium.org>
drivers/mtd/spi/spi_flash.c | patch | blob | history |
index 58b764120bfbfdfdf40153361092712c4a3c0f55..1fed2f7ac01e8f0b0d872f3195c02dc5dbf1fc27 100644 (file)
int spi_flash_cmd_read_fast(struct spi_flash *flash, u32 offset,
size_t len, void *data)
{
- u8 cmd[5];
+ u8 cmd[5], bank_sel;
+ u32 remain_len, read_len;
+ int ret = -1;
/* Handle memory-mapped SPI */
if (flash->memory_map)
memcpy(data, flash->memory_map + offset, len);
cmd[0] = CMD_READ_ARRAY_FAST;
- spi_flash_addr(offset, cmd);
cmd[4] = 0x00;
- return spi_flash_read_common(flash, cmd, sizeof(cmd), data, len);
+ while (len) {
+ bank_sel = offset / SPI_FLASH_16MB_BOUN;
+
+ ret = spi_flash_cmd_bankaddr_write(flash, bank_sel);
+ if (ret) {
+ debug("SF: fail to set bank%d\n", bank_sel);
+ return ret;
+ }
+
+ remain_len = (SPI_FLASH_16MB_BOUN * (bank_sel + 1) - offset);
+ if (len < remain_len)
+ read_len = len;
+ else
+ read_len = remain_len;
+
+ spi_flash_addr(offset, cmd);
+
+ ret = spi_flash_read_common(flash, cmd, sizeof(cmd),
+ data, read_len);
+ if (ret < 0) {
+ debug("SF: read failed\n");
+ break;
+ }
+
+ offset += read_len;
+ len -= read_len;
+ data += read_len;
+ }
+
+ return ret;
}
int spi_flash_cmd_poll_bit(struct spi_flash *flash, unsigned long timeout,