summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c3754e9)
raw | patch | inline | side by side (parent: c3754e9)
author | Ilya Yanok <ilya.yanok@cogentembedded.com> | |
Tue, 6 Nov 2012 13:06:34 +0000 (13:06 +0000) | ||
committer | Tom Rini <trini@ti.com> | |
Mon, 10 Dec 2012 15:54:02 +0000 (08:54 -0700) |
AM33XX with BCH8 can't work with nand_spl_simple correctly
because custom read_page implementation is required for proper
syndrome generation.
This simple driver mostly duplicates nand_spl_simple but has
nand_read_page changed to suit our needs.
Signed-off-by: Ilya Yanok <ilya.yanok@cogentembedded.com>
because custom read_page implementation is required for proper
syndrome generation.
This simple driver mostly duplicates nand_spl_simple but has
nand_read_page changed to suit our needs.
Signed-off-by: Ilya Yanok <ilya.yanok@cogentembedded.com>
drivers/mtd/nand/Makefile | patch | blob | history | |
drivers/mtd/nand/am335x_spl_bch.c | [new file with mode: 0644] | patch | blob |
index beb99cacb6636291e4c91a65f79710214e31cb35..5322f3a953c694dc350da9c2be43068a6e08b3d2 100644 (file)
ifdef CONFIG_SPL_NAND_SIMPLE
COBJS-y += nand_spl_simple.o
endif
+COBJS-$(CONFIG_SPL_NAND_AM33XX_BCH) += am335x_spl_bch.o
ifdef CONFIG_SPL_NAND_LOAD
COBJS-y += nand_spl_load.o
endif
diff --git a/drivers/mtd/nand/am335x_spl_bch.c b/drivers/mtd/nand/am335x_spl_bch.c
--- /dev/null
@@ -0,0 +1,238 @@
+/*
+ * (C) Copyright 2012
+ * Konstantin Kozhevnikov, Cogent Embedded
+ *
+ * based on nand_spl_simple code
+ *
+ * (C) Copyright 2006-2008
+ * Stefan Roese, DENX Software Engineering, sr@denx.de.
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License as
+ * published by the Free Software Foundation; either version 2 of
+ * the License, or (at your option) any later version.
+ *
+ * This program is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
+ * GNU General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc.
+ */
+
+#include <common.h>
+#include <nand.h>
+#include <asm/io.h>
+#include <linux/mtd/nand_ecc.h>
+
+static int nand_ecc_pos[] = CONFIG_SYS_NAND_ECCPOS;
+static nand_info_t mtd;
+static struct nand_chip nand_chip;
+
+#define ECCSTEPS (CONFIG_SYS_NAND_PAGE_SIZE / \
+ CONFIG_SYS_NAND_ECCSIZE)
+#define ECCTOTAL (ECCSTEPS * CONFIG_SYS_NAND_ECCBYTES)
+
+
+/*
+ * NAND command for large page NAND devices (2k)
+ */
+static int nand_command(int block, int page, uint32_t offs,
+ u8 cmd)
+{
+ struct nand_chip *this = mtd.priv;
+ int page_addr = page + block * CONFIG_SYS_NAND_PAGE_COUNT;
+ void (*hwctrl)(struct mtd_info *mtd, int cmd,
+ unsigned int ctrl) = this->cmd_ctrl;
+
+ while (!this->dev_ready(&mtd))
+ ;
+
+ /* Emulate NAND_CMD_READOOB */
+ if (cmd == NAND_CMD_READOOB) {
+ offs += CONFIG_SYS_NAND_PAGE_SIZE;
+ cmd = NAND_CMD_READ0;
+ }
+
+ /* Begin command latch cycle */
+ hwctrl(&mtd, cmd, NAND_CTRL_CLE | NAND_CTRL_CHANGE);
+
+ if (cmd == NAND_CMD_RESET) {
+ hwctrl(&mtd, NAND_CMD_NONE, NAND_NCE | NAND_CTRL_CHANGE);
+ while (!this->dev_ready(&mtd))
+ ;
+ return 0;
+ }
+
+ /* Shift the offset from byte addressing to word addressing. */
+ if (this->options & NAND_BUSWIDTH_16)
+ offs >>= 1;
+
+ /* Set ALE and clear CLE to start address cycle */
+ /* Column address */
+ hwctrl(&mtd, offs & 0xff,
+ NAND_CTRL_ALE | NAND_CTRL_CHANGE); /* A[7:0] */
+ hwctrl(&mtd, (offs >> 8) & 0xff, NAND_CTRL_ALE); /* A[11:9] */
+ /* Row address */
+ hwctrl(&mtd, (page_addr & 0xff), NAND_CTRL_ALE); /* A[19:12] */
+ hwctrl(&mtd, ((page_addr >> 8) & 0xff),
+ NAND_CTRL_ALE); /* A[27:20] */
+#ifdef CONFIG_SYS_NAND_5_ADDR_CYCLE
+ /* One more address cycle for devices > 128MiB */
+ hwctrl(&mtd, (page_addr >> 16) & 0x0f,
+ NAND_CTRL_ALE); /* A[31:28] */
+#endif
+ hwctrl(&mtd, NAND_CMD_NONE, NAND_NCE | NAND_CTRL_CHANGE);
+
+ if (cmd == NAND_CMD_READ0) {
+ /* Latch in address */
+ hwctrl(&mtd, NAND_CMD_READSTART,
+ NAND_CTRL_CLE | NAND_CTRL_CHANGE);
+ hwctrl(&mtd, NAND_CMD_NONE, NAND_NCE | NAND_CTRL_CHANGE);
+
+ /*
+ * Wait a while for the data to be ready
+ */
+ while (!this->dev_ready(&mtd))
+ ;
+ } else if (cmd == NAND_CMD_RNDOUT) {
+ hwctrl(&mtd, NAND_CMD_RNDOUTSTART, NAND_CTRL_CLE |
+ NAND_CTRL_CHANGE);
+ hwctrl(&mtd, NAND_CMD_NONE, NAND_NCE | NAND_CTRL_CHANGE);
+ }
+
+ return 0;
+}
+
+static int nand_is_bad_block(int block)
+{
+ struct nand_chip *this = mtd.priv;
+
+ nand_command(block, 0, CONFIG_SYS_NAND_BAD_BLOCK_POS,
+ NAND_CMD_READOOB);
+
+ /*
+ * Read one byte (or two if it's a 16 bit chip).
+ */
+ if (this->options & NAND_BUSWIDTH_16) {
+ if (readw(this->IO_ADDR_R) != 0xffff)
+ return 1;
+ } else {
+ if (readb(this->IO_ADDR_R) != 0xff)
+ return 1;
+ }
+
+ return 0;
+}
+
+static int nand_read_page(int block, int page, void *dst)
+{
+ struct nand_chip *this = mtd.priv;
+ u_char ecc_calc[ECCTOTAL];
+ u_char ecc_code[ECCTOTAL];
+ u_char oob_data[CONFIG_SYS_NAND_OOBSIZE];
+ int i;
+ int eccsize = CONFIG_SYS_NAND_ECCSIZE;
+ int eccbytes = CONFIG_SYS_NAND_ECCBYTES;
+ int eccsteps = ECCSTEPS;
+ uint8_t *p = dst;
+ uint32_t data_pos = 0;
+ uint8_t *oob = &oob_data[0] + nand_ecc_pos[0];
+ uint32_t oob_pos = eccsize * eccsteps + nand_ecc_pos[0];
+
+ nand_command(block, page, 0, NAND_CMD_READ0);
+
+ for (i = 0; eccsteps; eccsteps--, i += eccbytes, p += eccsize) {
+ this->ecc.hwctl(&mtd, NAND_ECC_READ);
+ nand_command(block, page, data_pos, NAND_CMD_RNDOUT);
+
+ this->read_buf(&mtd, p, eccsize);
+
+ nand_command(block, page, oob_pos, NAND_CMD_RNDOUT);
+
+ this->read_buf(&mtd, oob, eccbytes);
+ this->ecc.calculate(&mtd, p, &ecc_calc[i]);
+
+ data_pos += eccsize;
+ oob_pos += eccbytes;
+ oob += eccbytes;
+ }
+
+ /* Pick the ECC bytes out of the oob data */
+ for (i = 0; i < ECCTOTAL; i++)
+ ecc_code[i] = oob_data[nand_ecc_pos[i]];
+
+ eccsteps = ECCSTEPS;
+ p = dst;
+
+ for (i = 0 ; eccsteps; eccsteps--, i += eccbytes, p += eccsize) {
+ /* No chance to do something with the possible error message
+ * from correct_data(). We just hope that all possible errors
+ * are corrected by this routine.
+ */
+ this->ecc.correct(&mtd, p, &ecc_code[i], &ecc_calc[i]);
+ }
+
+ return 0;
+}
+
+int nand_spl_load_image(uint32_t offs, unsigned int size, void *dst)
+{
+ unsigned int block, lastblock;
+ unsigned int page;
+
+ /*
+ * offs has to be aligned to a page address!
+ */
+ block = offs / CONFIG_SYS_NAND_BLOCK_SIZE;
+ lastblock = (offs + size - 1) / CONFIG_SYS_NAND_BLOCK_SIZE;
+ page = (offs % CONFIG_SYS_NAND_BLOCK_SIZE) / CONFIG_SYS_NAND_PAGE_SIZE;
+
+ while (block <= lastblock) {
+ if (!nand_is_bad_block(block)) {
+ /*
+ * Skip bad blocks
+ */
+ while (page < CONFIG_SYS_NAND_PAGE_COUNT) {
+ nand_read_page(block, page, dst);
+ dst += CONFIG_SYS_NAND_PAGE_SIZE;
+ page++;
+ }
+
+ page = 0;
+ } else {
+ lastblock++;
+ }
+
+ block++;
+ }
+
+ return 0;
+}
+
+/* nand_init() - initialize data to make nand usable by SPL */
+void nand_init(void)
+{
+ /*
+ * Init board specific nand support
+ */
+ mtd.priv = &nand_chip;
+ nand_chip.IO_ADDR_R = nand_chip.IO_ADDR_W =
+ (void __iomem *)CONFIG_SYS_NAND_BASE;
+ board_nand_init(&nand_chip);
+
+ if (nand_chip.select_chip)
+ nand_chip.select_chip(&mtd, 0);
+
+ /* NAND chip may require reset after power-on */
+ nand_command(0, 0, 0, NAND_CMD_RESET);
+}
+
+/* Unselect after operation */
+void nand_deselect(void)
+{
+ if (nand_chip.select_chip)
+ nand_chip.select_chip(&mtd, -1);
+}