summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b4c5bbc)
raw | patch | inline | side by side (parent: b4c5bbc)
author | Taylor Hutt <thutt@chromium.org> | |
Mon, 29 Oct 2012 05:23:58 +0000 (05:23 +0000) | ||
committer | Tom Rini <trini@ti.com> | |
Fri, 2 Nov 2012 22:20:42 +0000 (15:20 -0700) |
Update the assignment of various physical memory buffers used by the
SATA controller to explicitly be denoted as physical addresses.
The memory is identity-mapped, so these function calls are a nop, but
they provide good semantic documentation for any maintainers.
The return value of virt_to_phys() is 'unsigned long'. On machines
where sizeof(unsigned long) != sizeof(pointer), a cast through
(uintptr_t) is needed to appease the compiler due to the potential of
losing the upper 32 bits of the address.
In compilation this scenario, a physical address could be 64-bits, yet
the C pointer environment only allows 32-bit addresses; the constraint
is that pointers cannot address more than 4Gb of memory and if
virt_to_phys() ever returns an out-of-range value for the physical
address, there are issues with emmory mapping which must be solved.
However, since the memory is identify mappeed, there is no problem
introducing the cast: the original pointer will reside in 32-bits, so
the physical address will also be within in 32-bits.
Signed-off-by: Taylor Hutt <thutt@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
SATA controller to explicitly be denoted as physical addresses.
The memory is identity-mapped, so these function calls are a nop, but
they provide good semantic documentation for any maintainers.
The return value of virt_to_phys() is 'unsigned long'. On machines
where sizeof(unsigned long) != sizeof(pointer), a cast through
(uintptr_t) is needed to appease the compiler due to the potential of
losing the upper 32 bits of the address.
In compilation this scenario, a physical address could be 64-bits, yet
the C pointer environment only allows 32-bit addresses; the constraint
is that pointers cannot address more than 4Gb of memory and if
virt_to_phys() ever returns an out-of-range value for the physical
address, there are issues with emmory mapping which must be solved.
However, since the memory is identify mappeed, there is no problem
introducing the cast: the original pointer will reside in 32-bits, so
the physical address will also be within in 32-bits.
Signed-off-by: Taylor Hutt <thutt@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
drivers/block/ahci.c | patch | blob | history |
diff --git a/drivers/block/ahci.c b/drivers/block/ahci.c
index 20c5336263536ae20ce611126841ec06f8e301dd..00de0868a3db6323759b060812a6862aa989b5a0 100644 (file)
--- a/drivers/block/ahci.c
+++ b/drivers/block/ahci.c
* First item in chunk of DMA memory: 32-slot command table,
* 32 bytes each in size
*/
- pp->cmd_slot = (struct ahci_cmd_hdr *)mem;
+ pp->cmd_slot =
+ (struct ahci_cmd_hdr *)(uintptr_t)virt_to_phys((void *)mem);
debug("cmd_slot = 0x%x\n", (unsigned)pp->cmd_slot);
mem += (AHCI_CMD_SLOT_SZ + 224);
/*
* Second item: Received-FIS area
*/
- pp->rx_fis = mem;
+ pp->rx_fis = virt_to_phys((void *)mem);
mem += AHCI_RX_FIS_SZ;
/*
* Third item: data area for storing a single command
* and its scatter-gather table
*/
- pp->cmd_tbl = mem;
+ pp->cmd_tbl = virt_to_phys((void *)mem);
debug("cmd_tbl_dma = 0x%x\n", pp->cmd_tbl);
mem += AHCI_CMD_TBL_HDR;
- pp->cmd_tbl_sg = (struct ahci_sg *)mem;
+ pp->cmd_tbl_sg =
+ (struct ahci_sg *)(uintptr_t)virt_to_phys((void *)mem);
writel_with_flush((u32) pp->cmd_slot, port_mmio + PORT_LST_ADDR);