]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/commitdiff
Merge branch 'master' of git://git.denx.de/u-boot-fdt
authorTom Rini <trini@ti.com>
Tue, 23 Oct 2012 02:54:48 +0000 (19:54 -0700)
committerTom Rini <trini@ti.com>
Tue, 23 Oct 2012 02:54:48 +0000 (19:54 -0700)
common/cmd_fdt.c
common/image.c
include/image.h
include/libfdt.h
lib/libfdt/Makefile
lib/libfdt/fdt_empty_tree.c [new file with mode: 0644]
lib/libfdt/fdt_rw.c

index e2225c4d5c64e188b50a2f9f205426dac11ba5df..a5e2cfcbfa8ede2fffd84d5ef1beb13e7f75ff8b 100644 (file)
@@ -35,6 +35,9 @@
 
 #define MAX_LEVEL      32              /* how deeply nested we will go */
 #define SCRATCHPAD     1024            /* bytes of scratchpad memory */
+#ifndef CONFIG_CMD_FDT_MAX_DUMP
+#define CONFIG_CMD_FDT_MAX_DUMP 64
+#endif
 
 /*
  * Global data (for the gd->bd)
@@ -44,6 +47,7 @@ DECLARE_GLOBAL_DATA_PTR;
 static int fdt_valid(void);
 static int fdt_parse_prop(char *const*newval, int count, char *data, int *len);
 static int fdt_print(const char *pathp, char *prop, int depth);
+static int is_printable_string(const void *data, int len);
 
 /*
  * The working_fdt points to our working flattened device tree.
@@ -60,6 +64,34 @@ void set_working_fdt_addr(void *addr)
        setenv("fdtaddr", buf);
 }
 
+/*
+ * Get a value from the fdt and format it to be set in the environment
+ */
+static int fdt_value_setenv(const void *nodep, int len, const char *var)
+{
+       if (is_printable_string(nodep, len))
+               setenv(var, (void *)nodep);
+       else if (len == 4) {
+               char buf[11];
+
+               sprintf(buf, "0x%08X", *(uint32_t *)nodep);
+               setenv(var, buf);
+       } else if (len%4 == 0 && len <= 20) {
+               /* Needed to print things like sha1 hashes. */
+               char buf[41];
+               int i;
+
+               for (i = 0; i < len; i += sizeof(unsigned int))
+                       sprintf(buf + (i * 2), "%08x",
+                               *(unsigned int *)(nodep + i));
+               setenv(var, buf);
+       } else {
+               printf("error: unprintable value\n");
+               return 1;
+       }
+       return 0;
+}
+
 /*
  * Flattened Device Tree command, see the help for parameter definitions.
  */
@@ -250,6 +282,117 @@ int do_fdt (cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[])
                        return 1;
                }
 
+       /********************************************************************
+        * Get the value of a property in the working_fdt.
+        ********************************************************************/
+       } else if (argv[1][0] == 'g') {
+               char *subcmd;           /* sub-command */
+               char *pathp;            /* path */
+               char *prop;             /* property */
+               char *var;              /* variable to store result */
+               int  nodeoffset;        /* node offset from libfdt */
+               const void *nodep;      /* property node pointer */
+               int  len = 0;           /* new length of the property */
+
+               /*
+                * Parameters: Node path, property, optional value.
+                */
+               if (argc < 5)
+                       return CMD_RET_USAGE;
+
+               subcmd = argv[2];
+
+               if (argc < 6 && subcmd[0] != 's')
+                       return CMD_RET_USAGE;
+
+               var    = argv[3];
+               pathp  = argv[4];
+               prop   = argv[5];
+
+               nodeoffset = fdt_path_offset(working_fdt, pathp);
+               if (nodeoffset < 0) {
+                       /*
+                        * Not found or something else bad happened.
+                        */
+                       printf("libfdt fdt_path_offset() returned %s\n",
+                               fdt_strerror(nodeoffset));
+                       return 1;
+               }
+
+               if (subcmd[0] == 'n' || (subcmd[0] == 's' && argc == 5)) {
+                       int reqIndex = -1;
+                       int startDepth = fdt_node_depth(
+                               working_fdt, nodeoffset);
+                       int curDepth = startDepth;
+                       int curIndex = -1;
+                       int nextNodeOffset = fdt_next_node(
+                               working_fdt, nodeoffset, &curDepth);
+
+                       if (subcmd[0] == 'n')
+                               reqIndex = simple_strtoul(argv[5], NULL, 16);
+
+                       while (curDepth > startDepth) {
+                               if (curDepth == startDepth + 1)
+                                       curIndex++;
+                               if (subcmd[0] == 'n' && curIndex == reqIndex) {
+                                       const char *nodeName = fdt_get_name(
+                                           working_fdt, nextNodeOffset, NULL);
+
+                                       setenv(var, (char *)nodeName);
+                                       return 0;
+                               }
+                               nextNodeOffset = fdt_next_node(
+                                       working_fdt, nextNodeOffset, &curDepth);
+                               if (nextNodeOffset < 0)
+                                       break;
+                       }
+                       if (subcmd[0] == 's') {
+                               /* get the num nodes at this level */
+                               char buf[11];
+
+                               sprintf(buf, "%d", curIndex + 1);
+                               setenv(var, buf);
+                       } else {
+                               /* node index not found */
+                               printf("libfdt node not found\n");
+                               return 1;
+                       }
+               } else {
+                       nodep = fdt_getprop(
+                               working_fdt, nodeoffset, prop, &len);
+                       if (len == 0) {
+                               /* no property value */
+                               setenv(var, "");
+                               return 0;
+                       } else if (len > 0) {
+                               if (subcmd[0] == 'v') {
+                                       int ret;
+
+                                       ret = fdt_value_setenv(nodep, len, var);
+                                       if (ret != 0)
+                                               return ret;
+                               } else if (subcmd[0] == 'a') {
+                                       /* Get address */
+                                       char buf[11];
+
+                                       sprintf(buf, "0x%08X", (uint32_t)nodep);
+                                       setenv(var, buf);
+                               } else if (subcmd[0] == 's') {
+                                       /* Get size */
+                                       char buf[11];
+
+                                       sprintf(buf, "0x%08X", len);
+                                       setenv(var, buf);
+                               } else
+                                       return CMD_RET_USAGE;
+                               return 0;
+                       } else {
+                               printf("libfdt fdt_getprop(): %s\n",
+                                       fdt_strerror(len));
+                               return 1;
+                       }
+               }
+
        /*
         * Print (recursive) / List (single level)
         */
@@ -611,12 +754,12 @@ static int is_printable_string(const void *data, int len)
        if (len == 0)
                return 0;
 
-       /* must terminate with zero */
-       if (s[len - 1] != '\0')
+       /* must terminate with zero or '\n' */
+       if (s[len - 1] != '\0' && s[len - 1] != '\n')
                return 0;
 
        /* printable or a null byte (concatenated strings) */
-       while (((*s == '\0') || isprint(*s)) && (len > 0)) {
+       while (((*s == '\0') || isprint(*s) || isspace(*s)) && (len > 0)) {
                /*
                 * If we see a null, there are three possibilities:
                 * 1) If len == 1, it is the end of the string, printable
@@ -672,19 +815,28 @@ static void print_data(const void *data, int len)
        }
 
        if ((len %4) == 0) {
-               const u32 *p;
-
-               printf("<");
-               for (j = 0, p = data; j < len/4; j ++)
-                       printf("0x%x%s", fdt32_to_cpu(p[j]), j < (len/4 - 1) ? " " : "");
-               printf(">");
+               if (len > CONFIG_CMD_FDT_MAX_DUMP)
+                       printf("* 0x%08x [0x%08x]", (unsigned int)data, len);
+               else {
+                       const u32 *p;
+
+                       printf("<");
+                       for (j = 0, p = data; j < len/4; j++)
+                               printf("0x%08x%s", fdt32_to_cpu(p[j]),
+                                       j < (len/4 - 1) ? " " : "");
+                       printf(">");
+               }
        } else { /* anything else... hexdump */
-               const u8 *s;
-
-               printf("[");
-               for (j = 0, s = data; j < len; j++)
-                       printf("%02x%s", s[j], j < len - 1 ? " " : "");
-               printf("]");
+               if (len > CONFIG_CMD_FDT_MAX_DUMP)
+                       printf("* 0x%08x [0x%08x]", (unsigned int)data, len);
+               else {
+                       const u8 *s;
+
+                       printf("[");
+                       for (j = 0, s = data; j < len; j++)
+                               printf("%02x%s", s[j], j < len - 1 ? " " : "");
+                       printf("]");
+               }
        }
 }
 
@@ -824,6 +976,10 @@ U_BOOT_CMD(
        "fdt resize                          - Resize fdt to size + padding to 4k addr\n"
        "fdt print  <path> [<prop>]          - Recursive print starting at <path>\n"
        "fdt list   <path> [<prop>]          - Print one level starting at <path>\n"
+       "fdt get value <var> <path> <prop>   - Get <property> and store in <var>\n"
+       "fdt get name <var> <path> <index>   - Get name of node <index> and store in <var>\n"
+       "fdt get addr <var> <path> <prop>    - Get start address of <property> and store in <var>\n"
+       "fdt get size <var> <path> [<prop>]  - Get size of [<property>] or num nodes and store in <var>\n"
        "fdt set    <path> <prop> [<val>]    - Set <property> [to <val>]\n"
        "fdt mknode <path> <node>            - Create a new node after <path>\n"
        "fdt rm     <path> [<prop>]          - Delete the node or <property>\n"
index f084d2baed3e0685937c6d4be3b73eb8e54add3a..750a98b6ba9e46880f222c7fc6796d4427241f0b 100644 (file)
@@ -2496,6 +2496,36 @@ int fit_image_hash_get_value(const void *fit, int noffset, uint8_t **value,
        return 0;
 }
 
+#ifndef USE_HOSTCC
+/**
+ * fit_image_hash_get_ignore - get hash ignore flag
+ * @fit: pointer to the FIT format image header
+ * @noffset: hash node offset
+ * @ignore: pointer to an int, will hold hash ignore flag
+ *
+ * fit_image_hash_get_ignore() finds hash ignore property in a given hash node.
+ * If the property is found and non-zero, the hash algorithm is not verified by
+ * u-boot automatically.
+ *
+ * returns:
+ *     0, on ignore not found
+ *     value, on ignore found
+ */
+int fit_image_hash_get_ignore(const void *fit, int noffset, int *ignore)
+{
+       int len;
+       int *value;
+
+       value = (int *)fdt_getprop(fit, noffset, FIT_IGNORE_PROP, &len);
+       if (value == NULL || len != sizeof(int))
+               *ignore = 0;
+       else
+               *ignore = *value;
+
+       return 0;
+}
+#endif
+
 /**
  * fit_set_timestamp - set node timestamp property
  * @fit: pointer to the FIT format image header
@@ -2759,6 +2789,9 @@ int fit_image_check_hashes(const void *fit, int image_noffset)
        char            *algo;
        uint8_t         *fit_value;
        int             fit_value_len;
+#ifndef USE_HOSTCC
+       int             ignore;
+#endif
        uint8_t         value[FIT_MAX_HASH_LEN];
        int             value_len;
        int             noffset;
@@ -2795,6 +2828,14 @@ int fit_image_check_hashes(const void *fit, int image_noffset)
                        }
                        printf("%s", algo);
 
+#ifndef USE_HOSTCC
+                       fit_image_hash_get_ignore(fit, noffset, &ignore);
+                       if (ignore) {
+                               printf("-skipped ");
+                               continue;
+                       }
+#endif
+
                        if (fit_image_hash_get_value(fit, noffset, &fit_value,
                                                        &fit_value_len)) {
                                err_msg = " error!\nCan't get hash value "
@@ -2820,6 +2861,11 @@ int fit_image_check_hashes(const void *fit, int image_noffset)
                }
        }
 
+       if (noffset == -FDT_ERR_TRUNCATED || noffset == -FDT_ERR_BADSTRUCTURE) {
+               err_msg = " error!\nCorrupted or truncated tree";
+               goto error;
+       }
+
        return 1;
 
 error:
index e5f6649291e24ccd524f67e211cd2bb63bf482a4..4e5863ff7fbd73fb6c22b981a2445f80b2213cc1 100644 (file)
@@ -511,6 +511,7 @@ static inline int image_check_target_arch(const image_header_t *hdr)
 #define FIT_HASH_NODENAME      "hash"
 #define FIT_ALGO_PROP          "algo"
 #define FIT_VALUE_PROP         "value"
+#define FIT_IGNORE_PROP                "uboot-ignore"
 
 /* image node */
 #define FIT_DATA_PROP          "data"
@@ -595,6 +596,9 @@ int fit_image_get_data(const void *fit, int noffset,
 int fit_image_hash_get_algo(const void *fit, int noffset, char **algo);
 int fit_image_hash_get_value(const void *fit, int noffset, uint8_t **value,
                                int *value_len);
+#ifndef USE_HOSTCC
+int fit_image_hash_get_ignore(const void *fit, int noffset, int *ignore);
+#endif
 
 int fit_set_timestamp(void *fit, int noffset, time_t timestamp);
 int fit_set_hashes(void *fit);
index de82ed5ffdf7f4d98049fbe60f544de96a1f0f40..c93ae28833e172c3bca7ee188da1c200f3eb27c5 100644 (file)
@@ -852,17 +852,17 @@ int fdt_setprop_inplace(void *fdt, int nodeoffset, const char *name,
                        const void *val, int len);
 
 /**
- * fdt_setprop_inplace_cell - change the value of a single-cell property
+ * fdt_setprop_inplace_u32 - change the value of a 32-bit integer property
  * @fdt: pointer to the device tree blob
  * @nodeoffset: offset of the node whose property to change
  * @name: name of the property to change
- * @val: cell (32-bit integer) value to replace the property with
+ * @val: 32-bit integer value to replace the property with
  *
- * fdt_setprop_inplace_cell() replaces the value of a given property
- * with the 32-bit integer cell value in val, converting val to
- * big-endian if necessary.  This function cannot change the size of a
- * property, and so will only work if the property already exists and
- * has length 4.
+ * fdt_setprop_inplace_u32() replaces the value of a given property
+ * with the 32-bit integer value in val, converting val to big-endian
+ * if necessary.  This function cannot change the size of a property,
+ * and so will only work if the property already exists and has length
+ * 4.
  *
  * This function will alter only the bytes in the blob which contain
  * the given property value, and will not alter or move any other part
@@ -871,7 +871,7 @@ int fdt_setprop_inplace(void *fdt, int nodeoffset, const char *name,
  * returns:
  *     0, on success
  *     -FDT_ERR_NOSPACE, if the property's length is not equal to 4
 *    -FDT_ERR_NOTFOUND, node does not have the named property
    -FDT_ERR_NOTFOUND, node does not have the named property
  *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
  *     -FDT_ERR_BADMAGIC,
  *     -FDT_ERR_BADVERSION,
@@ -879,13 +879,59 @@ int fdt_setprop_inplace(void *fdt, int nodeoffset, const char *name,
  *     -FDT_ERR_BADSTRUCTURE,
  *     -FDT_ERR_TRUNCATED, standard meanings
  */
-static inline int fdt_setprop_inplace_cell(void *fdt, int nodeoffset,
-                                          const char *name, uint32_t val)
+static inline int fdt_setprop_inplace_u32(void *fdt, int nodeoffset,
+                                         const char *name, uint32_t val)
 {
        val = cpu_to_fdt32(val);
        return fdt_setprop_inplace(fdt, nodeoffset, name, &val, sizeof(val));
 }
 
+/**
+ * fdt_setprop_inplace_u64 - change the value of a 64-bit integer property
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to change
+ * @val: 64-bit integer value to replace the property with
+ *
+ * fdt_setprop_inplace_u64() replaces the value of a given property
+ * with the 64-bit integer value in val, converting val to big-endian
+ * if necessary.  This function cannot change the size of a property,
+ * and so will only work if the property already exists and has length
+ * 8.
+ *
+ * This function will alter only the bytes in the blob which contain
+ * the given property value, and will not alter or move any other part
+ * of the tree.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, if the property's length is not equal to 8
+ *     -FDT_ERR_NOTFOUND, node does not have the named property
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+static inline int fdt_setprop_inplace_u64(void *fdt, int nodeoffset,
+                                         const char *name, uint64_t val)
+{
+       val = cpu_to_fdt64(val);
+       return fdt_setprop_inplace(fdt, nodeoffset, name, &val, sizeof(val));
+}
+
+/**
+ * fdt_setprop_inplace_cell - change the value of a single-cell property
+ *
+ * This is an alternative name for fdt_setprop_inplace_u32()
+ */
+static inline int fdt_setprop_inplace_cell(void *fdt, int nodeoffset,
+                                          const char *name, uint32_t val)
+{
+       return fdt_setprop_inplace_u32(fdt, nodeoffset, name, val);
+}
+
 /**
  * fdt_nop_property - replace a property with nop tags
  * @fdt: pointer to the device tree blob
@@ -945,11 +991,20 @@ int fdt_add_reservemap_entry(void *fdt, uint64_t addr, uint64_t size);
 int fdt_finish_reservemap(void *fdt);
 int fdt_begin_node(void *fdt, const char *name);
 int fdt_property(void *fdt, const char *name, const void *val, int len);
-static inline int fdt_property_cell(void *fdt, const char *name, uint32_t val)
+static inline int fdt_property_u32(void *fdt, const char *name, uint32_t val)
 {
        val = cpu_to_fdt32(val);
        return fdt_property(fdt, name, &val, sizeof(val));
 }
+static inline int fdt_property_u64(void *fdt, const char *name, uint64_t val)
+{
+       val = cpu_to_fdt64(val);
+       return fdt_property(fdt, name, &val, sizeof(val));
+}
+static inline int fdt_property_cell(void *fdt, const char *name, uint32_t val)
+{
+       return fdt_property_u32(fdt, name, val);
+}
 #define fdt_property_string(fdt, name, str) \
        fdt_property(fdt, name, str, strlen(str)+1)
 int fdt_end_node(void *fdt);
@@ -959,6 +1014,7 @@ int fdt_finish(void *fdt);
 /* Read-write functions                                               */
 /**********************************************************************/
 
+int fdt_create_empty_tree(void *buf, int bufsize);
 int fdt_open_into(const void *fdt, void *buf, int bufsize);
 int fdt_pack(void *fdt);
 
@@ -1068,14 +1124,14 @@ int fdt_setprop(void *fdt, int nodeoffset, const char *name,
                const void *val, int len);
 
 /**
- * fdt_setprop_cell - set a property to a single cell value
+ * fdt_setprop_u32 - set a property to a 32-bit integer
  * @fdt: pointer to the device tree blob
  * @nodeoffset: offset of the node whose property to change
  * @name: name of the property to change
  * @val: 32-bit integer value for the property (native endian)
  *
- * fdt_setprop_cell() sets the value of the named property in the
- * given node to the given cell value (converting to big-endian if
+ * fdt_setprop_u32() sets the value of the named property in the given
+ * node to the given 32-bit integer value (converting to big-endian if
  * necessary), or creates a new property with that value if it does
  * not already exist.
  *
@@ -1095,13 +1151,59 @@ int fdt_setprop(void *fdt, int nodeoffset, const char *name,
  *     -FDT_ERR_BADLAYOUT,
  *     -FDT_ERR_TRUNCATED, standard meanings
  */
-static inline int fdt_setprop_cell(void *fdt, int nodeoffset, const char *name,
-                                  uint32_t val)
+static inline int fdt_setprop_u32(void *fdt, int nodeoffset, const char *name,
+                                 uint32_t val)
 {
        val = cpu_to_fdt32(val);
        return fdt_setprop(fdt, nodeoffset, name, &val, sizeof(val));
 }
 
+/**
+ * fdt_setprop_u64 - set a property to a 64-bit integer
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to change
+ * @val: 64-bit integer value for the property (native endian)
+ *
+ * fdt_setprop_u64() sets the value of the named property in the given
+ * node to the given 64-bit integer value (converting to big-endian if
+ * necessary), or creates a new property with that value if it does
+ * not already exist.
+ *
+ * This function may insert or delete data from the blob, and will
+ * therefore change the offsets of some existing nodes.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, there is insufficient free space in the blob to
+ *             contain the new property value
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+static inline int fdt_setprop_u64(void *fdt, int nodeoffset, const char *name,
+                                 uint64_t val)
+{
+       val = cpu_to_fdt64(val);
+       return fdt_setprop(fdt, nodeoffset, name, &val, sizeof(val));
+}
+
+/**
+ * fdt_setprop_cell - set a property to a single cell value
+ *
+ * This is an alternative name for fdt_setprop_u32()
+ */
+static inline int fdt_setprop_cell(void *fdt, int nodeoffset, const char *name,
+                                  uint32_t val)
+{
+       return fdt_setprop_u32(fdt, nodeoffset, name, val);
+}
+
 /**
  * fdt_setprop_string - set a property to a string value
  * @fdt: pointer to the device tree blob
@@ -1133,6 +1235,147 @@ static inline int fdt_setprop_cell(void *fdt, int nodeoffset, const char *name,
 #define fdt_setprop_string(fdt, nodeoffset, name, str) \
        fdt_setprop((fdt), (nodeoffset), (name), (str), strlen(str)+1)
 
+/**
+ * fdt_appendprop - append to or create a property
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to append to
+ * @val: pointer to data to append to the property value
+ * @len: length of the data to append to the property value
+ *
+ * fdt_appendprop() appends the value to the named property in the
+ * given node, creating the property if it does not already exist.
+ *
+ * This function may insert data into the blob, and will therefore
+ * change the offsets of some existing nodes.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, there is insufficient free space in the blob to
+ *             contain the new property value
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+int fdt_appendprop(void *fdt, int nodeoffset, const char *name,
+                  const void *val, int len);
+
+/**
+ * fdt_appendprop_u32 - append a 32-bit integer value to a property
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to change
+ * @val: 32-bit integer value to append to the property (native endian)
+ *
+ * fdt_appendprop_u32() appends the given 32-bit integer value
+ * (converting to big-endian if necessary) to the value of the named
+ * property in the given node, or creates a new property with that
+ * value if it does not already exist.
+ *
+ * This function may insert data into the blob, and will therefore
+ * change the offsets of some existing nodes.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, there is insufficient free space in the blob to
+ *             contain the new property value
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+static inline int fdt_appendprop_u32(void *fdt, int nodeoffset,
+                                    const char *name, uint32_t val)
+{
+       val = cpu_to_fdt32(val);
+       return fdt_appendprop(fdt, nodeoffset, name, &val, sizeof(val));
+}
+
+/**
+ * fdt_appendprop_u64 - append a 64-bit integer value to a property
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to change
+ * @val: 64-bit integer value to append to the property (native endian)
+ *
+ * fdt_appendprop_u64() appends the given 64-bit integer value
+ * (converting to big-endian if necessary) to the value of the named
+ * property in the given node, or creates a new property with that
+ * value if it does not already exist.
+ *
+ * This function may insert data into the blob, and will therefore
+ * change the offsets of some existing nodes.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, there is insufficient free space in the blob to
+ *             contain the new property value
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+static inline int fdt_appendprop_u64(void *fdt, int nodeoffset,
+                                    const char *name, uint64_t val)
+{
+       val = cpu_to_fdt64(val);
+       return fdt_appendprop(fdt, nodeoffset, name, &val, sizeof(val));
+}
+
+/**
+ * fdt_appendprop_cell - append a single cell value to a property
+ *
+ * This is an alternative name for fdt_appendprop_u32()
+ */
+static inline int fdt_appendprop_cell(void *fdt, int nodeoffset,
+                                     const char *name, uint32_t val)
+{
+       return fdt_appendprop_u32(fdt, nodeoffset, name, val);
+}
+
+/**
+ * fdt_appendprop_string - append a string to a property
+ * @fdt: pointer to the device tree blob
+ * @nodeoffset: offset of the node whose property to change
+ * @name: name of the property to change
+ * @str: string value to append to the property
+ *
+ * fdt_appendprop_string() appends the given string to the value of
+ * the named property in the given node, or creates a new property
+ * with that value if it does not already exist.
+ *
+ * This function may insert data into the blob, and will therefore
+ * change the offsets of some existing nodes.
+ *
+ * returns:
+ *     0, on success
+ *     -FDT_ERR_NOSPACE, there is insufficient free space in the blob to
+ *             contain the new property value
+ *     -FDT_ERR_BADOFFSET, nodeoffset did not point to FDT_BEGIN_NODE tag
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_BADMAGIC,
+ *     -FDT_ERR_BADVERSION,
+ *     -FDT_ERR_BADSTATE,
+ *     -FDT_ERR_BADSTRUCTURE,
+ *     -FDT_ERR_BADLAYOUT,
+ *     -FDT_ERR_TRUNCATED, standard meanings
+ */
+#define fdt_appendprop_string(fdt, nodeoffset, name, str) \
+       fdt_appendprop((fdt), (nodeoffset), (name), (str), strlen(str)+1)
+
 /**
  * fdt_delprop - delete a property
  * @fdt: pointer to the device tree blob
index c965577dc093e7a21325b9e37b74ab9ebdb7645e..0693d4bf5585541d85e9f173d5e8aa2e16d95162 100644 (file)
@@ -27,7 +27,7 @@ LIB   = $(obj)libfdt.o
 
 SOBJS  =
 
-COBJS-libfdt += fdt.o fdt_ro.o fdt_rw.o fdt_strerror.o fdt_sw.o fdt_wip.o
+COBJS-libfdt += fdt.o fdt_ro.o fdt_rw.o fdt_strerror.o fdt_sw.o fdt_wip.o fdt_empty_tree.o
 
 COBJS-$(CONFIG_OF_LIBFDT) += $(COBJS-libfdt)
 COBJS-$(CONFIG_FIT) += $(COBJS-libfdt)
diff --git a/lib/libfdt/fdt_empty_tree.c b/lib/libfdt/fdt_empty_tree.c
new file mode 100644 (file)
index 0000000..f72d13b
--- /dev/null
@@ -0,0 +1,84 @@
+/*
+ * libfdt - Flat Device Tree manipulation
+ * Copyright (C) 2012 David Gibson, IBM Corporation.
+ *
+ * libfdt is dual licensed: you can use it either under the terms of
+ * the GPL, or the BSD license, at your option.
+ *
+ *  a) This library is free software; you can redistribute it and/or
+ *     modify it under the terms of the GNU General Public License as
+ *     published by the Free Software Foundation; either version 2 of the
+ *     License, or (at your option) any later version.
+ *
+ *     This library is distributed in the hope that it will be useful,
+ *     but WITHOUT ANY WARRANTY; without even the implied warranty of
+ *     MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
+ *     GNU General Public License for more details.
+ *
+ *     You should have received a copy of the GNU General Public
+ *     License along with this library; if not, write to the Free
+ *     Software Foundation, Inc., 51 Franklin St, Fifth Floor, Boston,
+ *     MA 02110-1301 USA
+ *
+ * Alternatively,
+ *
+ *  b) Redistribution and use in source and binary forms, with or
+ *     without modification, are permitted provided that the following
+ *     conditions are met:
+ *
+ *     1. Redistributions of source code must retain the above
+ *        copyright notice, this list of conditions and the following
+ *        disclaimer.
+ *     2. Redistributions in binary form must reproduce the above
+ *        copyright notice, this list of conditions and the following
+ *        disclaimer in the documentation and/or other materials
+ *        provided with the distribution.
+ *
+ *     THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND
+ *     CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES,
+ *     INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF
+ *     MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
+ *     DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
+ *     CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
+ *     SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT
+ *     NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
+ *     LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
+ *     HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
+ *     CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
+ *     OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
+ *     EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+ */
+#include "libfdt_env.h"
+
+#include <fdt.h>
+#include <libfdt.h>
+
+#include "libfdt_internal.h"
+
+int fdt_create_empty_tree(void *buf, int bufsize)
+{
+       int err;
+
+       err = fdt_create(buf, bufsize);
+       if (err)
+               return err;
+
+       err = fdt_finish_reservemap(buf);
+       if (err)
+               return err;
+
+       err = fdt_begin_node(buf, "");
+       if (err)
+               return err;
+
+       err =  fdt_end_node(buf);
+       if (err)
+               return err;
+
+       err = fdt_finish(buf);
+       if (err)
+               return err;
+
+       return fdt_open_into(buf, buf, bufsize);
+}
+
index 5c27a677e3536ed7320ee399113666975e5d545b..5ed23d6f1934699540b60cb437f0c740dc43956c 100644 (file)
@@ -293,6 +293,33 @@ int fdt_setprop(void *fdt, int nodeoffset, const char *name,
        return 0;
 }
 
+int fdt_appendprop(void *fdt, int nodeoffset, const char *name,
+                  const void *val, int len)
+{
+       struct fdt_property *prop;
+       int err, oldlen, newlen;
+
+       FDT_RW_CHECK_HEADER(fdt);
+
+       prop = fdt_get_property_w(fdt, nodeoffset, name, &oldlen);
+       if (prop) {
+               newlen = len + oldlen;
+               err = _fdt_splice_struct(fdt, prop->data,
+                                        FDT_TAGALIGN(oldlen),
+                                        FDT_TAGALIGN(newlen));
+               if (err)
+                       return err;
+               prop->len = cpu_to_fdt32(newlen);
+               memcpy(prop->data + oldlen, val, len);
+       } else {
+               err = _fdt_add_property(fdt, nodeoffset, name, len, &prop);
+               if (err)
+                       return err;
+               memcpy(prop->data, val, len);
+       }
+       return 0;
+}
+
 int fdt_delprop(void *fdt, int nodeoffset, const char *name)
 {
        struct fdt_property *prop;