author | Tom Rini <trini@ti.com> | |
Mon, 11 Mar 2013 16:02:40 +0000 (12:02 -0400) | ||
committer | Tom Rini <trini@ti.com> | |
Mon, 11 Mar 2013 16:16:13 +0000 (12:16 -0400) |
In master we had already taken a patch to fix the davinci GPIO code for
CONFIG_SOC_DM646X and in u-boot-ti we have additional patches to support
DA830 (which is CONFIG_SOC_DA8XX && !CONFIG_SOC_DA850). Resolve these
conflicts manually and comment the #else/#endif lines for clarity.
Conflicts:
arch/arm/include/asm/arch-davinci/gpio.h
drivers/gpio/da8xx_gpio.c
Signed-off-by: Tom Rini <trini@ti.com>
CONFIG_SOC_DM646X and in u-boot-ti we have additional patches to support
DA830 (which is CONFIG_SOC_DA8XX && !CONFIG_SOC_DA850). Resolve these
conflicts manually and comment the #else/#endif lines for clarity.
Conflicts:
arch/arm/include/asm/arch-davinci/gpio.h
drivers/gpio/da8xx_gpio.c
Signed-off-by: Tom Rini <trini@ti.com>
1 | 2 | |||
---|---|---|---|---|
MAINTAINERS | patch | | diff1 | | diff2 | | blob | history |
README | patch | | diff1 | | diff2 | | blob | history |
arch/arm/include/asm/arch-davinci/gpio.h | patch | | diff1 | | diff2 | | blob | history |
board/technexion/twister/twister.c | patch | | diff1 | | diff2 | | blob | history |
board/timll/devkit8000/devkit8000.c | patch | | diff1 | | diff2 | | blob | history |
boards.cfg | patch | | diff1 | | diff2 | | blob | history |
drivers/gpio/da8xx_gpio.c | patch | | diff1 | | diff2 | | blob | history |
drivers/mmc/bfin_sdh.c | patch | | diff1 | | diff2 | | blob | history |
include/configs/ea20.h | patch | | diff1 | | diff2 | | blob | history |
diff --combined MAINTAINERS
index 175bbe26669c38096240483e9c072d2b99c06206,8603085f3042db4075f6c9e27ebb888096a42a66..e792a8b4f6557ffcc9595d2e215199b1775161f8
--- 1/MAINTAINERS
--- 2/MAINTAINERS
+++ b/MAINTAINERS
igep0020 ARM ARMV7 (OMAP3xx SoC)
igep0030 ARM ARMV7 (OMAP3xx SoC)
+ igep0032 ARM ARMV7 (OMAP3xx SoC)
Eric Benard <eric@eukrea.com>
# Board CPU #
#########################################################################
- Mike Frysinger <vapier@gentoo.org>
+ Sonic Zhang <sonic.adi@gmail.com>
Blackfin Team <u-boot-devel@blackfin.uclinux.org>
BF506F-EZKIT BF506
BF538F-EZKIT BF538
BF548-EZKIT BF548
BF561-EZKIT BF561
+ BF609-EZKIT BF609
M.Hasewinkel (MHA) <info@ssv-embedded.de>
diff --combined README
index 398d70d67c2ff6b24e7d927b84b80202a7e13743,42544cead64ef8d45dbd8834de1c36d5f292ed5a..d51ece946c309a37fa3fcf5c1d91f0174e2b016f
+++ b/README
CONFIG_CMD_I2C * I2C serial bus support
CONFIG_CMD_IDE * IDE harddisk support
CONFIG_CMD_IMI iminfo
- CONFIG_CMD_IMLS List all found images
+ CONFIG_CMD_IMLS List all images found in NOR flash
+ CONFIG_CMD_IMLS_NAND List all images found in NAND flash
CONFIG_CMD_IMMAP * IMMR dump support
CONFIG_CMD_IMPORTENV * import an environment
CONFIG_CMD_INI * import data from an ini file into the env
CONFIG_CMD_READ * Read raw data from partition
CONFIG_CMD_REGINFO * Register dump
CONFIG_CMD_RUN run command in env variable
+ CONFIG_CMD_SANDBOX * sb command to access sandbox features
CONFIG_CMD_SAVES * save S record dump
CONFIG_CMD_SCSI * SCSI Support
CONFIG_CMD_SDRAM * print SDRAM configuration information
allows for a "silent" boot where a splash screen is
loaded very quickly after power-on.
+ CONFIG_SPLASHIMAGE_GUARD
+
+ If this option is set, then U-Boot will prevent the environment
+ variable "splashimage" from being set to a problematic address
+ (see README.displaying-bmps and README.arm-unaligned-accesses).
+ This option is useful for targets where, due to alignment
+ restrictions, an improperly aligned BMP image will cause a data
+ abort. If you think you will not have problems with unaligned
+ accesses (for example because your toolchain prevents them)
+ there is no need to set this option.
+
CONFIG_SPLASH_SCREEN_ALIGN
If this option is set the splash image can be freely positioned
=> vertically centered image
at x = dspWidth - bmpWidth - 9
+ CONFIG_SPLASH_SCREEN_PREPARE
+
+ If this option is set then the board_splash_screen_prepare()
+ function, which must be defined in your code, is called as part
+ of the splash screen display sequence. It gives the board an
+ opportunity to prepare the splash image data before it is
+ processed and sent to the frame buffer by U-Boot.
+
- Gzip compressed BMP image support: CONFIG_VIDEO_BMP_GZIP
If this option is set, additionally to standard BMP
that is executed before the actual U-Boot. E.g. when
compiling a NAND SPL.
+ - CONFIG_ARCH_MAP_SYSMEM
+ Generally U-Boot (and in particular the md command) uses
+ effective address. It is therefore not necessary to regard
+ U-Boot address as virtual addresses that need to be translated
+ to physical addresses. However, sandbox requires this, since
+ it maintains its own little RAM buffer which contains all
+ addressable memory. This option causes some memory accesses
+ to be mapped through map_sysmem() / unmap_sysmem().
+
- CONFIG_USE_ARCH_MEMCPY
CONFIG_USE_ARCH_MEMSET
If these options are used a optimized version of memcpy/memset will
diff --combined arch/arm/include/asm/arch-davinci/gpio.h
index fbbb1f33c3c9427b9710ad6aa1142e70261476d7,5206b122114e1eeb02f22d4cc855355fd8624ef1..06390c85e1092de192bf0b049927d5cebab76f77
#define davinci_gpio_bank67 ((struct davinci_gpio *)DAVINCI_GPIO_BANK67)
#define davinci_gpio_bank8 ((struct davinci_gpio *)DAVINCI_GPIO_BANK8)
- #if defined(CONFIG_SOC_DA8XX) && !defined(CONFIG_SOC_DA850)
+#define gpio_status() gpio_info()
+#define GPIO_NAME_SIZE 20
+ #if defined(CONFIG_SOC_DM644X)
+ /* GPIO0 to GPIO53, omit the V3.3 volts one */
+ #define MAX_NUM_GPIOS 70
++#elif defined(CONFIG_SOC_DA8XX) && !defined(CONFIG_SOC_DA850)
+#define MAX_NUM_GPIOS 128
#else
#define MAX_NUM_GPIOS 144
#endif
-
-#define gpio_status() gpio_info()
-#define GPIO_NAME_SIZE 20
#define GPIO_BANK(gp) (davinci_gpio_bank01 + ((gp) >> 5))
#define GPIO_BIT(gp) ((gp) & 0x1F)
diff --combined board/technexion/twister/twister.c
index 5f197a746af851403e1d775c191ab398c80e1da3,fa0ace019ae9051af82c6ca13059852cfc563364..a28c7043f926b429c7a78cc4c8c55ecaa02e57b2
!defined(CONFIG_SPL_BUILD)
int board_mmc_init(bd_t *bis)
{
- return omap_mmc_init(0, 0, 0);
+ return omap_mmc_init(0, 0, 0, -1, -1);
}
#endif
int spl_start_uboot(void)
{
int val = 0;
- if (!gpio_request(CONFIG_SPL_OS_BOOT_KEY, "U-Boot key")) {
- gpio_direction_input(CONFIG_SPL_OS_BOOT_KEY);
- val = gpio_get_value(CONFIG_SPL_OS_BOOT_KEY);
- gpio_free(CONFIG_SPL_OS_BOOT_KEY);
+ if (!gpio_request(SPL_OS_BOOT_KEY, "U-Boot key")) {
+ gpio_direction_input(SPL_OS_BOOT_KEY);
+ val = gpio_get_value(SPL_OS_BOOT_KEY);
+ gpio_free(SPL_OS_BOOT_KEY);
}
return val;
}
diff --combined board/timll/devkit8000/devkit8000.c
index 22b3fac398433d292f560e53f641bc5a1f0028d0,b88d9783cb627b91fcc52739588e3a0ecdfeecbd..ebff59e70b38b3d7cc595d98ab31100bd7061238
#if defined(CONFIG_GENERIC_MMC) && !defined(CONFIG_SPL_BUILD)
int board_mmc_init(bd_t *bis)
{
- omap_mmc_init(0, 0, 0);
- return 0;
+ return omap_mmc_init(0, 0, 0, -1, -1);
}
#endif
int spl_start_uboot(void)
{
int val = 0;
- if (!gpio_request(CONFIG_SPL_OS_BOOT_KEY, "U-Boot key")) {
- gpio_direction_input(CONFIG_SPL_OS_BOOT_KEY);
- val = gpio_get_value(CONFIG_SPL_OS_BOOT_KEY);
- gpio_free(CONFIG_SPL_OS_BOOT_KEY);
+ if (!gpio_request(SPL_OS_BOOT_KEY, "U-Boot key")) {
+ gpio_direction_input(SPL_OS_BOOT_KEY);
+ val = gpio_get_value(SPL_OS_BOOT_KEY);
+ gpio_free(SPL_OS_BOOT_KEY);
}
return !val;
}
diff --combined boards.cfg
index efe137d8b0758930770fe37a93e96f528c3b1e8e,136ea0ae293736929153c2191371701f74569b8e..198cc5ce8483ea33e3a1712a301516e815472de4
--- 1/boards.cfg
--- 2/boards.cfg
+++ b/boards.cfg
integratorcp_cm946es arm arm946es integrator armltd - integratorcp:CM946ES
ca9x4_ct_vxp arm armv7 vexpress armltd
am335x_evm arm armv7 am335x ti am33xx am335x_evm:SERIAL1,CONS_INDEX=1
+am335x_evm_spiboot arm armv7 am335x ti am33xx am335x_evm:SERIAL1,CONS_INDEX=1,SPI_BOOT
am335x_evm_uart1 arm armv7 am335x ti am33xx am335x_evm:SERIAL2,CONS_INDEX=2
am335x_evm_uart2 arm armv7 am335x ti am33xx am335x_evm:SERIAL3,CONS_INDEX=3
am335x_evm_uart3 arm armv7 am335x ti am33xx am335x_evm:SERIAL4,CONS_INDEX=4
am335x_evm_uart4 arm armv7 am335x ti am33xx am335x_evm:SERIAL5,CONS_INDEX=5
am335x_evm_uart5 arm armv7 am335x ti am33xx am335x_evm:SERIAL6,CONS_INDEX=6
+am335x_evm_usbspl arm armv7 am335x ti am33xx am335x_evm:SERIAL1,CONS_INDEX=1,SPL_USBETH_SUPPORT
pcm051 arm armv7 pcm051 phytec am33xx pcm051
highbank arm armv7 highbank - highbank
mx51_efikamx arm armv7 mx51_efikamx genesi mx5 mx51_efikamx:MACH_TYPE=MACH_TYPE_MX51_EFIKAMX,IMX_CONFIG=board/genesi/mx51_efikamx/imximage_mx.cfg
igep0020_nand arm armv7 igep00x0 isee omap3 igep00x0:MACH_TYPE=MACH_TYPE_IGEP0020,BOOT_NAND
igep0030 arm armv7 igep00x0 isee omap3 igep00x0:MACH_TYPE=MACH_TYPE_IGEP0030,BOOT_ONENAND
igep0030_nand arm armv7 igep00x0 isee omap3 igep00x0:MACH_TYPE=MACH_TYPE_IGEP0030,BOOT_NAND
+igep0032 arm armv7 igep00x0 isee omap3 igep00x0:MACH_TYPE=MACH_TYPE_IGEP0032,BOOT_ONENAND
am3517_evm arm armv7 am3517evm logicpd omap3
mt_ventoux arm armv7 mt_ventoux teejet omap3
omap3_zoom1 arm armv7 zoom1 logicpd omap3
omap4_panda arm armv7 panda ti omap4
omap4_sdp4430 arm armv7 sdp4430 ti omap4
omap5_evm arm armv7 omap5_evm ti omap5
+dra7xx_evm arm armv7 dra7xx ti omap5
s5p_goni arm armv7 goni samsung s5pc1xx
smdkc100 arm armv7 smdkc100 samsung s5pc1xx
origen arm armv7 origen samsung exynos
kzm9g arm armv7 kzm9g kmc rmobile
armadillo-800eva arm armv7 armadillo-800eva atmark-techno rmobile
zynq arm armv7 zynq xilinx zynq
+zynq_dcc arm armv7 zynq xilinx zynq zynq:ZYNQ_DCC
socfpga_cyclone5 arm armv7 socfpga_cyclone5 altera socfpga
actux1_4_16 arm ixp actux1 - - actux1:FLASH2X2
actux1_4_32 arm ixp actux1 - - actux1:FLASH2X2,RAM_32MB
bf548-ezkit blackfin blackfin
bf561-acvilon blackfin blackfin
bf561-ezkit blackfin blackfin
+ bf609-ezkit blackfin blackfin
blackstamp blackfin blackfin
blackvme blackfin blackfin
br4 blackfin blackfin
TQM834x powerpc mpc83xx tqm834x tqc
suvd3 powerpc mpc83xx km83xx keymile - suvd3:SUVD3
kmvect1 powerpc mpc83xx km83xx keymile - suvd3:KMVECT1
- tuge1 powerpc mpc83xx km83xx keymile - tuxx1:KM_DISABLE_APP2,TUGE1
- tuxx1 powerpc mpc83xx km83xx keymile
- kmsupx5 powerpc mpc83xx km83xx keymile - tuxx1:KM_DISABLE_APP2,KMSUPX5
+ tuge1 powerpc mpc83xx km83xx keymile - tuxx1:TUGE1
+ tuxx1 powerpc mpc83xx km83xx keymile - tuxx1:TUXX1
+ kmopti2 powerpc mpc83xx km83xx keymile - tuxx1:KMOPTI2
+ kmsupx5 powerpc mpc83xx km83xx keymile - tuxx1:KMSUPX5
sbc8548 powerpc mpc85xx sbc8548 - - sbc8548
sbc8548_PCI_33 powerpc mpc85xx sbc8548 - - sbc8548:PCI,33
sbc8548_PCI_33_PCIE powerpc mpc85xx sbc8548 - - sbc8548:PCI,33,PCIE
diff --combined drivers/gpio/da8xx_gpio.c
index 271b8d93f4352b1471e938169e00940ef84884c1,ed6a1180d469b0c6387653056fbccf8164c2a0ef..76648d27d426bc9e644378312e010d10629e329d
char name[GPIO_NAME_SIZE];
} gpio_registry[MAX_NUM_GPIOS];
+ #if defined(CONFIG_SOC_DA8XX)
#define pinmux(x) (&davinci_syscfg_regs->pinmux[x])
- #else
+#if defined(CONFIG_SOC_DA8XX) && !defined(CONFIG_SOC_DA850)
+static const struct pinmux_config gpio_pinmux[] = {
+ { pinmux(13), 8, 6 }, /* GP0[0] */
+ { pinmux(13), 8, 7 },
+ { pinmux(14), 8, 0 },
+ { pinmux(14), 8, 1 },
+ { pinmux(14), 8, 2 },
+ { pinmux(14), 8, 3 },
+ { pinmux(14), 8, 4 },
+ { pinmux(14), 8, 5 },
+ { pinmux(14), 8, 6 },
+ { pinmux(14), 8, 7 },
+ { pinmux(15), 8, 0 },
+ { pinmux(15), 8, 1 },
+ { pinmux(15), 8, 2 },
+ { pinmux(15), 8, 3 },
+ { pinmux(15), 8, 4 },
+ { pinmux(15), 8, 5 },
+ { pinmux(15), 8, 6 }, /* GP1[0] */
+ { pinmux(15), 8, 7 },
+ { pinmux(16), 8, 0 },
+ { pinmux(16), 8, 1 },
+ { pinmux(16), 8, 2 },
+ { pinmux(16), 8, 3 },
+ { pinmux(16), 8, 4 },
+ { pinmux(16), 8, 5 },
+ { pinmux(16), 8, 6 },
+ { pinmux(16), 8, 7 },
+ { pinmux(17), 8, 0 },
+ { pinmux(17), 8, 1 },
+ { pinmux(17), 8, 2 },
+ { pinmux(17), 8, 3 },
+ { pinmux(17), 8, 4 },
+ { pinmux(17), 8, 5 },
+ { pinmux(17), 8, 6 }, /* GP2[0] */
+ { pinmux(17), 8, 7 },
+ { pinmux(18), 8, 0 },
+ { pinmux(18), 8, 1 },
+ { pinmux(18), 8, 2 },
+ { pinmux(18), 8, 3 },
+ { pinmux(18), 8, 4 },
+ { pinmux(18), 8, 5 },
+ { pinmux(18), 8, 6 },
+ { pinmux(18), 8, 7 },
+ { pinmux(19), 8, 0 },
+ { pinmux(9), 8, 2 },
+ { pinmux(9), 8, 3 },
+ { pinmux(9), 8, 4 },
+ { pinmux(9), 8, 5 },
+ { pinmux(9), 8, 6 },
+ { pinmux(10), 8, 1 }, /* GP3[0] */
+ { pinmux(10), 8, 2 },
+ { pinmux(10), 8, 3 },
+ { pinmux(10), 8, 4 },
+ { pinmux(10), 8, 5 },
+ { pinmux(10), 8, 6 },
+ { pinmux(10), 8, 7 },
+ { pinmux(11), 8, 0 },
+ { pinmux(11), 8, 1 },
+ { pinmux(11), 8, 2 },
+ { pinmux(11), 8, 3 },
+ { pinmux(11), 8, 4 },
+ { pinmux(9), 8, 7 },
+ { pinmux(2), 8, 6 },
+ { pinmux(11), 8, 5 },
+ { pinmux(11), 8, 6 },
+ { pinmux(12), 8, 4 }, /* GP4[0] */
+ { pinmux(12), 8, 5 },
+ { pinmux(12), 8, 6 },
+ { pinmux(12), 8, 7 },
+ { pinmux(13), 8, 0 },
+ { pinmux(13), 8, 1 },
+ { pinmux(13), 8, 2 },
+ { pinmux(13), 8, 3 },
+ { pinmux(13), 8, 4 },
+ { pinmux(13), 8, 5 },
+ { pinmux(11), 8, 7 },
+ { pinmux(12), 8, 0 },
+ { pinmux(12), 8, 1 },
+ { pinmux(12), 8, 2 },
+ { pinmux(12), 8, 3 },
+ { pinmux(9), 8, 1 },
+ { pinmux(7), 8, 3 }, /* GP5[0] */
+ { pinmux(7), 8, 4 },
+ { pinmux(7), 8, 5 },
+ { pinmux(7), 8, 6 },
+ { pinmux(7), 8, 7 },
+ { pinmux(8), 8, 0 },
+ { pinmux(8), 8, 1 },
+ { pinmux(8), 8, 2 },
+ { pinmux(8), 8, 3 },
+ { pinmux(8), 8, 4 },
+ { pinmux(8), 8, 5 },
+ { pinmux(8), 8, 6 },
+ { pinmux(8), 8, 7 },
+ { pinmux(9), 8, 0 },
+ { pinmux(7), 8, 1 },
+ { pinmux(7), 8, 2 },
+ { pinmux(5), 8, 1 }, /* GP6[0] */
+ { pinmux(5), 8, 2 },
+ { pinmux(5), 8, 3 },
+ { pinmux(5), 8, 4 },
+ { pinmux(5), 8, 5 },
+ { pinmux(5), 8, 6 },
+ { pinmux(5), 8, 7 },
+ { pinmux(6), 8, 0 },
+ { pinmux(6), 8, 1 },
+ { pinmux(6), 8, 2 },
+ { pinmux(6), 8, 3 },
+ { pinmux(6), 8, 4 },
+ { pinmux(6), 8, 5 },
+ { pinmux(6), 8, 6 },
+ { pinmux(6), 8, 7 },
+ { pinmux(7), 8, 0 },
+ { pinmux(1), 8, 0 }, /* GP7[0] */
+ { pinmux(1), 8, 1 },
+ { pinmux(1), 8, 2 },
+ { pinmux(1), 8, 3 },
+ { pinmux(1), 8, 4 },
+ { pinmux(1), 8, 5 },
+ { pinmux(1), 8, 6 },
+ { pinmux(1), 8, 7 },
+ { pinmux(2), 8, 0 },
+ { pinmux(2), 8, 1 },
+ { pinmux(2), 8, 2 },
+ { pinmux(2), 8, 3 },
+ { pinmux(2), 8, 4 },
+ { pinmux(2), 8, 5 },
+ { pinmux(0), 1, 0 },
+ { pinmux(0), 1, 1 },
+};
++#else /* CONFIG_SOC_DA8XX && CONFIG_SOC_DA850 */
static const struct pinmux_config gpio_pinmux[] = {
{ pinmux(1), 8, 7 }, /* GP0[0] */
{ pinmux(1), 8, 6 },
{ pinmux(18), 8, 3 },
{ pinmux(18), 8, 2 },
};
- #endif
-#else
++#endif /* CONFIG_SOC_DA8XX && !CONFIG_SOC_DA850 */
++#else /* !CONFIG_SOC_DA8XX */
+ #define davinci_configure_pin_mux(a, b)
-#endif
++#endif /* CONFIG_SOC_DA8XX */
int gpio_request(unsigned gpio, const char *label)
{
diff --combined drivers/mmc/bfin_sdh.c
index 81d8e5432f941f94d7eea769bb09f4309d9fd8eb,0f98b961fd4418b5ac676473a8ee9d0d0bd4671c..26311741f5fa8b83bb51a9b1a1811571508b5c00
+++ b/drivers/mmc/bfin_sdh.c
#include <asm/mach-common/bits/sdh.h>
#include <asm/mach-common/bits/dma.h>
- #if defined(__ADSPBF50x__) || defined(__ADSPBF51x__)
- # define bfin_read_SDH_PWR_CTL bfin_read_RSI_PWR_CONTROL
- # define bfin_write_SDH_PWR_CTL bfin_write_RSI_PWR_CONTROL
+ #if defined(__ADSPBF50x__) || defined(__ADSPBF51x__) || defined(__ADSPBF60x__)
# define bfin_read_SDH_CLK_CTL bfin_read_RSI_CLK_CONTROL
# define bfin_write_SDH_CLK_CTL bfin_write_RSI_CLK_CONTROL
# define bfin_write_SDH_ARGUMENT bfin_write_RSI_ARGUMENT
# define bfin_write_SDH_STATUS_CLR bfin_write_RSI_STATUSCL
# define bfin_read_SDH_CFG bfin_read_RSI_CONFIG
# define bfin_write_SDH_CFG bfin_write_RSI_CONFIG
+ # if defined(__ADSPBF60x__)
+ # define bfin_read_SDH_BLK_SIZE bfin_read_RSI_BLKSZ
+ # define bfin_write_SDH_BLK_SIZE bfin_write_RSI_BLKSZ
+ # define bfin_write_DMA_START_ADDR bfin_write_DMA10_START_ADDR
+ # define bfin_write_DMA_X_COUNT bfin_write_DMA10_X_COUNT
+ # define bfin_write_DMA_X_MODIFY bfin_write_DMA10_X_MODIFY
+ # define bfin_write_DMA_CONFIG bfin_write_DMA10_CONFIG
+ # else
+ # define bfin_read_SDH_PWR_CTL bfin_read_RSI_PWR_CONTROL
+ # define bfin_write_SDH_PWR_CTL bfin_write_RSI_PWR_CONTROL
# define bfin_write_DMA_START_ADDR bfin_write_DMA4_START_ADDR
# define bfin_write_DMA_X_COUNT bfin_write_DMA4_X_COUNT
# define bfin_write_DMA_X_MODIFY bfin_write_DMA4_X_MODIFY
# define bfin_write_DMA_CONFIG bfin_write_DMA4_CONFIG
+ # endif
# define PORTMUX_PINS \
{ P_RSI_DATA0, P_RSI_DATA1, P_RSI_DATA2, P_RSI_DATA3, P_RSI_CMD, P_RSI_CLK, 0 }
#elif defined(__ADSPBF54x__)
sdh_cmd |= CMD_RSP;
if (flags & MMC_RSP_136)
sdh_cmd |= CMD_L_RSP;
+ #ifdef RSI_BLKSZ
+ sdh_cmd |= CMD_DATA0_BUSY;
+ #endif
bfin_write_SDH_ARGUMENT(arg);
bfin_write_SDH_COMMAND(sdh_cmd);
bfin_write_SDH_STATUS_CLR(CMD_SENT_STAT | CMD_RESP_END_STAT |
CMD_TIMEOUT_STAT | CMD_CRC_FAIL_STAT);
+ #ifdef RSI_BLKSZ
+ /* wait till card ready */
+ while (!(bfin_read_RSI_ESTAT() & SD_CARD_READY))
+ continue;
+ bfin_write_RSI_ESTAT(SD_CARD_READY);
+ #endif
return ret;
}
{
u16 data_ctl = 0;
u16 dma_cfg = 0;
- int ret = 0;
unsigned long data_size = data->blocksize * data->blocks;
/* Don't support write yet. */
if (data->flags & MMC_DATA_WRITE)
return UNUSABLE_ERR;
+ #ifndef RSI_BLKSZ
data_ctl |= ((ffs(data_size) - 1) << 4);
+ #else
+ bfin_write_SDH_BLK_SIZE(data_size);
+ #endif
data_ctl |= DTX_DIR;
bfin_write_SDH_DATA_CTL(data_ctl);
- dma_cfg = WDSIZE_32 | RESTART | WNR | DMAEN;
+ dma_cfg = WDSIZE_32 | PSIZE_32 | RESTART | WNR | DMAEN;
bfin_write_SDH_DATA_TIMER(-1);
/* kick off transfer */
bfin_write_SDH_DATA_CTL(bfin_read_SDH_DATA_CTL() | DTX_DMA_E | DTX_E);
- return ret;
+ return 0;
}
u32 status;
int ret = 0;
+ if (data) {
+ ret = sdh_setup_data(mmc, data);
+ if (ret)
+ return ret;
+ }
+
ret = sdh_send_cmd(mmc, cmd);
if (ret) {
+ bfin_write_SDH_COMMAND(0);
+ bfin_write_DMA_CONFIG(0);
+ bfin_write_SDH_DATA_CTL(0);
+ SSYNC();
printf("sending CMD%d failed\n", cmd->cmdidx);
return ret;
}
+
if (data) {
- ret = sdh_setup_data(mmc, data);
do {
udelay(1);
status = bfin_read_SDH_STATUS();
if (mmc->bus_width == 4) {
cfg = bfin_read_SDH_CFG();
- cfg &= ~0x80;
- cfg |= 0x40;
+ #ifndef RSI_BLKSZ
+ cfg &= ~PD_SDDAT3;
+ #endif
+ cfg |= PUP_SDDAT3;
bfin_write_SDH_CFG(cfg);
- clk_ctl |= WIDE_BUS;
+ clk_ctl |= WIDE_BUS_4;
}
bfin_write_SDH_CLK_CTL(clk_ctl);
sdh_set_clk(mmc->clock);
static int bfin_sdh_init(struct mmc *mmc)
{
const unsigned short pins[] = PORTMUX_PINS;
- u16 pwr_ctl = 0;
+ int ret;
/* Initialize sdh controller */
- peripheral_request_list(pins, "bfin_sdh");
+ ret = peripheral_request_list(pins, "bfin_sdh");
+ if (ret < 0)
+ return ret;
#if defined(__ADSPBF54x__)
bfin_write_DMAC1_PERIMUX(bfin_read_DMAC1_PERIMUX() | 0x1);
#endif
bfin_write_SDH_CFG(bfin_read_SDH_CFG() | CLKS_EN);
/* Disable card detect pin */
bfin_write_SDH_CFG((bfin_read_SDH_CFG() & 0x1F) | 0x60);
-
- pwr_ctl |= ROD_CTL;
- pwr_ctl |= PWR_ON;
- bfin_write_SDH_PWR_CTL(pwr_ctl);
+ #ifndef RSI_BLKSZ
+ bfin_write_SDH_PWR_CTL(PWR_ON | ROD_CTL);
+ #else
+ bfin_write_SDH_CFG(bfin_read_SDH_CFG() | PWR_ON);
+ #endif
return 0;
}
mmc->set_ios = bfin_sdh_set_ios;
mmc->init = bfin_sdh_init;
mmc->getcd = NULL;
+ mmc->getwp = NULL;
mmc->host_caps = MMC_MODE_4BIT;
mmc->voltages = MMC_VDD_32_33 | MMC_VDD_33_34;
diff --combined include/configs/ea20.h
index 03dfe0af2d02c3fd2943d423b16d50c1e7335a72,a8c08e8d95d15b19f94b7da8669018632adf41f3..90fc7c58d2053dad22377f3ffd112fef9d839fb4
+++ b/include/configs/ea20.h
#define CONFIG_MACH_DAVINCI_DA850_EVM
#define CONFIG_ARM926EJS /* arm926ejs CPU core */
#define CONFIG_SOC_DA8XX /* TI DA8xx SoC */
+#define CONFIG_SOC_DA850 /* TI DA850 SoC */
#define CONFIG_SYS_CLK_FREQ clk_get(DAVINCI_ARM_CLKID)
#define CONFIG_SYS_OSCIN_FREQ 24000000
#define CONFIG_SYS_TIMERBASE DAVINCI_TIMER0_BASE
"bootm ${kernel_addr_r}\0" \
"net_self_load=tftp ${kernel_addr_r} ${bootfile};" \
"tftp ${ramdisk_addr_r} ${ramdisk_file};\0" \
- "nand_nand=ubi part nand0,${as};ubifsmount rootfs;" \
+ "nand_nand=ubi part nand0,${as};ubifsmount ubi:rootfs;" \
"ubifsload ${kernel_addr_r} /boot/uImage;" \
"ubifsumount; run nandargs addip addtty " \
"addmtd addmisc addmem;clrlogo;" \
"bootm ${kernel_addr_r}\0" \
- "nand_nandrw=ubi part nand0,${as};ubifsmount rootfs;" \
+ "nand_nandrw=ubi part nand0,${as};ubifsmount ubi:rootfs;" \
"ubifsload ${kernel_addr_r} /boot/uImage;" \
"ubifsumount; run nandrwargs addip addtty " \
"addmtd addmisc addmem;clrlogo;" \
"u-boot=" __stringify(CONFIG_HOSTNAME) "/u-boot.bin\0" \
"load_magic=if sf probe 0;then sf " \
"read c0000000 0x10000 0x60000;fi\0" \
- "load_nand=ubi part nand0,${as};ubifsmount rootfs;" \
+ "load_nand=ubi part nand0,${as};ubifsmount ubi:rootfs;" \
"if ubifsload c0000014 /boot/u-boot.bin;" \
"then mw c0000008 ${filesize};else echo Error reading" \
" u-boot from nand!;fi\0" \