summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c97cd1b)
raw | patch | inline | side by side (parent: c97cd1b)
author | Scott Wood <scottwood@freescale.com> | |
Fri, 21 Sep 2012 00:05:12 +0000 (19:05 -0500) | ||
committer | Scott Wood <scottwood@freescale.com> | |
Mon, 26 Nov 2012 21:41:25 +0000 (15:41 -0600) |
Introduces CONFIG_SPL_RELOC_TEXT_BASE and CONFIG_SPL_RELOC_STACK.
Signed-off-by: Scott Wood <scottwood@freescale.com>
Cc: Andy Fleming <afleming@freescale.com>
Signed-off-by: Scott Wood <scottwood@freescale.com>
Cc: Andy Fleming <afleming@freescale.com>
README | patch | blob | history | |
board/freescale/p1_p2_rdb_pc/Makefile | patch | blob | history | |
board/freescale/p1_p2_rdb_pc/p1_p2_rdb_pc.c | patch | blob | history | |
board/freescale/p1_p2_rdb_pc/spl_minimal.c | [new file with mode: 0644] | patch | blob |
board/freescale/p1_p2_rdb_pc/tlb.c | patch | blob | history |
index ca2d10f8ed804317aa7f4fa30c51e64448b58ac8..44cd65a52feb00fe15c4ea4f459092aa17a2783f 100644 (file)
--- a/README
+++ b/README
CONFIG_SPL_TEXT_BASE
TEXT_BASE for linking the SPL binary.
+ CONFIG_SPL_RELOC_TEXT_BASE
+ Address to relocate to. If unspecified, this is equal to
+ CONFIG_SPL_TEXT_BASE (i.e. no relocation is done).
+
CONFIG_SPL_BSS_START_ADDR
Link address for the BSS within the SPL binary.
CONFIG_SPL_STACK
Adress of the start of the stack SPL will use
+ CONFIG_SPL_RELOC_STACK
+ Adress of the start of the stack SPL will use after
+ relocation. If unspecified, this is equal to
+ CONFIG_SPL_STACK.
+
CONFIG_SYS_SPL_MALLOC_START
Starting address of the malloc pool used in SPL.
index 0dcf7d1ab17e7262fc1db420261acfb37743cef0..5b45d72f511252e838be98bbfe16b2fdc28f9b05 100644 (file)
LIB = $(obj)lib$(BOARD).o
+MINIMAL=
+
+ifdef CONFIG_SPL_BUILD
+ifdef CONFIG_SPL_INIT_MINIMAL
+MINIMAL=y
+endif
+endif
+
+ifdef MINIMAL
+
+COBJS-y += spl_minimal.o tlb.o law.o
+
+else
+
COBJS-y += $(BOARD).o
COBJS-y += ddr.o
COBJS-y += law.o
COBJS-y += tlb.o
+endif
+
SRCS := $(SOBJS:.o=.S) $(COBJS-y:.o=.c)
OBJS := $(addprefix $(obj),$(COBJS-y))
SOBJS := $(addprefix $(obj),$(SOBJS))
diff --git a/board/freescale/p1_p2_rdb_pc/p1_p2_rdb_pc.c b/board/freescale/p1_p2_rdb_pc/p1_p2_rdb_pc.c
index aa39260ca7ed084589a444f52e9ac546dbdb0058..5b5b86c822e968db065913406700462d5f66af16 100644 (file)
*/
setbits_be32(&pgpio->gpdir, 0x02130000);
-#ifndef CONFIG_SYS_RAMBOOT
+#if !defined(CONFIG_SYS_RAMBOOT) && !defined(CONFIG_SPL)
/* init DDR3 reset signal */
setbits_be32(&pgpio->gpdir, 0x00200000);
setbits_be32(&pgpio->gpodr, 0x00200000);
diff --git a/board/freescale/p1_p2_rdb_pc/spl_minimal.c b/board/freescale/p1_p2_rdb_pc/spl_minimal.c
--- /dev/null
@@ -0,0 +1,131 @@
+/*
+ * Copyright 2011 Freescale Semiconductor, Inc.
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License as
+ * published by the Free Software Foundation; either version 2 of
+ * the License, or (at your option) any later version.
+ *
+ * This program is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
+ *
+ * GNU General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
+ * MA 02111-1307 USA
+ *
+ */
+
+#include <common.h>
+#include <ns16550.h>
+#include <asm/io.h>
+#include <nand.h>
+#include <asm/fsl_law.h>
+#include <asm/fsl_ddr_sdram.h>
+#include <asm/global_data.h>
+
+DECLARE_GLOBAL_DATA_PTR;
+
+/*
+ * Fixed sdram init -- doesn't use serial presence detect.
+ */
+void sdram_init(void)
+{
+ ccsr_ddr_t *ddr = (ccsr_ddr_t *)CONFIG_SYS_MPC85xx_DDR_ADDR;
+
+ __raw_writel(CONFIG_SYS_DDR_CS0_BNDS, &ddr->cs0_bnds);
+ __raw_writel(CONFIG_SYS_DDR_CS0_CONFIG, &ddr->cs0_config);
+#if CONFIG_CHIP_SELECTS_PER_CTRL > 1
+ __raw_writel(CONFIG_SYS_DDR_CS1_BNDS, &ddr->cs1_bnds);
+ __raw_writel(CONFIG_SYS_DDR_CS1_CONFIG, &ddr->cs1_config);
+#endif
+ __raw_writel(CONFIG_SYS_DDR_TIMING_3, &ddr->timing_cfg_3);
+ __raw_writel(CONFIG_SYS_DDR_TIMING_0, &ddr->timing_cfg_0);
+ __raw_writel(CONFIG_SYS_DDR_TIMING_1, &ddr->timing_cfg_1);
+ __raw_writel(CONFIG_SYS_DDR_TIMING_2, &ddr->timing_cfg_2);
+
+ __raw_writel(CONFIG_SYS_DDR_CONTROL_2, &ddr->sdram_cfg_2);
+ __raw_writel(CONFIG_SYS_DDR_MODE_1, &ddr->sdram_mode);
+ __raw_writel(CONFIG_SYS_DDR_MODE_2, &ddr->sdram_mode_2);
+
+ __raw_writel(CONFIG_SYS_DDR_INTERVAL, &ddr->sdram_interval);
+ __raw_writel(CONFIG_SYS_DDR_DATA_INIT, &ddr->sdram_data_init);
+ __raw_writel(CONFIG_SYS_DDR_CLK_CTRL, &ddr->sdram_clk_cntl);
+
+ __raw_writel(CONFIG_SYS_DDR_TIMING_4, &ddr->timing_cfg_4);
+ __raw_writel(CONFIG_SYS_DDR_TIMING_5, &ddr->timing_cfg_5);
+ __raw_writel(CONFIG_SYS_DDR_ZQ_CONTROL, &ddr->ddr_zq_cntl);
+ __raw_writel(CONFIG_SYS_DDR_WRLVL_CONTROL, &ddr->ddr_wrlvl_cntl);
+
+ /* Set, but do not enable the memory */
+ __raw_writel(CONFIG_SYS_DDR_CONTROL & ~SDRAM_CFG_MEM_EN, &ddr->sdram_cfg);
+
+ asm volatile("sync;isync");
+ udelay(500);
+
+ /* Let the controller go */
+ out_be32(&ddr->sdram_cfg, in_be32(&ddr->sdram_cfg) | SDRAM_CFG_MEM_EN);
+
+ set_next_law(0, CONFIG_SYS_SDRAM_SIZE_LAW, LAW_TRGT_IF_DDR_1);
+}
+
+void board_init_f(ulong bootflag)
+{
+ u32 plat_ratio;
+ ccsr_gur_t *gur = (void *)CONFIG_SYS_MPC85xx_GUTS_ADDR;
+#ifndef CONFIG_QE
+ ccsr_gpio_t *pgpio = (void *)(CONFIG_SYS_MPC85xx_GPIO_ADDR);
+#endif
+
+ /* initialize selected port with appropriate baud rate */
+ plat_ratio = in_be32(&gur->porpllsr) & MPC85xx_PORPLLSR_PLAT_RATIO;
+ plat_ratio >>= 1;
+ gd->bus_clk = CONFIG_SYS_CLK_FREQ * plat_ratio;
+
+ NS16550_init((NS16550_t)CONFIG_SYS_NS16550_COM1,
+ gd->bus_clk / 16 / CONFIG_BAUDRATE);
+
+ puts("\nNAND boot... ");
+
+#ifndef CONFIG_QE
+ /* init DDR3 reset signal */
+ __raw_writel(0x02000000, &pgpio->gpdir);
+ __raw_writel(0x00200000, &pgpio->gpodr);
+ __raw_writel(0x00000000, &pgpio->gpdat);
+ udelay(1000);
+ __raw_writel(0x00200000, &pgpio->gpdat);
+ udelay(1000);
+ __raw_writel(0x00000000, &pgpio->gpdir);
+#endif
+
+ /* Initialize the DDR3 */
+ sdram_init();
+
+ /* copy code to RAM and jump to it - this should not return */
+ /* NOTE - code has to be copied out of NAND buffer before
+ * other blocks can be read.
+ */
+ relocate_code(CONFIG_SPL_RELOC_STACK, 0, CONFIG_SPL_RELOC_TEXT_BASE);
+}
+
+void board_init_r(gd_t *gd, ulong dest_addr)
+{
+ nand_boot();
+}
+
+void putc(char c)
+{
+ if (c == '\n')
+ NS16550_putc((NS16550_t)CONFIG_SYS_NS16550_COM1, '\r');
+
+ NS16550_putc((NS16550_t)CONFIG_SYS_NS16550_COM1, c);
+}
+
+void puts(const char *str)
+{
+ while (*str)
+ putc(*str++);
+}
index 6d2246387a6967b17644e2c39417723802a909e0..0873dd750f1d5e026fc7c99d7f9093508bbce33b 100644 (file)
MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,
0, 1, BOOKE_PAGESZ_1M, 1),
-#ifndef CONFIG_NAND_SPL
+#ifndef CONFIG_SPL_BUILD
/* W**G* - Flash/promjet, localbus */
/* This will be changed to *I*G* after relocation to RAM. */
SET_TLB_ENTRY(1, CONFIG_SYS_FLASH_BASE, CONFIG_SYS_FLASH_BASE_PHYS,
SET_TLB_ENTRY(1, CONFIG_SYS_PMC_BASE, CONFIG_SYS_PMC_BASE_PHYS,
MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,
0, 10, BOOKE_PAGESZ_64K, 1),
-#endif
+#endif /* not SPL */
#ifdef CONFIG_SYS_NAND_BASE
/* *I*G - NAND */
0, 7, BOOKE_PAGESZ_1M, 1),
#endif
-#ifdef CONFIG_SYS_RAMBOOT
+#if defined(CONFIG_SYS_RAMBOOT) || defined(CONFIG_SPL)
/* *I*G - eSDHC/eSPI/NAND boot */
SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE, CONFIG_SYS_DDR_SDRAM_BASE,
MAS3_SX|MAS3_SW|MAS3_SR, 0,
0, 9, BOOKE_PAGESZ_1G, 1),
#endif
#endif
-
};
int num_tlb_entries = ARRAY_SIZE(tlb_table);