]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/commitdiff
i.MX28: Move SPL to arch/arm/cpu/arm926ejs/mx28
authorMarek Vasut <marek.vasut@gmail.com>
Fri, 2 Dec 2011 03:47:40 +0000 (03:47 +0000)
committerAlbert ARIBAUD <albert.u.boot@aribaud.net>
Fri, 9 Dec 2011 16:30:10 +0000 (17:30 +0100)
This moves SPL to common location so it can be reused by multiple boards. Also,
this commit adjusts M28 SoM to avoid breakage due to the move.

Signed-off-by: Marek Vasut <marek.vasut@gmail.com>
Cc: Wolfgang Denk <wd@denx.de>
Cc: Detlev Zundel <dzu@denx.de>
Cc: Stefano Babic <sbabic@denx.de>
arch/arm/cpu/arm926ejs/mx28/Makefile
arch/arm/cpu/arm926ejs/mx28/mx28_init.h [moved from board/denx/m28evk/m28_init.h with 100% similarity]
arch/arm/cpu/arm926ejs/mx28/spl_boot.c [new file with mode: 0644]
arch/arm/cpu/arm926ejs/mx28/spl_mem_init.c [moved from board/denx/m28evk/mem_init.c with 99% similarity]
arch/arm/cpu/arm926ejs/mx28/spl_power_init.c [moved from board/denx/m28evk/power_init.c with 99% similarity]
arch/arm/cpu/arm926ejs/mx28/start.S [moved from board/denx/m28evk/start.S with 100% similarity]
arch/arm/cpu/arm926ejs/mx28/u-boot-spl.lds [moved from board/denx/m28evk/u-boot-spl.lds with 97% similarity]
arch/arm/include/asm/arch-mx28/sys_proto.h
board/denx/m28evk/Makefile
board/denx/m28evk/spl_boot.c [moved from board/denx/m28evk/mmc_boot.c with 87% similarity]
include/configs/m28evk.h

index 7845310cfec12493245d9a20df5a454248275dcf..372de8a5e4c6de28bce2eb3cfccec16d56c7d689 100644 (file)
@@ -27,6 +27,10 @@ LIB  = $(obj)lib$(SOC).o
 
 COBJS  = clock.o mx28.o iomux.o timer.o
 
+ifdef  CONFIG_SPL_BUILD
+COBJS  += memsize.o spl_boot.o spl_mem_init.o spl_power_init.o
+endif
+
 SRCS   := $(START:.o=.S) $(COBJS:.o=.c)
 OBJS   := $(addprefix $(obj),$(COBJS))
 START  := $(addprefix $(obj),$(START))
@@ -36,6 +40,11 @@ all: $(obj).depend $(LIB)
 $(LIB):        $(OBJS)
        $(call cmd_link_o_target, $(OBJS))
 
+ifdef  CONFIG_SPL_BUILD
+memsize.c:
+       ln -sf $(TOPDIR)/common/memsize.c $@
+endif
+
 #########################################################################
 
 # defines $(obj).depend target
diff --git a/arch/arm/cpu/arm926ejs/mx28/spl_boot.c b/arch/arm/cpu/arm926ejs/mx28/spl_boot.c
new file mode 100644 (file)
index 0000000..3cd4c24
--- /dev/null
@@ -0,0 +1,87 @@
+/*
+ * Freescale i.MX28 Boot setup
+ *
+ * Copyright (C) 2011 Marek Vasut <marek.vasut@gmail.com>
+ * on behalf of DENX Software Engineering GmbH
+ *
+ * See file CREDITS for list of people who contributed to this
+ * project.
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License as
+ * published by the Free Software Foundation; either version 2 of
+ * the License, or (at your option) any later version.
+ *
+ * This program is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
+ * GNU General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
+ * MA 02111-1307 USA
+ */
+
+#include <common.h>
+#include <config.h>
+#include <asm/io.h>
+#include <asm/arch/iomux-mx28.h>
+#include <asm/arch/imx-regs.h>
+
+#include "mx28_init.h"
+
+/*
+ * This delay function is intended to be used only in early stage of boot, where
+ * clock are not set up yet. The timer used here is reset on every boot and
+ * takes a few seconds to roll. The boot doesn't take that long, so to keep the
+ * code simple, it doesn't take rolling into consideration.
+ */
+#define        HW_DIGCTRL_MICROSECONDS 0x8001c0c0
+void early_delay(int delay)
+{
+       uint32_t st = readl(HW_DIGCTRL_MICROSECONDS);
+       st += delay;
+       while (st > readl(HW_DIGCTRL_MICROSECONDS))
+               ;
+}
+
+void mx28_common_spl_init(const iomux_cfg_t *iomux_setup,
+                       const unsigned int iomux_size)
+{
+       mxs_iomux_setup_multiple_pads(iomux_setup, iomux_size);
+       mx28_power_init();
+       mx28_mem_init();
+       mx28_power_wait_pswitch();
+}
+
+/* Support aparatus */
+inline void board_init_f(unsigned long bootflag)
+{
+       for (;;)
+               ;
+}
+
+inline void board_init_r(gd_t *id, ulong dest_addr)
+{
+       for (;;)
+               ;
+}
+
+inline int printf(const char *fmt, ...)
+{
+       return 0;
+}
+
+inline void __coloured_LED_init(void) {}
+inline void __red_LED_on(void) {}
+void coloured_LED_init(void)
+       __attribute__((weak, alias("__coloured_LED_init")));
+void red_LED_on(void)
+       __attribute__((weak, alias("__red_LED_on")));
+void hang(void) __attribute__ ((noreturn));
+void hang(void)
+{
+       for (;;)
+               ;
+}
similarity index 99%
rename from board/denx/m28evk/mem_init.c
rename to arch/arm/cpu/arm926ejs/mx28/spl_mem_init.c
index 17d1f9b6a1644d90ebea21f16919e90c2273fbe5..00493b8bf9293adbc1401dcb665cbc04374339ff 100644 (file)
@@ -29,7 +29,7 @@
 #include <asm/arch/iomux-mx28.h>
 #include <asm/arch/imx-regs.h>
 
-#include "m28_init.h"
+#include "mx28_init.h"
 
 uint32_t dram_vals[] = {
        0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000,
similarity index 99%
rename from board/denx/m28evk/power_init.c
rename to arch/arm/cpu/arm926ejs/mx28/spl_power_init.c
index 27322b4ec18d1dcf3c6836ee12a1ca19fc4a13f2..a4dc2a31b7b275c918d40987555bdae72d7ad9ed 100644 (file)
@@ -28,7 +28,7 @@
 #include <asm/io.h>
 #include <asm/arch/imx-regs.h>
 
-#include "m28_init.h"
+#include "mx28_init.h"
 
 void mx28_power_clock2xtal(void)
 {
similarity index 97%
rename from board/denx/m28evk/u-boot-spl.lds
rename to arch/arm/cpu/arm926ejs/mx28/u-boot-spl.lds
index e296a92ed8b21b83d834c0819217a215d0d89449..893320f993579888626a973d8f2228e162d53a65 100644 (file)
@@ -37,7 +37,7 @@ SECTIONS
        . = ALIGN(4);
        .text   :
        {
-               board/denx/m28evk/start.o       (.text)
+               arch/arm/cpu/arm926ejs/mx28/start.o     (.text)
                *(.text)
        }
 
index a226ea4840988bc958f381be92b5df2b28f08af6..be1f7db2ae7b8aa6b22b560a12c4bb20a21dc16a 100644 (file)
@@ -29,4 +29,10 @@ int mx28_wait_mask_clr(struct mx28_register *reg, uint32_t mask, int timeout);
 
 int mxsmmc_initialize(bd_t *bis, int id, int (*wp)(int));
 
+#ifdef CONFIG_SPL_BUILD
+#include <asm/arch/iomux-mx28.h>
+void mx28_common_spl_init(const iomux_cfg_t *iomux_setup,
+                       const unsigned int iomux_size);
+#endif
+
 #endif /* __MX28_H__ */
index b6f002fe36f466e570c819b782e543e5468d3023..aa16c7d1560b763b3c77f385435c085a8876e9f2 100644 (file)
@@ -27,10 +27,8 @@ LIB  = $(obj)lib$(BOARD).o
 
 ifndef CONFIG_SPL_BUILD
 COBJS  := m28evk.o
-endif
-
-ifdef  CONFIG_SPL_BUILD
-COBJS  := mem_init.o mmc_boot.o power_init.o memsize.o
+else
+COBJS  := spl_boot.o
 endif
 
 SRCS   := $(COBJS:.o=.c)
@@ -41,11 +39,6 @@ $(LIB):      $(obj).depend $(OBJS)
 
 all:   $(ALL)
 
-ifdef  CONFIG_SPL_BUILD
-memsize.c:
-       ln -sf $(TOPDIR)/common/memsize.c $@
-endif
-
 #########################################################################
 
 # defines $(obj).depend target
similarity index 87%
rename from board/denx/m28evk/mmc_boot.c
rename to board/denx/m28evk/spl_boot.c
index 86d3ab5e1cb2565010df73aad2f1720b44712183..86d7d876daf0e166fffdcc223855b6f32f72f75e 100644 (file)
@@ -1,5 +1,5 @@
 /*
- * Freescale i.MX28 Boot setup
+ * DENX M28 Boot setup
  *
  * Copyright (C) 2011 Marek Vasut <marek.vasut@gmail.com>
  * on behalf of DENX Software Engineering GmbH
 #include <config.h>
 #include <asm/io.h>
 #include <asm/arch/iomux-mx28.h>
-
-#include "m28_init.h"
-
-/*
- * This delay function is intended to be used only in early stage of boot, where
- * clock are not set up yet. The timer used here is reset on every boot and
- * takes a few seconds to roll. The boot doesn't take that long, so to keep the
- * code simple, it doesn't take rolling into consideration.
- */
-#define        HW_DIGCTRL_MICROSECONDS 0x8001c0c0
-void early_delay(int delay)
-{
-       uint32_t st = readl(HW_DIGCTRL_MICROSECONDS);
-       st += delay;
-       while (st > readl(HW_DIGCTRL_MICROSECONDS))
-               ;
-}
+#include <asm/arch/imx-regs.h>
+#include <asm/arch/sys_proto.h>
 
 #define        MUX_CONFIG_LED  (MXS_PAD_3V3 | MXS_PAD_4MA | MXS_PAD_NOPULL)
 #define        MUX_CONFIG_LCD  (MXS_PAD_3V3 | MXS_PAD_4MA)
@@ -109,10 +94,6 @@ const iomux_cfg_t iomux_setup[] = {
        MX28_PAD_GPMI_RDY2__CAN0_TX,
        MX28_PAD_GPMI_RDY3__CAN0_RX,
 
-       /* I2C */
-       MX28_PAD_I2C0_SCL__I2C0_SCL,
-       MX28_PAD_I2C0_SDA__I2C0_SDA,
-
        /* TSC2007 */
        MX28_PAD_SAIF0_MCLK__GPIO_3_20 | MUX_CONFIG_TSC,
 
@@ -235,39 +216,5 @@ const iomux_cfg_t iomux_setup[] = {
 
 void board_init_ll(void)
 {
-       mxs_iomux_setup_multiple_pads(iomux_setup, ARRAY_SIZE(iomux_setup));
-       mx28_power_init();
-       mx28_mem_init();
-       mx28_power_wait_pswitch();
-}
-
-/* Support aparatus */
-inline void board_init_f(unsigned long bootflag)
-{
-       for (;;)
-               ;
-}
-
-inline void board_init_r(gd_t *id, ulong dest_addr)
-{
-       for (;;)
-               ;
-}
-
-inline int printf(const char *fmt, ...)
-{
-       return 0;
-}
-
-inline void __coloured_LED_init(void) {}
-inline void __red_LED_on(void) {}
-void coloured_LED_init(void)
-       __attribute__((weak, alias("__coloured_LED_init")));
-void red_LED_on(void)
-       __attribute__((weak, alias("__red_LED_on")));
-void hang(void) __attribute__ ((noreturn));
-void hang(void)
-{
-       for (;;)
-               ;
+       mx28_common_spl_init(iomux_setup, ARRAY_SIZE(iomux_setup));
 }
index d4bd207d58b92544a2e5a45d6c0d63c3add3598b..cdf7636c2fcffe7d531cfdb48bce4cbab5d57781 100644 (file)
@@ -48,8 +48,8 @@
  */
 #define        CONFIG_SPL
 #define        CONFIG_SPL_NO_CPU_SUPPORT_CODE
-#define        CONFIG_SPL_START_S_PATH         "board/denx/m28evk"
-#define        CONFIG_SPL_LDSCRIPT             "board/denx/m28evk/u-boot-spl.lds"
+#define        CONFIG_SPL_START_S_PATH         "arch/arm/cpu/arm926ejs/mx28"
+#define        CONFIG_SPL_LDSCRIPT     "arch/arm/cpu/arm926ejs/mx28/u-boot-spl.lds"
 
 /*
  * U-Boot Commands