summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 02a58b9)
raw | patch | inline | side by side (parent: 02a58b9)
author | Ajay Kumar <ajaykumar.rs@samsung.com> | |
Sun, 13 Jan 2013 23:32:16 +0000 (23:32 +0000) | ||
committer | Minkyu Kang <mk7.kang@samsung.com> | |
Mon, 14 Jan 2013 10:17:28 +0000 (19:17 +0900) |
Previously, the call to draw_logo() was happening irrespective
of whether we have selected logo or LCD console.
With this patch we call draw_logo() only when CONFIG_CMD_BMP is selected.
This would even fix the following compilation warning:
exynos_fb.c: In function 'draw_logo':
exynos_fb.c:74:8: warning: variable 'addr' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:9: warning: variable 'y' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:6: warning: variable 'x' set but not used
[-Wunused-but-set-variable]
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
of whether we have selected logo or LCD console.
With this patch we call draw_logo() only when CONFIG_CMD_BMP is selected.
This would even fix the following compilation warning:
exynos_fb.c: In function 'draw_logo':
exynos_fb.c:74:8: warning: variable 'addr' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:9: warning: variable 'y' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:6: warning: variable 'x' set but not used
[-Wunused-but-set-variable]
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
drivers/video/exynos_fb.c | patch | blob | history |
index 183bca07c5899ca42190ece283a56e47bdc2ceac..ee0ed06d6fe60d711a420b8710e996cb487fa9e8 100644 (file)
lcd_set_flush_dcache(1);
}
+#ifdef CONFIG_CMD_BMP
static void draw_logo(void)
{
int x, y;
}
addr = panel_info.logo_addr;
-#ifdef CONFIG_CMD_BMP
bmp_display(addr, x, y);
-#endif
}
+#endif
static void lcd_panel_on(vidinfo_t *vid)
{
if (panel_info.logo_on) {
memset(lcd_base, 0, panel_width * panel_height *
(NBITS(panel_info.vl_bpix) >> 3));
+#ifdef CONFIG_CMD_BMP
draw_logo();
+#endif
}
lcd_panel_on(&panel_info);