]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/commitdiff
patman: Add Cover-letter-cc tag to Cc cover letter to people
authorSimon Glass <sjg@chromium.org>
Wed, 20 Mar 2013 16:43:00 +0000 (16:43 +0000)
committerSimon Glass <sjg@chromium.org>
Thu, 4 Apr 2013 21:04:34 +0000 (14:04 -0700)
The cover letter is sent to everyone who is on the Cc list for any of
the patches in the series. Sometimes it is useful to send just the cover
letter to additional people, so that they are aware of the series, but
don't need to wade through all the individual patches.

Add a new Cover-letter-cc tag for this purpose.

Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
tools/patman/README
tools/patman/patchstream.py
tools/patman/series.py

index 86d366fe9bf5c817be59d084cd45ea0e88fcc083..9922f2a37ae788c9c9b41ceb97a765b822fcfa1b 100644 (file)
@@ -182,6 +182,10 @@ END
        Sets the cover letter contents for the series. The first line
        will become the subject of the cover letter
 
+Cover-letter-cc: email / alias
+       Additional email addresses / aliases to send cover letter to (you
+       can add this multiple times)
+
 Series-notes:
 blah blah
 blah blah
@@ -263,7 +267,13 @@ will create a patch which is copied to x86, arm, sandbox, mikef, ag and
 afleming.
 
 If you have a cover letter it will get sent to the union of the CC lists of
-all of the other patches.
+all of the other patches. If you want to sent it to additional people you
+can add a tag:
+
+Cover-letter-cc: <list of addresses>
+
+These people will get the cover letter even if they are not on the To/Cc
+list for any of the patches.
 
 
 Example Work Flow
index 91542adb9b0c6f0afdc4c22308c486790847ac60..5c2d3bc9b0cef923b8377320971e82c2e7d7c13e 100644 (file)
@@ -42,6 +42,9 @@ re_signoff = re.compile('^Signed-off-by:')
 # The start of the cover letter
 re_cover = re.compile('^Cover-letter:')
 
+# A cover letter Cc
+re_cover_cc = re.compile('^Cover-letter-cc: *(.*)')
+
 # Patch series tag
 re_series = re.compile('^Series-(\w*): *(.*)')
 
@@ -153,6 +156,7 @@ class PatchStream:
         # Handle state transition and skipping blank lines
         series_match = re_series.match(line)
         commit_match = re_commit.match(line) if self.is_log else None
+        cover_cc_match = re_cover_cc.match(line)
         tag_match = None
         if self.state == STATE_PATCH_HEADER:
             tag_match = re_tag.match(line)
@@ -205,6 +209,10 @@ class PatchStream:
             self.in_section = 'cover'
             self.skip_blank = False
 
+        elif cover_cc_match:
+            value = cover_cc_match.group(1)
+            self.AddToSeries(line, 'cover-cc', value)
+
         # If we are in a change list, key collected lines until a blank one
         elif self.in_change:
             if is_blank:
index 6c5c5702e84bf82ad9eaf0b51e62b75d7f9fabeb..44ad931cf8758eb1b758d1e0e5b44f3d212da81e 100644 (file)
@@ -27,7 +27,8 @@ import gitutil
 import terminal
 
 # Series-xxx tags that we understand
-valid_series = ['to', 'cc', 'version', 'changes', 'prefix', 'notes', 'name'];
+valid_series = ['to', 'cc', 'version', 'changes', 'prefix', 'notes', 'name',
+                'cover-cc']
 
 class Series(dict):
     """Holds information about a patch series, including all tags.
@@ -43,6 +44,7 @@ class Series(dict):
     def __init__(self):
         self.cc = []
         self.to = []
+        self.cover_cc = []
         self.commits = []
         self.cover = None
         self.notes = []
@@ -69,6 +71,7 @@ class Series(dict):
             value: Tag value (part after 'Series-xxx: ')
         """
         # If we already have it, then add to our list
+        name = name.replace('-', '_')
         if name in self:
             values = value.split(',')
             values = [str.strip() for str in values]
@@ -140,7 +143,8 @@ class Series(dict):
         print 'Prefix:\t ', self.get('prefix')
         if self.cover:
             print 'Cover: %d lines' % len(self.cover)
-            all_ccs = itertools.chain(*self._generated_cc.values())
+            cover_cc = gitutil.BuildEmailList(self.get('cover_cc', ''))
+            all_ccs = itertools.chain(cover_cc, *self._generated_cc.values())
             for email in set(all_ccs):
                     print '      Cc: ',email
         if cmd:
@@ -232,7 +236,8 @@ class Series(dict):
             self._generated_cc[commit.patch] = list
 
         if cover_fname:
-            print >>fd, cover_fname, ', '.join(set(all_ccs))
+            cover_cc = gitutil.BuildEmailList(self.get('cover_cc', ''))
+            print >>fd, cover_fname, ', '.join(set(cover_cc + all_ccs))
 
         fd.close()
         return fname