]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/history - arch
mx51evk: Add DVI output support
[glsdk/glsdk-u-boot.git] / arch /
2013-01-13 Troy Kiskymx31/mx35/mx51/mx53/mx6: add watchdog
2013-01-09 Fabio Estevammx6: Add workaround for ARM errata
2013-01-08 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-01-08 Albert ARIBAUDMerge branch 'u-boot-ti/master' into 'u-boot-arm/master'
2012-12-22 Albert ARIBAUDMerge samsung, imx, tegra into u-boot-arm/master
2012-12-19 Allen MartinMerge remote-tracking branch 'u-boot/master' into u...
2012-12-14 Scott WoodMerge remote-tracking branch 'origin/master'
2012-12-13 Joe Hershbergerenv: Use getenv_yesno() more generally
2012-12-12 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-mips
2012-12-12 Joe Hershbergermips: serial: Fix busted manual relocation
2012-12-12 Daniel SchwierzeckMIPS: constify mips_io_port_base
2012-12-11 Simon GlassAdd strcasecmp() and strncasecmp()
2012-12-11 Piotr Wilczekexynos:pinmux: Add pinmux support for i2c
2012-12-11 Piotr Wilczekexynos:cpu: Add Exynos4 I2C spacing
2012-12-11 Piotr Wilczekexynos:clock: Add i2c clock
2012-12-11 Marek Vasutmxs: i2c: Implement algorithm to set up arbitrary i2c...
2012-12-10 Nikita Kiryanovgpio: add gpio_is_valid() to omap_gpio API
2012-12-10 Davide Bonfantidavinci: fixed cpu reset
2012-12-10 Lokesh Vutlaomap: emif: configure emif only when required
2012-12-10 Robert P. J. DayOMAP: Tweak omap-common/Makefile since reset.S -> reset.c
2012-12-10 Robert P. J. Dayomap4: Add comments on some "#endif"s for readability.
2012-12-10 Robert P. J. Dayomap3: Add a few comments to "#endif"s for readability.
2012-12-10 Peter BaradaPass sdrc timing values through board_sdrc_timings...
2012-12-10 Mansoor Ahamedam33xx: add ELM support
2012-12-10 Ilya Yanokam33xx: NAND support
2012-12-10 Ilya YanokOMAP: include sys_proto.h from boot-common
2012-12-10 Andreas Bießmannomap3/mem.c: remove unused defines
2012-12-10 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot into...
2012-12-08 Daniel SchwierzeckMIPS: constify address pointer in test_bit()
2012-12-08 Zhi-zhou ZhangMIPS: fix a latent bug on initialize $gp
2012-12-08 Stefano BabicMerge branch 'master' of git://git.denx.de/u-boot into...
2012-12-07 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-x86
2012-12-07 Otavio Salvadormxs: SPL: Generalize memory initialization
2012-12-06 Simon Glassx86: Build vga video code only if CONFIG_VIDEO_VGA...
2012-12-06 Simon Glassx86: Remove video_init() prototype from u-boot-x86.h
2012-12-06 Stefan Reinauerx86: drop unused code in coreboot.c
2012-12-06 Stefan Reinauerx86: Remove coreboot_ from file name
2012-12-06 Vadim Bendeburyx86: Provide a way to throttle port80 accesses
2012-12-06 Vadim Bendeburyx86: Provide tick counter and frequency reference for...
2012-12-06 Duncan Lauriex86: Issue SMI to finalize Coreboot in final stage
2012-12-06 Duncan Lauriex86: Fix MTRR clear to detect which MTRR to use
2012-12-06 Stefan Reinauerx86: Emit port 80 post codes in show_boot_progress()
2012-12-06 Simon Glassx86: fdt: Create basic .dtsi file for coreboot
2012-12-06 Gabe Blackx86: coreboot: Set CONFIG_ARCH_DEVICE_TREE correctly
2012-12-06 Gabe Blackx86: Add support for CONFIG_OF_CONTROL
2012-12-06 Stefan Reinauerx86: Add CONFIG_DELAY_ENVIRONMENT to delay environment...
2012-12-06 Gabe Blackx86: Add back cold- and warm-boot flags
2012-12-06 Gabe Blackx86: Override calculate_relocation_address to use the...
2012-12-06 Gabe Blackx86: Make calculate_relocation_address an overridable...
2012-12-06 Gabe Blackx86: Make the upper bound on relocated symbols closed...
2012-12-06 Gabe Blackx86: Reorder x86's post relocation memory layout
2012-12-06 Gabe Blackx86: Initialise SPI if enabled
2012-12-06 Gabe Blackx86: Implement arch_phys_memset so that it can wipe...
2012-12-06 Gabe Blackx86: Increase the size of the phys_size_t and phys_addr...
2012-12-06 Duncan Lauriex86: Fix off-by-one error in do_elf_reloc_fixups()
2012-12-06 Duncan Lauriex86: Ignore memory >4GB when parsing Coreboot tables
2012-12-06 Simon Glassx86: Fix indirect jmp warning in zimage.c
2012-12-06 Stefan Reinauerx86: Clean up MTRR 7 right before jumping to the kernel
2012-12-06 Graeme Russx86: Import MSR/MTRR code from Linux
2012-12-06 Stefan Reinauerx86: Provide a function to clean up just before booting...
2012-12-06 Stefan Reinauerx86: Add basic cache operations
2012-12-06 Gabe Blackx86: Fill in the dram info using the e820 map on corebo...
2012-12-06 Vadim Bendeburyx86: Add a CBMEM timestamp generated right before the...
2012-12-06 Vadim Bendeburyx86: Enable coreboot timestamp facility support in...
2012-12-06 Vadim Bendeburyx86: Add function to read time stamp counter
2012-12-06 Bill Richardsonx86: gpio: Add GPIO driver for Intel ICH6 and later.
2012-12-05 Stefan Roesempc5200: Add SPL support
2012-12-05 Stefan RoeseSPL: Port SPL framework to powerpc
2012-12-05 Stefan Roesepowerpc: Extract EPAPR_MAGIC constants into processor.h
2012-12-04 Marek Vasutmxs: Staticize SPL functions
2012-12-04 Marek Vasutmxs: Properly setup VDDD in power supply setup code
2012-12-04 Marek Vasutmxs: Implement common function to setup VDDx
2012-12-04 Marek Vasutmx28: Rename regs-power.h to regs-power-mx28.h
2012-12-04 Marek Vasutmx28: Remove SET, CLR, TOG ops from PLLxCTRL1 registers
2012-12-03 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-x86
2012-11-30 Stefan Reinauerx86: Don't spam POST80 codes with slow IO functions
2012-11-30 Stefan Reinauerx86: Fix typo in pcat_timer.c
2012-11-30 Gabe Blackx86: Include types.h explicitly in the i386 version...
2012-11-30 Gabe Blackx86: Add a dummy implementation for timer_get_us
2012-11-30 Gabe Blackx86: Add a default implementation for cleanup_before_li...
2012-11-30 Gabe Blackx86: Add an fdt pointer to the global data structure
2012-11-30 Gabe Blackx86: Allow compiling out realmode/bios code
2012-11-30 Simon Glassx86: coreboot: Decode additional coreboot sysinfo tags
2012-11-30 Stefan Reinauerx86: coreboot: Drop sysinfo.c
2012-11-30 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-sh
2012-11-30 Yoshihiro Shimodash: fix trigger_address_error()
2012-11-29 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-fdt
2012-11-28 Tom RiniMerge branch 'master' of git://www.denx.de/git/u-boot-x86
2012-11-28 Gabe Blackx86: coreboot: Implement recursively scanning PCI busses
2012-11-28 Gabe Blackx86: coreboot: Tell u-boot about PCI bus 0 when initial...
2012-11-28 Stefan Reinauerx86: coreboot: Move non-board specific files to coreboo...
2012-11-28 Gabe Blackx86: Add some missing includes
2012-11-28 Gabe Blackx86: Allow excluding reset vector code from u-boot
2012-11-28 Simon Glassx86: Add initial memory barrier macros
2012-11-28 Graeme Russx86: Add ilog2 to bitops
2012-11-28 Graeme Russx86: Remove duplicate PCI init
2012-11-28 Graeme Russx86: Put global data on the stack
2012-11-28 Graeme Russx86: Forward declare gd_t
2012-11-28 Tom RiniMerge branch 'master' of git://www.denx.de/git/u-boot...
2012-11-28 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-mips
next