Allow newlines within command environment vars
[glsdk/glsdk-u-boot.git] / common / main.c
2012-08-09 Simon GlassAllow newlines within command environment vars
2012-08-09 Simon GlassAdd run_command_list() to run a list of commands
2012-05-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-usb
2012-05-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-nand...
2012-05-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-net
2012-05-15 Joe Hershbergernet: cosmetic: net.c checkpatch compliance
2012-04-30 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-blackfin
2012-04-30 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-nds32
2012-04-29 Wolfgang DenkMerge branch 'marex@denx.de' of git://git.denx.de/u...
2012-04-23 Timo KetolaFix the behaviour of the 'run' command
2012-04-09 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-nios
2012-03-06 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-x86
2012-03-06 Simon GlassConvert cmd_usage() calls in common to use a return...
2012-03-06 Simon GlassAdd cmd_process() to process commands in one place
2012-03-06 Simon GlassCreate a single cmd_call() function to handle command...
2012-03-06 Simon GlassDon't include standard parser if hush is used
2012-03-06 Simon GlassStop using builtin_run_command()
2012-03-06 Simon GlassRename run_command2() to run_command()
2012-03-06 Simon GlassRename run_command() to builtin_run_command()
2012-03-06 Simon GlassRemove CMD_PXE's static on run_command()
2012-02-17 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-x86
2012-02-13 Wolfgang DenkMerge branch 'sf' of git://git.denx.de/u-boot-blackfin
2012-02-13 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-blackfin
2012-02-12 Heiko Schochercommon, menu: show menu on startup if CONFIG_MENU_SHOW...
2012-02-12 Heiko Schochercommon: add possibility for readline_into_buffer timeout
2011-10-21 Wolfgang DenkMerge branch 'master' of /home/wd/git/u-boot/master
2011-10-17 Jason HobbsAdd pxe command
2011-10-17 Jason HobbsReplace space and tab checks with isblank
2011-10-17 Jason Hobbscosmetic: remove unneeded curly braces
2011-10-17 Jason Hobbscommon: add run_command2 for running simple or hush...
2011-10-17 Jason Hobbscommon, menu: use abortboot for menu timeout
2011-08-04 Albert ARIBAUDMerge commit '7b2fac7654f7420c2787f74ec3b1540fa3b343e9'
2011-08-02 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-ppc4xx
2011-08-02 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-blackfin
2011-07-28 Andreas Bießmannunify version_string
2011-07-26 Andreas Pretzschautomatic update from FIT image: add optional address...
2011-07-25 Jason Hobbscosmetic, main: correct indentation/spacing issues
2011-07-25 Jason Hobbscosmetic, main: clean up declarations of abortboot
2011-06-23 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-arm
2011-06-22 Wolfgang DenkARM: drop unsupported 'trab' board
2011-01-09 Mike Frysingercmd editing: mark erase/tab seqs constant
2010-12-22 Wolfgang DenkMerge branch 'next' of ../next
2010-12-16 Wolfgang DenkMerge branch 'master' of ../master into next
2010-11-28 Mike Frysingerautocomplete: remove runtime handler install
2010-11-28 Mike Frysingerdo_reset: unify duplicate prototypes
2010-11-28 Mike Frysingerdo_bootd: unify duplicate prototypes
2010-10-17 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-imx
2010-10-11 Wolfgang DenkMerge branch 'at91' of git://git.denx.de/u-boot-atmel
2010-10-11 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-imx
2010-10-11 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-x86
2010-10-11 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-mpc85xx
2010-10-11 Wolfgang DenkMerge branch 'sf' of git://git.denx.de/u-boot-blackfin
2010-10-06 Peter TyserReplace MAX_CMDBUF_SIZE references with CONFIG_SYS_CBSIZE
2010-09-07 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-samsung
2010-08-10 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-marvell
2010-08-10 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-ti
2010-08-10 Wolfgang DenkMerge branch 'master' of ../master
2010-08-08 Mike Frysingercmd editing: optimize/shrink output blanking
2010-08-03 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-samsung
2010-08-03 Wolfgang DenkMerge branch 'master' of /home/wd/git/u-boot/master
2010-07-24 Wolfgang Denkcmd_usage(): simplify return code handling
2010-07-06 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot
2010-07-04 Wolfgang DenkMake sure that argv[] argument pointers are not modified.
2010-06-30 Wolfgang DenkMerge branch 'master' of ssh://gemini/home/wd/git/u...
2010-06-29 Wolfgang DenkMerge branch 'master' into next
2010-06-29 Wolfgang DenkMerge branch 'next' of git://git.denx.de/u-boot-ti...
2010-06-29 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-sh...
2010-06-23 Wolfgang DenkRemove AmigaOneG3SE board
2010-04-19 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot-arm
2010-04-10 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-blackfin
2010-04-10 Jens ScharsigFIX: watchdog timeout, while waiting for input
2010-04-01 Wolfgang DenkMerge branch 'next'
2010-03-29 Wolfgang DenkMerge remote branch 'origin/master' into next
2010-03-23 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot-arm
2010-03-22 Wolfgang DenkMerge remote branch 'origin/master' into next
2010-03-21 Wolfgang DenkMerge remote branch 'origin/master' into next
2010-03-21 John Schmollercmd history: Match history buffer size to console buffer
2010-03-21 John Schmollerconsole: Fix console buffer overrun
2010-03-11 Wolfgang DenkMove CONFIG_UPDATE_TFTP code after CONFIG_PREBOOT
2009-11-09 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot-arm
2009-10-28 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-sparc
2009-10-27 Peter Tyserreadline(): Add ability to modify a string buffer
2009-10-27 Peter Tysercread_line(): Remove unused variables
2009-10-27 Peter TyserCheck for NULL prompt in readline_into_buffer()
2009-05-15 Emil MedveRemove inline qualifier from show_boot_progress()
2009-02-23 Haavard SkinnemoenMerge branch 'mimc200' into next
2009-02-23 Haavard SkinnemoenMerge branch 'cleanups' into next
2009-02-01 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-arm
2009-02-01 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-net
2009-01-28 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-nand...
2009-01-28 Peter TyserStandardize command usage messages with cmd_usage()
2009-01-25 Ben WarrenMerge git://git.denx.de/u-boot into u-boot
2009-01-24 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-mpc85xx
2009-01-24 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-mpc83xx
2009-01-24 Peter Korsgaardcommon/main: support bootdelay=0 for CONFIG_AUTOBOOT_KEYED
2008-12-17 Haavard SkinnemoenMerge branch 'fixes' into cleanups
2008-10-21 Stefan RoeseMerge branch 'master' of /home/stefan/git/u-boot/u...
2008-10-21 Markus KlotzbuecherMerge git://git.denx.de/u-boot into x1
2008-10-18 Wolfgang DenkMerge 'next' branch
2008-10-18 Jean-Christophe... rename CFG_ macros to CONFIG_SYS
next