]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/history - common
sf: Place the sf calls in proper order
[glsdk/glsdk-u-boot.git] / common /
2013-05-10 SRICHARAN RARM: OMAP: Cleanup boot parameters usage
2013-04-18 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm...
2013-04-17 Jaehoon Chungmmc: support the correct card version for eMMC
2013-04-17 Maxime Larocqueprintenv: Correct out-of-memory condition check.
2013-04-16 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-x86
2013-04-16 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2013-04-15 Simon Glassx86: Allow setup code to manage its own global data
2013-04-15 Simon Glassx86: Fix DRAM bank size init with generic board
2013-04-15 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2013-04-15 Tom RiniMerge branch 'tpm' of git://git.denx.de/u-boot-x86
2013-04-14 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-04-14 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-04-13 Albert ARIBAUDMerge branch 'u-boot-ti/master' into 'u-boot-arm/master'
2013-04-12 Che-liang Chioutpm: Add TPM command library
2013-04-12 Albert ARIBAUDMerge branch 'u-boot/master' into 'u-boot-arm/master'
2013-04-11 Joe Hershbergerenv: Add redundant env support to UBI env
2013-04-11 Joe Hershbergerenv: Add support for UBI environment
2013-04-11 Joe Hershbergermtd: Make mtdparts work with pre-reloc env
2013-04-11 Joe Hershbergerubi: ubifs: Turn off verbose prints
2013-04-11 Joe Hershbergerubi: Expose a few simple functions from the cmd_ubi
2013-04-11 Vadim BendeburyDo not call board_early_init_f() twice
2013-04-11 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-usb
2013-04-10 Tom Rinicmd_nand.c: Fix CONFIG_CMD_NAND_YAFFS
2013-04-10 Tom Rininand: Extend nand_(read|write)_skip_bad with *actual...
2013-04-08 Tom RiniMerge branch 'patman' of git://git.denx.de/u-boot-x86
2013-04-08 Mingkai Hucmd_sf: include header file common.h before div64.h
2013-04-08 York Suncommon/cmd_test: Avoid macro expansion
2013-04-05 Tom RiniRevert "env: fix potential stack overflow in environmen...
2013-04-04 Tom RiniMerge branch 'master' of git://www.denx.de/git/u-boot...
2013-04-04 Albert ARIBAUDMerge branch 'u-boot-samsung/master' into 'u-boot-arm...
2013-04-04 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-04-02 Stephen Warrenmmc: don't allow extra cmdline arguments
2013-04-02 Rob Herringenv: fix potential stack overflow in environment functions
2013-04-01 York SunConsolidate bool type
2013-03-31 Tom RiniMerge branch 'agust@denx.de' of git://git.denx.de/u...
2013-03-29 Anatolij Gustschinvideo: bcm2835: fix build issues
2013-03-29 Anatolij GustschinMerge branch 'for-v2013.04'
2013-03-29 Akshay Saraswatgen: Add sha h/w acceleration to hash
2013-03-29 Pali RohárNew command bootmenu: ANSI terminal boot menu support
2013-03-29 Anatolij Gustschinmenu: export menu_default_choice() function
2013-03-29 Pali Rohármenu: Add support for user defined item choice function
2013-03-28 Albert ARIBAUDMerge branch 'u-boot/master' into 'u-boot-arm/master'
2013-03-27 Steven Stallionimage: Add support for Plan 9
2013-03-27 Tom Rinicmd_ext4: BREAK and correct ext4write parameter order
2013-03-27 Tom Rinienv_callback: Mark find_env_callback as static
2013-03-26 Albert ARIBAUDMerge branch 'u-boot-tegra/master' into 'u-boot-arm...
2013-03-26 Albert ARIBAUDMerge branch 'u-boot-samsung/master' into 'u-boot-arm...
2013-03-21 Andre RenaudFix bitmap offsets for non 8-bit LCDs
2013-03-21 Jeroen Hofsteecommon/lcd.c: move the macro's to the c file
2013-03-21 Jeroen Hofsteecommon/lcd: cosmetic: clean up a bit
2013-03-21 Jeroen Hofsteecommon/lcd.c: remove global lcd_base
2013-03-21 Jeroen Hofsteecommon/lcd.c: cleanup use of global variables
2013-03-21 Wolfgang Denkcommon/lcd.c: cleanup use of global variables
2013-03-20 Tom RiniMerge branch 'spi' of git://git.denx.de/u-boot-x86
2013-03-20 Stephen Warrenlcd: calculate line_length after lcd_ctrl_init()
2013-03-19 Simon Glasssf: Use unsigned type for buffers
2013-03-18 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-usb
2013-03-18 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2013-03-18 Lukasz Majewskiusb:gadget: USB Mass Storage Gadget support
2013-03-16 Pantelis Antonioudfu: Fix crash when wrong number of arguments given
2013-03-16 Pantelis Antonioudfu: Only perform DFU board_usb_init() for TRATS
2013-03-15 Simon Glassx86: Enable generic board support
2013-03-15 Simon Glassx86: Adjust board_r.c for x86
2013-03-15 Simon Glassx86: Adjust board_f.c for x86
2013-03-15 Simon GlassAdjust board_r.c for ppc
2013-03-15 Simon GlassAdjust board_f.c for ppc
2013-03-15 Simon GlassAdd CONFIG_SYS_SYM_OFFSETS to support offset symbols
2013-03-15 Simon GlassAdd spl load feature
2013-03-15 Simon GlassIntroduce generic post-relocation board_r.c
2013-03-15 Simon GlassIntroduce generic pre-relocation board_f.c
2013-03-15 Albert ARIBAUDMerge branch 'u-boot-tegra/master' into 'u-boot-arm...
2013-03-15 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-03-12 Albert ARIBAUDRefactor linker-generated arrays
2013-03-12 Tom Rinicmd_mem.c: Fix warning when CONFIG_CMD_MEMTEST is not set
2013-03-12 Joe HershbergerCONFIG_BOOTDELAY default should not affect runtime
2013-03-12 Barak Wasserstromcommon/main: move set_working_fdt_addr to enable usage...
2013-03-12 Wolfgang Denkenv: fix "env ask" command
2013-03-12 Tom Rinicmd_fat.c: Note in fatread help about alignment require...
2013-03-12 Albert ARIBAUDMerge branch 'u-boot-atmel/master' into 'u-boot-arm...
2013-03-12 Akshay SaraswatTMU: Add TMU support in dtt command
2013-03-11 Robert P. J. Daycmd_df.c: Delete this clearly unused source file.
2013-03-11 Robert P. J. Daycmd_mtdparts.c: Correct "reseting" to "resetting" in...
2013-03-11 Joe HershbergerAllow u-boot to be silent without forcing Linux to be
2013-03-11 Stephen Warrencmd_part: don't print cmd name twice in help
2013-03-11 Wolfgang DenkFeature Removal: disable "mtest" command by default
2013-03-11 Tom RiniMerge u-boot/master into u-boot-ti/master
2013-03-11 Nikita Kiryanovlcd: implement a callback for splashimage
2013-03-11 Enric Balletbo i... SPL: ONENAND: Support SPL to boot u-boot from OneNAND.
2013-03-08 Nikita Kiryanovlcd: add option for board specific splash screen prepar...
2013-03-08 Nikita Kiryanovmmc: add support for write protection
2013-03-07 Otavio Salvadorled: Use STATUS_LED_ON and STATUS_LED_OFF when calling...
2013-03-05 Stefano BabicMerge branch 'master' of git://git.denx.de/u-boot-arm
2013-03-04 Daniel Schwierzeckbootm: fix conditional compilation for bootm ramdisk...
2013-03-04 Joe Hershbergerenv: Avoid clobbering an edited variable on ctrl-c
2013-03-04 Simon Glasssandbox: Add 'sb' command to access filesystem features
2013-03-04 Tom RiniMerge branch 'mem' of git://git.denx.de/u-boot-x86
2013-03-04 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-blackfin
2013-03-04 Sonic Zhangblackfin: bf60x: Port blackfin core architecture code...
2013-03-01 Stefano BabicSPL: Change description for spl command
2013-03-01 Simon Glasshash: Use lower case for hash algorithm names
next