HACK: ARM: DRA7xx: Add Ethernet crossbar setting
[glsdk/glsdk-u-boot.git] / net /
2013-03-26 Albert ARIBAUDMerge branch 'u-boot-samsung/master' into 'u-boot-arm...
2013-03-15 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-03-12 Albert ARIBAUDMerge branch 'u-boot-atmel/master' into 'u-boot-arm...
2013-03-11 Tom RiniMerge u-boot/master into u-boot-ti/master
2013-03-04 Tom RiniMerge branch 'mem' of git://git.denx.de/u-boot-x86
2013-03-01 Simon Glassnet: Use new numeric setenv functions
2013-01-17 Kim PhillipsMerge remote-tracking branch 'mpc83xx/next'
2013-01-09 Albert ARIBAUDMerge 'u-boot-atmel/master' into 'u-boot-arm/master'
2013-01-08 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-01-08 Albert ARIBAUDMerge branch 'u-boot-ti/master' into 'u-boot-arm/master'
2012-12-22 Albert ARIBAUDMerge samsung, imx, tegra into u-boot-arm/master
2012-12-21 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-usb
2012-12-19 Allen MartinMerge remote-tracking branch 'u-boot/master' into u...
2012-12-18 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-net
2012-12-15 Joe Hershbergernet: Fix endianness bug in link-local
2012-12-15 Simon Glassnet: Add tftp speed indication
2012-12-14 Scott WoodMerge remote-tracking branch 'origin/master'
2012-12-13 Joe Hershbergerenv: Add a bootfile env handler
2012-12-13 Joe Hershbergerenv: Use getenv_yesno() more generally
2012-11-10 Stefano BabicMerge git://git.denx.de/u-boot
2012-11-05 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-avr32
2012-11-05 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2012-11-04 Kim Phillipsnet/: sparse fixes
2012-10-15 Tom RiniMerge branch 'agust@denx.de-next' of git://git.denx...
2012-10-05 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2012-10-04 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-arm
2012-10-03 Joe Hershbergernet: fix netconsole filtering
2012-10-01 Ilya YanokOMAP: networking support for SPL
2012-10-01 Ilya Yanoknet/bootp: add VCI support for BOOTP also
2012-09-30 Albert ARIBAUDMerge remote-tracking branch 'u-boot/master'
2012-09-27 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-net
2012-09-27 Brian Rzyckinet: Quietly ignore DHCP Option 28 (Broadcast Address)
2012-09-27 Benoît Thébaudeaunet: eth_write_hwaddr: Return error for invalid MACs
2012-09-24 Joe Hershbergernet: Filter incoming netconsole packets by IP
2012-09-24 Joe Hershbergernet: Improve the speed of netconsole
2012-09-24 Tetsuyuki Kobayashinet: bugfix: NetSetTimeout assumes CONFIG_SYS_HZ=1000
2012-09-24 Michael Walleapi: net: fix length check in eth_receive()
2012-07-31 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-micro...
2012-07-30 Wolfgang DenkMerge branch 'next' of git://git.denx.de/u-boot
2012-07-24 Joe Hershbergernet: Make sure the ethaddr is updated in net_init()
2012-07-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-usb
2012-07-20 Wolfgang DenkMerge branch 'sf' of git://git.denx.de/u-boot-blackfin
2012-07-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-net
2012-07-19 benoit.thebaudeau... net: link_local: fix build
2012-07-19 benoit.thebaudeau... net: bootp: fix build
2012-07-18 Wolfgang DenkMerge branch 'next' of git://git.denx.de/u-boot-video
2012-07-12 Tetsuyuki Kobayashinet: nfs: make NFS_TIMEOUT configurable
2012-07-12 Wolfgang DenkMerge branch 'next' of git://git.denx.de/u-boot-net...
2012-07-12 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-i2c
2012-07-11 Joe Hershbergernet: Inline the new eth_setenv_enetaddr_by_index function
2012-07-11 Rob Herringnet: allow setting env enetaddr from net device setting
2012-07-11 Jayachandran Chand... net: tftp: fix type of block arg to store_block
2012-07-10 Mike Frysingernet: fix typo in arp clean up
2012-07-10 Wolfgang DenkMinor Coding Style cleanup
2012-07-08 Kim Phillipsnet: make net_rand.h inclusion depend on BOOTP_RANDOM_DELAY
2012-07-08 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-arm
2012-07-07 Michael Wallenet: add helper to generate random mac address
2012-07-07 Michael Wallenet: use common rand()/srand() functions
2012-05-23 Joe Hershbergernet: Allow filtering on debug traces in the net subsystem
2012-05-23 Joe Hershbergernet: Work-around for brain-damaged Cisco equipment...
2012-05-23 Joe Hershbergernet: Add link-local addressing support
2012-05-23 Joe Hershbergernet: Separate ArpRequest() into lower-level func
2012-05-23 Joe Hershbergernet: Don't copy every packet that waits for an ARP
2012-05-23 Joe Hershbergernet: Fix net buffer initialization
2012-05-23 Joe Hershbergernet: Remove unused parameter from NetInitLoop()
2012-05-23 Joe Hershbergernet: Remove static allocation for MAC address in PingSend()
2012-05-23 Joe Hershbergernet: Add option CONFIG_BOOTP_MAY_FAIL
2012-05-23 Joe Hershbergernet: Fix unused variable compile warning
2012-05-23 Joe Hershbergernet: Add net_update_ether() to handle ARP and Ping...
2012-05-23 Joe Hershbergernet: Refactor to separate the UDP handler from the...
2012-05-23 Joe Hershbergernet: Refactor to protect access to the NetState variable
2012-05-23 Joe Hershbergernet: Refactor to use NetSendPacket instead of eth_send...
2012-05-23 Joe Hershbergernet: Refactor ping receive handler
2012-05-23 Joe Hershbergernet: Move debug trace to point of action
2012-05-23 Joe Hershbergernet: Refactor bootp packet length computations
2012-05-23 Joe Hershbergernet: Refactor packet length computations
2012-05-23 Joe Hershbergernet: Refactor NetSendUDPPacket to share more code
2012-05-23 Joe Hershbergernet: Refactor IP, UPD, and ICMP header writing functions
2012-05-23 Joe Hershbergernet: cosmetic: Replace magic numbers in arp.c with...
2012-05-23 Joe Hershbergernet: cosmetic: Rename tmp to reply_ip_addr in arp.c
2012-05-23 Joe Hershbergernet: cosmetic: Alphabetize includes in net.c
2012-05-23 Joe Hershbergernet: cosmetic: Rename OPT_SIZE to OPT_FIELD_SIZE
2012-05-23 Joe Hershbergernet: cosmetic: Rename CDPHandler to cdp_receive
2012-05-23 Joe Hershbergernet: cosmetic: Rename "x" to "eth_proto"
2012-05-23 Joe Hershbergernet: cosmetic: Add a more explicit comment about 802.2
2012-05-23 Joe Hershbergernet: cosmetic: Rename parameter len to payload_len
2012-05-23 Joe Hershbergernet: cosmetic: Un-typedef ICMP_t
2012-05-23 Joe Hershbergernet: cosmetic: Un-typedef ARP_t
2012-05-23 Joe Hershbergernet: cosmetic: Un-typedef VLAN_Ethernet_t
2012-05-23 Joe Hershbergernet: cosmetic: Un-typedef Ethernet_t
2012-05-23 Joe Hershbergernet: cosmetic: Split struct ip_udp_hdr into ip_hdr
2012-05-23 Joe Hershbergernet: cosmetic: Un-typedef IP_t
2012-05-23 Joe Hershbergernet: Move RARP receive logic out of net.c
2012-05-23 Joe Hershbergernet: Move PING out of net.c
2012-05-23 Joe Hershbergernet: Move ARP out of net.c
2012-05-23 Joe Hershbergernet: Encapsulate CDP packet identification
2012-05-23 Joe Hershbergernet: Move CDP out of net.c
2012-05-23 Joe Hershbergernet: Move MAC-seeded rand out of bootp.c
2012-05-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-usb
2012-05-20 Wolfgang DenkMerge branch 'master' of git://git.denx.de/u-boot-nand...
next