Merge branch 'u-boot/master' into 'u-boot-arm/master'
Conflicts:
drivers/video/exynos_fb.c
Conflicts:
drivers/video/exynos_fb.c
arm/km: add support for kmsuv31 board
This board is from a u-boot point of view a mixture between kmnusa and
a standard km_kirkwood board. We have our u-boot environment in the spi
NOR flash, but we have a direct connection between the kirkwood and the
piggy. A FPGA is connected via the PCIe interface. So we only have to
select the specific features in the board setup.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-By: Prafulla Wadaskar <prafulla@marvell.com>
This board is from a u-boot point of view a mixture between kmnusa and
a standard km_kirkwood board. We have our u-boot environment in the spi
NOR flash, but we have a direct connection between the kirkwood and the
piggy. A FPGA is connected via the PCIe interface. So we only have to
select the specific features in the board setup.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-By: Prafulla Wadaskar <prafulla@marvell.com>
arm/km: use CONFIG_NAND_ECC_BCH
Switch from 1-bit ecc to 4-bit ecc.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-By: Prafulla Wadaskar <prafulla@marvell.com>
Switch from 1-bit ecc to 4-bit ecc.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-By: Prafulla Wadaskar <prafulla@marvell.com>
arm/km: rename BOARD_LATE_INIT to CONFIG_BOARD_LATE_INIT
commit 9660e442 cosmetic: s/BOARD_LATE_INIT/CONFIG_BOARD_LATE_INIT
removes BOARD_LATE_INIT and uses CONFIG_BOARD_LATE_INIT instead.
Therefore we have to use this define.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <prafulla@marvell.com>
commit 9660e442 cosmetic: s/BOARD_LATE_INIT/CONFIG_BOARD_LATE_INIT
removes BOARD_LATE_INIT and uses CONFIG_BOARD_LATE_INIT instead.
Therefore we have to use this define.
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <prafulla@marvell.com>
kirkwood_nand: allow usage of NAND_ECC_SOFT_BCH
If CONFIG_NAND_ECC_BCH is set use 4-bit error correction code instead of
the 1-bit error correction code on the NAND device.
Signed-off-by: Gerlando Falauto <gerlando.falauto@keymile.com>
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Scott Wood <scottwood@freescale.com>
If CONFIG_NAND_ECC_BCH is set use 4-bit error correction code instead of
the 1-bit error correction code on the NAND device.
Signed-off-by: Gerlando Falauto <gerlando.falauto@keymile.com>
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Merge branch 'u-boot-ti/master' into 'u-boot-arm/master'
mx31pdk: Remove watchdog support
The conversion of mx31pdk to SPL NAND fixed the boot issue, but we start seeing
resets in loop, which prevents us from reaching the U-boot prompt.
Until the proper fix can be identified, disable watchdog, so that mx31pdk
can be functional again.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Stefano Babic <sbabic@denx.de>
The conversion of mx31pdk to SPL NAND fixed the boot issue, but we start seeing
resets in loop, which prevents us from reaching the U-boot prompt.
Until the proper fix can be identified, disable watchdog, so that mx31pdk
can be functional again.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Stefano Babic <sbabic@denx.de>
arm: Make all linker scripts compatible with per-symbol sections
Let all ARM linker scripts handle properly -ffunction-sections
and -fdata-sections. This will be useful for future changes in order to create
symbol-specific sections in common .S files.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Let all ARM linker scripts handle properly -ffunction-sections
and -fdata-sections. This will be useful for future changes in order to create
symbol-specific sections in common .S files.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm1176: Remove unused MMU setup from start.S
Following the removal of the smdk6400 board, the MMU setup code in
arm1176/start.S becomes unused, so remove it. It will still be possible to
restore it later from the Git history if necessary, in which case it should be
moved out of the relocate_code() function.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Following the removal of the smdk6400 board, the MMU setup code in
arm1176/start.S becomes unused, so remove it. It will still be possible to
restore it later from the Git history if necessary, in which case it should be
moved out of the relocate_code() function.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: Remove deprecated and now unused NAND SPL
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: Remove support for unused s3c64xx
Following the removal of the smdk6400 board, the s3c64xx SoC becomes unused, so
remove associated code. It will still be possible to restore it later from the
Git history if necessary.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Following the removal of the smdk6400 board, the s3c64xx SoC becomes unused, so
remove associated code. It will still be possible to restore it later from the
Git history if necessary.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Revert "mkconfig: start deprecating Makefile config targets"
This reverts commit 1285a2808a254f3d1a809c1a541f0c0f746e03d7 since the migration
of boards from Makefile to boards.cfg is now complete.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
This reverts commit 1285a2808a254f3d1a809c1a541f0c0f746e03d7 since the migration
of boards from Makefile to boards.cfg is now complete.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: Remove support for smdk6400
The migration of boards from Makefile to boards.cfg was due for v2012.03, but
smdk6400 did not follow, and it does not build, so move it to scrapyard. It will
still be possible to restore it from the Git history before fixing it.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
The migration of boards from Makefile to boards.cfg was due for v2012.03, but
smdk6400 did not follow, and it does not build, so move it to scrapyard. It will
still be possible to restore it from the Git history before fixing it.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
imx: Add u-boot-with-nand-spl.imx make target
This image combines the SPL with the i.MX header, the FCB and U-Boot.
For i.MX25/35/51, the FCB is ignored by the boot ROM, so this image is just
useful because it can be programmed on a NAND Flash page boundary.
For i.MX53, the FCB is required by the boot ROM.
This does not support i.MX6 so far because its FCB is more complicated.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
This image combines the SPL with the i.MX header, the FCB and U-Boot.
For i.MX25/35/51, the FCB is ignored by the boot ROM, so this image is just
useful because it can be programmed on a NAND Flash page boundary.
For i.MX53, the FCB is required by the boot ROM.
This does not support i.MX6 so far because its FCB is more complicated.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
imx: Add u-boot-with-spl.imx make target
This image combines the SPL with the i.MX header and U-Boot. This is a
convenient way of having a single image to program on some boot devices.
The i.MX header has to be added to the SPL before appending U-Boot, so that the
boot ROM loads only the SPL.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
This image combines the SPL with the i.MX header and U-Boot. This is a
convenient way of having a single image to program on some boot devices.
The i.MX header has to be added to the SPL before appending U-Boot, so that the
boot ROM loads only the SPL.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
.gitignore: Add /SPL
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Makefile: Move SHELL setup to config.mk
make never uses the SHELL variable from the environment. Instead, it
uses /bin/sh, or the value assigned to the SHELL variable by the Makefile. This
makes the export of the SHELL variable useless for sub-makes (but still useful
for the environment of recipes). However, we want all makes to use the same
shell.
This patch fixes this issue by moving the SHELL variable setup and export to the
top config.mk, so that all Makefile-s including it use the same shell.
Since BASH is used by default, this makes it possible to use things
like 'echo -e ...' in sub-makes, which would otherwise fail e.g. with /bin/sh
symlinked to /bin/dash on Ubuntu.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
make never uses the SHELL variable from the environment. Instead, it
uses /bin/sh, or the value assigned to the SHELL variable by the Makefile. This
makes the export of the SHELL variable useless for sub-makes (but still useful
for the environment of recipes). However, we want all makes to use the same
shell.
This patch fixes this issue by moving the SHELL variable setup and export to the
top config.mk, so that all Makefile-s including it use the same shell.
Since BASH is used by default, this makes it possible to use things
like 'echo -e ...' in sub-makes, which would otherwise fail e.g. with /bin/sh
symlinked to /bin/dash on Ubuntu.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
arm: Remove unused relocate_code() parameters
Commit e05e5de7fae5bec79617e113916dac6631251156 made the 2 1st parameters of
ARM's relocate_code() useless since it moved the code handling them to crt0.S.
So, drop these parameters.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Commit e05e5de7fae5bec79617e113916dac6631251156 made the 2 1st parameters of
ARM's relocate_code() useless since it moved the code handling them to crt0.S.
So, drop these parameters.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm926ejs: Remove deprecated and now unused NAND SPL
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
nand: mxc: Switch NAND SPL to generic SPL
This also fixes support for mx31pdk and tx25, which had been broken by commit
e05e5de7fae5bec79617e113916dac6631251156.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
This also fixes support for mx31pdk and tx25, which had been broken by commit
e05e5de7fae5bec79617e113916dac6631251156.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
imx: Fix automatic make targets for imx images
Automatically build the 'u-boot.imx' (i.e. imx header + u-boot.bin) and 'SPL'
(i.e. imx header + u-boot-spl.bin) make targets for all imx processors
supporting this header, so for arm926ejs, arm1136 and armv7. Some combinations
were missing.
At the same time, fix the build of SPL targets not supporting the imx header on
arm1136. For arm1136, the 'SPL' make target was forced to build in all cases if
CONFIG_SPL_BUILD was defined, even for non-imx platforms or imx setups without
an imx header.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Automatically build the 'u-boot.imx' (i.e. imx header + u-boot.bin) and 'SPL'
(i.e. imx header + u-boot-spl.bin) make targets for all imx processors
supporting this header, so for arm926ejs, arm1136 and armv7. Some combinations
were missing.
At the same time, fix the build of SPL targets not supporting the imx header on
arm1136. For arm1136, the 'SPL' make target was forced to build in all cases if
CONFIG_SPL_BUILD was defined, even for non-imx platforms or imx setups without
an imx header.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Makefile: Change CONFIG_SPL_PAD_TO to image offset
Change CONFIG_SPL_PAD_TO from a link address to an image offset since this is
more handy and closer to the purpose of this config.
Automatically define CONFIG_SPL_PAD_TO to CONFIG_SPL_MAX_SIZE (or 0 without
CONFIG_SPL_MAX_SIZE).
Test that CONFIG_SPL_PAD_TO >= CONFIG_SPL_MAX_SIZE if CONFIG_SPL_PAD_TO is
non-zero.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Change CONFIG_SPL_PAD_TO from a link address to an image offset since this is
more handy and closer to the purpose of this config.
Automatically define CONFIG_SPL_PAD_TO to CONFIG_SPL_MAX_SIZE (or 0 without
CONFIG_SPL_MAX_SIZE).
Test that CONFIG_SPL_PAD_TO >= CONFIG_SPL_MAX_SIZE if CONFIG_SPL_PAD_TO is
non-zero.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
autoconfig.mk: Make it possible to define configs from other configs
Give more flexibility to define configs that can be interpreted by make, e.g. to
define fallback values of configs like in the example below.
Before this change, the config lines:
#define CONFIG_SPL_MAX_SIZE 2048
#define CONFIG_SPL_PAD_TO CONFIG_SPL_MAX_SIZE
would have been changed in autoconfig.mk into:
CONFIG_SPL_MAX_SIZE=2048
CONFIG_SPL_PAD_TO="CONFIG_SPL_MAX_SIZE"
Hence, a make recipe using as an argument to $(OBJCOPY):
--pad-to=$(CONFIG_SPL_PAD_TO)
would have issued:
--pad-to="CONFIG_SPL_MAX_SIZE"
which means nothing for $(OBJCOPY) and makes it fail.
Thanks to this change, the config lines above are changed in autoconfig.mk into:
CONFIG_SPL_MAX_SIZE=2048
CONFIG_SPL_PAD_TO=$(CONFIG_SPL_MAX_SIZE)
Hence, the make recipe above now issues:
--pad-to=2048
as expected from the defined config.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
Give more flexibility to define configs that can be interpreted by make, e.g. to
define fallback values of configs like in the example below.
Before this change, the config lines:
#define CONFIG_SPL_MAX_SIZE 2048
#define CONFIG_SPL_PAD_TO CONFIG_SPL_MAX_SIZE
would have been changed in autoconfig.mk into:
CONFIG_SPL_MAX_SIZE=2048
CONFIG_SPL_PAD_TO="CONFIG_SPL_MAX_SIZE"
Hence, a make recipe using as an argument to $(OBJCOPY):
--pad-to=$(CONFIG_SPL_PAD_TO)
would have issued:
--pad-to="CONFIG_SPL_MAX_SIZE"
which means nothing for $(OBJCOPY) and makes it fail.
Thanks to this change, the config lines above are changed in autoconfig.mk into:
CONFIG_SPL_MAX_SIZE=2048
CONFIG_SPL_PAD_TO=$(CONFIG_SPL_MAX_SIZE)
Hence, the make recipe above now issues:
--pad-to=2048
as expected from the defined config.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
arm: crt0.S: Remove bogus .globl
The purpose of .globl is to export symbols for ld, not to declare external
symbols.
By the way, use the ENTRY() and ENDPROC() macros to define functions rather than
using .global directly.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
The purpose of .globl is to export symbols for ld, not to declare external
symbols.
By the way, use the ENTRY() and ENDPROC() macros to define functions rather than
using .global directly.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code(): Use __image_copy_end for end of relocation
Use __image_copy_end instead of __bss_start for the end of the image to
relocate. This is the same as commit 033ca72, but applied to all ARM start.S.
This is a more appropriate symbol naming for an image copy & relocate feature,
and this also saves a useless copy of data put between __image_copy_end and
__bss_start in linker scripts (e.g. relocation information, or MMU
initialization tables used only before jumping to the relocated image).
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Use __image_copy_end instead of __bss_start for the end of the image to
relocate. This is the same as commit 033ca72, but applied to all ARM start.S.
This is a more appropriate symbol naming for an image copy & relocate feature,
and this also saves a useless copy of data put between __image_copy_end and
__bss_start in linker scripts (e.g. relocation information, or MMU
initialization tables used only before jumping to the relocated image).
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code(): Remove useless relocation offset computation
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm1136: Remove redundant relocate_code() return
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: relocate_code() is no longer noreturn
Commit e05e5de7fae5bec79617e113916dac6631251156 made ARM's relocate_code()
return to its caller, but it did not update its declaration accordingly.
Fixing this function declaration fixes dropped C code following calls to
relocate_code().
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Commit e05e5de7fae5bec79617e113916dac6631251156 made ARM's relocate_code()
return to its caller, but it did not update its declaration accordingly.
Fixing this function declaration fixes dropped C code following calls to
relocate_code().
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
arm: start.S: Fix _TEXT_BASE for SPL
_TEXT_BASE must be set to CONFIG_SPL_TEXT_BASE for generic SPL, and to
CONFIG_SYS_TEXT_BASE for non-SPL builds.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
_TEXT_BASE must be set to CONFIG_SPL_TEXT_BASE for generic SPL, and to
CONFIG_SYS_TEXT_BASE for non-SPL builds.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Reviewed-by: Tom Rini <trini@ti.com>
nand: mxc: Use appropriate page number in syndrome functions
The syndrome functions should use the page number passed as argument instead of
the page number saved upon NAND_CMD_READ0.
This does not make any difference if the NAND_NO_AUTOINCR option is set, but
otherwise this fixes accesses to the wrong pages.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
The syndrome functions should use the page number passed as argument instead of
the page number saved upon NAND_CMD_READ0.
This does not make any difference if the NAND_NO_AUTOINCR option is set, but
otherwise this fixes accesses to the wrong pages.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
nand: mxc: Fix debug trace in mxc_nand_read_oob_syndrome()
The page number indicated in the debug trace of mxc_nand_read_oob_syndrome() did
not match the page being worked on.
By the way, replace the GCC-specific __FUNCTION__ with __func__.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
The page number indicated in the debug trace of mxc_nand_read_oob_syndrome() did
not match the page being worked on.
By the way, replace the GCC-specific __FUNCTION__ with __func__.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
imx: mx53ard: Add support for NAND Flash
Add support for the Samsung K9LAG08U0M NAND Flash (2-GiB MLC NAND Flash, 2-kiB
pages, 256-kiB blocks, 30-ns R/W cycles, 1 CS) on mx53ard.
eNFC_CLK_ROOT is set up with a cycle time of 37.5 ns (400 MHz / 3 / 5) for this
board, which satisfies the 30-ns NF R/W cycle requirement.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
Add support for the Samsung K9LAG08U0M NAND Flash (2-GiB MLC NAND Flash, 2-kiB
pages, 256-kiB blocks, 30-ns R/W cycles, 1 CS) on mx53ard.
eNFC_CLK_ROOT is set up with a cycle time of 37.5 ns (400 MHz / 3 / 5) for this
board, which satisfies the 30-ns NF R/W cycle requirement.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
imx: mx5: lowlevel_init: Simplify code
Don't use several instructions to build constant values.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Stefano Babic <sbabic@denx.de>
Don't use several instructions to build constant values.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Stefano Babic <sbabic@denx.de>
nand: mxc: Add support for i.MX5
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
nand: mxc: Prepare to add support for i.MX5
Add some abstraction to NFC definitions so that some parts of the current code
can also be used for future i.MX5 code.
Clean up a few things by the way.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
Add some abstraction to NFC definitions so that some parts of the current code
can also be used for future i.MX5 code.
Clean up a few things by the way.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
mtd: nand: mxc_nand: Fix is_16bit_nand()
Currently is_16bit_nand() is a per SoC function and it decides the bus nand
width by reading some boot related registers.
This method works when NAND is the boot medium, but does not work if another
boot medium is used. For example: booting from a SD card and then using NAND
to store the environment variables, would lead to the following error:
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
Use CONFIG_SYS_NAND_BUSWIDTH_16BIT symbol to decide the bus width.
If it is defined in the board file, then consider 16-bit NAND bus-width,
otherwise assume 8-bit NAND is used.
This also aligns with Documentation/devicetree/bindings/mtd/nand.txt, which
states:
nand-bus-width : 8 or 16 bus width if not present 8
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Reviewed-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Currently is_16bit_nand() is a per SoC function and it decides the bus nand
width by reading some boot related registers.
This method works when NAND is the boot medium, but does not work if another
boot medium is used. For example: booting from a SD card and then using NAND
to store the environment variables, would lead to the following error:
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
Use CONFIG_SYS_NAND_BUSWIDTH_16BIT symbol to decide the bus width.
If it is defined in the board file, then consider 16-bit NAND bus-width,
otherwise assume 8-bit NAND is used.
This also aligns with Documentation/devicetree/bindings/mtd/nand.txt, which
states:
nand-bus-width : 8 or 16 bus width if not present 8
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Reviewed-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
mtd: nand: Introduce CONFIG_SYS_NAND_BUSWIDTH_16BIT
Introduce CONFIG_SYS_NAND_BUSWIDTH_16BIT option so that other NAND controller
drivers could use it when a 16-bit NAND is deployed.
drivers/mtd/nand/ndfc has CONFIG_SYS_NDFC_16BIT, so just rename it, so that
other NAND drivers could reuse the same symbol.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Reviewed-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Introduce CONFIG_SYS_NAND_BUSWIDTH_16BIT option so that other NAND controller
drivers could use it when a 16-bit NAND is deployed.
drivers/mtd/nand/ndfc has CONFIG_SYS_NDFC_16BIT, so just rename it, so that
other NAND drivers could reuse the same symbol.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Reviewed-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
env: Add redundant env support to UBI env
Allow the user to specify two UBI volumes to use for the environment
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
Allow the user to specify two UBI volumes to use for the environment
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
env: Add support for UBI environment
UBI is a better place for the environment on NAND devices because it
handles wear-leveling and bad blocks.
Gluebi is needed in Linux to access the env as an MTD partition.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
UBI is a better place for the environment on NAND devices because it
handles wear-leveling and bad blocks.
Gluebi is needed in Linux to access the env as an MTD partition.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
mtd: Make mtdparts work with pre-reloc env
The env in UBI needs to look up the mtd partition as part of relocation,
which happens before relocation. Make the mtdparts code capable of
working on the default env to start with.
The code tries to set values in the env as well, but again, the env
isn't there yet, so add a check to setenv to not allow sets before the
env is relocated.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
The env in UBI needs to look up the mtd partition as part of relocation,
which happens before relocation. Make the mtdparts code capable of
working on the default env to start with.
The code tries to set values in the env as well, but again, the env
isn't there yet, so add a check to setenv to not allow sets before the
env is relocated.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
ubi: ubifs: Turn off verbose prints
The prints are out of control. SILENCE!
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
The prints are out of control. SILENCE!
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
ubi: ubifs: Add documentation for README
Describe the needed CONFIG tokens to enable UBI and UBIFS support.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
Describe the needed CONFIG tokens to enable UBI and UBIFS support.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
ubi: Expose a few simple functions from the cmd_ubi
Part, Read, and Write functionality that will be used by env_ubi.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
Part, Read, and Write functionality that will be used by env_ubi.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
ubi: Fix broken cleanup code in attach_by_scanning
The unwind code was not reversing operations correctly and was causing
a hang on any error condition.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
The unwind code was not reversing operations correctly and was causing
a hang on any error condition.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
Do not call board_early_init_f() twice
Apparently due to a missed rebase conflict resolution
board_early_init_f() is included twice in the list of initialization
functions.
Leave only the first occurrence.
. built and boot an Exynos 5250 target
Signed-off-by: Vadim Bendebury <vbendeb@chromium.org>
Apparently due to a missed rebase conflict resolution
board_early_init_f() is included twice in the list of initialization
functions.
Leave only the first occurrence.
. built and boot an Exynos 5250 target
Signed-off-by: Vadim Bendebury <vbendeb@chromium.org>
Merge branch 'master' of git://git.denx.de/u-boot-usb
omap5912-osk: Fix get_timer() and CONFIG_SYS_HZ
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap5912-osk: Increase flash partition for u-boot
The current u-boot binary needs more than 128KB of flash space and so
move the u-boot environment from an offset of 128KB to 256KB in flash
to ensure the enviroment does not overlap with u-boot.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The current u-boot binary needs more than 128KB of flash space and so
move the u-boot environment from an offset of 128KB to 256KB in flash
to ensure the enviroment does not overlap with u-boot.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap5912-osk: Fix device initialisation
In the current u-boot, the device pin multiplexing and clock
initialisation needs to be early during the boot process and before
board_init() is called. U-boot is currently crashing on this board
because this is not being done early enough. Therefore, add a s_init()
function for the omap5912-osk board to do this.
Also fix the stack pointer so that it is pointing to the end of the
internal RAM and not the beginning as this was also causing the device
to crash.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
In the current u-boot, the device pin multiplexing and clock
initialisation needs to be early during the boot process and before
board_init() is called. U-boot is currently crashing on this board
because this is not being done early enough. Therefore, add a s_init()
function for the omap5912-osk board to do this.
Also fix the stack pointer so that it is pointing to the end of the
internal RAM and not the beginning as this was also causing the device
to crash.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap5912-osk: Fix booting from NOR flash
The omap5912-osk board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash at address
0x00000000.
The omap5912-osk board only has 32MB of RAM and so fix the comment
in the omap5912-osk config.mk file as well.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The omap5912-osk board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash at address
0x00000000.
The omap5912-osk board only has 32MB of RAM and so fix the comment
in the omap5912-osk config.mk file as well.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap5912-osk: Fix DRAM initialisation
The size of the DRAM for the omap5912-osk board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap5912-osk board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The size of the DRAM for the omap5912-osk board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap5912-osk board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap5_uevm: Correct to 2MiB aligned partitions on eMMC
This has a 2MiB erase block size eMMC, so make sure we align on that for
best possible performance.
Signed-off-by: Tom Rini <trini@ti.com>
This has a 2MiB erase block size eMMC, so make sure we align on that for
best possible performance.
Signed-off-by: Tom Rini <trini@ti.com>
OMAP4: Fix bug in omap4460_volts struct
The omap4460_volts struct was incorrectly referencing tps62361
instead of twl6030 as PMIC for the core and mm voltages (the
tps is used for mpu supply only). This shall lead to bad OPP
settings while booting kernel. Fixing it.
Fix some comments as well.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
The omap4460_volts struct was incorrectly referencing tps62361
instead of twl6030 as PMIC for the core and mm voltages (the
tps is used for mpu supply only). This shall lead to bad OPP
settings while booting kernel. Fixing it.
Fix some comments as well.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
powerpc/lib: fix unsafe register handling in wait_ticks
If watchdog is enabled, the arch/powerpc/lib/ticks.S::wait_ticks() function
calls the function specified by the WATCHDOG_RESET macro.
The wait_ticks function depends on the registers r0, r6 and r7 being
preserved however that is not guaranteed, e.g. if the reset function is a
C function this will probably overwrite r0 and cause an endless loop.
The following patch changes to using r14+r15 instead of r6+r7 (to resemble
what would have been generated by a C compiler) and saves all necessary
registers on the stack.
The patch has been tested on a custom MPC5125 based machine using the 512x
powerpc architecture.
Signed-off-by: Mats Karrman <mats.karrman@tritech.se>
Cc: Wolfgang Denk <wd@denx.de>
Acked-by: Joakim Tjernlund <joakim.tjernlund@transmode.se>
Tested-by: Stefan Roese <sr@denx.de>
If watchdog is enabled, the arch/powerpc/lib/ticks.S::wait_ticks() function
calls the function specified by the WATCHDOG_RESET macro.
The wait_ticks function depends on the registers r0, r6 and r7 being
preserved however that is not guaranteed, e.g. if the reset function is a
C function this will probably overwrite r0 and cause an endless loop.
The following patch changes to using r14+r15 instead of r6+r7 (to resemble
what would have been generated by a C compiler) and saves all necessary
registers on the stack.
The patch has been tested on a custom MPC5125 based machine using the 512x
powerpc architecture.
Signed-off-by: Mats Karrman <mats.karrman@tritech.se>
Cc: Wolfgang Denk <wd@denx.de>
Acked-by: Joakim Tjernlund <joakim.tjernlund@transmode.se>
Tested-by: Stefan Roese <sr@denx.de>
am335x: Update timings for the beaglebone again
After further testing we can run DDR at 400MHz so update the timings
again.
Tested-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
After further testing we can run DDR at 400MHz so update the timings
again.
Tested-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
powerpc/usb: Fix usb device-tree fix-up
Fix USB device-tree fixup to properly handle device-tree fixup and
print appropriate message when wrong/junk "dr_mode" or "phy_type"
are mentioned in hwconfig string
Signed-off-by: Ramneek Mehresh <ramneek.mehresh@freescale.com>
Fix USB device-tree fixup to properly handle device-tree fixup and
print appropriate message when wrong/junk "dr_mode" or "phy_type"
are mentioned in hwconfig string
Signed-off-by: Ramneek Mehresh <ramneek.mehresh@freescale.com>
am335x_evm: Enable DFU for NAND and MMC, provide example alt_infos
- Add CONFIG_DFU_NAND, CONFIG_DFU_MMC
- Set dfu_alt_info_nand, dfu_alt_info_emmc and dfu_alt_info_mmc to show
working examples for those cases.
- Increase CONFIG_SYS_MAXARGS due to hush parsing bugs that would
otherwise disallow 'setenv dfu_alt_info ${dfu_alt_info_nand}'.
- Enable CONFIG_FAT_WRITE to allow updating on MMC
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
- Add CONFIG_DFU_NAND, CONFIG_DFU_MMC
- Set dfu_alt_info_nand, dfu_alt_info_emmc and dfu_alt_info_mmc to show
working examples for those cases.
- Increase CONFIG_SYS_MAXARGS due to hush parsing bugs that would
otherwise disallow 'setenv dfu_alt_info ${dfu_alt_info_nand}'.
- Enable CONFIG_FAT_WRITE to allow updating on MMC
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
am335x_evm: Add CONFIG_CMD_MTDPARTS and relevant defaults
Signed-off-by: Tom Rini <trini@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
am335x_evm: Define CONFIG_SYS_CACHELINE_SIZE
drivers/usb/gadget/composite.c requires that this is defined early.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Tom Rini <trini@ti.com>
drivers/usb/gadget/composite.c requires that this is defined early.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Tom Rini <trini@ti.com>
dfu: NAND specific routines for DFU operation
Support for NAND storage devices to work with the DFU framework.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Scott Wood <scottwood@freescale.com>
Support for NAND storage devices to work with the DFU framework.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Scott Wood <scottwood@freescale.com>
cmd_nand.c: Fix CONFIG_CMD_NAND_YAFFS
The flag changed from WITH_INLINE_OOB to WITH_YAFFS_OOB by accident in
418396e.
Signed-off-by: Tom Rini <trini@ti.com>
The flag changed from WITH_INLINE_OOB to WITH_YAFFS_OOB by accident in
418396e.
Signed-off-by: Tom Rini <trini@ti.com>
nand: Extend nand_(read|write)_skip_bad with *actual and limit parameters
We make these two functions take a size_t pointer to how much space
was used on NAND to read or write the buffer (when reads/writes happen)
so that bad blocks can be accounted for. We also make them take an
loff_t limit on how much data can be read or written. This means that
we can now catch the case of when writing to a partition would exceed
the partition size due to bad blocks. To do this we also need to make
check_skip_len count not just complete blocks used but partial ones as
well. All callers of nand_(read|write)_skip_bad are adjusted to call
these with the most sensible limits available.
The changes were started by Pantelis and finished by Tom.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
We make these two functions take a size_t pointer to how much space
was used on NAND to read or write the buffer (when reads/writes happen)
so that bad blocks can be accounted for. We also make them take an
loff_t limit on how much data can be read or written. This means that
we can now catch the case of when writing to a partition would exceed
the partition size due to bad blocks. To do this we also need to make
check_skip_len count not just complete blocks used but partial ones as
well. All callers of nand_(read|write)_skip_bad are adjusted to call
these with the most sensible limits available.
The changes were started by Pantelis and finished by Tom.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
dfu: Change indentation of defines in <dfu.h>
Signed-off-by: Tom Rini <trini@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
dfu: Support larger than memory transfers.
Previously we didn't support upload/download larger than available
memory. This is pretty bad when you have to update your root filesystem
for example.
This patch removes that limitation (and the crashes when you transfered
any file larger than 4MB) by making raw image writes be done in chunks
and making file maximum size be configurable.
The sequence number is a 16 bit counter; make sure we handle rollover
correctly. This fixes the wrong transfers for large (> 256MB) images.
Also utilize a variable to handle initialization, so that we don't rely
on just the counter sent by the host.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
Previously we didn't support upload/download larger than available
memory. This is pretty bad when you have to update your root filesystem
for example.
This patch removes that limitation (and the crashes when you transfered
any file larger than 4MB) by making raw image writes be done in chunks
and making file maximum size be configurable.
The sequence number is a 16 bit counter; make sure we handle rollover
correctly. This fixes the wrong transfers for large (> 256MB) images.
Also utilize a variable to handle initialization, so that we don't rely
on just the counter sent by the host.
Signed-off-by: Pantelis Antoniou <panto@antoniou-consulting.com>
Signed-off-by: Tom Rini <trini@ti.com>
README: Document current DFU CONFIG options
Add documentation for the current DFU config options. DFU is a standard
USB device class so more information is available from usb.org
Signed-off-by: Tom Rini <trini@ti.com>
Add documentation for the current DFU config options. DFU is a standard
USB device class so more information is available from usb.org
Signed-off-by: Tom Rini <trini@ti.com>
am335x/ti814x: Correct MMC_BOOT_DEVICES_START/END
Given that on TI814x we have MMC1/2 swapped, we also need to swap them
in MMC_BOOT_DEVICES_START/END
Reported-by: Peter Korsgaard <jacmet@sunsite.dk>
Signed-off-by: Tom Rini <trini@ti.com>
Given that on TI814x we have MMC1/2 swapped, we also need to swap them
in MMC_BOOT_DEVICES_START/END
Reported-by: Peter Korsgaard <jacmet@sunsite.dk>
Signed-off-by: Tom Rini <trini@ti.com>
patman: Add Series-process-log tag to sort/uniq change logs
For some series with lots of changes it is annoying that duplicate change
log items are not caught. It is also helpful sometimes to sort the change
logs.
Add a Series-process-log tag to enable this, which can be placed in a
commit to control this.
The change to the Cc: line is to fix a checkpatch warning.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
For some series with lots of changes it is annoying that duplicate change
log items are not caught. It is also helpful sometimes to sort the change
logs.
Add a Series-process-log tag to enable this, which can be placed in a
commit to control this.
The change to the Cc: line is to fix a checkpatch warning.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
patman: Add -a option to refrain from test-applying the patches
Especially with the Linux kernel, it takes a long time (a minute or more)
to test-apply the patches, so patman becomes significantly less useful.
The only real problem that is found with this apply step is trailing spaces.
Provide a -a option to skip this step, for those working with clean patches.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
Especially with the Linux kernel, it takes a long time (a minute or more)
to test-apply the patches, so patman becomes significantly less useful.
The only real problem that is found with this apply step is trailing spaces.
Provide a -a option to skip this step, for those working with clean patches.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
patman: Don't barf if the word 'commit' starts a line
Patman's regular expression for detecting the start of a
commit in a git log was a little simplistic and could be
confused if the git log itself had the word "commit" as
the start of a line (as this commit does). Make patman
a little more robust.
Signed-off-by: Doug Anderson <dianders@chromium.org>
Acked-by: Simon Glass <sjg@chromium.org>
Patman's regular expression for detecting the start of a
commit in a git log was a little simplistic and could be
confused if the git log itself had the word "commit" as
the start of a line (as this commit does). Make patman
a little more robust.
Signed-off-by: Doug Anderson <dianders@chromium.org>
Acked-by: Simon Glass <sjg@chromium.org>
patman: Provide option to ignore bad aliases
Often it happens that patches include tags which don't have aliases. It
is annoying that patman fails in this case, and provides no option to
continue other than adding empty tags to the .patman file.
Correct this by adding a '-t' option to ignore tags that don't exist.
Print a warning instead.
Since running the tests is not a common operation, move this to --test
instead, to reserve -t for this new option.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
Often it happens that patches include tags which don't have aliases. It
is annoying that patman fails in this case, and provides no option to
continue other than adding empty tags to the .patman file.
Correct this by adding a '-t' option to ignore tags that don't exist.
Print a warning instead.
Since running the tests is not a common operation, move this to --test
instead, to reserve -t for this new option.
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
Merge branch 'patman' of git://git.denx.de/u-boot-x86
cmd_sf: include header file common.h before div64.h
The header file div64.h includes <asm/types.h> which defines
the phys_addr_t according to the macro CONFIG_PHYS_64BIT, while
the macro CONFIG_PHYS_64BIT is included in common.h which comes
after div64.h, so in order to get consistent type definition for
phys_addr_t, common.h should be included before div64.h, Or else,
the parameters of phys_addr_t type will be passed wrongly when
CONFIG_PHYS_64BIT is defined.
Signed-off-by: Mingkai Hu <Mingkai.Hu@freescale.com>
The header file div64.h includes <asm/types.h> which defines
the phys_addr_t according to the macro CONFIG_PHYS_64BIT, while
the macro CONFIG_PHYS_64BIT is included in common.h which comes
after div64.h, so in order to get consistent type definition for
phys_addr_t, common.h should be included before div64.h, Or else,
the parameters of phys_addr_t type will be passed wrongly when
CONFIG_PHYS_64BIT is defined.
Signed-off-by: Mingkai Hu <Mingkai.Hu@freescale.com>
common/cmd_test: Avoid macro expansion
cmd_test.c adds "true" and "false" as new commands. We need to avoid macro
expansion for U_BOOT_CMD.
Signed-off-by: York Sun <yorksun@freescale.com>
cmd_test.c adds "true" and "false" as new commands. We need to avoid macro
expansion for U_BOOT_CMD.
Signed-off-by: York Sun <yorksun@freescale.com>
dfu: Increase DFU buffer size from 4MiB to 8MiB
Increase size of DMA buffer from 4MiB to 8MiB. This is necessary due to
uImage size increase.
Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Increase size of DMA buffer from 4MiB to 8MiB. This is necessary due to
uImage size increase.
Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
dfu:ext4:fix: Change ext4write command order of parameters
Following commit:
"cmd_ext4: BREAK and correct ext4write parameter order"
SHA1:0171d52c410cbaa9290b1b214e695697c835bfe5
introduced cleanup of ext4write semantics to be consistent with other
filesystem's writing commands (e.g. fatwrite).
This commit provides correct ext4write command generation at DFU eMMC
code.
Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Following commit:
"cmd_ext4: BREAK and correct ext4write parameter order"
SHA1:0171d52c410cbaa9290b1b214e695697c835bfe5
introduced cleanup of ext4write semantics to be consistent with other
filesystem's writing commands (e.g. fatwrite).
This commit provides correct ext4write command generation at DFU eMMC
code.
Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
omap5_common.h: Use fallback CONFIG_SYS_BAUDRATE_TABLE
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
omap5_uevm.h: Move uEVM-specific choices to omap5_uevm.h
The omap5_uevm platform has eMMC, and it makes sense to say that our
default env storage shall reside there. Other platforms may not, so
move this choice to the EVM config. In addition, we should provide some
way to partition the flash for later usage, so take advantage of the GPT
partition table support code and allow that to be setup with some
reasonable defaults.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
The omap5_uevm platform has eMMC, and it makes sense to say that our
default env storage shall reside there. Other platforms may not, so
move this choice to the EVM config. In addition, we should provide some
way to partition the flash for later usage, so take advantage of the GPT
partition table support code and allow that to be setup with some
reasonable defaults.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
OMAP3/4/5/AM33xx: Correct logic for checking FAT or RAW MMC
In the case of booting from certain peripherals, such as UART, we must
not see what the device descriptor says for RAW or FAT mode because in
addition to being nonsensical, it leads to a hang. This is why we have
a test currently for the boot mode being within range. The problem
however is that on some platforms we get MMC2_2 as the boot mode and not
the defined value for MMC2, and in others we get the value for MMC2_2.
This is required to fix eMMC booting on omap5_uevm.
Tested on am335x_evm (UART, NAND, SD), omap3_beagle (NAND, SD on
classic, SD only on xM rev C5) and omap5_uevm (SD, eMMC).
Signed-off-by: Tom Rini <trini@ti.com>
In the case of booting from certain peripherals, such as UART, we must
not see what the device descriptor says for RAW or FAT mode because in
addition to being nonsensical, it leads to a hang. This is why we have
a test currently for the boot mode being within range. The problem
however is that on some platforms we get MMC2_2 as the boot mode and not
the defined value for MMC2, and in others we get the value for MMC2_2.
This is required to fix eMMC booting on omap5_uevm.
Tested on am335x_evm (UART, NAND, SD), omap3_beagle (NAND, SD on
classic, SD only on xM rev C5) and omap5_uevm (SD, eMMC).
Signed-off-by: Tom Rini <trini@ti.com>
arm: omap4: Fix SDRAM AUTO DETECTION
Commit "8602114 omap: emif: configure emif only when required"
breaks SDRAM_AUTO_DETECTION.
The issue is dmm_init() depends on emif_sizes[](SDRAM Auto detection)
done in do_sdram_init(). The above commit moves dmm_init() above
do_sdram_init() because of which dmm_init() uses uninitialized
emif_sizes[].
So instead of using global emif_sizes[], get sdram details locally
and calculate emif sizes.
Reported-by: Michael Cashwell <mboards@prograde.net>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Commit "8602114 omap: emif: configure emif only when required"
breaks SDRAM_AUTO_DETECTION.
The issue is dmm_init() depends on emif_sizes[](SDRAM Auto detection)
done in do_sdram_init(). The above commit moves dmm_init() above
do_sdram_init() because of which dmm_init() uses uninitialized
emif_sizes[].
So instead of using global emif_sizes[], get sdram details locally
and calculate emif sizes.
Reported-by: Michael Cashwell <mboards@prograde.net>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
OMAP: Fix copy-paste bug that did not enable UART4 clock
V2 fixes line wrap issue of the patch itself.
UART3 was enabled twice instead of UART4.
One more cosmetic change in a comment on EMIF clock.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
Reviewed-by: R Sricharan <r.sricharan@ti.com>
V2 fixes line wrap issue of the patch itself.
UART3 was enabled twice instead of UART4.
One more cosmetic change in a comment on EMIF clock.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
Reviewed-by: R Sricharan <r.sricharan@ti.com>
doc/feature-removal-schedule.txt: Add CONFIG_SYS_(CLOCKS|PADS)_ENABLE_ALL
We shall remove these OMAP4/5-specific options in v2013.07, barring
insufficient progress on the kernel side.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
We shall remove these OMAP4/5-specific options in v2013.07, barring
insufficient progress on the kernel side.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
ARM: OMAP4/5: Make bootz as the default boot command
So with OMAP added to multi platform kernel,
the uImage no more contains a valid load address.
With the uboot already supporting zImage,
change the default boot command to bootz
instead.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
So with OMAP added to multi platform kernel,
the uImage no more contains a valid load address.
With the uboot already supporting zImage,
change the default boot command to bootz
instead.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
ARM: OMAP4/5: Change the default boot command to work with device tree
Now with kernel moving to all device tree, the default
boot command is changed to pass the device tree blob.
Also, adding the findfdt command to get the dt-blob
based on the board.
Thanks to Tom Rini <trini@ti.com> for suggesting this.
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Now with kernel moving to all device tree, the default
boot command is changed to pass the device tree blob.
Also, adding the findfdt command to get the dt-blob
based on the board.
Thanks to Tom Rini <trini@ti.com> for suggesting this.
Signed-off-by: Sricharan R <r.sricharan@ti.com>
omap5: Allow use of a plain text env file
For production systems it is better to use script images since
they are protected by checksums and carry valuable information
like name and timestamp. Also, you can't validate the content
passed to env import.
But for development, it is easier to use the env import command and
plain text files instead of script-images.
Since both OMAP5evm/uevm boards are used primarily for development,
we allow U-Boot to load env var from a text file in case that an
boot.scr script-image is not present.
The variable uenvcmd (if existent) will be executed (using run) after
uEnv.txt was loaded. If uenvcmd doesn't exist the default boot sequence
will be started.
Inspired by commit: d70f54808dfa83b574e1239c3eccbcf3317343e1
(omap4: allow the use of a plain text env file instead boot scripts)
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Tested-by: Sricharan R <r.sricharan@ti.com>
For production systems it is better to use script images since
they are protected by checksums and carry valuable information
like name and timestamp. Also, you can't validate the content
passed to env import.
But for development, it is easier to use the env import command and
plain text files instead of script-images.
Since both OMAP5evm/uevm boards are used primarily for development,
we allow U-Boot to load env var from a text file in case that an
boot.scr script-image is not present.
The variable uenvcmd (if existent) will be executed (using run) after
uEnv.txt was loaded. If uenvcmd doesn't exist the default boot sequence
will be started.
Inspired by commit: d70f54808dfa83b574e1239c3eccbcf3317343e1
(omap4: allow the use of a plain text env file instead boot scripts)
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Tested-by: Sricharan R <r.sricharan@ti.com>
ARM: OMAP5: Set fdt_high to enable booting with Device tree
While booting with dt blob, if fdt_high is not set to
0xffffffff, the dt blob gets relocated to a high ram address,
which the kernel is not able to use without HIGHMEM.
So set it to 0xffffffff to avoid the issue.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
While booting with dt blob, if fdt_high is not set to
0xffffffff, the dt blob gets relocated to a high ram address,
which the kernel is not able to use without HIGHMEM.
So set it to 0xffffffff to avoid the issue.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
ARM: OMAP5: Rename omap5_evm to omap5_uevm
The omap5-uevm is the reference board name for OMAP5 soc
based platform. So rename it accordingly.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
The omap5-uevm is the reference board name for OMAP5 soc
based platform. So rename it accordingly.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
omap2420-h4: Fix get_timer() and CONFIG_SYS_HZ
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Add device tree support
Enable device-tree support for the omap2420-h4 board.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
Enable device-tree support for the omap2420-h4 board.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Fix booting from NOR flash
The omap2420-h4 board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash. Please note
that OMAP maps the NOR flash to address 0x08000000 by default and so
use this as the default address for the NOR flash.
Also remove legacy code that attempts to calculate where in flash the
sdata structure, that holds the memory interface configuration data,
is located. By changing the default linker location for code to flash
this is no longer necessary.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The omap2420-h4 board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash. Please note
that OMAP maps the NOR flash to address 0x08000000 by default and so
use this as the default address for the NOR flash.
Also remove legacy code that attempts to calculate where in flash the
sdata structure, that holds the memory interface configuration data,
is located. By changing the default linker location for code to flash
this is no longer necessary.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Fix DRAM initialisation
The size of the DRAM for the omap2420-h4 board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap2420-h4 board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The size of the DRAM for the omap2420-h4 board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap2420-h4 board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
tricorder: enable hw assisted BCH8 in SPL and u-boot
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <weber@corscience.de>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <weber@corscience.de>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
omap_gpmc: add support for hw assisted BCH8
The kernel states:
---8<---
The OMAP3 GPMC hardware BCH engine computes remainder polynomials, it does not
provide automatic error location and correction: this step is implemented using
the BCH library.
--->8---
And we do so in u-boot.
This implementation uses the same layout for BCH8 but it is fix. The current
provided layout does only work with 64 Byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Cc: Mansoor Ahamed <mansoor.ahamed@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
The kernel states:
---8<---
The OMAP3 GPMC hardware BCH engine computes remainder polynomials, it does not
provide automatic error location and correction: this step is implemented using
the BCH library.
--->8---
And we do so in u-boot.
This implementation uses the same layout for BCH8 but it is fix. The current
provided layout does only work with 64 Byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Cc: Mansoor Ahamed <mansoor.ahamed@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
omap_gpmc: change nandecc command
With uppcoming BCH support on OMAP devices we need to decide between differnt
algorithms when switching the ECC engine. Currently we support 1-bit hammign
and 8-bit BCH on HW backend.
In order to switch between differnet ECC algorithms we need to change the
interface of omap_nand_switch_ecc() also.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
With uppcoming BCH support on OMAP devices we need to decide between differnt
algorithms when switching the ECC engine. Currently we support 1-bit hammign
and 8-bit BCH on HW backend.
In order to switch between differnet ECC algorithms we need to change the
interface of omap_nand_switch_ecc() also.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
omap3/omap_gpmc.h: add ooblayout for BCH8 as in kernel
This patch adds BCH8 ooblayout for NAND as provided by
0e618ef0a6a33cf7ef96c2c824402088dd8ef48c in linux kernel. This Layout is
currently only provided for 64 byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
This patch adds BCH8 ooblayout for NAND as provided by
0e618ef0a6a33cf7ef96c2c824402088dd8ef48c in linux kernel. This Layout is
currently only provided for 64 byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
asm/omap_gpmc.h: consolidate common defines
arch/arm/include/asm/arch-am33xx/omap_gpmc.h and
arch/arm/include/asm/arch-omap3/omap_gpmc.h are almost the same, consolidate
the common parts into a new header.
Introduce a new asm/omap_gpmc.h which defines the command part and pulls in
the architecture specific one.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
arch/arm/include/asm/arch-am33xx/omap_gpmc.h and
arch/arm/include/asm/arch-omap3/omap_gpmc.h are almost the same, consolidate
the common parts into a new header.
Introduce a new asm/omap_gpmc.h which defines the command part and pulls in
the architecture specific one.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
omap3/cpu.h: add BCH support
This patch adds the BCH result registers to register mapping for OMAP3 gpmc.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
This patch adds the BCH result registers to register mapping for OMAP3 gpmc.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
omap3_beagle: Flush UART3 xmit on enable if TEMT is broken
Flush UART3 xmit on enable if TEMT is broken
On some OMAP3 devices when UART3 is configured for boot mode before SPL starts
only THRE bit is set. We have to empty the transmitter before initialization
starts. This patch avoids the use of CONFIG_SYS_NS16550_BROKEN_TEMT.
Signed-off-by: Manfred Huber <man.huber@arcor.de>
Tested-by: Javier Martinez Canillas <javier@dowhile0.org>
Tested-by: Andreas Bießmann <andreas.devel@googlemail.com>
Flush UART3 xmit on enable if TEMT is broken
On some OMAP3 devices when UART3 is configured for boot mode before SPL starts
only THRE bit is set. We have to empty the transmitter before initialization
starts. This patch avoids the use of CONFIG_SYS_NS16550_BROKEN_TEMT.
Signed-off-by: Manfred Huber <man.huber@arcor.de>
Tested-by: Javier Martinez Canillas <javier@dowhile0.org>
Tested-by: Andreas Bießmann <andreas.devel@googlemail.com>
am335x: Enable MMC1 clock
We must not assume ROM has enabled the clock for MMC1.
Reported-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Peter Korsgaard <jacmet@sunsite.dk>
We must not assume ROM has enabled the clock for MMC1.
Reported-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Peter Korsgaard <jacmet@sunsite.dk>
pcm051: Enable DDR PHY dynamic power down bit
This is done already for am335x in
59dcf970d11ebff5d9f4bbbde79fda584e9e7ad4 and also applies for pcm051.
It powers down the IO receiver when not performing read which helps
reducing the overall power consuption in low power states
(suspend/standby).
Signed-off-by: Lars Poeschel <poeschel@lemonage.de>
This is done already for am335x in
59dcf970d11ebff5d9f4bbbde79fda584e9e7ad4 and also applies for pcm051.
It powers down the IO receiver when not performing read which helps
reducing the overall power consuption in low power states
(suspend/standby).
Signed-off-by: Lars Poeschel <poeschel@lemonage.de>
musb: set MUSB speed based on CONFIG
Do not config MUSB to highspeed mode if CONFIG_USB_GADGET_DUALSPEED
is not set, in which case Ether gadget only operates in fullspeed.
Reviewed-by: Tom Rini <trini@ti.com>
Signed-off-by: Bin Liu <b-liu@ti.com>
Do not config MUSB to highspeed mode if CONFIG_USB_GADGET_DUALSPEED
is not set, in which case Ether gadget only operates in fullspeed.
Reviewed-by: Tom Rini <trini@ti.com>
Signed-off-by: Bin Liu <b-liu@ti.com>