glsdk/glsdk-u-boot.git
9 years agoARM: OMAP3+: Detect reset type
Lokesh Vutla [Tue, 29 May 2012 19:26:41 +0000 (19:26 +0000)]
ARM: OMAP3+: Detect reset type

Certain modules are not affected by means of
a warm reset and need not be configured again.
Adding an API to detect the reset reason warm/cold.

This will be used to skip the module configurations
that are retained across a warm reset.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoarm: bugfix: Move vector table before jumping relocated code
Tetsuyuki Kobayashi [Mon, 25 Jun 2012 02:40:57 +0000 (02:40 +0000)]
arm: bugfix: Move vector table before jumping relocated code

Interrupts and exceptions doesn't work in relocated code.
It badly use IRQ_STACK_START_IN in rom area as interrupt stack.
It is because the vecotr table is not moved to ram area.
This patch moves vector table before jumping relocated code.

Signed-off-by: Tetsuyuki Kobayashi <koba@kmckk.co.jp>
Tested-by: Tom Rini <trini@ti.com>
9 years agoKirkwood: Add support for Ka-Ro TK71
Marek Vasut [Tue, 3 Jul 2012 03:02:20 +0000 (03:02 +0000)]
Kirkwood: Add support for Ka-Ro TK71

Signed-off-by: Marek Vasut <marex@denx.de>
Cc: Prafulla Wadaskar <prafulla@marvell.com>
Cc: Wolfgang Denk <wd@denx.de>
9 years agoarm/km: use spi claim bus to switch between SPI and NAND
Valentin Longchamp [Wed, 13 Jun 2012 03:01:03 +0000 (03:01 +0000)]
arm/km: use spi claim bus to switch between SPI and NAND

We overwrite these weak functions from the kirkwood spi code to
use our own method to be able to switch between the SPI NOR and
the NAND flash. This is needed e.g. to update the u-boot. The former
command do_spi_toggle can therefore be removed. And the usage of
this command is removed from the u-boot update command in the
u-boot environment.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
Signed-off-by: Prafulla Wadaskar <prafulla@marvell.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/kirkwood: protect the ENV_SPI #defines
Valentin Longchamp [Wed, 13 Jun 2012 03:03:52 +0000 (03:03 +0000)]
arm/kirkwood: protect the ENV_SPI #defines

So that they can be redefined by some boards specific values.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoARM: don't probe PHY address for LaCie boards
Simon Guinot [Tue, 5 Jun 2012 13:16:00 +0000 (13:16 +0000)]
ARM: don't probe PHY address for LaCie boards

The command miiphy_read(name, 0xEE, 0xEE, (u16 *) &devadr) always
returns 8 for the PHY address. It is the reset value for the PHY
Address Register. Obviously, this default value could be incorrect.
Moreover, as the PHY address is well known, there is no need to
auto-detect it.

Now, the PHY address must given as a parameter to the PHY initialization
function. Additionally this patch also fixes some aesthetic issues.

Signed-off-by: Simon Guinot <simon.guinot@sequanux.org>
9 years agolacie_kw: fix CONFIG_SYS_KWD_CONFIG for inetspace_v2
Simon Guinot [Tue, 5 Jun 2012 13:15:59 +0000 (13:15 +0000)]
lacie_kw: fix CONFIG_SYS_KWD_CONFIG for inetspace_v2

Signed-off-by: Simon Guinot <simon.guinot@sequanux.org>
9 years agolacie_kw: fix SDRAM banks number for net2big_v2
Simon Guinot [Tue, 5 Jun 2012 13:15:58 +0000 (13:15 +0000)]
lacie_kw: fix SDRAM banks number for net2big_v2

Signed-off-by: Simon Guinot <simon.guinot@sequanux.org>
9 years agoKirkwood: add lschlv2 and lsxhl board support
Michael Walle [Tue, 5 Jun 2012 11:33:17 +0000 (11:33 +0000)]
Kirkwood: add lschlv2 and lsxhl board support

This patch adds support for both the Linkstation Live (LS-CHLv2) and
Linkstation Pro (LS-XHL) by Buffalo.

Signed-off-by: Michael Walle <michael@walle.cc>
Cc: Prafulla Wadaskar <prafulla@marvell.com>
9 years agonet: add helper to generate random mac address
Michael Walle [Tue, 5 Jun 2012 11:33:16 +0000 (11:33 +0000)]
net: add helper to generate random mac address

Add new function eth_random_enetaddr() to generate a locally administered
ethernet address.

Signed-off-by: Michael Walle <michael@walle.cc>
Acked-by: Joe Hershberger <joe.hershberger@gmail.com>
9 years agonet: use common rand()/srand() functions
Michael Walle [Tue, 5 Jun 2012 11:33:15 +0000 (11:33 +0000)]
net: use common rand()/srand() functions

Replace rand() with the functions from lib/. The link-local network code
stores its own seed, derived from the MAC address. Thus making it
independent from calls to srand() in other modules.

Signed-off-by: Michael Walle <michael@walle.cc>
Acked-by: Joe Hershberger <joe.hershberger@ni.com>
9 years agolib: add rand() function
Michael Walle [Tue, 5 Jun 2012 11:33:14 +0000 (11:33 +0000)]
lib: add rand() function

It's a PRNG using the simple and fast xorshift method.

Signed-off-by: Michael Walle <michael@walle.cc>
Cc: Wolfgang Denk <wd@denx.de>
9 years agokwboot: boot kirkwood SoCs over a serial link
Luka Perkov [Sun, 27 May 2012 11:44:51 +0000 (11:44 +0000)]
kwboot: boot kirkwood SoCs over a serial link

The kwboot program boots boards based on Marvell's Kirkwood platform
via Xmodem over their integrated UART.

Signed-off-by: Daniel Stodden <daniel.stodden@googlemail.com>
Acked-by: Luka Perkov <uboot@lukaperkov.net>
Tested-By: Holger Brunck <holger.brunck@keymile.com>
Tested-By: David Purdy <david.c.purdy@gmail.com>
Tested-by: Simon Guinot <simon.guinot@sequanux.org>
9 years agokw_spi: add weak functions board_spi_claim/release_bus
Valentin Longchamp [Fri, 1 Jun 2012 01:31:03 +0000 (01:31 +0000)]
kw_spi: add weak functions board_spi_claim/release_bus

This allows a final, board specific, step in the claim/relase_bus
function for the SPI controller, which may be needed for some hardware
designs.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agokw_spi: support spi_claim/release_bus functions
Valentin Longchamp [Fri, 1 Jun 2012 01:31:02 +0000 (01:31 +0000)]
kw_spi: support spi_claim/release_bus functions

These two function nows ensure that the MPP is configured correctly for
the SPI controller before any SPI access, and restore the initial
configuration when the access is over.

Since the used pins for the SPI controller can differ (2 possibilities
for each signal), the used pins are configured with CONFIG_SYS_KW_SPI_MPP.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agokw_spi: backup and reset the MPP of the chosen CS pin
Valentin Longchamp [Fri, 1 Jun 2012 01:31:01 +0000 (01:31 +0000)]
kw_spi: backup and reset the MPP of the chosen CS pin

This was not done before, and in the case of a shared pin (for MPP0
between NF_IO[2] and CSn) this could lead to problems.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agokirkwood: fix calls to kirkwood_mpp_conf
Valentin Longchamp [Fri, 1 Jun 2012 01:31:00 +0000 (01:31 +0000)]
kirkwood: fix calls to kirkwood_mpp_conf

With the new second save argument introduced by the previous patch, all
the calls to the function had to be fixed.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agokirkwood: add save functionality kirkwood_mpp_conf function
Valentin Longchamp [Fri, 1 Jun 2012 01:30:59 +0000 (01:30 +0000)]
kirkwood: add save functionality kirkwood_mpp_conf function

If a second non NULL argument is given to the kirkwood_mpp_conf
function, it will be used to store the current configuration of the MPP
registers. mpp_save  must be a preallocated table of the same size as
mpp_list and it must be zero terminated as well.

A later call to kirkwood_mpp_conf function with this saved list as first
(mpp_conf) argment will set the configuration back.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agokm_arm: use filesize for erase in update command
Valentin Longchamp [Fri, 25 May 2012 01:57:21 +0000 (01:57 +0000)]
km_arm: use filesize for erase in update command

We used to have an arbitrary value, which can be a problem if we have a
u-boot image that is bigger than this value.

This patch is dependant on the whole km/arm series and will be included
in the v3 of the series if there is one.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: enable mii cmd
Valentin Longchamp [Fri, 25 May 2012 01:57:20 +0000 (01:57 +0000)]
arm/km: enable mii cmd

This is useful to debug the switch initialization

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: remove CONFIG_RESET_PHY_R
Holger Brunck [Fri, 25 May 2012 01:57:19 +0000 (01:57 +0000)]
arm/km: remove CONFIG_RESET_PHY_R

This is already defined in the generic kirkwood header.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: change maintainer for mgcoge3un
Holger Brunck [Fri, 25 May 2012 01:57:18 +0000 (01:57 +0000)]
arm/km: change maintainer for mgcoge3un

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
Acked-By: Heiko Schocher <hs@denx.de>
cc: Prafulla Wadaskar <prafulla@marvell.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>

9 years agoarm/km: fix wrong comment in SDRAM config for mgcoge3un
Holger Brunck [Fri, 25 May 2012 01:57:17 +0000 (01:57 +0000)]
arm/km: fix wrong comment in SDRAM config for mgcoge3un

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: use ARRAY_SIZE macro
Holger Brunck [Fri, 25 May 2012 01:57:16 +0000 (01:57 +0000)]
arm/km: use ARRAY_SIZE macro

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: rename CONFIG option CONFIG_KM_DEF_ENV_UPDATE
Holger Brunck [Fri, 25 May 2012 01:57:16 +0000 (01:57 +0000)]
arm/km: rename CONFIG option CONFIG_KM_DEF_ENV_UPDATE

This config option sounds like the it is responsible for the
update of  the environment, but it is the u-boot update handling.
Therefore we adapt it to a more apropriate naming.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Prafulla Wadaskar <prafulla@marvell.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: add piggy mac adress offset for mgcoge3un
Holger Brunck [Fri, 25 May 2012 01:57:14 +0000 (01:57 +0000)]
arm/km: add piggy mac adress offset for mgcoge3un

On mgcoge3un the piggy mac adress is at offset 3.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoarm/km: add board type to boards.cfg
Holger Brunck [Fri, 25 May 2012 01:57:13 +0000 (01:57 +0000)]
arm/km: add board type to boards.cfg

Some other kirkwood boards from keymile will follow. They will have some
small differences, but we want to use the km_kirkwood.h for all to
distinguish them. This patch a preparation for this.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Gerlando Falauto <gerlando.falauto@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

9 years agoAT91SAM9*: Change kernel address in dataflash to match u-boot's size
Alexandre Belloni [Mon, 2 Jul 2012 04:26:58 +0000 (04:26 +0000)]
AT91SAM9*: Change kernel address in dataflash to match u-boot's size

On at91sam platforms, u-boot grew larger than the allocated size in
dataflash, the layout was:
bootstrap  0x00000000
ubootenv   0x00004200
uboot      0x00008400
kernel     0x00042000
fs         0x00252000

u-boot with the defconfig doesn't seem to fit in 0x42000 - 0x8400 =
0x39C00 bytes anymore.

Now, the layout is:
bootstrap  0x00000000
ubootenv   0x00004200
uboot      0x00008400
kernel     0x00084000
fs         0x00294000

Signed-off-by: Alexandre Belloni <alexandre.belloni@piout.net>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoATMEL/PIO: Enable new feature of PIO on Atmel device
Bo Shen [Sun, 20 May 2012 15:50:00 +0000 (15:50 +0000)]
ATMEL/PIO: Enable new feature of PIO on Atmel device

Enable new PIO feature supported by Atmel SoC.
Using CPU_HAS_PIO3 micro to enable PIO new feature.

Signed-off-by: Bo Shen <voice.shen@atmel.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoehci-atmel: fix compiler warning
Andreas Bießmann [Thu, 28 Jun 2012 02:50:37 +0000 (02:50 +0000)]
ehci-atmel: fix compiler warning

Commit 7a101e946cba55e32d3d1265e30456c810046da3 introduced following warning:
---8<---
ehci-atmel.c: In function 'ehci_hcd_init':
ehci-atmel.c:49:2: warning: suggest parentheses around comparison in operand of '&' [-Wparentheses]
ehci-atmel.c: In function 'ehci_hcd_stop':
ehci-atmel.c:79:2: warning: suggest parentheses around comparison in operand of '&' [-Wparentheses]
--->8---

This patch fixes it.

Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
cc: Bo Shen <voice.shen@atmel.com>
cc: Marek Vasut <marex@denx.de>

9 years agoAT91: at91sam9m10g45ek : Enable EHCI instead OHCI
Bo Shen [Wed, 27 Jun 2012 21:24:10 +0000 (21:24 +0000)]
AT91: at91sam9m10g45ek : Enable EHCI instead OHCI

Enable EHCI support instead OHCI

Signed-off-by: Bo Shen <voice.shen@atmel.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoAtmel : usb : add EHCI driver for Atmel SoC
Bo Shen [Wed, 27 Jun 2012 21:58:20 +0000 (21:58 +0000)]
Atmel : usb : add EHCI driver for Atmel SoC

Some Atmel SoC support USB EHCI, add the EHCI driver to support it.

To enable the USB EHCI, add the following configuration options into
board relative configuration file and remove USB OHCI options.

    #define CONFIG_USB_EHCI
    #define CONFIG_USB_EHCI_ATMEL
    #define CONFIG_SYS_USB_EHCI_MAX_ROOT_PORTS     2

Signed-off-by: Bo Shen <voice.shen@atmel.com>
Acked-by: Marek Vasut <marex@denx.de>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoFix: AT91SAM9263 nor flash usage
esw@bus-elektronik.de [Mon, 19 Mar 2012 05:18:17 +0000 (05:18 +0000)]
Fix: AT91SAM9263 nor flash usage

Fix: board doesn't boot from norflash
 Fix: environment can't write to flash (end address/start address not on sector boundary)

Signed-off-by: Jens Scharsig (BuS Elektronik) <esw@bus-elektronik.de>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoFix: broken boot message at serial line on AT91SAM9263-EK board
esw@bus-elektronik.de [Mon, 19 Mar 2012 04:25:59 +0000 (04:25 +0000)]
Fix: broken boot message at serial line on AT91SAM9263-EK board

Signed-off-by: Jens Scharsig (BuS Elektronik) <esw@bus-elektronik.de>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
9 years agoi.MX6 USDHC: Use the ESDHC clock
Michael Langer [Thu, 14 Jun 2012 03:44:33 +0000 (03:44 +0000)]
i.MX6 USDHC: Use the ESDHC clock

The commit "i.mx: fsl_esdhc: add the i.mx6q support" (4692708d) introduces
support for the i.MX6Q MMC host controller USDHC.

MXC_IPG_PERCLK sets the clock to 66MHz. This seems to be the default clock
of the ESDHC IP found in < i.MX6 silicon. However, the default clock for the USDHC
IP found in i.MX6 is 200MHz (MXC_ESDHC_CLK). This difference will cause a 3 times
higher clock on SD_CLK than expected (see fsl_esdh.c -> set_sysctl()).

Signed-off-by: Michael Langer <michael.langer@de.bosch.com>
CC: Stefano Babic <sbabic@denx.de>
CC: Jason Liu <r64343@freescale.com>
Acked-by: Stefano Babic <sbabic@denx.de>
9 years agomx28evk: Fix boot by adjusting HW_DRAM_CTL29 register
Fabio Estevam [Tue, 19 Jun 2012 07:24:56 +0000 (07:24 +0000)]
mx28evk: Fix boot by adjusting HW_DRAM_CTL29 register

commit acc4959fc1 (Revert "i.MX28: Enable additional DRAM address bits")
broke mx28evk boot.

Fix it by properly adjusting the HW_DRAM_CTL29 register value.

Suggested-by: Marek Vasut <marex@denx.de>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Marek Vasut <marex@denx.de>
9 years agoi.MX28: Add function to adjust memory parameters
Marek Vasut [Tue, 29 May 2012 19:43:13 +0000 (19:43 +0000)]
i.MX28: Add function to adjust memory parameters

This function can be overridden at run-time and allows implementors
of new boards based on the i.MX28 chip to fine-tune the memory params.
It is possible to write into the dram_vals array because when the SPL
runs, it is located SRAM. Therefore the location is writable. There is
no possibility of these data to be read-only.

Signed-off-by: Marek Vasut <marex@denx.de>
Cc: Wolfgang Denk <wd@denx.de>
Cc: Detlev Zundel <dzu@denx.de>
Cc: Stefano Babic <sbabic@denx.de>
Cc: Fabio Estevam <festevam@gmail.com>
9 years agomx28evk: Fix PSWITCH key position
Fabio Estevam [Sat, 12 May 2012 08:16:46 +0000 (08:16 +0000)]
mx28evk: Fix PSWITCH key position

Fix the position for PSWITCH key.

The good benefit of doing this is that boot time is greatly reduced:
from 5 seconds to less then 1 second.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Marek Vasut <marex@denx.de>
9 years agomx53smd: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:30 +0000 (21:53 +0000)]
mx53smd: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53loco: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:29 +0000 (21:53 +0000)]
mx53loco: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53evk: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:28 +0000 (21:53 +0000)]
mx53evk: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53ard: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:27 +0000 (21:53 +0000)]
mx53ard: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx35pdk: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:26 +0000 (21:53 +0000)]
mx35pdk: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agoimx31_phycore: Remove CONFIG_SYS_I2C_SLAVE definition
Fabio Estevam [Sat, 2 Jun 2012 21:53:25 +0000 (21:53 +0000)]
imx31_phycore: Remove CONFIG_SYS_I2C_SLAVE definition

According to include/i2c.h:

"/*
 * Many boards/controllers/drivers don't support an I2C slave interface so
 * provide a default slave address for them for use in common code.  A real
 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
 * support a slave interface.
 */
#ifndef CONFIG_SYS_I2C_SLAVE
#define CONFIG_SYS_I2C_SLAVE 0xfe
#endif
"

As the mxc_i2c driver does not support slave mode, there is no need
to define CONFIG_SYS_I2C_SLAVE in i.MX board file.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53ard: Remove unused CONFIG_MII_GASKET
Fabio Estevam [Thu, 7 Jun 2012 08:05:41 +0000 (08:05 +0000)]
mx53ard: Remove unused CONFIG_MII_GASKET

CONFIG_MII_GASKET is not defined anywhere, so remove it.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx6: Avoid writing to read-only bits in imximage.cfg
Vikram Narayanan [Tue, 12 Jun 2012 04:50:33 +0000 (04:50 +0000)]
mx6: Avoid writing to read-only bits in imximage.cfg

If in case this is valid according to the latest datasheet, ignore this patch.
Acked-by: Marek Vasut <marex@denx.de>
9 years agom28evk: use same notation to alloc the 128kB stack
Otavio Salvador [Sat, 12 May 2012 13:40:11 +0000 (13:40 +0000)]
m28evk: use same notation to alloc the 128kB stack

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Acked-by: Wolfgang Denk <wd@denx.de>
9 years agom28evk: drop duplicated definition of CONFIG_OF_LIBFDT
Otavio Salvador [Tue, 15 May 2012 10:59:30 +0000 (10:59 +0000)]
m28evk: drop duplicated definition of CONFIG_OF_LIBFDT

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Cc: Marek Vasut <marex@denx.de>
Cc: Stefano Babic <sbabic@denx.de>
Cc: Wolfgang Denk <wd@denx.de>
Acked-by: Marek Vasut <marex@denx.de>
9 years agomx28evk: fix board config include guardian macro name
Otavio Salvador [Sat, 12 May 2012 13:40:16 +0000 (13:40 +0000)]
mx28evk: fix board config include guardian macro name

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Acked-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx28evk: ensure command definition is in alphabetic order
Otavio Salvador [Sat, 12 May 2012 13:40:13 +0000 (13:40 +0000)]
mx28evk: ensure command definition is in alphabetic order

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Acked-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agom28evk: fix board config include guardian macro name
Otavio Salvador [Sat, 12 May 2012 13:40:15 +0000 (13:40 +0000)]
m28evk: fix board config include guardian macro name

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Acked-by: Marek Vasut <marex@denx.de>
9 years agoMX28: Fix a typo in mx28_reg_8 macro
Otavio Salvador [Fri, 11 May 2012 05:37:59 +0000 (05:37 +0000)]
MX28: Fix a typo in mx28_reg_8 macro

The macro mistakenly referred to 32bit struct instead of 8bit one.

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Cc: Fabio Estevam <fabio.estevam@freescale.com>
Cc: Marek Vasut <marex@denx.de>
Acked-by: Marek Vasut <marex@denx.de>
9 years agomx6qsabrelite: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:40:03 +0000 (07:40 +0000)]
mx6qsabrelite: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Jason Liu <r64343@freescale.com>
9 years agomx6qarm2: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:40:02 +0000 (07:40 +0000)]
mx6qarm2: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Jason Liu <r64343@freescale.com>
9 years agoima3-mx53: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:40:01 +0000 (07:40 +0000)]
ima3-mx53: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agovision2: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:40:00 +0000 (07:40 +0000)]
vision2: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agoefikamx: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:59 +0000 (07:39 +0000)]
efikamx: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Cc: Marek Vasut <marex@denx.de>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx51evk: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:58 +0000 (07:39 +0000)]
mx51evk: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53smd: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:57 +0000 (07:39 +0000)]
mx53smd: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53ard: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:56 +0000 (07:39 +0000)]
mx53ard: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53evk: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:55 +0000 (07:39 +0000)]
mx53evk: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53loco: Remove unused SOBJS
Fabio Estevam [Tue, 29 May 2012 07:39:54 +0000 (07:39 +0000)]
mx53loco: Remove unused SOBJS

There is no .S file in this directory, so just remove SOBJS.

Cc: Jason Liu <r64343@freescale.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Marek Vasut <marex@denx.de>
9 years agomx53: Fix mask for SATA reference clock
Fabio Estevam [Fri, 11 May 2012 14:39:11 +0000 (14:39 +0000)]
mx53: Fix mask for SATA reference clock

SATA_ALT_REF_CLK field corresponds to bits 1 and 2 of offset 0x180c.

Fix the mask for these bits.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agomx53loco: Fix revision of Dialog boards
Fabio Estevam [Tue, 29 May 2012 05:54:39 +0000 (05:54 +0000)]
mx53loco: Fix revision of Dialog boards

Original code was assuming that the fuse revision version for all mx53loco boards
based on Dialog PMIC was the same, which is not the case.

Force the revision of all Dialog-based boards to 0.

This fixes a kernel crash when PMIC is accessed in the 2.6.35 kernel
for Dialog rev E boards.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
9 years agoi.mx: i.mx6x: NO_MUX_I/NO_PAD_I not set correctly
Jason Liu [Wed, 11 Apr 2012 01:18:02 +0000 (01:18 +0000)]
i.mx: i.mx6x: NO_MUX_I/NO_PAD_I not set correctly

If one PAD does not have mux or pad config register, we need
set the NO_MUX_I/NO_PAD_I to 0, the old value is not correct

Signed-off-by: Jason Liu <jason.hui@linaro.org>
CC: Stefano Babic <sbabic@denx.de>
Acked-by: Stefano Babic <sbabic@denx.de>
9 years agoEXYNOS: SMDK5250: Enable the pinmux setup
Rajeshwari Shinde [Wed, 6 Jun 2012 19:54:30 +0000 (19:54 +0000)]
EXYNOS: SMDK5250: Enable the pinmux setup

Use the pinmux configuration function for SMDK5250.

Signed-off-by: Abhilash Kesavan <a.kesavan@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Chander Kashyap <chander.kashyap@linaro.org>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
9 years agoEXYNOS5: PINMUX: Added default pinumx settings
Rajeshwari Shinde [Wed, 6 Jun 2012 19:54:29 +0000 (19:54 +0000)]
EXYNOS5: PINMUX: Added default pinumx settings

This patch performs the pinmux configuration in a common file.
As of now only EXYNOS5 pinmux for SDMMC, UART and Ethernet is
supported.

Signed-off-by: Abhilash Kesavan <a.kesavan@samsung.com>
Signed-off-by: Che-Liang Chiou <clchiou@chromium.org>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Chander Kashyap <chander.kashyap@linaro.org>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
9 years agomisc:pmic:trats: Correct procedure of enabling/disabling USB regulators
Łukasz Majewski [Wed, 25 Apr 2012 23:30:18 +0000 (23:30 +0000)]
misc:pmic:trats: Correct procedure of enabling/disabling USB regulators

In the MAX8997, LDO regulators needs to preserve previously set voltage
values.

Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
9 years agoTRATS: initialize panel_info data structure in board file
Donghwa Lee [Wed, 25 Apr 2012 13:29:39 +0000 (13:29 +0000)]
TRATS: initialize panel_info data structure in board file

panel_info data structure is gloable variable, so, I have initialized it
in board file. If it is initialized in init_panel_info() like existing,
it can't be used in drv_lcd_init() in common/lcd.c because
init_panel_info() is called after drv_lcd_init().

Signed-off-by: Donghwa Lee <dh09.lee@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Acked-by: Anatolij Gustschin <agust@denx.de>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
9 years agoExynos: fix cpuinfo and cpu detecting
Minkyu Kang [Thu, 26 Apr 2012 06:48:32 +0000 (15:48 +0900)]
Exynos: fix cpuinfo and cpu detecting

Since Exynos architecture have new SoCs,
need to fix cpuinfo correctly.

Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Tested-by: Jaehoon Chung <jh80.chung@samsung.com>
Cc: Chander Kashyap <chander.kashyap@linaro.org>
9 years agocm-t35: print PCB revision information
Nikita Kiryanov [Thu, 24 May 2012 04:01:24 +0000 (04:01 +0000)]
cm-t35: print PCB revision information

Buffer the PCB revision to avoid multiple eeprom accesses
for the same data and print it as a part of board information.

Signed-off-by: Nikita Kiryanov <nikita@compulab.co.il>
Signed-off-by: Igor Grinberg <grinberg@compulab.co.il>
Signed-off-by: Tom Rini <trini@ti.com>
9 years agocm-t35: fix legacy board revision representation
Nikita Kiryanov [Thu, 24 May 2012 04:01:23 +0000 (04:01 +0000)]
cm-t35: fix legacy board revision representation

Legacy eeprom layout represents the revision number syntactically
(i.e. revision 1.00 is written as 0x100). This is inconsistent with
the representation in newer layouts, where it is defined semantically
(i.e. 0x64).

This patch fixes the issue by replacing the syntactic representation
with the semantic one.

Signed-off-by: Nikita Kiryanov <nikita@compulab.co.il>
Signed-off-by: Igor Grinberg <grinberg@compulab.co.il>
9 years agocm-t35: fix incorrect BOARD_REV_SIZE value
Nikita Kiryanov [Thu, 24 May 2012 04:01:22 +0000 (04:01 +0000)]
cm-t35: fix incorrect BOARD_REV_SIZE value

Non-legacy layouts have an extended revision field,
but only the first 2 bytes are the PCB revision.

Signed-off-by: Nikita Kiryanov <nikita@compulab.co.il>
Signed-off-by: Igor Grinberg <grinberg@compulab.co.il>
9 years agocm-t35: reduce the environment size
Igor Grinberg [Thu, 24 May 2012 04:01:21 +0000 (04:01 +0000)]
cm-t35: reduce the environment size

Reduce the environment size (128KB => 16KB) to improve the environment
operations time (e.g. reading, ecc calculation).
Also, remove the unused CONFIG_SYS_ENV_SECT_SIZE.

Signed-off-by: Igor Grinberg <grinberg@compulab.co.il>
9 years agoARM: OMAP4: Correct the lpddr2 io settings register value.
SRICHARAN R [Thu, 24 May 2012 00:30:25 +0000 (00:30 +0000)]
ARM: OMAP4: Correct the lpddr2 io settings register value.

To meet certain timing requirements on the lpddr2 cmd and data phy
interfaces ,lpddr iopads have to be configured as differential buffers
and a Vref has to be internally generated and provided to these buffers.

Correcting the above settings here.

Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoOMAP5: Change voltages for omap5432
Lokesh Vutla [Tue, 22 May 2012 00:03:27 +0000 (00:03 +0000)]
OMAP5: Change voltages for omap5432

Change voltages for OMAP5432

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: DPLL core lock for OMAP5432
Lokesh Vutla [Tue, 22 May 2012 00:03:26 +0000 (00:03 +0000)]
OMAP5: DPLL core lock for OMAP5432

No need to Unlock DPLL initially.
DDR3 can work at normal OPP from initialozation

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: EMIF: Add support for DDR3 device
Lokesh Vutla [Tue, 22 May 2012 00:03:25 +0000 (00:03 +0000)]
OMAP5: EMIF: Add support for DDR3 device

In OMAP5432 EMIF controlller supports DDR3 device.
This patch adds support for ddr3 device intialization and configuration.
Initialization sequence is done as specified in JEDEC specs.
This also adds support for ddr3 leveling.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: ADD precalculated timings for ddr3
Lokesh Vutla [Tue, 22 May 2012 00:03:24 +0000 (00:03 +0000)]
OMAP5: ADD precalculated timings for ddr3

Adding precalculated timings for ddr3 with 1cs
adding required registers for ddr3

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: Configure the io settings for omap5432 uevm board
Lokesh Vutla [Tue, 22 May 2012 00:03:23 +0000 (00:03 +0000)]
OMAP5: Configure the io settings for omap5432 uevm board

This patch adds the IO settings required for OMAP5432 uevm's DDR3 pads

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: ADD chip detection for OMAP5432 SOC
Lokesh Vutla [Tue, 22 May 2012 00:03:22 +0000 (00:03 +0000)]
OMAP5: ADD chip detection for OMAP5432 SOC

This patch adds chip detection for OMAP5432

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoOMAP5: Adding correct Control id code for OMAP5430
Lokesh Vutla [Tue, 22 May 2012 00:03:21 +0000 (00:03 +0000)]
OMAP5: Adding correct Control id code for OMAP5430

Control id code for omap5430 ES1.0 is hard coded with a wrong value.
This patch corrects the value

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
9 years agoomap3evm: Add CONFIG_CMD_ASKENV
Tom Rini [Mon, 21 May 2012 11:20:47 +0000 (11:20 +0000)]
omap3evm: Add CONFIG_CMD_ASKENV

Signed-off-by: Tom Rini <trini@ti.com>
9 years agoomap3_beagle: Add CONFIG_CMD_ASKENV
Tom Rini [Mon, 21 May 2012 11:20:46 +0000 (11:20 +0000)]
omap3_beagle: Add CONFIG_CMD_ASKENV

Signed-off-by: Tom Rini <trini@ti.com>
9 years agoomap3evm: Set BOOTDELAY to 3
Tom Rini [Mon, 21 May 2012 11:20:45 +0000 (11:20 +0000)]
omap3evm: Set BOOTDELAY to 3

We reduce the bootdelay from 10s to 3s to give users a short but usable
window to interrupt the boot process if needed.

Signed-off-by: Tom Rini <trini@ti.com>
9 years agoOMAP3 Beagle: Set BOOTDELAY to 3
Tom Rini [Mon, 21 May 2012 11:20:44 +0000 (11:20 +0000)]
OMAP3 Beagle: Set BOOTDELAY to 3

We change the bootdelay to give users a little bit longer to break in if
needed.

Signed-off-by: Tom Rini <trini@ti.com>
9 years agoomap24xx_i2c: Add AM33XX support
Tom Rini [Mon, 21 May 2012 06:46:33 +0000 (06:46 +0000)]
omap24xx_i2c: Add AM33XX support

The same places that check for CONFIG_OMAP44XX need to check for
CONFIG_AM33XX as we share the same i2c block.

Cc: Heiko Schocher <hs@denx.de>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Heiko Schocher <hs@denx.de>
9 years agoam33xx: Fix i2c sampling rate typo
Tom Rini [Mon, 21 May 2012 06:46:32 +0000 (06:46 +0000)]
am33xx: Fix i2c sampling rate typo

Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Heiko Schocher <hs@denx.de>
9 years agoam33xx: Fill in more cm_wkuppll / cm_perpll
Tom Rini [Mon, 21 May 2012 06:46:31 +0000 (06:46 +0000)]
am33xx: Fill in more cm_wkuppll / cm_perpll

Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Heiko Schocher <hs@denx.de>
9 years agoam335x: Correct i2c sysc offset
Tom Rini [Mon, 21 May 2012 06:46:30 +0000 (06:46 +0000)]
am335x: Correct i2c sysc offset

Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Heiko Schocher <hs@denx.de>
9 years agoRevert "I2C: OMAP: detect more devices when probing an i2c bus"
Tom Rini [Mon, 21 May 2012 06:46:29 +0000 (06:46 +0000)]
Revert "I2C: OMAP: detect more devices when probing an i2c bus"

This reverts commit 0e57968a215d1b9d271f3fa5bebeddeaea0c8075.

The short version of the original commit is that some i2c devices cannot
be probed via read as they NAK the first cycle, so try and probe via a
write that we abort before it writes to the device.  This however is not
allowed by the TRM for any of these parts.  The section on I2C_CON
(table 17-35 I2C_CON for am/dm37x for example) says you must not change
the register while STT has been set.  On these parts, the unpredictable
behavior that the chip exhibits is not problematic.  On OMAP4 however it
results in the chip being in a bad state:
Panda # i2c probe
Valid chip addresses: 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12
13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A
2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40 41 42
43 44 45 46 47 48 49 4A 4B 4C 4D 4E 4F 50 51 52 53 54 55 56 57 58 59 5A
5B 5C 5D 5E 5F 60 61 62 63 64 65 66 67 68 69 6A 6B 6C 6D 6E 6F 70 71 72
73 74 75 76 77 78 79 7A 7B 7C 7D 7E 7F
Panda # i2c md 50 0
timed out in wait_for_pin: I2C_STAT=0
I2C read: I/O error
Error reading the chip.

We must revert the original behavior to bring probe back into line with
the TRM.

Cc: Nick Thompson <nick.thompson@ge.com>
Cc: Heiko Schocher <hs@denx.de>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Heiko Schocher <hs@denx.de>
9 years agoDaVinci: fix ddr2 vtp i/o calibration
Troy Kisky [Fri, 18 May 2012 13:21:59 +0000 (13:21 +0000)]
DaVinci: fix ddr2 vtp i/o calibration

Previously, only the low 5 bits (NCH) were being transfered
from DDRVTPR to DDRVTPIOCR, the bits 5-9 where zeroed.

VTP_RECAL should be bit 15, not 18.

The only mainline board affected by this change is davinci_sonata.
The other Davinci boards define CONFIG_SKIP_LOWLEVEL_INIT.

However, if the program that loads u-boot on these boards
copied the code from u-boot, they will need fixed as well.

Signed-off-by: Troy Kisky <troy.kisky@boundarydevices.com>
Please get tested by acks before applying, where tested by
means an overnight memory test.

Thanks
Troy

9 years agoARM: OMAP5: Correct the DRAM_ADDR_SPACE_END macro.
SRICHARAN R [Thu, 17 May 2012 00:12:09 +0000 (00:12 +0000)]
ARM: OMAP5: Correct the DRAM_ADDR_SPACE_END macro.

OMAP5 evm board has 2GB of memory. So correct the
macro to take in to account of the full dram size.

Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoARM: OMAP5: Align memory used for testing to the power of 2
SRICHARAN R [Thu, 17 May 2012 00:12:08 +0000 (00:12 +0000)]
ARM: OMAP5: Align memory used for testing to the power of 2

get_ram_size checks the given memory range for valid ram,
but expects the size of memory to be aligned to the power
of 2. In case of OMAP5 evm board the memory available is
2GB - 16MB(used for TRAP section) = 2032MB.

So always ensure that the size of memory used for testing is
aligned to the power of 2.

Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoARM: OMAP5: dmm: Create a tiler trap section.
SRICHARAN R [Thu, 17 May 2012 00:12:07 +0000 (00:12 +0000)]
ARM: OMAP5: dmm: Create a tiler trap section.

The unmapped entries in tiler space are set with
values 0xFF. So creating a DMM section of
size 16MB at 0xFF000000 with ADDRSPACE set to 0x2.

This way all the unmapped entry accesses to tiler
will be trapped by the EMIF and a error response
is sent to the L3 interconnect. L3 errors are
inturn reported to MPU.

Note that here the tiler trap section is overlapping
with the actual ddr physical space and we lose 16MB
out of the total 2GB.

Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoARM: OMAP4+: dmm: Take care of overlapping dmm and trap sections.
SRICHARAN R [Thu, 17 May 2012 00:12:06 +0000 (00:12 +0000)]
ARM: OMAP4+: dmm: Take care of overlapping dmm and trap sections.

The DMM sections can be overlapping with each other, with
sections 3 to 0 having the highest to lowest priority in that
order. There could also be a section that is used trap the
unmapped Tiler entries and this trap section could be
overlapping with the actual sdram area.

So take care of the above scenarios while calculating the
size of the actual ram.

Signed-off-by: R Sricharan <r.sricharan@ti.com>
9 years agoarm,davinci: update for enbw_cmc board
Heiko Schocher [Mon, 14 May 2012 20:24:14 +0000 (20:24 +0000)]
arm,davinci: update for enbw_cmc board

- change gpio pin settings:

  - gpio pin 6[13] (PLC reset) default value low
  - gpio pin 6[0] (TPM reset) default value low
  - 4 new GPIO pins
      pin  i/o   name
    - 3[9] input Board Type
    - 2[7] input HW-ID0
    - 2[6] input HW-ID1
    - 2[3] input HW-ID2

- read board type and hw id from gpio pins on the enbw_cmc board,
  and use board type for setting up different gpio pin settings.

- do not pass "davinci_mmc.use_dma=0" to linux, as MMC now
  works with DMA.

- update logbuf support:
  store post word in RTC scratch register

- add support for configuring KSZ8864RMN switch through
  a config file on u-boot startup. For more infos see:
  doc/README.switch_config

Signed-off-by: Heiko Schocher <hs@denx.de>
Cc: Wolfgang Denk <wd@denx.de>
Cc: Tom Rini <tom.rini@gmail.com>
Cc: Christian Riesch <christian.riesch@omicron.at>
Cc: Sandeep Paulraj <s-paulraj@ti.com>
9 years agoam33xx: Do not call init_timer twice
Tom Rini [Mon, 14 May 2012 12:38:18 +0000 (12:38 +0000)]
am33xx: Do not call init_timer twice

We do not need to call init_timer both in SPL and U-Boot itself, just
SPL needs to initialize the timer.

Signed-off-by: Tom Rini <trini@ti.com>
9 years agoomap4/5: Use CPUDIR for .lds script
Thomas Weber [Mon, 14 May 2012 10:28:54 +0000 (10:28 +0000)]
omap4/5: Use CPUDIR for .lds script

Signed-off-by: Thomas Weber <thomas@tomweber.eu>
9 years agotegra: trimslice: fix a couple typos
Stephen Warren [Wed, 30 May 2012 06:45:50 +0000 (06:45 +0000)]
tegra: trimslice: fix a couple typos

Fix the .dts file USB unit addresses not to duplicate each-other.

Fix the board name string to indicate the vendor is Compulab not NVIDIA.

Signed-off-by: Stephen Warren <swarren@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Acked-by: Igor Grinberg <grinberg@compulab.co.il>