glsdk/glsdk-u-boot.git
8 years agoMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
Albert ARIBAUD [Mon, 14 Jan 2013 16:00:02 +0000 (17:00 +0100)]
Merge branch 'u-boot-imx/master' into 'u-boot-arm/master'

8 years agoMerge branch 'u-boot-samsung/master' into 'u-boot-arm/master'
Albert ARIBAUD [Mon, 14 Jan 2013 14:21:00 +0000 (15:21 +0100)]
Merge branch 'u-boot-samsung/master' into 'u-boot-arm/master'

8 years agovideo: exynos_fb: Make a call to draw_logo only when CONFIG_CMD_BMP is selected
Ajay Kumar [Sun, 13 Jan 2013 23:32:16 +0000 (23:32 +0000)]
video: exynos_fb: Make a call to draw_logo only when CONFIG_CMD_BMP is selected

Previously, the call to draw_logo() was happening irrespective
of whether we have selected logo or LCD console.
With this patch we call draw_logo() only when CONFIG_CMD_BMP is selected.

This would even fix the following compilation warning:
exynos_fb.c: In function 'draw_logo':
exynos_fb.c:74:8: warning: variable 'addr' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:9: warning: variable 'y' set but not used
[-Wunused-but-set-variable]
exynos_fb.c:73:6: warning: variable 'x' set but not used
[-Wunused-but-set-variable]

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agovideo: exynos_dp: Remove unused variable disp_info
Ajay Kumar [Sun, 13 Jan 2013 23:32:15 +0000 (23:32 +0000)]
video: exynos_dp: Remove unused variable disp_info

Remove unused variable disp_info to fix the following compilation warning:
exynos_dp.c: In function 'exynos_init_dp':
exynos_dp.c:860:23: warning: variable 'disp_info' set but not used
[-Wunused-but-set-variable]

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoI2C: S3C24X0: Resolve build error for VCMA9
Rajeshwari Shinde [Sun, 13 Jan 2013 19:49:36 +0000 (19:49 +0000)]
I2C: S3C24X0: Resolve build error for VCMA9

This patch resolves the following build errors for I2C driver in
VCMA9:

In file included from s3c24x0_i2c.c:40:0:
s3c24x0_i2c.h:38:17: error: field 'id' has incomplete type
s3c24x0_i2c.c:70:39: error: 'CONFIG_MAX_I2C_NUM' undeclared here (not
in a function) s3c24x0_i2c.c:70:31: warning: 'i2c_bus' defined but
not used [-Wunused-variable] s3c24x0_i2c.c:72:12: warning:
'i2c_busses' defined but not used [-Wunused-variable]

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agomx51evk: Add DVI output support
Fabio Estevam [Wed, 9 Jan 2013 04:55:09 +0000 (04:55 +0000)]
mx51evk: Add DVI output support

Add DVI output support and make it the default video output.

Currently the CLAA WVGA panel is supported, but this panel has to be purchased
separately, so using the DVI output as the default would allow more people to
try the splash screen feature on a mx51evk.

If someone still wants to use the CLAA WVGA, just set the panel variable as:
set panel claa

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx6qsabresd: Fix booting the kernel from SDHC3
Fabio Estevam [Thu, 10 Jan 2013 09:00:53 +0000 (09:00 +0000)]
mx6qsabresd: Fix booting the kernel from SDHC3

Since commit de7d02aeb (mx6qsabresd: add usdhc2 and usdhc4 support)
SDHC3 device node is no longer 0, which breaks loading a uImage from SDHC3.

Fix it by adapting the default environment to use CONFIG_SYS_MMC_ENV_DEV as the
correct mmc node for loading the kernel from.

While at it, go back to using SDHC3 as the default mmc, since we have Yocto
images that generate an SD card containing U-boot,kernel and rootfs, so it is
more convenient to keep using SDHC3 as it was originally.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx6qsabre{auto, sd}: Add support to dynamically choose between fdt use or not
Otavio Salvador [Thu, 10 Jan 2013 09:45:09 +0000 (09:45 +0000)]
mx6qsabre{auto, sd}: Add support to dynamically choose between fdt use or not

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Tested-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx6qsabrelite: Add support to dynamically choose between fdt use or not
Otavio Salvador [Thu, 10 Jan 2013 09:45:08 +0000 (09:45 +0000)]
mx6qsabrelite: Add support to dynamically choose between fdt use or not

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
8 years agomx53loco: Add support to dynamically choose between fdt use or not
Otavio Salvador [Thu, 10 Jan 2013 09:45:07 +0000 (09:45 +0000)]
mx53loco: Add support to dynamically choose between fdt use or not

The CONFIG_SYS_CBSIZE has been change to 512 to avoid runtime errors as:

,---[ Runtime error ]
| Hit any key to stop autoboot:  0
| MX53LOCO U-Boot > pri netboot
| netboot=echo Booting from net ...; run netargs; if test ...
| prefetch abort
| pc : [<20747368>]          lr : [<20747365>]
| sp : af566e20  ip : 00000000     fp : 00000000
| r10: 00000002  r9 : af6dfc28     r8 : af566f58
| r7 : af6dfc10  r6 : 00000001     r5 : 00000002  r4 : 74206669
| r3 : 00000000  r2 : 00000060     r1 : 00000020  r0 : 0000018e
| Flags: nZCv  IRQs off  FIQs off  Mode SVC_32
| Resetting CPU ...
|
| resetting ...
`---

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
8 years agomx28evk: Add support to dynamically choose between fdt use or not
Otavio Salvador [Thu, 10 Jan 2013 09:45:06 +0000 (09:45 +0000)]
mx28evk: Add support to dynamically choose between fdt use or not

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
8 years agomx28evk: We shouldn't hardcode a rootfs filesystem type
Otavio Salvador [Thu, 10 Jan 2013 09:45:05 +0000 (09:45 +0000)]
mx28evk: We shouldn't hardcode a rootfs filesystem type

For a generic environment, we shouldn't have a fixed rootfs filesystem
so we drop it from env.

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
8 years agomx6qsabrelite: Use tabs to environment setting
Otavio Salvador [Thu, 10 Jan 2013 09:45:04 +0000 (09:45 +0000)]
mx6qsabrelite: Use tabs to environment setting

This rework the environment to use tabs for environment setting as
done in other boards.

Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
8 years agomx31/mx35/mx51/mx53/mx6: add watchdog
Troy Kisky [Mon, 22 Oct 2012 15:19:01 +0000 (15:19 +0000)]
mx31/mx35/mx51/mx53/mx6: add watchdog

Use a common watchdog driver for all these cpus.

Signed-off-by: Troy Kisky <troy.kisky@boundarydevices.com>
Acked-by: Stefano Babic <sbabic@denx.de>
8 years agoarm: at91sam9x5: add dataflash boot support
Bo Shen [Thu, 6 Dec 2012 21:37:04 +0000 (21:37 +0000)]
arm: at91sam9x5: add dataflash boot support

Add dataflash boot support on at91sam9x5ek board

Signed-off-by: Bo Shen <voice.shen@atmel.com>
Acked-by: Andreas Bießmann <andreas.devel@googlemail.com>
8 years agom68k/lib: fix serial driver relocation
angelo [Fri, 23 Nov 2012 12:23:39 +0000 (12:23 +0000)]
m68k/lib: fix serial driver relocation

Fix coldfire serial driver bindings no more relocated to ram after last
changes to drivers/serial/serial.c (regression).
Serial initialization in ram has to be called after that gd->reloc_off is
calculated.

Signed-off-by: Angelo Dureghello <sysamfw@gmail.com>
Cc: Jason Jin <jason.jin@freescale.com>
Acked-by: Jens Scharsig (BuS Elektronik) <esw@bus-elektronik.de>
Tested-by: Jens Scharsig (BuS Elektronik) <esw@bus-elektronik.de>
8 years agoMerge branch 'master' of git://git.denx.de/u-boot-arm
Tom Rini [Fri, 11 Jan 2013 21:38:24 +0000 (14:38 -0700)]
Merge branch 'master' of git://git.denx.de/u-boot-arm

8 years agoMerge branch 'u-boot-ti/master' into 'u-boot-arm/master'
Albert ARIBAUD [Fri, 11 Jan 2013 17:17:33 +0000 (18:17 +0100)]
Merge branch 'u-boot-ti/master' into 'u-boot-arm/master'

8 years agoEXYNOS5: Enable console multiplexing in u-boot
Ajay Kumar [Thu, 10 Jan 2013 21:06:11 +0000 (21:06 +0000)]
EXYNOS5: Enable console multiplexing in u-boot

We enable console multiplexing and use both serial and LCD for stdout/stderr.
Initially, u-boot output console is observed via serial port.
If you also have a DP panel connected onto your SMDK5250 board,
you can switch to LCD console by typing "setenv stdout lcd".
You can always switch back to serial using "setenv stdout serial".
You can switch error console(stderr) as well, using similar commands.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: Make all display related code dependent on CONFIG_LCD
Ajay Kumar [Thu, 10 Jan 2013 21:06:10 +0000 (21:06 +0000)]
EXYNOS5: Make all display related code dependent on CONFIG_LCD

u-boot compilation fails for smdk5250 when we deselect CONFIG_LCD
from the main config file.

Following error was observed:
drivers/video/libvideo.o: In function `exynos_lcd_init':
/home/ajay/u-boot-samsung/drivers/video/exynos_fb.c:68: undefined reference to `lcd_set_flush_dcache'

This is because exynos video drivers have dependency on CONFIG_LCD.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoExynos: clock: add CLK_DIV_FSYS3 at set_mmc_clk
Jaehoon Chung [Thu, 27 Dec 2012 22:30:33 +0000 (22:30 +0000)]
Exynos: clock: add CLK_DIV_FSYS3 at set_mmc_clk

Mobile storage is used the CLK_DIV_FSYS3 value.

Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com>
Signed-off-by: kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoExynos: clock: support get_mmc_clk for exynos
Jaehoon Chung [Thu, 27 Dec 2012 22:30:32 +0000 (22:30 +0000)]
Exynos: clock: support get_mmc_clk for exynos

To get exactly clock value for mmc, support the get_mmc_clk() like
set_mmc_clk().

Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoOMAP3: igep00x0: add CONFIG_SYS_NS16550_BROKEN_TEMT
Javier Martinez Canillas [Mon, 7 Jan 2013 01:35:21 +0000 (01:35 +0000)]
OMAP3: igep00x0: add CONFIG_SYS_NS16550_BROKEN_TEMT

IGEP board PC16550D (ns16550) UART doesn't set the
Transmitter Empty (TEMT) Bit in SPL. This makes
U-Boot to hang while waiting for TEMT. Add the
CONFIG_SYS_NS16550_BROKEN_TEMT config option to
avoid this issue.

Signed-off-by: Javier Martinez Canillas <javier.martinez@collabora.co.uk>
8 years agoserial/ns16550: add an option to avoid hanging on broken platforms
Javier Martinez Canillas [Mon, 7 Jan 2013 01:35:20 +0000 (01:35 +0000)]
serial/ns16550: add an option to avoid hanging on broken platforms

Some platforms (e.g. IGEPv2 board) has a broken ns16550 UART that
does not set the TEMT bit when the transmitter is empty in SPL.
This makes U-Boot to hang while waiting for TEMT to be set.

Add a new option to avoid this:

CONFIG_SYS_NS16550_BROKEN_TEMT

16550 UART set the Transmitter Empty (TEMT) Bit when all output
has finished and the transmitter is totally empty. U-Boot waits
for this bit to be set to initialize the serial console. On some
broken platforms this bit is not set in SPL making U-Boot to
hang while waiting for TEMT. Define this option to avoid it.

Signed-off-by: Javier Martinez Canillas <javier.martinez@collabora.co.uk>
8 years agoMakefile: remove MLO.byteswap on clobber
Nishanth Menon [Wed, 2 Jan 2013 07:59:24 +0000 (07:59 +0000)]
Makefile: remove MLO.byteswap on clobber

On clobber, do a cleanup even for SPL build else, we'd have
MLO.byteswap remaining for certain platforms like am33xx SPL builds

Signed-off-by: Nishanth Menon <nm@ti.com>
8 years agoOMAP3: igep00x0: add CONFIG_SPL_BOARD_INIT for CONFIG_SPL_NAND_SUPPORT
Javier Martinez Canillas [Fri, 28 Dec 2012 02:51:53 +0000 (02:51 +0000)]
OMAP3: igep00x0: add CONFIG_SPL_BOARD_INIT for CONFIG_SPL_NAND_SUPPORT

When booting an IGEPv2 board from NAND with SPL, U-Boot hangs
trying to read the OMAP General Purpose Memory Controller (GPMC).

The reason is that the GPMC initialization function is called
inside spl_board_init() and this function is only executed when
CONFIG_SPL_BOARD_INIT is defined.

Signed-off-by: Javier Martinez Canillas <javier.martinez@collabora.co.uk>
Acked-by: Enric Balletbo i Serra <eballetbo@iseebcn.com>
8 years agoPrepare v2013.01-rc3
Tom Rini [Thu, 10 Jan 2013 21:44:40 +0000 (14:44 -0700)]
Prepare v2013.01-rc3

Signed-off-by: Tom Rini <trini@ti.com>
8 years agobootm: relocate names of sub-command table for archs with CONFIG_NEEDS_MANUAL_RELOC
Daniel Schwierzeck [Mon, 7 Jan 2013 06:54:52 +0000 (06:54 +0000)]
bootm: relocate names of sub-command table for archs with CONFIG_NEEDS_MANUAL_RELOC

To make bootm sub-command feature working on archs with CONFIG_NEEDS_MANUAL_RELOC,
the name pointers in the sub-command table need to be relocated.

Signed-off-by: Daniel Schwierzeck <daniel.schwierzeck@gmail.com>
8 years agoarm: Tabify code for MMC initialization
Taylor Hutt [Fri, 30 Nov 2012 13:01:23 +0000 (13:01 +0000)]
arm: Tabify code for MMC initialization

The two modified lines were indented with spaces.
They are now indented with tabs.

Signed-off-by: Taylor Hutt <thutt@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: Move bootstage record for board_init_f() to after arch_cpu_init()
Simon Glass [Fri, 30 Nov 2012 13:01:22 +0000 (13:01 +0000)]
arm: Move bootstage record for board_init_f() to after arch_cpu_init()

The timer may be inited in arch_cpu_init() so it is not safe to make a
bootstage mark before this is called. Arrange the code to fix this.

Note: The question was raised as to why we don't keep all archs in sync.
PowerPC doesn't have specific bootstage markers at present (although it
does use boot progress). I hope that the generic board series will solve
this problem in general, but in the meantime this is a real problem, and
only in ARM.

We now get a correct time for board_init_f:

Timer summary in microseconds:
       Mark    Elapsed  Stage
          0          0  reset
    100,000    100,000  spl_start
    848,530    748,530  board_init_f
    907,301     58,771  board_init_r
    910,478      3,177  board_init

Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: Make interrupts.o and reset.o in libarm also appear in SPL
Tom Wai-Hong Tam [Fri, 30 Nov 2012 13:01:21 +0000 (13:01 +0000)]
arm: Make interrupts.o and reset.o in libarm also appear in SPL

SPL u-boot may call do_reset() which depends on interrupts.o and reset.o.
So make them also appear in SPL.

Signed-off-by: Tom Wai-Hong Tam <waihong@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoAdd option to display customised memory information
Simon Glass [Fri, 30 Nov 2012 13:01:20 +0000 (13:01 +0000)]
Add option to display customised memory information

Some boards want to report more than just memory size. For example, it
might be useful to display the memory type (DDR2, DDR3) or manufacturer.

Add a weak function to support this requirement, accessed through a new
'meminfo' command.

Any example of the DRAM: output is below, just for illustration:

SMDK5250 # meminfo
DRAM:  2 GiB Elpida DDR3 @ 800MHz

Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: Add CONFIG_DISPLAY_BOARDINFO_LATE to display board info on LCD
Simon Glass [Fri, 30 Nov 2012 13:01:19 +0000 (13:01 +0000)]
arm: Add CONFIG_DISPLAY_BOARDINFO_LATE to display board info on LCD

This option displays board info after stdio is running, so that it will
appear on the LCD. If it is displayed earlier, the board info will appear
on the serial console but not on the LCD.

Here follows a blow-by-blow description.

1a. Without CONFIG_DISPLAY_BOARDINFO_LATE, on serial:

U-Boot 2011.12-02550-g037e1c5-dirty (Nov 15 2012 - 14:29:42) for SMDK5250

CPU:   S5PC520 @ 1700MHz

Board: Google Snow, rev 0
I2C:   ready
DRAM:  2 GiB Elpida DDR3 @ 800MHz
MMC:   S5P MSHC0: 0, S5P MSHC1: 1
SF: Detected W25Q32 with page size 4 KiB, total 4 MiB
*** Warning - bad CRC, using default environment

In:    mkbp-keyb
Out:   lcd
Err:   lcd
Net:   No ethernet found.
Hit any key to stop autoboot:  0
SMDK5250 #

1b. Without CONFIG_DISPLAY_BOARDINFO_LATE, on LCD (note machine info
is missing):

In:    mkbp-keyb
Out:   lcd
Err:   lcd
Net:   No ethernet found.
Hit any key to stop autoboot:  0
SMDK5250 #

2a. With CONFIG_DISPLAY_BOARDINFO_LATE, on serial:

U-Boot 2011.12-02550-g037e1c5 (Nov 15 2012 - 14:27:40) for SMDK5250

CPU:   S5PC520 @ 1700MHz
I2C:   ready
DRAM:  2 GiB Elpida DDR3 @ 800MHz
MMC:   S5P MSHC0: 0, S5P MSHC1: 1
SF: Detected W25Q32 with page size 4 KiB, total 4 MiB
*** Warning - bad CRC, using default environment

Model: Google Snow
In:    mkbp-keyb
Out:   lcd
Err:   lcd
Net:   No ethernet found.
Hit any key to stop autoboot:  0
SMDK5250 #

2b. With CONFIG_DISPLAY_BOARDINFO_LATE, on LCD (note machine info is present):

Model: Google Snow
In:    mkbp-keyb
Out:   lcd
Err:   lcd
Net:   No ethernet found.
Hit any key to stop autoboot:  0
SMDK5250 #

Since the LCD is all that a typical user sees, it is useful to display
the model there.

We may be able to rearrange things some other way one day, but at
present this seems like a convenient way of getting the required
behaviour.

Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoDocument the CONFIG_DISPLAY_BOARDINFO option
Simon Glass [Fri, 30 Nov 2012 13:01:18 +0000 (13:01 +0000)]
Document the CONFIG_DISPLAY_BOARDINFO option

Add a short note about this in the README.

Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: Add CONFIG_DELAY_ENVIRONMENT to delay environment loading
Simon Glass [Fri, 30 Nov 2012 13:01:17 +0000 (13:01 +0000)]
arm: Add CONFIG_DELAY_ENVIRONMENT to delay environment loading

This option delays loading of the environment until later, so that only the
default environment will be available to U-Boot.

This can address the security risk of untrusted data being used during boot.

Any time you load untrusted data you expose yourself to a bug in the
code. The attacker gets to choose the data so can sometimes carefully
craft it to exploit a bug. We try to avoid touching user-controlled
data during a verified boot unless strictly necessary. Since the
default environment is good enough in this case (or you would just
change it), this gets around the problem by just not loading the
environment.

When CONFIG_DELAY_ENVIRONMENT is defined, it is convenient to have a
run-time way of enabling loading of the environment. Add this to the
fdt as /config/delay-environment.

Note: This patch depends on http://patchwork.ozlabs.org/patch/194342/

Signed-off-by: Doug Anderson <dianders@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
Reviewed-by: Doug Anderson <dianders@chromium.org>
8 years agoarm: Move fdt check earlier so that board_early_init_f() can use it
Simon Glass [Fri, 30 Nov 2012 13:01:16 +0000 (13:01 +0000)]
arm: Move fdt check earlier so that board_early_init_f() can use it

We want to use the fdt inside board_early_init_f(), so check for its
presence earlier in the pre-reloc init sequence.

So far ARM and microblaze are the only only ones that use
CONFIG_OF_CONTROL. Microblaze does not have the same init loop, and in
particular does not have the board_early_init_f() call. So a patch for
microblaze would have no meaning.

Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: Keep track of the tlb size as well as its location
Gabe Black [Fri, 30 Nov 2012 13:01:15 +0000 (13:01 +0000)]
arm: Keep track of the tlb size as well as its location

It may be necessary to know where the TLB area ends as well as where it
starts. This allows board code to complete a secure memory erase without
destroying the page tables.

Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agoarm: move flush_dcache_all() to just before disable cache
Arun Mankuzhi [Fri, 30 Nov 2012 13:01:14 +0000 (13:01 +0000)]
arm: move flush_dcache_all() to just before disable cache

In Cortex-A15 architecture, when we run cache invalidate
the cache clean operation executes automatically.
So if there are any dirty cache lines before disabling the L2 cache
these will be synchronized with the main memory when
invalidate_dcache_all() runs in the last part of U-boot

The two functions after flush_dcache_all is using the stack. So this
data will be on the cache. After disable when invalidate is called the
data will be flushed from cache to memory. This corrupts the stack in
invalida_dcache_all. So this change is required to avoid the u-boot
hang.

So flush has to be done just before clearing CR_C bit

Signed-off-by: Arun Mankuzhi <arun.m@samsung.com>
Signed-off-by: Simon Glass <sjg@chromium.org>
8 years agocfi_flash: Report Advanced Sector Protection (PPB) with flinfo cmd
Stefan Roese [Thu, 6 Dec 2012 14:44:12 +0000 (15:44 +0100)]
cfi_flash: Report Advanced Sector Protection (PPB) with flinfo cmd

Report the usage of the Advanced Sector Protection (PPB) to the user
upon 'flinfo' command. E.g:

Bank # 1: CFI conformant flash (16 x 16)  Size: 64 MB in 512 Sectors
  AMD Standard command set, Manufacturer ID: 0x01, Device ID: 0x227E2301
  Advanced Sector Protection (PPB) enabled
  Erase timeout: 16384 ms, write timeout: 2 ms
  Buffer write timeout: 5 ms, buffer size: 32 bytes

  Sector Start Addresses:
  FC000000 E      FC020000 E RO   FC040000 E      FC060000 E      FC080000 E
  ...

Signed-off-by: Stefan Roese <sr@denx.de>
Cc: Anatolij Gustschin <agust@denx.de>
Cc: Holger Brunck <holger.brunck@keymile.com>
Tested-by: Holger Brunck <holger.brunck@keymile.com>
8 years agocfi_flash: Enable PPB protection for all AMD cmdset flash chips
Stefan Roese [Thu, 6 Dec 2012 14:44:11 +0000 (15:44 +0100)]
cfi_flash: Enable PPB protection for all AMD cmdset flash chips

Not only Spansion supports the Persistent Protection Bits (PPB) locking.
Other devices like the Micron JS28F512M29EWx also support this type
of locking/unlocking. Detection of support is done in the same way as
done for the Spansion chips - via the 0x49 CFI word.

This patch enables this PPB protection mechanism for all AMD type
(AMD commandset) chips.

Signed-off-by: Stefan Roese <sr@denx.de>
Cc: Anatolij Gustschin <agust@denx.de>
Cc: Holger Brunck <holger.brunck@keymile.com>
Tested-by: Holger Brunck <holger.brunck@keymile.com>
8 years agocfi_flash: Read PPB sector protection from device for AMD/Spansion chips
Stefan Roese [Thu, 6 Dec 2012 14:44:10 +0000 (15:44 +0100)]
cfi_flash: Read PPB sector protection from device for AMD/Spansion chips

Patch 66863b05 [cfi_flash: add support for Spansion flash PPB sector
protection] introduced the PPB (Persistent Protection Bit) locking for
Spansion chips. But right now the sector protection status (locked vs
unlocked) is set to unlocked for all sectors upon bootup. The real
sector protection status is ignored.

This patch now reads the current sector protection status and uses
it for these AMD/Spansion flash chips.

Signed-off-by: Stefan Roese <sr@denx.de>
Cc: Anatolij Gustschin <agust@denx.de>
Cc: Holger Brunck <holger.brunck@keymile.com>
Tested-by: Holger Brunck <holger.brunck@keymile.com>
8 years agocfi_flash: Add manufact_match helper function
Stefan Roese [Thu, 6 Dec 2012 14:44:09 +0000 (15:44 +0100)]
cfi_flash: Add manufact_match helper function

Consolidate manufacturer matching into the function manufact_match()
and use it.

Signed-off-by: Stefan Roese <sr@denx.de>
Tested-by: Holger Brunck <holger.brunck@keymile.com>
8 years agomtd/cfi: add support for SST 4KB sector granularity
Angelo Dureghello [Sat, 1 Dec 2012 00:14:18 +0000 (01:14 +0100)]
mtd/cfi: add support for SST 4KB sector granularity

Add support for SST 4KB sector granularity.

Many recent SST flashes, i.e. SST39VF3201B and similar of this family
are declared CFI-conformant from SST. They support CFI query, but implement
2 different sector sizes in the same memory: a 64KB sector (they call it
"block", std AMD erase cmd=0x30), and a 4KB sector (they call it "sector",
erase cmd=0x50). Also, CFI query on these chips, reading from address 0x2dh
of cfi query struct, detects a number of secotrs for the 4KB granularity
(flinfo shows it).

For all other aspects, they are CFI compliant, so, as Linux do, i think
it's a good idea to handle these chips in the CFI driver, with a fixup
to allow 4KB granularity, as should be expected, instead of 64KB.

Signed-off-by: Angelo Dureghello <sysamfw@gmail.com>
Signed-off-by: Stefan Rose <sr@denx.de>
8 years agovideo: Modify exynos_fimd driver to support LCD console
Ajay Kumar [Tue, 8 Jan 2013 20:42:25 +0000 (20:42 +0000)]
video: Modify exynos_fimd driver to support LCD console

Currently, exynos FIMD driver is being used to support only TIZEN LOGOs.
In order to get LCD console, we need to enable half word swap feature
of FIMD and use 16 BPP.
LCD console and proprietary Logo cannot be used simultaneously.
We use "logo_on" field inside vidinfo_t structure to decide whether
user wants Logo or Console.
Define CONFIG_CMD_BMP and make logo_on = 1 to get Logo on screen.
Use logo_on = 0 to get output console on LCD.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS: Add dummy definition to fix compilation dependency on CONFIG_EXYNOS_MIPI_DSIM
Ajay Kumar [Tue, 8 Jan 2013 20:42:24 +0000 (20:42 +0000)]
EXYNOS: Add dummy definition to fix compilation dependency on CONFIG_EXYNOS_MIPI_DSIM

When only DP is used, we need not enable CONFIG_EXYNOS_MIPI_DSIM.
But if we do not select CONFIG_EXYNOS_MIPI_DSIM, exynos_fb.c throws
error saying exynos_mipi_dsi_init() not defined. So, we add
dummy definition for exynos_mipi_dsi_init when CONFIG_EXYNOS_MIPI_DSIM
is not defined.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Donghwa Lee <dh09.lee@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: Change parent clock of FIMD to MPLL
Ajay Kumar [Tue, 8 Jan 2013 20:42:23 +0000 (20:42 +0000)]
EXYNOS5: Change parent clock of FIMD to MPLL

With VPLL as source clock to FIMD,
Exynos DP Initializaton was failing sometimes with unstable clock.
Changing FIMD source to MPLL resolves this issue.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Donghwa Lee <dh09.lee@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: Add support for FIMD and DP
Ajay Kumar [Tue, 8 Jan 2013 20:42:26 +0000 (20:42 +0000)]
EXYNOS5: Add support for FIMD and DP

Add panel_info structure required by LCD driver
and DP panel platdata for SMDK5250.
Add GPIO configuration for LCD.
Enable FIMD and DP support on SMDK5250.
DP Panel size: 2560x1600.
We use 16BPP resolution to get LCD console.

Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Acked-by: Simon Glass <sjg@chomium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoPMIC: MAX77686: Add FDT Support
Rajeshwari Shinde [Tue, 8 Jan 2013 21:03:40 +0000 (21:03 +0000)]
PMIC: MAX77686: Add FDT Support

This patch adds fdt support to MAX77686.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: Add device node for PMIC
Rajeshwari Shinde [Tue, 8 Jan 2013 21:03:39 +0000 (21:03 +0000)]
EXYNOS5: Add device node for PMIC

Add device node for MAX77686

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add compatible strings for PMIC
Rajeshwari Shinde [Tue, 8 Jan 2013 21:03:38 +0000 (21:03 +0000)]
EXYNOS5: FDT: Add compatible strings for PMIC

Add required compatible information for PMIC

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoMerge 'u-boot-atmel/master' into 'u-boot-arm/master'
Albert ARIBAUD [Wed, 9 Jan 2013 19:01:48 +0000 (20:01 +0100)]
Merge 'u-boot-atmel/master' into 'u-boot-arm/master'

8 years agomx53loco: Add support for SEIKO 4.3'' WVGA panel
Fabio Estevam [Wed, 9 Jan 2013 05:10:16 +0000 (05:10 +0000)]
mx53loco: Add support for SEIKO 4.3'' WVGA panel

Add support for the Seiko 4.3'' WVGA panel on mx53loco.

By default, the CLAA WVGA panel is selected.

In order to support the Seiko panel, the enviroment variable 'panel' must be
set to 'seiko'.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx6: Add workaround for ARM errata
Fabio Estevam [Fri, 4 Jan 2013 16:07:26 +0000 (16:07 +0000)]
mx6: Add workaround for ARM errata

Add workaround for the following ARM errata: 743622 and 751472.

The motivation for this change is the following kernel commit 62e4d357a
(ARM: 7609/1: disable errata work-arounds which access
secure registers), which removes the errata from multiplatform kernel.

Since imx has been converted to multiplatform in the kernel, we need to apply
such workarounds into the bootloader.

Workaround code has been taken from arch/arm/mm/proc-v7.S from 3.7.1 kernel.

Explanation of each erratum is provided at "Chip Errata for the i.MX 6Dual/6Quad"
document available at: cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agoMerge branch 'u-boot-marvell/master' into 'u-boot-arm/master'
Albert ARIBAUD [Wed, 9 Jan 2013 15:57:03 +0000 (16:57 +0100)]
Merge branch 'u-boot-marvell/master' into 'u-boot-arm/master'

8 years agoMerge branch 'master' of git://git.denx.de/u-boot-arm
Tom Rini [Wed, 9 Jan 2013 15:13:22 +0000 (08:13 -0700)]
Merge branch 'master' of git://git.denx.de/u-boot-arm

8 years agoFix SPL build for non-ARM targets
Albert ARIBAUD [Tue, 8 Jan 2013 22:57:20 +0000 (23:57 +0100)]
Fix SPL build for non-ARM targets

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agovideo:cache:fix: Enable dcache flush at LCD subsystem for Exynos based boards
Łukasz Majewski [Tue, 8 Jan 2013 03:48:40 +0000 (03:48 +0000)]
video:cache:fix: Enable dcache flush at LCD subsystem for Exynos based boards

lcd_set_flush_dcache(1) function is called from exynos_fb.c configuration file
to enable lcd_sync function.

Signed-off-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Tested-by: Lukasz Majewski <l.majewski@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agomv-common.h: increase malloc arena to 4MiB
Andreas Bießmann [Mon, 29 Oct 2012 13:58:55 +0000 (13:58 +0000)]
mv-common.h: increase malloc arena to 4MiB

This will fix the following error:

---8<---
UBIFS error (pid 0): ubifs_mount: Error reading superblock on volume 'ubi:root' errno=-12!
--->8---

Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: prafulla@marvell.com
Cc: dimax.main@gmail.com
Tested-by: Alex Xol <dimax.main@gmail.com>
8 years agoarch-kirkwood: Ethernet port macro returning incorrect address
Luke Lowrey [Mon, 25 Jun 2012 06:37:09 +0000 (06:37 +0000)]
arch-kirkwood: Ethernet port macro returning incorrect address

Modified the arch-kirkwood header so KWGBE_PORT_SERIAL_CONTROL1_REG(x)
returns the correct address.

Originally calling KWGBE_PORT_SERIAL_CONTROL1_REG(1) returned the
address for port 0 and vice versa.

Doesn't have any knock on effects to the u-boot code as the only
time they're used is to do the same function to both addresses

Signed-off-by: Luke Lowrey <luke@chamsys.co.uk>
Acked-by: Prafulla Wadaskar <Prafulla@marvell.com>
Acked-by: Heiko Schocher <hs@denx.de>
8 years agolsxl: unset ncip for rescue mode
Michael Walle [Thu, 4 Oct 2012 06:54:25 +0000 (06:54 +0000)]
lsxl: unset ncip for rescue mode

Instead of using the serverip we get from the DHCP server, implicitly use
the broadcast address, which is automatically set when no ncip environment
variable is set. That way it isn't necessary to use a special DHCP
configuration to set the netconsole peer.

Signed-off-by: Michael Walle <michael@walle.cc>
Cc: Prafulla Wadaskar <prafulla@marvell.com>
8 years agoARM: lacie_kw: add support for WIRELESS_SPACE
Albert ARIBAUD [Mon, 26 Nov 2012 11:27:37 +0000 (11:27 +0000)]
ARM: lacie_kw: add support for WIRELESS_SPACE

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agokirkwood: make MPP arrays static const
Albert ARIBAUD [Mon, 26 Nov 2012 11:27:36 +0000 (11:27 +0000)]
kirkwood: make MPP arrays static const

This saves stack and code memory for local copy, and
consumes initialized data memory. For 22 of the 29
kirkwood-based boards, this results in a global saving
of about 30 bytes. For 7 of them, it results in an
increase of 6 to 14 bytes.

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agomv88e61xx: refactor PHY and SWITCH level-code
Albert ARIBAUD [Mon, 26 Nov 2012 11:27:35 +0000 (11:27 +0000)]
mv88e61xx: refactor PHY and SWITCH level-code

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agoarm/km: remove duplicate code
Valentin Longchamp [Fri, 2 Nov 2012 00:15:10 +0000 (00:15 +0000)]
arm/km: remove duplicate code

This patch removes 2 small portions of board specific code that are
duplicated with common ARM code and thus unnecessary. These 2 portions
of code concern the mach id that is given by u-boot to the Linux kernel
to identify the system's MACH.

The first one was the possibility to change the MACH thanks to the
'mach_id' enviroment variable. This is possible thanks to the 'machid'
env variable (see arch/arm/lib/bootm.c:boot_jump_linux()).

The seconde one is the setting of the bi_arch_number. This is already
done in arch/arm/lib/board.c:board_init_f() since km_arm.h does #define
CONFIG_MACH_TYPE.

Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Holger Brunck <holger.brunck@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <Prafulla@marvell.com>
8 years agokm/common: cosmetic change reported from checkpatch
Holger Brunck [Fri, 2 Nov 2012 00:15:09 +0000 (00:15 +0000)]
km/common: cosmetic change reported from checkpatch

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>
Acked-by: Prafulla Wadaskar <Prafulla@marvell.com>
8 years agokm/common: drop unneeded std* environment variables
Holger Brunck [Fri, 2 Nov 2012 00:15:08 +0000 (00:15 +0000)]
km/common: drop unneeded std* environment variables

These variables are only used if CONFIG_SYS_CONSOLE_IS_IN_ENV
is set. This isn't the case, so we can drop them safely.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
cc: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

8 years agoarm/km: fix memory settings
Holger Brunck [Fri, 2 Nov 2012 00:15:07 +0000 (00:15 +0000)]
arm/km: fix memory settings

On kmcoge5un we faced some serious problems with the memory during
temperature tests. Reason was that we overwrite some registers for
memory settings which have to leave untouched. These where registers
0x20148 , 0x2014c and 0x20154.
So writing these registers is prohibited and this patch removes them
from all km related config files. Even if the problem was only
seen on kmcoge5un.

Signed-off-by: Holger Brunck <holger.brunck@keymile.com>
Signed-off-by: Valentin Longchamp <valentin.longchamp@keymile.com>
cc: Prafulla Wadaskar <prafulla@marvell.com>

8 years agoMerge branch 'master' of git://git.denx.de/u-boot-arm
Tom Rini [Tue, 8 Jan 2013 15:28:27 +0000 (08:28 -0700)]
Merge branch 'master' of git://git.denx.de/u-boot-arm

8 years agoarm: remove useless code in start.S files
Albert ARIBAUD [Tue, 8 Jan 2013 10:18:03 +0000 (10:18 +0000)]
arm: remove useless code in start.S files

Remove code such as unneeded includes or labels.
These removals have no functional effect.

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agoarm: move C runtime setup code in crt0.S
Albert ARIBAUD [Tue, 8 Jan 2013 10:18:02 +0000 (10:18 +0000)]
arm: move C runtime setup code in crt0.S

Move all the C runtime setup code from every start.S
in arch/arm into arch/arm/lib/crt0.S. This covers
the code sequence from setting up the initial stack
to calling into board_init_r().

Also, rewrite the C runtime setup and make functions
board_init_*() and relocate_code() behave according to
normal C semantics (no jumping across the C stack any
more, etc).

Some SPL targets had to be touched because they use
start.S explicitly or for some reason; the relevant
maintainers and custodians are cc:ed.

Signed-off-by: Albert ARIBAUD <albert.u.boot@aribaud.net>
8 years agoMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
Albert ARIBAUD [Tue, 8 Jan 2013 13:59:37 +0000 (14:59 +0100)]
Merge branch 'u-boot-imx/master' into 'u-boot-arm/master'

8 years agoMerge branch 'u-boot-ti/master' into 'u-boot-arm/master'
Albert ARIBAUD [Tue, 8 Jan 2013 12:15:45 +0000 (13:15 +0100)]
Merge branch 'u-boot-ti/master' into 'u-boot-arm/master'

This required manual merging drivers/mtd/nand/Makefile
and adding am335x_evm support for CONFIG_SPL_NAND_DRIVERS

8 years agoSMDK5250: Enable VBus for USB 2.0 controller
Vivek Gautam [Mon, 7 Jan 2013 23:37:18 +0000 (23:37 +0000)]
SMDK5250: Enable VBus for USB 2.0 controller

This patch enables Vbus required for USB 2.0 controller.

Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add compatible strings for USB
Rajeshwari Shinde [Mon, 7 Jan 2013 23:35:05 +0000 (23:35 +0000)]
EXYNOS5: FDT: Add compatible strings for USB

Add required compatible information for USB

Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: Add device node for USB.
Rajeshwari Shinde [Mon, 7 Jan 2013 23:35:04 +0000 (23:35 +0000)]
EXYNOS5: Add device node for USB.

This patch adds the device node required for USB

Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEHCI: Exynos: Add fdt support
Rajeshwari Shinde [Mon, 7 Jan 2013 23:35:03 +0000 (23:35 +0000)]
EHCI: Exynos: Add fdt support

Adding fdt support to ehci-exynos in order to parse
register base addresses from the device node.

Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoSPI: EXYNOS: Add FDT support to driver.
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:23 +0000 (20:03 +0000)]
SPI: EXYNOS: Add FDT support to driver.

This patch adds FDT support to the SPI driver.

Signed-off-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add SPI device node data
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:22 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add SPI device node data

Add SPI device node data for exynos.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5 : FDT: Add Aliases for SPI device
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:21 +0000 (20:03 +0000)]
EXYNOS5 : FDT: Add Aliases for SPI device

This patch adds aliases for SPI.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add compatible strings for SPI
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:20 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add compatible strings for SPI

Add required compatible information for SPI driver.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoSound: Add FDT support to CMD.
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:19 +0000 (20:03 +0000)]
Sound: Add FDT support to CMD.

This patch adds FDT support to sound init in CMD.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoSound: WM8994: Add FDT support to codec
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:18 +0000 (20:03 +0000)]
Sound: WM8994: Add FDT support to codec

This patch adds FDT support to the codec.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoSound: Add FDT support to driver
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:17 +0000 (20:03 +0000)]
Sound: Add FDT support to driver

This patch adds FDT support to the sound driver.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add compatible strings for sound
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:16 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add compatible strings for sound

Add required compatible information for sound driver.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add sound and codec device node
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:15 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add sound and codec device node

Adds sound and codec device node parameters

Signed-off-by: R. Chandrasekar <rcsekar@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add sound device node data
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:14 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add sound device node data

Add sound device node data for exynos

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoSMDK5250: Initialise I2C using FDT
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:13 +0000 (20:03 +0000)]
SMDK5250: Initialise I2C using FDT

This patch initialises I2C using FDT.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Heiko Schocher <hs@denx.de>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoI2C: Driver changes for FDT support
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:12 +0000 (20:03 +0000)]
I2C: Driver changes for FDT support

Functions added to get the I2C bus number and reset I2C bus using
FDT node.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Heiko Schocher <hs@denx.de>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT : Decode peripheral id
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:11 +0000 (20:03 +0000)]
EXYNOS5: FDT : Decode peripheral id

Api is added to decode peripheral id based on the interrupt number
of the peripheral.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoFDT: Add compatible string for I2C
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:10 +0000 (20:03 +0000)]
FDT: Add compatible string for I2C

Add required compatible information for I2C driver.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Heiko Schocher <hs@denx.de>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5 : FDT: Add Aliases for I2C device
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:09 +0000 (20:03 +0000)]
EXYNOS5 : FDT: Add Aliases for I2C device

This patch adds aliases for I2C.

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Acked-by: Heiko Schocher <hs@denx.de>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoEXYNOS5: FDT: Add I2C device node data
Rajeshwari Shinde [Wed, 26 Dec 2012 20:03:08 +0000 (20:03 +0000)]
EXYNOS5: FDT: Add I2C device node data

Add I2C device node data for exynos

Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agoarm:exynos4:pinmux: Modify the gpio function for mmc
Piotr Wilczek [Wed, 2 Jan 2013 21:31:00 +0000 (21:31 +0000)]
arm:exynos4:pinmux: Modify the gpio function for mmc

This patch add pinmux settings for Exynos4 for mmc0 and mmc2

Signed-off-by: Piotr Wilczek <p.wilczek@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
CC: Albert ARIBAUD <albert.u.boot@aribaud.net>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
8 years agotools: imximage: Load a size that is multiple of 512
Fabio Estevam [Thu, 3 Jan 2013 08:24:33 +0000 (08:24 +0000)]
tools: imximage: Load a size that is multiple of 512

In order to mx53 ROM to properly load the U-boot image, its header size should
be multiple of 512 bytes.

This issue was observed with gcc 4.6.2/4.7.3, which caused data aborts:

U-Boot 2013.01-rc2-00172-gf8cfcf1-dirty (Dec 26 2012 - 13:13:28)

Board: MX53 LOCO
I2C:   ready
DRAM:  1 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
In:    serial
Out:   serial
Err:   serial
CPU:   Freescale i.MX53 family rev2.1 at 1000 MHz
Reset cause: WDOG
Net:   FEC
Warning: FEC using MAC address from net device

Hit any key to stop autoboot:  0
data abort

    MAYBE you should read doc/README.arm-unaligned-accesses

pc : [<aff72220>]          lr : [<aff721fc>]
sp : af565e20  ip : af566918     fp : 00000000
r10: 00000003  r9 : affabb5b     r8 : af565f58
r7 : 00000000  r6 : 36747fff     r5 : af5668e8  r4 : 36747fff
r3 : af5668ec  r2 : af5668eb     r1 : 00000000  r0 : af5668e8
Flags: NzcV  IRQs off  FIQs off  Mode SVC_32
Resetting CPU ...

resetting ...

,and this patch fixes it.

Also, even though the ROUND macro is already defined in common.h,
the reason for redefining it in image.h is explained by Stefano Babic:

"I will remark a previous comment - even if including common.h seems a
good idea to avoid duplications, it makes tools like mkimage to depend
on the selected board, because <board>_config must run. Even if this is
not a problem for us u-boot developers, it becomes an issue when these
tools are included in distros (like u-boot-tools in Ubuntu) and cannot
be packaged."

Signed-off-by: Troy Kisky <troy.kisky@boundarydevices.com>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx53loco: Improve error handling on power_init()
Fabio Estevam [Fri, 28 Dec 2012 04:05:29 +0000 (04:05 +0000)]
mx53loco: Improve error handling on power_init()

Make the error handling more robust.

Check if each one of the PMIC writes fail and if they do, just return
immediately.

Also, print the cause for the failures.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx53loco: Remove unneeded 'retval' variable
Fabio Estevam [Fri, 28 Dec 2012 04:05:28 +0000 (04:05 +0000)]
mx53loco: Remove unneeded 'retval' variable

commit c73368150 (pmic: Extend PMIC framework to support multiple instances
of PMIC devices) introduced an extra 'retval' variable, but this is not
necessary since we have already the variable 'ret' in place.

So use 'ret' to store the return values from the pmic related calls and remove
'retval'.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx51evk: Remove unneeded comment
Fabio Estevam [Thu, 27 Dec 2012 05:46:33 +0000 (05:46 +0000)]
mx51evk: Remove unneeded comment

Looks like the original comment came from a copy and paste from mx31ads.h.

It does not have a context on mx51evk anymore, so delete it.

Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
8 years agomx6qsabresd: use on-board eMMC to store environment
Shawn Guo [Sun, 30 Dec 2012 14:15:00 +0000 (14:15 +0000)]
mx6qsabresd: use on-board eMMC to store environment

It makes more sense to use on-board eMMC to store environments.  The
boot partition 1 is selected by default.

Signed-off-by: Shawn Guo <shawn.guo@linaro.org>
8 years agomx6qsabresd: add usdhc2 and usdhc4 support
Shawn Guo [Sun, 30 Dec 2012 14:14:59 +0000 (14:14 +0000)]
mx6qsabresd: add usdhc2 and usdhc4 support

The on-board number of available usdhc devices is something board
specific.  The patch moves CONFIG_SYS_FSL_USDHC_NUM out of
mx6qsabre_common.h and adds usdhc2 and usdhc4 support for mx6qsabresd
board.

To keep the default mmc device for environment same as before (usdhc3),
it moves CONFIG_SYS_MMC_ENV_DEV out of mx6qsabre_common.h and changes
it to 1 for mx6qsabresd.

Signed-off-by: Shawn Guo <shawn.guo@linaro.org>
8 years agofsl_esdhc: add MMC_MODE_HC host_caps
Shawn Guo [Sun, 30 Dec 2012 14:14:58 +0000 (14:14 +0000)]
fsl_esdhc: add MMC_MODE_HC host_caps

All esdhc variants we know should support high capacity MMC cards,
so let's add MMC_MODE_HC host_caps unconditionally to support those
MMC cards (capacity > 2 GB).

Signed-off-by: Shawn Guo <shawn.guo@linaro.org>